powered by CADENAS

Social Share

Amazon

Pencil case (7879 views - Consumer products)

A pencil case or pencil box is a container used to store pencils. A pencil case can also contain a variety of other stationery such as sharpeners, pens, glue sticks, erasers, scissors and rulers. Pencil cases can be made from a variety of materials such as wood or metal. Some pencil cases have a hard and rigid shell encasing the pens inside, while others use a softer material such as plastic, leather or cotton. Soft versions are typically fastened with a zipper. Decorated versions are popular with schoolchildren depending on age and gender. The intent of having a pencil case is for easy portability of small items such as pencils. They may also contain other stationery such as pens and glue sticks. Some pencil cases double as make up bags. Early pencil cases were round or cylindrical in shape. Some early pencil cases were decorated with jasper (one from 1860) or platinum (from 1874). In 1946, the first patent for a pencil case was placed in the United States. This patent was made by Verona Pearl Amoth, who also invented other tools of the field like replaceable erasers for pencils.
Go to Article

Explanation by Hotspot Model

Pencil case

Pencil case

Pencil case

Licensed under Creative Commons Attribution 3.0 (Honza Groh).

A pencil case or pencil box is a container used to store pencils. A pencil case can also contain a variety of other stationery such as sharpeners, pens, glue sticks, erasers, scissors and rulers.

Pencil cases can be made from a variety of materials such as wood or metal. Some pencil cases have a hard and rigid shell encasing the pens inside, while others use a softer material such as plastic, leather or cotton. Soft versions are typically fastened with a zipper. Decorated versions are popular with schoolchildren depending on age and gender.

The intent of having a pencil case is for easy portability of small items such as pencils. They may also contain other stationery such as pens and glue sticks. Some pencil cases double as make up bags.

Early pencil cases were round or cylindrical in shape. Some early pencil cases were decorated with jasper (one from 1860) or platinum (from 1874).[1] In 1946, the first patent for a pencil case was placed in the United States. This patent was made by Verona Pearl Amoth, who also invented other tools of the field like replaceable erasers for pencils.

  1. ^ Nadelhoffer, Hans (2007). Cartier. Chronicle Books. p. 201. ISBN 081186099X. 

See also



This article uses material from the Wikipedia article "Pencil case", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Consumer products

.max, Maya, Challenge, Competition, Rendering, 3D, Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D, 3D library