powered by CADENAS

Social Share

Amazon

GoPro (3358 views - Consumer products)

GoPro, Inc. (marketed as GoPro and sometimes stylised as GoPRO) is an American technology company founded in 2002 by Nick Woodman. It manufactures eponymous action cameras and develops its own mobile apps and video-editing software. Founded as Woodman Labs, Inc, the company eventually focused on the connected sports genre, developing its line of action cameras and, later, video editing software. It developed a quadcopter drone, Karma, released in October 2016. In January 2018, Karma was discontinued and the company hired JPMorgan Chase to pursue options of selling the company. However, a month later, the CEO denied this.
Go to Article

Explanation by Hotspot Model

GoPro

GoPro

GoPro
GoPro, Inc.
Formerly called
Woodman Labs, Inc.
Public
Traded as NASDAQGPRO
Industry
Founded 2002; 16 years ago (2002)
Founder Nick Woodman
Headquarters San Mateo, California, U.S.
Area served
Worldwide
Key people
Products
Revenue US$ 1.18 billion (2017)[1]
(US$ 163.46 million) (loss,2017)[1]
(US$ 182.87 million) (loss,2017)[1]
Total assets US$ 0.85 billion (2017)[1]
Number of employees
963 (2018)
Subsidiaries
Website www.gopro.com

GoPro, Inc.[2] (marketed as GoPro and sometimes stylised as GoPRO) is an American technology company founded in 2002 by Nick Woodman. It manufactures eponymous action cameras and develops its own mobile apps and video-editing software. Founded as Woodman Labs, Inc, the company eventually focused on the connected sports genre, developing its line of action cameras and, later, video editing software.

It developed a quadcopter drone, Karma, released in October 2016. In January 2018, Karma was discontinued and the company hired JPMorgan Chase to pursue options of selling the company. [3] However, a month later, the CEO denied this.[4]

History

The company was founded by Nick Woodman in 2002.[5] He was motivated by a 2002 surfing trip to Australia in which he was hoping to capture quality action photos, but could not because amateur photographers could not get close enough or buy quality equipment at reasonable prices.[6] His desire for a camera system that could capture the professional angles inspired the 'GoPro' name.[7][8]

Woodman raised a portion of his initial capital by selling bead and shell belts for under US $20 from his VW van[9] and, later, fashionable camera straps. He also received over $230,000 from his parents to invest in the business.[10][11]

In 2004, the company sold its first camera system, which used 35 mm film.[7] Digital still and video cameras were later introduced. As of 2014, a fixed-lens HD video camera with a wide 170-degree lens was available; two or more can be paired to create 360 video.[7][12]

On June 4, 2014, the company announced the appointment of former Microsoft executive Tony Bates as President reporting directly to Woodman.[13]

In January 2016, GoPro partnered with Periscope for live streaming.[14]

After growing the number of employees by more than 500 in 2015, the company responded to weak sales in the fourth quarter by cutting about 7% of its workforce (100 workers) in January 2016.[15]

At its peak, a share of GoPro was valued at $86, but on March 26, 2018, only $4.81.[16]

In November 2016, the company announced it was laying off an additional 200 employees in an effort to reduce costs. The company also announced that President Tony Bates would be stepping down at the end of 2016.[17] 270 more employees were laid off in March 2017,[18] and 250 additional layoffs followed in January 2018, bringing the company's workforce to "just under 1,000"[19]

Corporate actions

On March 30, 2011, GoPro acquired CineForm. The acquisition included the CineForm 444 video codec used in the film Slumdog Millionaire. The company claimed that the codec "makes HD and 3D editing faster and more convenient without sacrificing image quality". It was incorporated in the company's 3D Hero System shortly after the acquisition.[20][21]

In March 2013, GoPro issued a DMCA takedown notice to website DigitalRev.com, which had posted a review[22] of its product, citing trademark use as a breach of copyright. This notice was retracted 10 days later, citing "erroneous enforcement".[23][24]

On February 29, 2016, GoPro spent $105 million and acquired two start-ups, namely, Stupeflix and Vemory, for their video editing tools Replay and Splice.[25][26]

IPO

On February 7, 2014, GoPro submitted a confidential filing for an initial public offering (IPO) with the Securities and Exchange Commission (SEC).[27]

On May 19, 2014, GoPro filed its S-1 with the SEC without specifying the number of shares or their price. The company stated that they hoped to raise at least $100 million through the sale of shares, using the money to pay off debt in full ($111 million as of March 31, 2014) and "to acquire or invest in complementary businesses, technologies or assets". They said that they planned to list on the NASDAQ stock exchange using the symbol 'GPRO.'[28][29]

The expected price range was $21 to $24 a share; on June 25, 2014, GoPro sold 17.8 million shares to initial investors at $24 per share (totaling $427.2M).[30] At the IPO price the company was valued at $2.95 billion.[28] 1.5 percent of those shares were allotted to LOYAL3, a technology platform that allows small investors to participate.[31][32]

One reason for GoPro's decision to go public was the potential to become a media company to generate additional revenue from the content its cameras create.[33][34]

Product lines

HERO cameras

Woodman worked on his first camera for two years after founding the company, eventually introducing the GoPro 35mm HERO in September 2004 at San Diego's Action Sports Retailer trade show.[35] In its first year GoPro sold $150,000 worth of products.[35] In 2006 the company introduced its first Digital HERO, with 10 second video capability, and generated $800,000 in revenue. The following year GoPro sales quadrupled to $3.4 million.[35]

In 2014, the company was selling the HERO3+ in editions of different colors. It was capable of filming in 16:9 aspect ratio, supporting 4K UHD video and 12 MP still photographs.[36] The HERO4 was introduced on 24 September 2014.[37]

On September 28th 2017, GoPro released the Hero 6 camera, which claims improved stabilization over the Hero 5 models and is capable of capturing 4K video in 60 FPS.

GoPro KARMA & GoPro KARMA Grip

The GoPro Karma was GoPro's consumer drone, until its discontinuation in January 2018.

In 2014, GoPro entered into discussions with DJI for a private label model built with the GoPro branding. After the failure of these negotiations, GoPro entered into an agreement with 3D Robotics (3DR) for a similar partnership based on 3DR's flight controllers. 3DR failed to meet their agreed upon timelines. As a result, GoPro took full control of the development process in mid-2015.

Scheduled to be released early 2016, the GoPro Karma project was delayed several times before the GoPro Karma was announced with an introduction date of October 23, 2016. The Karma was released along with newer models of the HERO5 and Session cameras and features a removable handheld stabilizer (gimbal) integrated into the design. After a few customers complained about power failure during operation, GoPro recalled Karma drones and gave customers full refunds.[38]

In February 2017, GoPro re-launched the Karma Drone.[39] However, in January 2018, GoPro Inc. said that it will be cutting more than 20 percent of its global workforce and putting an end to its drone business after a disappointing fourth quarter. The company said it expects sales of about $340 million, well short of its own previous projection of as much as $480 million and the average analyst estimate of $472 million. Their revenue took an $80 million hit due to discounting for its Karma drones, as well as its Hero line of cameras, over the holiday season. [40]

GoPro Fusion

In November 2017, GoPro launched the Fusion camera[41], an omnidirectional camera which is capable of recording 360-degree footage. The Fusion was the first GoPro to feature an increased maximum resolution of 5.2K[42].

Accessories

GoPro produces various mounting accessories for its cameras including a 3-way mount, suction cup, chest harness, jaws-type flexible clamp, dog harness, surfing mount, etc.[43]

Video editing

The company developed GoPro Studio, simple video editing software to edit camera footage.[44] It was reported that GoPro intended to also become a content provider, also with a new app for the HERO5 called GoPro Quik to share, and edit videos easier.[34] You can also edit and shoot photos and videos using the GoPro app released in 2015.

Content company

In April 2014, GoPro was listed by Adweek as one of the "Top 10 Best Brand Channels on YouTube" based on a combination of views, shares, comments and overall engagement.[45] Content is uploaded daily, an additional source of revenue for the company.[46]

As part of its transformation to a media company in 2014, GoPro created additional channels with GoPro content on YouTube, Virgin America, and Xbox Live.[33] This was extended to the PlayStation Network in 2015.[47]

HD HERO cameras

As of October 2014, GoPro sells three fixed-lens cameras, two without viewfinders and one including a touchscreen viewfinder. A 2-bit LCD on the front of the camera allows access to its menu system, which is controlled by the front and top shutter buttons. The HERO4 Black has dimensions of 41 mm × 59 mm × 30 mm and weighs 88 grams (152 grams with housing). Still images from 6 to 12 megapixels can be captured. The cameras are sold with a clear polycarbonate HD Housing with a glass lens that is rated shockproof and waterproof to 131 feet (40 m), with a quick-release buckle on the top and threads at the bottom to attach to all of the GoPro mounts. The housing has metal buttons that connect to the camera's controls and has a "skeleton" backdoor option to allow audio recording when the camera is used with a mount but without the need to be watertight or shockproof.[48][non-primary source needed]

Products

HERO cameras

35mm

The 35mm camera (model #001) became available on April 13, 2005. It had dimensions of 2.5 by 3 inches (64 by 76 mm) and weighed 0.45 pounds (200 g). It included the camera, a clear case with quick release, a camera strap and ski glove adapter lash. It could pivot "on the fly" and be functional to a depth in water of about 15 feet (5 m). It was described as a "reusable wrist camera" and included a roll of 24 exposure Kodak 400 film.

Digital

The Digital HERO released in 2006 (Model: SQ907 mini-cam) had a 640×460 camera and shot VGA definition 320X240 (10 fps) video for a maximum of 10 seconds. The Digital HERO1 had 32 MB internal memory without SD slot.

Digital 3

The Digital HERO3 released in 2007 had a 3-megapixel camera and shot standard definition 512×384 video. It was rated up to 30 m (98.4 feet) in depth.[49]

Digital 5

The Digital HERO5 was first introduced on December 5, 2006. It had a 5 megapixel still photo sensor and supported standard definition (512×384) video capture. It ran on two AAA batteries, had 16 MB of internal memory and could function with a 2 GB SD card. Its housing was rated to 100 ft/30 meters depth. Its dimensions were 2.6 × 1.75 × 1.25 inches (66 × 44 × 32 mm). The camera is not designed to work with the newer HD HERO line of housings, although the standard screw mounts are indeed compatible.

Digital Wide

HD

The HD Hero shoots video at a maximum of 1080p 30fps, or 720p 60fps.

960

HD HERO 960 - shoots a maximum of 960p video[50] and is not compatible with GoPro's electronic accessories although the camera is compatible with all GoPro mounts. It was first listed on August 6, 2010.[51]

LED

The HD HERO Naked, released with a range of accessories, shoots a maximum of 1080p video on its 100 MP sensor.[52] The Naked camera line forms the basis for other bundles, which are differentiated by the types of mounts they have (HD Helmet HERO, HD Motorsports HERO, HD Surf HERO). It was first listed on January 25, 2010.

Specifications
  • Sensor size: 1/2.5-inch (5.75 mm × 4.28 mm)
  • Pixel size: 2.2 μm
  • Image formats:
Mode Size fps FOV
R1 848 × 480 60 170°
R2 1280 × 720 30 170°
R3 1280 × 720 60 170°
R4 1280 × 960 30 170°
R5 1920 × 1080 30 127°
Photo 2592 × 1944 0 170°

HERO2

The HERO2 was launched on October 24, 2011. It has an 11 MP image sensor, improved low-light capability and records at up to 120 fps.[53] It was sold with three different accessory packages as the Outdoor, Motorsports, and Surf Editions.[54]

HERO3

In late 2012, GoPro announced the HERO3 line of cameras.[55] These cameras came in three editions: black, silver and white.

All three versions of the HERO3 come in a 30% smaller and 25% lighter package, with WiFi built in. The change of the physical dimensions of the cameras compared to the previous generations (HERO1 and HERO2 were physically identical) means that some accessories for HD HERO Original and HERO2 are not compatible with HERO3, so GoPro made new versions of those accessories specifically for HERO3 (and mostly for HERO3+, see below). Those new versions of accessories are usually not compatible with older Hero camera generations. However, a lot of other accessories are compatible with all HD Hero camera generations.

The HERO3 Silver and Black cameras have significantly less battery endurance than the HD HERO Original and HERO2.[56] For example, in 720p resolution with 25/30 fps, while HD HERO Original and HERO2 have a stated battery runtime of 3 hours, HERO3 Silver Edition has a stated battery runtime of 2 hours, and HERO3 Black Edition has a stated battery runtime of 1.5 hours (the Black Edition's "most economical" setting is 1080p/30 fps, so this also partially contributes to its poor battery runtime).

The Black Edition[57][not in citation given] has a new 12 MP sensor that can capture 4K UHD digital video at 15 fps, 2.7K video at 30 fps, 1440p at 48 fps, 1080p at 60 fps, 960p at 100 fps, 720p at 120 fps and WVGA at 240 fps. The Black edition also includes the WiFi Remote. The Black Edition cannot record at 25/30 fps in 720p and WVGA resolutions; it can only record at very fast frame rates in those resolutions. This is a deliberate firmware limitation, as the manufacturer does not expect that this high-end camera model will be used at these lower resolutions and frame rates.

The Silver Edition uses the same 11 MP sensor as the HERO2, and the White edition uses the same 5 MP sensor as the HD HERO Original.

HERO3+

In October 2013, GoPro released the HERO3+, available in Black and Silver Editions,[58] replacing the HERO3 generation. The HERO3 White Edition remains as GoPro's low-end device.

The HERO3+ camera models claim dramatically improved low light performance and have a waterproof enclosure which is 20% lighter and 15% smaller than the HERO3's, according to the GoPro website. The HERO3+ camera housing is 20% smaller than the HERO3. The cameras are claimed to have improved image sharpness (close focus down to 7" vs about 3 ft on the HERO3, at the expense of distant focus which is slightly less sharp[clarification needed] with HERO3+), and better audio functionality with wind noise reduction. Battery life is claimed to be 30% longer than for the HERO3 model (both through better efficiency and a higher-capacity battery of the same dimensions).[56][59]

The Black Edition has video modes of 1440p48,[60] 1080p60, 960p100 and 720p120 as well as 4K15 and 2.7K30 and can shoot 12 MP stills at up to 30 fps. The HERO3+ Black Edition also offers an optional function in firmware (called "SuperView") which increases the field of view. It has additional functions, including dynamic low light situation adjustment, higher-quality recording modes (higher bitrates, no white balance applied, etc.) etc. The Black Edition continues to include a Wifi Remote. It does not have the ability to record 25/30 fps in 720p and WVGA modes (it can only record at very fast frame rates in those lower resolutions). This is an intentional firmware limitation. The battery runtime of HERO3+ Black Edition is significantly longer than HERO3 Black Edition but 30–50% lower than the battery runtime of the older HERO2 and HERO1.

The Silver Edition has video modes of 1080p60 and 720p120 and can shoot 10 MP stills at up to 10 fps.[61] In contrast to the Black Edition, the Silver Edition can record at 25/30 fps (or higher) in all supported resolutions. HERO3+ Silver Edition also has about 25%-50% longer battery runtime during recording than HERO3+ Black Edition (they both use the same batteries).[59] The difference in runtime depends on the resolution/fps combination, and whether WiFi and GoPro mobile application are used during recording. The difference in runtime increases as the fps is lowered and the additional functions are deactivated on both cameras. The battery runtime of HERO3+ Silver Edition is similar to the battery runtime of HERO2 and HERO1.

The HERO3 HD camera was awarded the 2013 Technology & Engineering Emmy Award for its contribution to television.[62]

HERO

The GoPro Hero can capture 5mp still images and has a 5fps burst option. It is able to record 1080P at 30 or 25fps and 720P at 60 or 50fps on to a MicroSD card up to 32GB. It has an LCD non touch display on the front and is waterproof up to 40m. It was released along side the HERO4 Black and HERO4 Silver.[63]

HERO4

In September 2014, GoPro announced the HERO4, available in Black Edition and Silver Edition,[51] which replace their respective HERO3+ generation predecessors. The HERO Session, a budget camera, was also announced.

The HERO4 Black Edition still has a 12 megapixel (MP) CMOS and a f/2.8 fixed maximum aperture and focus free. It adds Bluetooth connectivity, Highlight tag, Protune Available for photo and a new processor claimed by GoPro to be twice as fast as that of the HERO3+ Black Edition, doubling the frame rates in most resolutions. The HERO4 Black Edition can record 4K UHD video (3840×2160) at a frame rate of 24, 25 and 30 fps.[64] In Superview mode, 4K is only possible at 25 fps. Many other rates and resolutions are available. The HERO4 Black Edition still shoots stills at a maximum of 12 MP with a maximum burst rate of 30 fps. With Wi-Fi disabled at 4K/30, GoPro claims the HERO4 Black Edition battery life to be 65 minutes, increasing to a maximum of 1h 50' at 720p/240.[65] The HERO4 Black battery is in a different form factor than its predecessors. Initial side-by-side comparisons of HERO3+ and HERO4 Black edition video results suggest that the newer model has more detail at long range and similar performance at close range.

The HERO4 Silver Edition is basically a HERO3 Black Edition with the addition of a micro speaker,[66] built-in touchscreen display, Protune for photo and highlight tag (the first GoPro with this), a lower clocked Cortex-A9 and missing the Black Edition's integrated analog-to-digital converter which supports a wider variety of professional low-sensitivity external microphones.[67] The video modes supported by the HERO4 Silver Edition are similar to those of the HERO3+ Black, due to the higher processing speed and thermal requirements of encoding 4K video (3840×2160), but it supports Wi-Fi, Bluetooth and contains the same[68][69] Ambarella Inc. A9[70] system on a chip (SoC) as in the HERO4 Black.

The HERO Session, released July 6, 2015, is 50% smaller and 40% lighter compared to other versions of the GoPro HERO4 camera.[71]

The HERO4 models maintain the H.264 video codec of previous versions and MP4 file formats. GoPro claims the mono microphone in both the Black and Silver Editions has twice the dynamic range of that in the HERO3+, and that the HERO4 Black and Silver Editions have improved low-light performance.

Model HERO Session[72] Hero4 Silver[73] Hero4 Black[74]
Sensor Size 1/3.2" 1/2.3" 1/2.3"
Aperture f/2.8 f/2.8 f/2.8
Dimensions 38 x 38 x 38 mm 41 x 59 x 30 mm 41 x 59 x 30 mm
Weight 74 g 83 g (147 g with case) 88 g (152 g with case)
Still Image Resolution 8 MP 12 MP 12 MP
Video Modes 1440p30 1080p60 720p100 480p120 4k15 2.7k30 1080p60 720p120 480p240 4k30 2.7k60 1440p80 1080p120 720p240 480p240
Photo burst 10 fps 10 fps 30 fps
Connectivity WiFi, Bluetooth WiFi, Bluetooth WiFi, Bluetooth
Water Resistance 10 m 40 m (with case) 40 m (with case)
Touchscreen no 1.5 inches (38 mm) 320x240 optional extra
HERO+LCD

In June 2015, the company started to sell the GoPro HERO+LCD, which provides video recording at 1080p at 60 fps/and 8 megapixel photos. GoPro HERO+LCD has a touchscreen to preview the shot to frame the scene and letting the user navigate the menu.[75] A new feature in the camera was instant camera editing. GoPro HERO+LCD is waterproof, because it is built directly into a waterproof case (waterproof to 131 feet (40 m)). The device also includes a feature HiLight Tagging and built-in video editing function, which allows the user to put a label on the main points while shooting video or in the process of view, which makes it possible to quickly find desired footage later. It also has built-in Wi-Fi and Bluetooth, and user-friendly modes like QuikCapture, SuperView and Auto Low Light.

HERO+

In October 2015, GoPro released its third entry level camera: GoPro HERO+.[51] This camera is the same as the previous HERO+LCD with its 1080p 60 fps / 720p 60 fps video resolution, 8 MP / 5 fps burst photo resolution, built-in Wi-Fi and Bluetooth, waterproof up to 40 m and other modes like Superview, Auto Low Light, QuikCapture and Timelapse mode which automatically captures photos at set time intervals from 0.5 to 60 seconds. However, it does not have an LCD built-in touchscreen display and it is slightly lighter than HERO+LCD. The HERO+ weighs 123 g whereas the HERO+LCD weighs 127 g. The housing also remained the same.

HERO5

HERO5 Black and HERO5 Session were introduced in September 2016.[76] They are waterproof up to 10 m, support 4K video recording at up to 30 fps and 1080p at up to 120 fps, automatic upload of footage to cloud and voice controls.

Model HERO5 Session[77] HERO5 Black
Video Modes 4K30, 1440p60, 1080p90 4K30, 1440p80, 1080p120
Still Image Resolution 10 MP 12 MP
Photo burst 30 fps 30 fps
Connectivity WiFi, Bluetooth WiFi, Bluetooth
Water Resistance 10 m 10 m
Wired Connectors USB-C USB-C, micro HDMI
Battery built-in 1000 mAh, Li-Ion replaceable 1220 mAh, Li-Ion
Screen none touchscreen, 51 mm
Location Capture none GPS

HERO6

The HERO6 Black was introduced on September 28, 2017. The camera is waterproof up to 10 m, supports 4K HEVC video recording at up to 60 fps and 1080p at up to 240 fps, automatic upload of footage to cloud, voice controls and 5 GHz Wi-Fi. It will be the first GoPro with its own custom system on a chip (SoC) the GP1.

Model HERO6 Black
Video Modes 4K60, 2.7K120, 1080p240
Video Formats H.264/MPEG-4_AVC, H.265 (HEVC)
Still Image Resolution 12 MP
Photo burst 30 fps
Connectivity 5Ghz/2.4Ghz Wi-Fi, Bluetooth
Water Resistance 10 m
Wired Connectors USB-C, micro HDMI
Battery replaceable 1220 mAh, Li-Ion
Screen touchscreen, 51 mm, pinch zoom
Location Capture GPS

HERO (2018)

The HERO (2018 edition) is a new entry level camera, introduced on April 7, 2018.[78] The new model offers some similar features and functionality to the HERO5 and HERO6, like a touchscreen and built in timelapse video mode, but with slightly lower resolution and framerate, and lacking the GPS functionality and exposure control.

Model Hero (2018 edition)
Video Modes 1920x1080 (Full HD), 2560x1440 (Quad HD)
Video Formats H.264/MPEG-4_AVC, H.265 (HEVC)
Still Image Resolution 10 MP
Photo burst 10 fps
Connectivity 2.4Ghz Wi-Fi, Bluetooth
Water Resistance 10 m
Wired Connectors USB-C, micro HDMI
Battery replaceable 1220 mAh, Li-Ion
Screen touchscreen, 51 mm
Location Capture - (no GPS)

GoPro KARMA Drone

Karma Drone became available October 23, 2016. The drone is compatible with the HERO5 and HERO4 Black and Silver. The Drone has 20 minutes of battery life.[79] The stabilizer can be taken out and attached to a Karma grip. The Karma grip has greater than 1-hour battery life.

On November 8, 2016, Go Pro announced the recall of the Karma Drone following reports of loss of electrical power on the drone during operation.[80] On February 1, 2017, the company announced that the Karma Drone will return to stores with a redesigned battery latch.[81]

On January 9, 2018, GoPro announced that it was discontinuing the Karma drone and that it was exiting the drone marketplace.[82]

GoPro Omni

A camera rig that synchronizes six GoPro HERO4 Black cameras allowing users to stitch and make virtual reality 360° videos.

GoPro Fusion

The Fusion is an omnidirectional camera that was released November 2017 for $699.99.

GoPro Session

The Session is a mini camera released by GoPro. This camera is controlled by the GoPro app because on the camera there is only one button and most of the camera’s actual features are on the app. The GoPro Session can go an estimated amount of 10 meters or 33 feet underwater.

Chips

Starting from the Hero6 GoPro stopped using Ambarella SoC's and started making their own, starting with the GP1

GoPro GP1

The GoPro GP1 is their own System-on-Chip with the main task of image processing. It replaces the earlier used Ambarella SoC's and launched in the GoPro Hero6.[83] The SoC is designed in collaberation with Socionext.

The GP1 encodes video in the H.265 codec, also known as HEVC. The available resolutions are 4K60, 2.7K120 and 1080p240 unstabilized or 4K30, 2.7K60 and 1080p120 digitally stabilized.

See also



This article uses material from the Wikipedia article "GoPro", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Consumer products

.max, Maya, Challenge, Competition, Rendering, 3D, Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D, 3D library