powered by CADENAS

Social Share

Amazon

Moka pot (12388 views - Food Drinks Beverages)

The moka pot is a stove-top or electric coffee maker that brews coffee by passing boiling water pressurized by steam through ground coffee. Named after the Yemenite city of Mocha, it was invented by Luigi De Ponti. It was patented for the first time in Italy by an engineer named Alfonso Bialetti in 1933. Bialetti Industrie continues to produce the same model under the name "Moka Express." The moka pot is most commonly used in Europe (especially Italy, Portugal, Hungary, Spain and Switzerland) and in Latin America. It has become an iconic design, displayed in modern industrial art and design museums such as the Wolfsonian-FIU, Museum of Modern Art, the Cooper–Hewitt, National Design Museum, the Design Museum, and the London Science Museum. Moka pots come in different sizes, from one to eighteen 50 ml (2 imp fl oz; 2 US fl oz) servings. The original design and many current models are made from aluminium with Bakelite handles.
Go to Article

Explanation by Hotspot Model

Moka pot

Moka pot

Moka pot
Manufacturer Bialetti
Release date 1933

The moka pot is a stove-top or electric coffee maker that brews coffee by passing boiling water pressurized by steam through ground coffee. Named after the Yemenite city of Mocha, it was invented by Luigi De Ponti[1]. It was patented for the first time in Italy by an engineer named Alfonso Bialetti in 1933.[2] Bialetti Industrie continues to produce the same model under the name "Moka Express."

The moka pot is most commonly used in Europe (especially Italy, Portugal, Hungary, Spain and Switzerland) and in Latin America. It has become an iconic design, displayed in modern industrial art and design museums such as the Wolfsonian-FIU, Museum of Modern Art, the Cooper–Hewitt, National Design Museum, the Design Museum,[3] and the London Science Museum. Moka pots come in different sizes, from one to eighteen 50 ml (2 imp fl oz; 2 US fl oz) servings.[4] The original design and many current models are made from aluminium with Bakelite handles.

Variations and brands

Moka pots are used over a flame or electric range and are traditionally made of aluminium, though they are sometimes made out of stainless steel or other alloys.

"Brikka" is a modified moka pot manufactured by Bialetti. It incorporates a weighted valve as a pressure regulator on top of the nozzle that allows pressure to build up inside the water tank in a manner similar to a pressure cooker. As pressure builds up more quickly in this method (since there is much less leakage of vapour) compared to the standard moka pot, it reaches the level required for water to rise through the ground coffee in a shorter time. However, the weighted valve allows pressure to accumulate and temperature to rise somewhat further before the liquid bursts through the nozzle. The result is coffee brewed at a higher pressure and temperature than the standard pot, making it more similar to espresso and therefore with more visible crema.[citation needed]

How the moka pot works

"Mukka Express" is a modified moka pot also manufactured by Bialetti that allows milk to be frothed and mixed with the coffee during brewing. The name, "Mukka", is a pun on the Italian for milk-cow, mucca. Bialetti also manufactures several stainless steel moka pots, e.g., Musa, Class, and Venus.

Alessi is an Italian kitchenware manufacturer known for their moka pots. Cuisinox also markets several models of moka pots in both aluminium and stainless steel.[citation needed]

Also the design oriented Italian kitchenware manufacturer Serafino Zani is known for his moka pots: "Finlandia" designed by Tapio Wirkkala, "Mach" designed by Isao Hosoe and awarded with the Good Design Award (Chicago) 1993, "Thema" in stainess steel with titanium, and "Genesis" in stainless steel and copper, both designed by Tarcisio Zani.

Vev Viganò is an Italian manufacturer that specialises in stainless steel moka pots. Their product lines include Kontessa, Itaca, Vespress, and Carioca. In 2004 they produced a caffettiera 'UFO' designed by Vinod Gangotra, designed to receive two coffee cups that sit in recesses on the upper half of the machine and collect the coffee as it's brewed. The upper part is made from cast aluminium whilst the lower from stainless steel.[citation needed]

Bellman makes a stainless steel moka pot, the "CX-25 Series", operating at higher pressure and capable of creating a crema. It also has a wand to steam liquids, such as milk for cappuccino.[5]

The brand Volturno has been manufacturing moka pots in Argentina for many decades;[6] the name Volturno is sometimes used synonymously with moka pot there.[7]

Top Moka, another Italian manufacturer, offers two different styles of moka pots in a wide variety of colours. The more traditional Top Moka pot comes in sizes varying from two- to six-shot boilers. They also make mini moka pots in one- and two-shot sizes that use dispensing arcs rather than the standard collection chamber. Both are available with aluminium boilers for standard cooktops or titanium-alloy boilers for induction stoves.[8]

G.A.T. is also an Italian company based in Brescia involved in the production of Italian moka coffee-makers since 1986. The range of coffee-makers that G.A.T. proposes is wide and complete (more than 50 models), allowing one to choose among various products, materials, and prices, following the different market needs or personal liking.

After the Second World War, the Italian moka expanded all over the South Europe and it became the standard way of domestically making coffee. Its popularity led to non-Italian South European manufacturers making copies or new designs inspired in the original Italian design.

Another part of the world the Italian moka reached after the Second World War was Australia. Most post-war Italian migrants used the moka pot in their homes which eventually lead to many Australians of non-Italian backgrounds to also use the pot in their homes. It was widely available in many of the Italian-style delis and supermarkets that existed in Australia.

Brewing coffee with a moka pot

Funnel with ground coffee
Moka pot brewing
Coffee being brewed

The boiler (marked A in the diagram) is filled with water almost up to the safety release valve (some models have an etched water level sign) and the funnel-shaped metal filter (B) is inserted. Finely-ground coffee is added to the filter as shown below. Then the upper part (C, which has a second metal filter at the bottom) is tightly screwed onto the base. The pot is placed on a suitable heat source, the water is brought to its boiling point, and thereby steam is created in the boiler.

A gasket ensures a tightly closed unit and allows for pressure to safely build up in the lower section, where a safety valve provides a necessary release in case this pressure should get too high (with clean filters, that should not happen).

The steam eventually reaches a high enough pressure to gradually force the surrounding boiling water up the funnel through the coffee powder and into the upper chamber (C), where the coffee is collected. Although the "boiler" on a moka pot contains steam at elevated temperature and pressure, the water forced up through the grounds is no hotter than that used in other brewing methods – up to 90 °C, depending on the stage of extraction.[9][10]

When the lower chamber is almost empty, bubbles of steam mix with the upstreaming water, producing a characteristic gurgling noise. This "strombolian phase" allows a mixture of superheated steam and water to pass through the coffee, which leads to undesirable results, and therefore brewing should be stopped by removing the pot from the stove as soon as this stage is reached.[9]

Maintenance

Moka pots require periodic replacement of the rubber seal and the filters, and a check that the safety release valve is not blocked. When the rubber seal is new, it might alter the coffee taste, so do a couple of "dry runs" without coffee or with used coffee grounds to "prime" it.

Moka pot dimensions

Several models of Bialetti moka pots

The moka pot comes in various sizes based on the number of 50 mL (2 imp fl oz; 2 US fl oz) espresso cups they produce. The following table are the standard sizes for the Bialetti Moka Express.

Bialetti "Moka Express"
Espresso
cups
Metric units US units
Volume (mL) height (mm) base (mm) Volume (US fl oz) height (in) base (in)
1 60 133 64 2 5 14 2 12
3 200 159 83 6 12 6 14 3 14
6 300 216 102 10 8 12 4
9 550 254 105 18 12 10 4 18
12 775 292 127 25 11 12 5

Moka coffee characteristics

The flavour of moka pot coffee depends greatly on bean variety, roast level, fineness of grind, water profile, and the level of heat used.

Moka pots are sometimes referred to as stove-top espresso makers and produce coffee with an extraction ratio similar to (but somewhat higher than) that of a conventional espresso machine.[9] The resultant brew has increased extraction of caffeine and flavours from the grounds versus filter coffee, resulting in a stronger brew than that obtained by drip brewing.[citation needed] Furthermore, depending on bean variety and grind selection, moka pots can create a foam emulsion, known as crema.[citation needed]

However a typical moka coffee is extracted at relatively low pressures of 1 to 2 bar (100 to 200 kPa),[9] while standards for espresso coffee specify a pressure of 9 bar (900 kPa).[11][12] Therefore, moka coffee is not considered to be a true espresso and has different flavour characteristics.[citation needed]

See also



This article uses material from the Wikipedia article "Moka pot", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Food Drinks Beverages

food,liquor,alcohol,drink,beverage,coke