powered by CADENAS

Social Share

Amazon

Toast (9703 views - Food Drinks Beverages)

Toast is sliced bread that has been browned by exposure to radiant heat. This browning is the result of a Maillard reaction altering the flavor of the bread and making it firmer so that it is easier to spread toppings on it. Toasting is a common method of making stale bread more palatable. Bread is often toasted using a toaster, but toaster ovens are also used. Though many types of bread can be toasted the most commonly used is "toast bread", referring to bread that is already sliced and bagged upon purchase and may be white, brown, or multigrain. Toast is commonly eaten with butter or margarine and sweetened toppings, such as jam or jelly. Regionally, savoury spreads, such as peanut butter or yeast extracts, may also be popular. When buttered, toast may also be served as an accompaniment to savoury dishes, especially soups or stews, or topped with heartier ingredients like eggs or baked beans as a light meal. Toast is a common breakfast food. While slices of bread are most common, bagels and English muffins are also toasted. Scientific studies in the early 2000s found that toast may contain carcinogens caused by the browning process.
Go to Article

Explanation by Hotspot Model

Toast

Toast

Toast
A slice of bread, untoasted (left) and toasted (right)
Type Bread
Main ingredients Sliced bread
Cookbook: Toast  Media: Toast

Toast is sliced bread that has been browned by exposure to radiant heat. This browning is the result of a Maillard reaction altering the flavor of the bread and making it firmer so that it is easier to spread toppings on it. Toasting is a common method of making stale bread more palatable. Bread is often toasted using a toaster, but toaster ovens are also used. Though many types of bread can be toasted the most commonly used is "toast bread", referring to bread that is already sliced and bagged upon purchase and may be white, brown, or multigrain.

Toast is commonly eaten with butter or margarine and sweetened toppings, such as jam or jelly. Regionally, savoury spreads, such as peanut butter or yeast extracts, may also be popular. When buttered, toast may also be served as an accompaniment to savoury dishes, especially soups or stews, or topped with heartier ingredients like eggs or baked beans as a light meal. Toast is a common breakfast food. While slices of bread are most common, bagels and English muffins are also toasted. Scientific studies in the early 2000s found that toast may contain carcinogens caused by the browning process.[1][2]

Etymology and history

The word "toast", which means "sliced bread singed by heat" comes from the Latin torrere, "to burn".[3] The first reference to toast in print is in a recipe for Oyle Soppys (flavoured onions stewed in a gallon of stale beer and a pint of oil) that dates from 1430.[4] In the 1400s and 1500s, toast was discarded or eaten after it was used as a flavouring for drinks.[4] In the 1600s, toast was still thought of as something that was "put it into drinks. Shakespeare gave this line to Falstaff in The Merry Wives of Windsor, 1616: "Go, fetch me a quart of Sacke [sherry], put a tost in 't."[4] By the 1700s, there were references to "toast" as a gesture that indicates sexual attraction for a person: "Ay, Madam, it has been your Life's whole Pride of late to be the Common Toast of every Publick Table."[4]

Toast has been used as an element of American haute cuisine since at least the 1850s.[5]

Preparation

A classic two-slot toaster

In a modern home kitchen, the usual method of toasting bread is by the use of a toaster, an electrical appliance made for that purpose. To use a modern toaster, sliced bread is placed into the narrow slots on the top of the toaster, the toaster is tuned to the correct setting (some may have more elaborate settings than others) and a lever on the front is pushed down. The toast is ready when the lever pops up along with the toast. If the bread is insufficiently toasted, the lever can be pressed down again.

Bread toasted in a conventional toaster can "sweat" when it is served (i.e. water collects on the surface of the cooled toast). This occurs because moisture in the bread becomes steam while being toasted due to heat and when cooled the steam condenses into water droplets on the surface of the bread.[6]

It can also be toasted by a conveyor toaster which are often used in hotels, restaurants and other food service locations. These work by having one heating element on the top and one on the bottom with a metal conveyor belt in the middle which carries the toast between the two heating elements. This allows toast to be made consistently as more slices can be added at any time without waiting for previous ones to pop up.

Bread can also be toasted under a grill (or broiler), in an open oven, or lying on an oven rack. This "oven toast" is usually buttered before toasting. Toaster ovens are special small appliances made for toasting bread or for heating small amounts of other foods.

Bread can also be toasted by holding it near but not directly over an open flame, such as a campfire or fireplace; special toasting utensils (e.g. toasting forks) are made for this purpose. Before the invention of modern cooking appliances such as toasters and grills, bread has been produced in ovens for millennia, toast can be made in the same oven.

Many brands of ready sliced bread are available, some specifically marketing their suitability for toasting.

Consumption

Toast is most commonly eaten with butter or margarine spread over it, and may be served with preserves, spreads, or other toppings in addition to or instead of butter. Toast with jam or marmalade is popular. A few other condiments that can be enjoyed with toast are chocolate spread, cream cheese, and peanut butter. Yeast extracts such as Marmite in the UK, New Zealand and South Africa, and Vegemite in Australia are national traditions. Some sandwiches, such as the BLT,[7] call for toast to be used rather than bread.

Toast is an important component of many breakfasts, and is also important in some traditional bland specialty diets for people with gastrointestinal problems such as diarrhea.

In the United Kingdom, a dish popular with children is a soft-boiled egg eaten with toast soldiers at breakfast. Strips of toast (the soldiers) are dipped into the runny yolk of a boiled egg through a hole made in the top of the eggshell, and eaten.[8]

In southern Sri Lanka it is common for toast to be paired with a curry soup and mint tea.

By 2013 "artisanal toast" had become a significant food trend in upscale American cities like San Francisco, where some commentators decried the increasing number of restaurants and bakeries selling freshly made toast at what was perceived to be an unreasonably high price.[9][10]

Health concerns

Toasted bread slices may contain Benzo[a]pyrene and high levels of acrylamide, a carcinogen generated during the browning process.[1] High acrylamide levels can also be found in other heated carbohydrate-rich foods.[2] The darker the surface colour of the toast, the higher its concentration of acrylamide.[1] That is why, according to the recommendations made by the British Food Standards Agency, bread should be toasted to the lightest colour acceptable.[11]

Cultural references

The slang idiom "you're toast", "I'm toast" or "we're toast" is used to express a state of being "outcast", "finished", "burned, scorched, wiped out, [or] demolished" (without even the consolation of being remembered, as with the slang term "you're history")."[3] The first known use of "toast" as a metaphorical term for "you're dead" was in the 1984 film Ghostbusters, in which Bill Murray's character declares "This chick is toast" before the Ghostbusters attempt to burn the villain with their nuclear-powered weapons.[4] "Hey, dude. You're toast, man", which appeared in The St. Petersburg Times of Oct. 1, 1987, is the "...earliest [printed] citation the Oxford English Dictionary research staff has of this usage."[3]

Another popular idiom associated with the word "toast" is the expression "to toast someone's health", which is typically done by one or more persons at a gathering by raising a glass in salute to the individual. This meaning is derived from the early meaning of toast, which from the 1400s to the 1600s meant warmed bread that was placed in a drink. By the 1700s, there were references to the drink in which toast was dunked being used in a gesture that indicates respect: "Ay, Madam, it has been your Life's whole Pride of late to be the Common Toast of every Public Table."[4][better source needed]

Humorous observations have been made about buttered toast. It has been noted that buttered toast has a perceived tendency, when dropped, to land with the buttered side to the floor, the least desirable outcome. Although the concept of "dropped buttered toast" was originally a pessimistic joke, a 2001 study of the buttered toast phenomenon found that when dropped from a table, a buttered slice of toast landed butter-side down at least 62% of the time.[12] The phenomenon is widely believed to be attributable to the combination of the size of the toast and the height of the typical dining table, which means that the toast will not rotate far enough to right itself before encountering the floor.[13][14] A joke that plays on this tendency is the buttered cat paradox; if cats always land on their feet and buttered toast always lands buttered side down, it questions what happens when buttered toast is attached to a cat's back.

Other foods which are toasted

Cheese and marshmallows are also toasted by exposure to dry radiant heat.[15][16] A toasted cheese sandwich features toasted cheese and toasted bread. Bagels, English muffins and Pop Tart pastries are foods that can be toasted too.

See also



This article uses material from the Wikipedia article "Toast", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Food Drinks Beverages

food,liquor,alcohol,drink,beverage,coke