powered by CADENAS

Social Share

Amazon

Hose reel (2157 views - Plant Design)

A Hose Reel is a cylindrical spindle made of either metal, fiberglass, or plastic and is used for storing a hose. The most common styles of hose reels are spring driven (which is self retracting), hand crank, or motor driven. Hose reels are categorized by the diameter and length of the hose they hold, the pressure rating and the rewind method. Hose reels can either be fixed in a permanent location, or portable and attached to a truck, trailer, or cart.
Go to Article

Explanation by Hotspot Model

Hose reel

Hose reel

A Hose Reel is a cylindrical spindle made of either metal, fiberglass, or plastic and is used for storing a hose. The most common styles of hose reels are spring driven (which is self retracting), hand crank, or motor driven. Hose reels are categorized by the diameter and length of the hose they hold, the pressure rating and the rewind method. Hose reels can either be fixed in a permanent location, or portable and attached to a truck, trailer, or cart.



This article uses material from the Wikipedia article "Hose reel", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Plant Design

Aveva Tribon, Aveva PDMS, Intergraph Smartplant, Intergraph Smartmarine, Offshore, Onshore, Marine, Shipyard, Plantdesign