Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Slippers are light footwear that are easy to put on and off and are intended to be worn indoors, particularly at home.[1]
The recorded history of slippers can be traced back to the 12th century when the Vietnamese had been wearing slippers. But in the West, the record can only be traced to 1478.[2]
The historical record of slippers in the west is about in Sultan when people wear them indoors to slip.[3]
This section needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (June 2016) (Learn how and when to remove this template message) |
The following is a partial list of types of slippers:
Some slippers are made to resemble something other than a slipper and are sold as a novelty item. The slippers are usually made from soft and colorful materials and may come in the shapes of animals, animal paws, vehicles, cartoon characters, etc.
Contrary to popular belief, not all shoes with a soft fluffy interior are slippers. By definition, any shoe with a rubber sole and laces is a normal outdoor shoe. In India, rubber chappals (flip-flops) are worn as indoor shoes.[4]
The fictional character Cinderella is said to have worn glass slippers; in modern parlance, they would probably be called glass high heels. This motif was introduced in Charles Perrault's 1697 version of the tale, "Cendrillon ou la petite pantoufle de verre" ("Cinderella, or The Little Glass Slipper"). For some years it was debated that this detail was a mistranslation and the slippers in the story were instead made of fur (French: vair), but this interpretation has since been discredited by folklorists.[5]
Derek "The Slipper Man" Fan holds the Guinness World Records record for wearing a pair of dress slippers for 23 years straight as of June 30, 2007.[6]
The ruby slippers worn by Judy Garland in The Wizard of Oz sold for a record $165,000.[6]
Grandpa's Slippers is an award-winning book by Joy Watson.[7]
In Hawaii, slippers, or "slippahs" is used for describing traditional flip-flops.
Wikimedia Commons has media related to Slippers. |
This article uses material from the Wikipedia article "Slipper", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,fashion,clothes,shoes,hat,glasses,wearables,iot,hardware