Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Yosarian).
A smile is a facial expression formed primarily by flexing the muscles at the sides of the mouth. It is believed it takes about 42 muscles to smile.[1] Some smiles include a contraction of the muscles at the corner of the eyes, an action known as a "Duchenne smile". Smiles performed without the eye contraction may be perceived as insincere.
Among humans, smiling is an expression denoting pleasure, sociability, happiness, joy or amusement. It is distinct from a similar but usually involuntary expression of anxiety known as a grimace. Although cross-cultural studies have shown that smiling is a means of communication throughout the world,[2] there are large differences among different cultures, with some using smiles to convey confusion or embarrassment.
Primatologist Signe Preuschoft traces the smile back over 30 million years of evolution to a "fear grin" stemming from monkeys and apes who often used barely clenched teeth to portray to predators that they were harmless, or to signal submission to more dominant group members. The smile may have evolved differently among species and especially among humans.[3] Apart from Biology as an academic discipline that interprets the smile, those who study kinesics and psychology such as Freitas-Magalhaes view the smile as an affect display that can communicate feelings such as love, happiness, glee, pride, contempt, and embarrassment. Also, other types of primates can express this gesture as a symbol of happiness and fun.
A smile seems to have a favorable influence upon others and makes one likable and more approachable.[4] In the social context, smiling and laughter have different functions in the order of sequence in social situations:
Smiling is a signaling system that evolved from a need to communicate information of many different forms. One of these is advertisement of sexual interest. Female smiles are appealing to heterosexual males, increasing physical attractiveness and enhancing sex appeal. However, recent research indicates a man's smile may or may not be most effective in attracting heterosexual women, and that facial expressions such as pride or even shame might be more effective. The researchers ignored the role of smiles in other sexual preferences.[6]
The influence of smiling on others is not necessarily benign. It may take the form of positive reinforcement, possibly for an underhand manipulative and abusive purpose.[7] See also superficial smile.
While smiling is perceived as a positive emotion most of the time, there are many cultures that perceive smiling as a negative expression and consider it unwelcoming. Too much smiling can be viewed as a sign of shallowness or dishonesty.[9] In some parts of Asia, people may smile when they are embarrassed or in emotional pain. Some people may smile at others to indicate a friendly greeting. A smile may be reserved for close friends and family members. Many people in the former Soviet Union area consider smiling at strangers in public to be unusual and even suspicious behavior. [10]
Cheek dimples are visible indentations of the epidermis, caused by underlying flesh, which form on some people's cheeks, especially when they smile. Dimples are genetically inherited and are a dominant trait. A rarer form is the single dimple, which occurs on one side of the face only. Anatomically, dimples may be caused by variations in the structure of the facial muscle known as zygomaticus major. Specifically, the presence of a double or bifid zygomaticus major muscle may explain the formation of cheek dimples.[11]
This bifid variation of the muscle originates as a single structure from the zygomatic bone. As it travels anteriorly, it then divides with a superior bundle that inserts in the typical position above the corner of the mouth. An inferior bundle inserts below the corner of the mouth.
While conducting research on the physiology of facial expressions in the mid-19th century, French neurologist Guillaume Duchenne identified two distinct types of smiles. A Duchenne smile involves contraction of both the zygomatic major muscle (which raises the corners of the mouth) and the orbicularis oculi muscle (which raises the cheeks and forms crow's feet around the eyes).[12] The Duchenne smile has been described as "smizing", as in "smiling with the eyes".[13]
A non-Duchenne smile involves only the zygomatic major muscle.[14] "Research with adults initially indicated that joy was indexed by generic smiling, any smiling involving the raising of the lip corners by the zygomatic major [...]. More recent research suggests that smiling in which the muscle around the eye contracts, raising the cheeks high (Duchenne smiling), is uniquely associated with positive emotion."[15]
The Pan Am smile, also known as the "Botox smile", is the name given to a fake smile, in which only the zygomatic major muscle is voluntarily contracted to show politeness. It is named after the now defunct airline Pan American World Airways, whose flight attendants would always flash every passenger the same perfunctory smile.[16] Botox was introduced for cosmetic use in 2002.[17] Chronic use of Botox injections to deal with eye wrinkle can result in the paralysis of the small muscles around the eyes, preventing the appearance of a Duchenne smile.
In animals, the baring of teeth is often used as a threat or warning display—known as a snarl—or a sign of submission. For chimpanzees, it can also be a sign of fear. However, not all animal displays of teeth convey negative acts or emotions. For example, Barbary macaques demonstrate an open mouth display as a sign of playfulness which likely has similar roots and purposes as the human smile.[18]
This article uses material from the Wikipedia article "Smile", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D