Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Panzerkampfwagen V Panther | |
---|---|
Panther Ausf. D tanks, 1943. The D model can best be recognized by the drum-shaped cupola. | |
Type | Medium tank |
Place of origin | Nazi Germany |
Service history | |
In service |
|
Used by |
Nazi Germany France Limited use by other militaries (see Postwar and foreign use) |
Wars | World War II |
Production history | |
Designer | MAN AG |
Designed | 1942 |
Manufacturer | MAN, Daimler-Benz, MNH |
Unit cost |
117,100 Reichmarks (Without weapons, optics, or radio) 176.100 Reichmarks (combat ready)[1] |
Produced | 1943–1945 (1946- 9 postwar for the British Army) |
No. built | about 6,000[2] |
Variants | Ausf. D, Ausf. A, Ausf. G, Befehlspanzer (command tank), Beobachtungspanzer (artillery observer vehicle), Bergepanther (armoured recovery vehicle) |
Specifications | |
Weight | 44.8 tonnes (44.1 long tons; 49.4 short tons)[3] |
Length |
6.87 m (22 ft 6 in) 8.66 metres (28 ft 5 in) gun forward[3] |
Width |
3.27 m (10 ft 9 in)[3] 3.42 m (11 ft 3 in) with skirts |
Height | 2.99 m (9 ft 10 in) |
Crew | 5 (driver, radio-operator/hull machine gunner, commander, gunner, loader) |
| |
Armour | up to 80 mm (sloped at 35°) |
Main armament |
|
Secondary armament | |
Engine |
V-12 petrol Maybach HL230 P30[3] 700 PS (690 hp, 515 kW) |
Power/weight | 15.39 PS (11.5 kW)/tonne (13.77 hp/ton) |
Transmission | ZF AK 7-200. 7 forward 1 reverse[3] |
Suspension | double torsion bar, interleaved road wheels |
Fuel capacity | 720 litres (160 imp gal; 190 US gal) |
Operational range |
Road: 200 km (120 mi) Cross-country: 100 km (62 mi) [4] |
Speed |
55 km/h (34 mph) (first models) 46 km/h (29 mph) (later models) |
The Panther is a German medium tank deployed during World War II on the Eastern and Western Fronts in Europe from mid-1943 to the war's end in 1945. It had the ordnance inventory designation of Sd.Kfz. 171. It was designated as the Panzerkampfwagen V Panther until 27 February 1944, when Hitler ordered that the Roman numeral "V" be deleted. Contemporary English language reports sometimes refer to it as the Mark V.
The Panther was intended to counter the Soviet T-34 and to replace the Panzer III and Panzer IV. Nevertheless, it served alongside the Panzer IV and the heavier Tiger I until the end of the war. It is considered one of the best tanks of World War II for its excellent firepower and protection, although its reliability was less impressive.[5]
The Panther was a compromise. While having essentially the same engine as the Tiger I, it had more efficient frontal hull armour,[6] better gun penetration, was lighter and faster, and could traverse rough terrain better than the Tiger I. The trade-off was weaker side armour, which made it vulnerable to flanking fire. The Panther proved to be effective in open country and long range engagements, but did not provide enough high explosive firepower against infantry.[7]
The Panther was far cheaper to produce than the Tiger I, and only slightly more expensive than the Panzer IV. Key elements of the Panther design, such as its armour, transmission, and final drive, were simplifications made to improve production rates and address raw material shortages. The overall design remained somewhat over-engineered.[8][9] The Panther was rushed into combat at the Battle of Kursk despite numerous unresolved technical problems, leading to high losses due to mechanical failure. Most design flaws were rectified by late 1943 and the spring of 1944, though the bombing of production plants, increasing shortages of high quality alloys for critical components, shortage of fuel and training space, and the declining quality of crews all impacted the tank's effectiveness.
Though officially classified as a medium tank, its weight is more like that of a heavy tank, as its weight of 44.8 tons puts it roughly in the same category as the American M26 Pershing (41.7 tons), British Churchill (40.7 tons) and the Soviet IS-2 (46 tons) heavy tanks. The tank had a very high power to weight ratio however, making it extremely mobile regardless of its weight. Its weight still caused heavy tank-esque problems however, such as an inability to cross certain bridges.
The Panther was born out of a project started in 1938 to replace the Panzer III and Panzer IV tanks. The initial requirements of the VK 20 series called for a fully tracked vehicle weighing 20 tonnes and design proposals by Krupp, Daimler Benz and MAN ensued. These designs were abandoned and Krupp dropped out of the competition entirely as the requirements increased to a vehicle weighing 30 tonnes, a direct reaction to the encounters with the Soviet T-34 and KV-1 tanks and against the advice of Wa Pruef 6.[Notes 1][10] The T-34 outclassed the existing models of the Panzer III and IV.[11][12] At the insistence of General Heinz Guderian, a special tank commission was created to assess the T-34.[13] Among the features of the Soviet tank considered most significant were the sloping armour, which gave much improved shot deflection and also increased the effective armour thickness against penetration, the wide track, which improved mobility over soft ground, and the 76.2 mm (3.00 in) gun, which had good armour penetration and fired an effective high explosive round. Daimler-Benz (DB), which designed the successful Panzer III and StuG III, and Maschinenfabrik Augsburg-Nürnberg AG (MAN) were given the task of designing a new 30- to 35-tonne tank, designated VK 30.02, by April 1942.
The DB design resembled the T-34 in its hull and turret and was also to be powered by a diesel engine. It was also driven from the rear drive sprocket with the turret situated forward. The incorporation of a diesel engine promised increased operational range, reduced flammability and allowed for more efficient use of petroleum reserves. Hitler himself considered a diesel engine imperative for the new tank.[14] DB's proposal used an external leaf spring suspension, in contrast to the MAN proposal of twin torsion bars. Wa Pruef 6's opinion was that the leaf spring suspension was a disadvantage and that using torsion bars would allow greater internal hull width. It also opposed the rear drive because of the potential for track fouling. Daimler Benz still preferred the leaf springs over a torsion bar suspension as it resulted in a silhouette about 200 mm (7.9 in) shorter and rendered complex shock absorbers unnecessary. The employment of a rear drive provided additional crew space and also allowed for a better slope on the front hull, which was considered important in preventing penetration by armour-piercing shells.[10]
The MAN design embodied more a conventional configuration, with the transmission and drive sprocket in the front and a centrally mounted turret. It had a petrol engine and eight torsion-bar suspension axles per side. Because of the torsion bar suspension and the drive shaft running under the turret basket, the MAN Panther was higher and had a wider hull than the DB design. The Henschel firm's design concepts for their Tiger I tank's suspension/drive components, using its characteristic Schachtellaufwerk format – large, overlapping, interleaved road wheels with a "slack-track" using no return rollers for the upper run of track, also features shared with almost all German military half-track designs since the late 1930s – were repeated with the MAN design for the Panther. These multiple large, rubber-rimmed steel wheels distributed ground pressure more evenly across the track. The MAN proposal also complemented Rheinmetall's already designed turret modified from that of the VK 45.01 (H),[15] and used a virtually identical Maybach V12 engine to the Tiger I heavy tank's Maybach HL230 powerplant model.
The two designs were reviewed from January to March 1942. Reichminister Todt, and later, his replacement Albert Speer, both recommended the DB design to Hitler because of its advantages over the initial MAN design. At the final submission, MAN refined its design, having learned from the DB proposal apparently through a leak by a former employee in the Wa Pruef 6, senior engineer Heinrich Ernst Kniepkamp and others.[14] On 5 March 1942, Albert Speer reported that Hitler considered the Daimler-Benz design to be superior to MAN's design.[16] A review by a special commission appointed by Hitler in May 1942 selected the MAN design. Hitler approved this decision after reviewing it overnight. One of the principal reasons given for this decision was that the MAN design used an existing turret designed by Rheinmetall-Borsig, while the DB design would have required a brand new turret and engine to be designed and produced, delaying the commencement of production.[17] This time-saving measure compromised the subsequent development of the design.[18]
Albert Speer recounts in his autobiography Inside the Third Reich
Since the Tiger had originally been designed to weigh fifty tons but as a result of Hitler's demands had gone up to fifty seven tons, we decided to develop a new thirty ton tank whose very name, Panther, was to signify greater agility. Though light in weight, its motor was to be the same as the Tiger's, which meant it could develop superior speed. But in the course of a year Hitler once again insisted on clapping so much armor on it, as well as larger guns, that it ultimately reached forty eight tons, the original weight of the Tiger.[19]
A mild steel prototype of the MAN design was produced by September 1942 and, after testing at Kummersdorf, was officially accepted. It was put into immediate production. The start of production was delayed, mainly because of a shortage of specialized machine tools needed for the machining of the hull. Finished tanks were produced in December and suffered from reliability problems as a result. The demand for this tank was so high that the manufacturing was soon expanded beyond MAN to include Daimler-Benz (Berlin-Marienfelde, former DMG plant), Maschinenfabrik Niedersachsen Hanover (MNH, subsidiary of Eisenwerk Wülfel/Hanomag) and Henschel & Sohn in Kassel.
The initial production target was 250 tanks per month at the MAN plant Nuremberg. This was increased to 600 per month in January 1943. Despite determined efforts, this figure was never reached due to disruption by Allied bombing, and manufacturing and resource bottlenecks. Production in 1943 averaged 148 per month. In 1944, it averaged 315 a month (3,777 having been built that year), peaking with 380 in July and ending around the end of March 1945, with at least 6,000 built in total. Front-line combat strength peaked on 1 September 1944 at 2,304 tanks, but that same month a record number of 692 tanks were reported lost.[2]
Allied bombing was first directed at the common chokepoint for both Panther and Tiger production: the Maybach engine plant. This was bombed the night of 27/28 April 1944 and production was halted for five months. A second factory had already been planned, the Auto Union Siegmar plant (the former Wanderer car factory), and this came on line in May 1944.[20] The targeting of Panther factories began with a bombing raid on the DB plant on 6 August 1944, and again on the night of 23/24 August. MAN was struck on 10 September, 3 October and 19 October 1944, and then again on 3 January and 20/21 February 1945. MNH was not attacked until 14 and 28 March 1945.[21]
In addition to interfering with tank production goals, the bombing forced a steep drop in the production of spare parts, which as a percentage of tank production dropped from 25–30 percent in 1943 to 8 percent in late 1944. This compounded the problems with reliability and the numbers of operational Panthers, as tanks in the field had to be cannibalized for parts.[22]
The Panther was the third most produced German armoured fighting vehicle, after the Sturmgeschütz III assault gun/tank destroyer at 9,408 units, and the Panzer IV tank at 8,298 units.
Model | Number | Date | Notes |
---|---|---|---|
Prototype | 2 | Sep 1942 | Designated V1 and V2 |
Ausf. D | 842 | Jan 1943 to Sept 1943 | |
Ausf. A | 2,200 | Aug 1943 to Aug 1944 | Sometimes called Ausf. A2 |
Ausf. G | ~2,961 | Mar 1944 to Apr 1945 | |
Befehlspanzer Panther | 329 | May 1943 to Apr 1945 | Converted on the production line[citation needed] |
Beobachtungspanzer Panther | 1 | 1944 | Converted |
Bergepanther | 339 | 1943 to 1945 | 61 more converted from rebuilt chassis |
Manufacturer | % of total |
---|---|
Maschinenfabrik Augsburg-Nürnberg (M.A.N.) | 35% |
Daimler-Benz | 31% |
Maschinenfabrik Niedersachsen-Hannover | 31% |
Other | 3% |
The cost of a Panther tank has been given as 117,100 Reichmarks (RM)[citation needed]. This compared with 82,500 RM for the StuG III, 96,163 RM for the Panzer III, 103,462 RM for the Panzer IV, and 250,800 RM for the Tiger I. These figures did not include the cost of the armament and radio.[25][26] Using slave labour on the production lines greatly reduced costs, but also greatly increased the risk of sabotage. French army studies in 1947 found that many Panthers had been sabotaged during production.[27] The Germans increasingly strove for production methods that would allow higher production rates and lower cost. By comparison the total cost of the early production Tiger I in 1942–1943 has been stated to be as high as 800,000 RM.[28]
The process of streamlining the production of German armoured fighting vehicles first began after Speer became Reichminister in early 1942, and steadily accelerated through to 1944; the production of the Panther tank coincided with this period of increased manufacturing efficiency. At the beginning of the war, German armoured fighting vehicle manufacturers had employed labour-intensive and costly manufacturing methods unsuitable for the needs of mass production; even with streamlined production methods, Germany never approached the efficiency of Allied manufacturing during World War II.[29]
The weight of the production model was increased to 45 tonnes from the original plans for a 35 tonne tank. Hitler was briefed thoroughly on the comparison between the MAN and DB designs in the report by Guderian's tank commission. Armour protection appeared to be inadequate, while "the motor mounted on the rear appeared to him correct". He agreed that the "decisive factor was the possibility of quickly getting the tank into production". On 15 May 1942, Oberst Fichtner informed MAN that Hitler had decided in favour of the MAN Panther and ordered series production. The upper glacis plate was to be increased from 60 mm (2.4 in) to 80 mm (3.1 in). Hitler demanded that an increase to 100 mm (3.9 in) should be attempted and that at least all vertical surfaces were to be 100 mm (3.9 in); the turret front plate was increased from 80 mm (3.1 in) to 100 mm (3.9 in).[30]
The Panther was rushed into combat before all of its teething problems had been corrected. Reliability was considerably improved over time, and the Panther proved to be a very effective fighting vehicle,[31] but some design flaws, such as its weak final drive units, were never corrected.
The crew had five members: driver, radio operator (who also fired the bow machine gun), gunner, loader, and commander.
The first 250 Panthers were powered by a Maybach HL 210 P30 engine, V-12 petrol engine, which delivered 650 metric hp at 3,000 rpm and had three simple air filters.[32] Starting in May 1943, the Panthers were built using the 700 metric hp (690 hp, 515 kW) at 3,000 rpm, 23.1 litre Maybach HL 230 P30 V-12 petrol engine. To save aluminium, the light alloy block used in the HL 210 was replaced by a cast iron block. Two multistage "cyclone" air filters were used to improve dust removal.[33][34] Due to the use of low grade petrol, the engine power output was reduced. With a capacity of 730 litres (160 imperial gallons; 190 US gallons) of fuel, a fully fuelled Panther's range was 200 km (120 mi) on surfaced roads and 100 km (62 mi) cross country.[4]
The HL 230 P30 engine was a very compact tunnel crankcase design, and it kept the space between the cylinder walls to a minimum. The crankshaft was composed of seven "discs" or main journals, each with an outer race of roller bearings, and a crankshaft pin between each disc. To reduce the length of the engine by an inch or so, and reduce unbalanced rocking moment caused by a normal offset-Vee type engine, the two banks of 6 cylinders of the V-12 were not offset – the "big ends" of the connecting rods of each cylinder pair in the "V" where they mated with the crankpin were thus at the same spot with respect to the engine block's length rather than offset; this required a "fork and blade" matched pair of connecting rods for each transversely oriented pair of cylinders. Usually, "V"-form engines have their transversely paired cylinders' connecting rods' "big ends" simply placed side by side on the crankpin, with their transverse pairs of cylinders offset slightly to allow the connecting rod big ends to attach side by side while still being in the cylinder bore centerline. This compact arrangement with the connecting rods was the source of considerable problems initially.[35] Blown head gaskets were another problem, which was corrected with improved seals in September 1943. Improved bearings were introduced in November 1943. An engine governor was also added in November 1943 that reduced the maximum engine speed to 2500 rpm. An eighth crankshaft bearing was added beginning in January 1944 to reduce motor failures.[36]
The engine compartment space was designed to be watertight so that the Panther could ford water obstacles; however, this made the engine compartment underventilated and prone to overheating. The fuel connectors in the early models were not insulated, leading to the leakage of fuel fumes into the engine compartment, which caused engine fires in the early Panthers. Additional ventilation was added to draw off these gases, which only partly solved the problem of engine fires.[37] Other measures taken to reduce this problem included improving the coolant circulation inside the motor and adding a reinforced membrane spring to the fuel pump.[38] Despite the risks of fire, the fighting compartment was relatively safe due to a solid firewall that separated it from the engine compartment.[39]
Engine reliability improved over time. A French assessment in 1947 of their stock of captured Normandy Panther A tanks concluded that the engine had an average life of 1,000 km (620 mi) and maximum life of 1,500 km (930 mi).[40]
The suspension consisted of front drive sprockets, rear idlers and eight double-interleaved rubber-rimmed steel road wheels on each side — in the so-called Schachtellaufwerk design, suspended on a dual torsion bar suspension. The dual torsion bar system, designed by Professor Ernst Lehr, allowed for a wide travel stroke and rapid oscillations with high reliability, thus allowing for relatively high speed travel over undulating terrain. The extra space required for the bars running across the length of the bottom of the hull, below the turret basket, increased the overall height of the tank. When damaged by mines, the torsion bars often required a welding torch for removal.[41]
The Panther's suspension was overengineered and the Schachtellaufwerk interleaved road wheel system made replacing inner road wheels time consuming (though it could operate with missing or broken wheels). The interleaved wheels also had a tendency to become clogged with mud, rocks and ice, and could freeze solid overnight in the harsh winter weather that followed the autumn rasputitsa mud season on the Eastern Front. Shell damage could cause the road wheels to jam together and become difficult to separate.[42] Interleaved wheels had long been standard on all German half-tracks. The extra wheels did provide better flotation and stability, and also provided more armour protection for the thin hull sides than smaller wheels or non-interleaved wheel systems, but the complexity meant that no other country ever adopted this design for their tanks.[43] In September 1944, and again in March/April 1945, M.A.N. built a limited number of Panthers with overlapping, non-interleaved steel-rimmed 80 cm diameter roadwheels originally designed for Henschel's Tiger II and late series Tiger I Ausf. E tanks. These steel-rimmed roadwheels were introduced from chassis number 121052 due to raw material shortages.[44]
From November 1944 through February 1945, a conversion process began to use sleeve bearings in the Panther tank, as there was a shortage of ball bearings. The sleeve bearings were primarily used in the running gear; plans were also made to convert the transmission to sleeve bearings, but were not carried out due to the ending of Panther production.[45]
Steering was accomplished through a seven-speed AK 7-200 synchromesh gearbox, designed by Zahnradfabrik Friedrichshafen (ZF), and a MAN single radius steering system, operated by steering levers. Each gear had a fixed radius of turning, ranging from 5 m (16 ft) for 1st gear up to 80 m (260 ft) for 7th gear. The driver was expected to judge the sharpness of a turn ahead of time and shift into the appropriate gear to turn the tank. The driver could also engage the brakes on one side to force a sharper turn.[46] This manual steering was a much simplified design, compared to the sophisticated dual-radius hydraulically controlled steering system of the Tiger tanks.
The AK 7-200 transmission was also capable of pivot turns, but this high-torque method of turning could cause failures of the final drive.[47]
The Panthers' main weakness was its final drive unit. The problems stemmed from several factors. The original MAN proposal had called for the Panther to have an epicyclic gearing (planetary) system in the final drive, similar to that used in the Tiger I.[48] Germany suffered from a shortage of gear-cutting machine tools and, unlike the Tiger tanks, the Panther was intended to be mass-produced. To achieve the goal of higher production rates, numerous simplifications were made to the design and its manufacture. This process was aggressively pushed forward, sometimes against the wishes of designers and army officers, by the Chief Director of Armament and War Production, Karl-Otto Saur (who worked under, and later succeeded, Reichminister Speer). Consequently, the final drive was changed to a double spur system.[49] Although much simpler to produce, the double spur gears had inherently higher internal impact and stress loads, making them prone to failure under the high torque requirements of the heavy Panther tank. Because of the significant numbers of breakdowns, the Wehrmacht was forced to move the Panther D and Tiger I tanks by rail, throughout 1943. The tanks could not participate in major movements of more than 100 km without adversely affecting unit strengths due to breakdowns.[50]
Initial production Panthers had a face-hardened glacis plate (the main front hull armour piece), but as armour-piercing capped rounds became the standard in all armies (thus defeating the benefits of face-hardening, which caused uncapped rounds to shatter), this requirement was deleted in March 1943. By August 1943, Panthers were being built only with a homogeneous steel glacis plate.[51] The front hull had 80 mm (3.1 in) of armour angled at 55 degrees from the vertical, welded but also interlocked for strength. The combination of well-sloped and thick armour meant that heavy Allied weapons, such as the Soviet 122 mm A-19, 100 mm BS-3 and US 90 mm M3[52] were needed to assure penetration of the upper glacis at all combat ranges.[53][dubious – discuss]
The armour for the side hull and superstructure (the side sponsons) was much thinner (40–50 mm (1.6–2.0 in)). The thinner side armour was necessary to keep the tanks' weight down, but it made the Panther vulnerable to hits from the side by all Allied tank and anti-tank guns. German tactical doctrine for the use of the Panther emphasized the importance of flank protection.[54] 5 mm (0.20 in) thick spaced armour, known as Schürzen, intended to provide protection for the lower side hull from Soviet anti-tank rifle fire, was fitted on the hull side. Zimmerit coating against magnetic mines started to be applied at the factory on late Ausf D models beginning in September 1943;[55] an order for field units to apply Zimmerit to older versions of the Panther was issued in November 1943.[56] In September 1944, orders to stop all application of Zimmerit were issued, based on false rumours that hits on the Zimmerit had caused vehicle fires.[57]
Panther crews were aware of the weak side armour and made augmentations by hanging track links or spare roadwheels onto the turret and/or the hull sides.[58] The rear hull top armour was only 16 mm (0.63 in) thick, and had two radiator fans and four air intake louvres over the engine compartment that were vulnerable to strafing by aircraft.[59]
As the war progressed, Germany was forced to reduce or no longer use certain critical alloys in the production of armour plate, such as those including nickel, tungsten and molybdenum; this resulted in lower impact resistance levels compared to earlier armour.[60] Allied bombers struck the Knaben mine in Norway and stopped a key source of molybdenum; supplies from Finland and Japan were also cut off. The loss of molybdenum, and its replacement with other substitutes to maintain hardness, as well as a general loss of quality control, resulted in an increased brittleness in German armour plate, which developed a tendency to fracture when struck with a shell. Testing by U.S. Army officers in August 1944 in Isigny, France showed catastrophic cracking of the armour plate on two out of three Panthers examined.[61][62]
The main gun was a Rheinmetall-Borsig 7.5 cm KwK 42 (L/70) with semi-automatic shell ejection and a supply of 79 rounds (82 on Ausf. G). The main gun used three different types of ammunition: APCBC-HE (Pzgr. 39/42), HE (Sprgr. 42) and APCR (Pzgr. 40/42), the last of which was usually in short supply. While it was of a calibre common on Allied tanks, the Panther's gun was one of the most powerful of World War II, due to the large propellant charge and the long barrel, which gave it a very high muzzle velocity and excellent armour-piercing qualities — among Allied tank guns of similar calibre, only the British Sherman Firefly conversion's Ordnance QF 17-pounder gun, of 3 inch (76.2mm) calibre, and a 55 calibre long (L/55) barrel, had more potential hitting power. The flat trajectory also made hitting targets much easier, since accuracy was less sensitive to errors in range estimation and increased the chance of hitting a moving target, though these same attributes made the gun a poor infantry-support weapon using HE ammo. The Panther's 75 mm gun had more penetrating power than the main gun of the Tiger I heavy tank, the 8.8 cm KwK 36 L/56,[63] although the larger 88 mm projectile might inflict more damage if it did penetrate.[64]
The tank typically had two MG 34 armoured fighting vehicle variant machine guns featuring an armoured barrel sleeve. An MG 34 machine gun was located co-axially with the main gun on the gun mantlet; an identical MG 34 was located on the glacis plate and fired by the radio operator. Initial Ausf. D and early Ausf. A models used a "letterbox" flap enclosing its underlying thin, vertical arrowslit-like aperture, through which the machine gun was fired.[65] In later Ausf A and all Ausf G models (starting in late November-early December 1943), a ball mount in the glacis plate with a K.Z.F.2 machine gun sight was installed for the hull machine gun.[66]
The front of the turret was a curved 100 mm (3.9 in) thick cast armour mantlet. Its transverse-cylindrical shape meant that it was more likely to deflect shells, but the lower section created a shot trap. If a non-penetrating hit bounced downwards off its lower section, it could penetrate the thin forward hull roof armour, and plunge down into the front hull compartment.[67] Penetrations of this nature could have catastrophic results, since the compartment housed the driver and radio operator sitting along both sides of the massive gearbox and steering unit. Also, four magazines containing main gun ammunition were located between the driver/radio operator seats and the turret, directly underneath the gun mantlet when the turret was facing forward.[68]
From September 1944, a slightly redesigned mantlet with a flattened and much thicker lower "chin" design started to be fitted to Panther Ausf G models, the chin being intended to prevent such deflections. Conversion to the "chin" design was gradual, and Panthers continued to be produced to the end of the war with the rounded gun mantlet.[69]
The Ausf A model introduced a new cast armour commander's cupola, replacing the forged cupola. It featured a steel hoop to which a third MG 34 or either the coaxial or the bow machine gun could be mounted for use in the anti-aircraft role.[70]
The first Panthers (Ausf D) had a hydraulic motor that could traverse the turret at a maximum rate of one complete revolution in one minute, independent of engine speed. This was improved in the Ausf A model with a hydraulic traverse that varied with engine speed; one full turn taking 46 seconds at an engine speed of 1,000 rpm but only 15 seconds if the engine was running at 3,000 rpm.[71] This arrangement was a weakness, as traversing the Panther's turret rapidly onto a target required close coordination between the gunner and driver, who had to run the engine to maximum speed. By comparison, the M4 Sherman's electrically traversed turret rotated at up to 360 degrees in 15 seconds and was independent of engine speed, which gave it an advantage over the Panther in close-quarters combat.[72] A hand traverse wheel was provided for the Panther gunner to make fine adjustment of his aim.[71]
Ammunition storage for the main gun was a weak point. All the ammunition for the main armament was stored in the hull, with a significant amount stored in the sponsons. In the Ausf D and A models, 18 rounds were stored next to the turret on each side, for a total of 36 rounds. In the Ausf G, which had deeper sponsons, 24 rounds were stored on each side of the turret, for a total of 48 rounds. In all models, four rounds were also stored in the left sponson between the driver and the turret. An additional 36 rounds were stored inside the hull of the Ausf D and A models – 27 in the forward hull compartment directly underneath the mantlet. In the Ausf G, the hull ammunition storage was reduced to 27 rounds total, with 18 rounds in the forward hull compartment. For all models, three rounds were kept under the turntable of the turret.[73] The stowage of 52 rounds of ammunition in the side sponsons made this area the most vulnerable point on the Panther since penetration here usually led to catastrophic ammunition fires.[74]
The loader was stationed in the right side of the turret. With the turret facing forward, he had access only to the right sponson and hull ammunition,[75] and so these served as the main ready-ammunition bins.
Panthers were supplied to form Panzer Abteilung 51 (Tank Battalion 51) on 9 January, and then Panzer Abteilung 52 on 6 February 1943.[76]
The first production Panther tanks were plagued with mechanical problems. The engine was dangerously prone to overheating and suffered from connecting rod or bearing failures. Petrol leaks from the fuel pump or carburettor, as well as motor oil leaks from gaskets, produced fires in the engine compartment; which resulted in the total writeoff of three Panthers due to fires.[77][78] Transmission and final drive breakdowns were the most common and difficult to repair. A large list of other problems were detected in these early Panthers, and so from April through May 1943 all Panthers were shipped to Falkensee and Nürnberg for a major rebuilding program. This did not correct all of the problems, so a second program was started at Grafenwoehr and Erlangen in June 1943. Reliability improved with the Ausf. A and later G of the Panther, with availability rates going from an average of 37% by end of 1943[79] to an average of 54% in 1944.[80] By mid-1944, the Panther was at its peak performance and widely regarded as the most formidable tank on the battlefield.[31]
The Panther tank was seen as a necessary component of Operation Citadel, and the attack was delayed several times because of their mechanical problems and to receive more Panthers, with the eventual start date of the battle only six days after the last Panthers had been delivered to the front. This resulted in major problems in Panther units during the Battle of Kursk, as tactical training at the unit level, coordination by radio, and driver training were all seriously deficient.[81]
It was not until 23–29 June 1943 that a total of 200 rebuilt Panthers were finally issued to Panther Regiment von Lauchert, of the XLVIII Panzer Corps (4 Panzer Army). Two were immediately lost due to motor fires on disembarking from the trains.[81] By 5 July, when the Battle of Kursk started, there were only 184 operational Panthers. Within two days, this had dropped to 40.[81] On 17 July 1943, after Hitler had ordered a stop to the German offensive, Gen. Heinz Guderian sent in the following preliminary assessment of the Panthers:
Due to enemy action and mechanical breakdowns, the combat strength sank rapidly during the first few days. By the evening of 10 July there were only 10 operational Panthers in the front line. 25 Panthers had been lost as total writeoffs (23 were hit and burnt and two had caught fire during the approach march). 100 Panthers were in need of repair (56 were damaged by hits and mines and 44 by mechanical breakdown). 60 percent of the mechanical breakdowns could be easily repaired. Approximately 40 Panthers had already been repaired and were on the way to the front. About 25 still had not been recovered by the repair service ... On the evening of 11 July, 38 Panthers were operational, 31 were total write-offs and 131 were in need of repair. A slow increase in the combat strength is observable. The large number of losses by hits (81 Panthers up to 10 July) attests to the heavy fighting.[81]During Zitadelle the Panthers claimed 267 destroyed tanks.[82]
A later report on 20 July 1943 showed 41 Panthers as operational, 85 as repairable, 16 severely damaged and needing repair in Germany, 56 burnt out because of enemy action, and two destroyed by motor fires.[83]
Before the Germans ended their offensive at Kursk, the Soviets began their counteroffensive, and succeeded in pushing the Germans back into a steady retreat. Thus, a report on 11 August 1943 showed that the number of total write-offs in Panthers swelled to 156, with only 9 operational. The German Army was forced into a fighting retreat, and increasingly lost Panthers in combat as well as from abandoning and destroying damaged vehicles.[83]
The Panther demonstrated its capacity to destroy any Soviet armoured fighting vehicle from long distance during the Battle of Kursk, and had a very high overall kill ratio.[84] It constituted less than seven percent of the estimated 2,400–2,700 total armoured fighting vehicles deployed by the Germans in this battle,[85] and its effectiveness was limited by its mechanical problems and the in-depth layered defence system of the Soviets at Kursk. Its greatest historical role in the battle may have been a highly negative one—its contribution to the decisions to delay the original start of Operation Zitadelle for a total of two months, time which the Soviets used to build up an enormous concentration of minefields, anti-tank guns, trenches and artillery defences.[86]
After the losses of the Battle of Kursk, the German Army went into a permanent state of retreat from the Red Army. The numbers of Panthers were slowly built up again on the Eastern Front, and the operational percentage increased as reliability improved. In March 1944 Guderian reported: "Almost all the bugs have been worked out", although many units continued to report significant mechanical problems, especially with the final drive.[87] The greatly outnumbered Panthers came to be used as mobile reserves to fight off major attacks.[88]
The highest total number of operational Panthers on the Eastern Front was achieved in September 1944, when some 522 were listed as operational out of a total of 728. Throughout the rest of the war Germany continued to keep the great majority of Panther forces on the Eastern Front, where the situation progressively worsened for them. The last recorded status, on 15 March 1945, listed 740 on the Eastern Front, of which 361 were operational.[89] By this time the Red Army had entered East Prussia and was advancing through Poland.
In August 1944 Panthers were deployed during the Warsaw Uprising as mobile artillery and troop support. At least two of them were captured in the early days of the conflict and used in actions against the Germans, including the liberation of the Gęsiówka concentration camp on 5 August, when the soldiers of "Wacek" platoon used the captured Panther (named "Magda") to destroy the bunkers and watchtowers of the camp. Most of the Germans in the camp were killed; the insurgents had lost two people and liberated almost 350 people. After several days the captured tanks were immobilized due to the lack of fuel and batteries and were set ablaze to prevent them from being recaptured.[90]
Photographs have proven the existence of Soviet-used Panthers in some units. A manual on the operation of the Panther was published in 1944 by the Red Army. Most Panthers ended up in trophy collections. Some Soviet officers proposed re-arming them with 85 mm guns, but this was not done. After the war, Red Army had an overall surplus of tanks, so it had no use for captured Panthers.
At the time of the invasion of Normandy in June 1944, there were initially only two Panther-equipped Panzer regiments in the Western Front, with a total of 156 Panthers between them. From June through August 1944, an additional seven Panther regiments were sent into France, reaching a maximum strength of 432 in a status report dated 30 July 1944.[91]
The majority of the German tank forces in Normandy – six and a half divisions – were drawn into the fighting around the town of Caen, where they checked the Anglo-Canadian forces of the 21st Army Group. The numerous operations undertaken to secure the town became collectively known as the Battle of Caen. While there were sectors of heavy wooded bocage around Caen, there were also many open fields, which allowed the Panther to engage the attacking enemy armour at long range. Conversely, by the time of the Normandy Campaign, British Divisional Anti-tank Regiments were well equipped with the excellent 17-pounder gun (the 17pdr also replaced the US gun on some M10 Tank Destroyers in British service), making it equally as perilous for Panthers to attack across these same fields. The British had begun converting regular M4 Shermans to carry the 17-pounder gun (nicknamed Firefly) prior to the D-day landings, and while limited numbers meant that during Normandy not more than one Sherman in four was of the Firefly variant, the lethality of the gun against German armour made them priority targets for German gunners.
US forces in the meantime, facing one and a half German panzer divisions, mainly the Panzer Lehr Division, struggled in the heavy, low-lying bocage terrain west of Caen. Against the M4 Shermans of the Allied tank forces during this time, the Panther tank proved to be most effective when fighting in open country and shooting at long range — its combination of superior armour and firepower allowed it to engage at distances from which the Shermans could not respond.[92] The Panther struggled in the bocage country of Normandy, and was vulnerable to side and close-in attacks in the built-up areas of cities and small towns.[93] The commander of the Panzer Lehr Division, Gen. Fritz Bayerlein, reported on the difficulties experienced by the Panther tank in the fighting in Normandy:
While the PzKpfw IV could still be used to advantage, the PzKpfw V [Panther] proved ill adapted to the terrain. The Sherman because of its maneuverability and height was good ... [the Panther was] poorly suited for hedgerow terrain because of its width. Long gun barrel and width of tank reduce maneuverability in village and forest fighting. It is very front-heavy and therefore quickly wears out the front final drives, made of low-grade steel. High silhouette. Very sensitive power-train requiring well-trained drivers. Weak side armor; tank top vulnerable to fighter-bombers. Fuel lines of porous material that allow gasoline fumes to escape into the tank interior causing a grave fire hazard. Absence of vision slits makes defense against close attack impossible.[93]
But Bayerlein still appreciated the Panther's virtues when used in the right conditions, writing: "An ideal vehicle for tank battles and infantry support. The best tank in existence for its weight".[93]
Through September and October, a series of new Panzerbrigades equipped with Panther tanks were sent into France to try to stop the Allied advance with counter-attacks.[94] This culminated in the Battle of Arracourt (18–29 September 1944), in which the mostly Panther-equipped German forces suffered heavy losses fighting against the 4th Armored Division of Patton's 3rd Army, which were still primarily equipped with 75 mm M4 Sherman tanks and yet came away from the battle with only a few losses. The Panther units were newly formed, poorly trained and tactically disorganized; most units ended up stumbling into ambushes against seasoned U.S. tank crews.[95]
A status report on 15 December 1944 listed an all-time high of 471 Panthers assigned to the Western Front, with 336 operational (71 percent). This was one day before the start of the Battle of the Bulge; 400 of the tanks assigned to the Western Front were in units sent into the offensive.[96]
The Panther once again demonstrated its prowess in open country, where it could hit its targets at long range with near-impunity, and its vulnerability in the close-in fighting of the small towns of the Ardennes, where they suffered heavy losses.[97] A status report on 15 January 1945 showed only 97 operational Panthers left in the units involved in the operation, out of 282 still in their possession. Total writeoffs were listed as 198.[98]
The Operation Greif commando mission included five Panthers assigned to Panzerbrigade 150, disguised to look like M10 Tank Destroyers by welding on additional plates, applying US-style camouflage paint and markings.[96] This was carried out as part of a larger operation that involved soldiers disguised as Americans to attack US troops from the rear. The disguised Panthers were detected and destroyed.
In February 1945, eight Panzer divisions with a total of 271 Panthers were transferred from the West to the Eastern Front. Only five Panther battalions remained in the west.[99]
One of the top German Panther commanders was SS-Oberscharführer Ernst Barkmann of the 2nd SS-Panzer Regiment "Das Reich". By the end of the war, he had some 80 tank kills claimed.[100]
From 1943, Panther turrets were mounted in fixed fortifications; some were normal production models, but most were made specifically for the task, with additional roof armour to withstand artillery fire. Two types of turret emplacements were used; (Pantherturm III – Betonsockel — concrete base) and (Pantherturm I – Stahluntersatz — steel sub-base). They housed ammunition storage and fighting compartment along with crew quarters. A total of 182 of these were installed in the fortifications of the Atlantic Wall and Siegfried Line (Westwall), 48 in the Gothic Line and Hitler Line, 36 on the Eastern Front, and two for training and experimentation, for a total of 268 installations by March 1945. They proved to be costly to attack, and difficult to destroy.[101]
From September 1943, one Panzer battalion with 96 Panthers constituted the Panzer regiment of a Panzer-Division 43.[102]
From 3 August 1944, the new Panzer-Division 44 organisation called for a Panzer division to consist of one Panzer regiment with two Panzer battalions – one of 96 Panzer IVs and one of 96 Panthers. Actual strengths tended to differ, and became far lower after losses.[103]
The Tiger I and Panther tanks were German responses to encountering the T-34 in 1941. Soviet firing tests against a captured Tiger in April 1943 showed that the T-34's 76 mm gun could not penetrate the front of the Tiger I; and could only penetrate the side at very close range. An existing Soviet 85 mm anti-aircraft gun, the D-5T, also proved disappointing. Several captured German Tiger I tanks were shipped to Chelyabinsk, where they were subjected to 85 mm fire from various angles. The 85 mm gun could not reliably penetrate the Tiger I except at ranges within the lethal envelope of the Tiger I's own 88 mm gun.[104] The Soviets had already embarked on the 85 mm gun upgrade path before encountering the Panther tank at the Battle of Kursk.[105][106]
After much development work, the first T-34-85 tanks entered combat in March 1944. The production version of the T-34's new 85 mm gun had to be aimed at the Panther's turret front and mantlet to penetrate, while the Panther's main gun could penetrate the T-34's glacis from 800 m (870 yd) at 30 degrees.[107] Although the T-34-85 tank was not quite the equal of the Panther in the anti-tank role, it was much better than the 76.2 mm-armed versions and made up for it with proven reliability, more effective fragmentation shells, and production in greater quantities.[108] New tank destroyers based on the T-34 hull, such as the SU-85 and SU-100, were also developed. A Wa Pruef 1 report dated 5 October 1944 estimated that when set at a 30-degree angle the T-34-85's upper glacis could be penetrated by the Panther's 7.5 cm KwK 42 from 300 m (330 yd), the mantlet from 1,200 m (1,300 yd) and the turret front from 2,000 m (2,200 yd) while the T-34-85's 85 mm ZiS-S-53 could penetrate the Panther's frontal turret from 500 m (550 yd). From the side, the two were equivalent as both tanks could penetrate the other from ranges over 2,000 m (2,200 yd), further than any practical engagement distance.[109]
The Battle of Kursk convinced the Soviets of the need for even greater firepower. A Soviet analysis of the battle in August 1943 showed that a Corps artillery piece, the A-19 122 mm gun, had done well against the German armoured fighting vehicles in that battle, and so development work on the 122 mm equipped IS-2 began in late 1943. First encounters with enemy tanks revealed that the 122 mm BR-471 shell could punch through the Panther's frontal armour at a range of 600–700 m (660–770 yd).[110] The early results of the IS-2's combat employment, which were confirmed by firing tests in Kubinka 1944, compelled the designers to seek innovative solutions.[111] According to German tactical instructions, a Panther had to close to 600 m (660 yd) to guarantee penetration of the IS-2's frontal armour, while the IS-2 could penetrate the Panther at ranges of 1,000 m (1,100 yd).[112][Notes 2]
A Wa Pruef 1 report states that when set at a 30-degree angle the glacis plate of the Panther could not be penetrated by the 122 mm D-25T AP shell, the lower glacis could be penetrated from 100 m (110 yd), the turret mantlet from 500 m (550 yd) and the turret front from 1,500 m (1,600 yd).[109] The Panther's 75 mm gun could penetrate the IS-2 model 1943's mantlet from 400 m (440 yd), turret from 800 m (870 yd), and driver's front plate from 600 m (660 yd). From the side, the Panther's armour was penetrable by the 122 mm D-25T from over 3,500 m (3,800 yd).[109] The Panther carried more ammunition and had a faster firing cycle: for every 1-1.5 shots of the IS-2, the Panther and Tiger could fire 3-4 times.[113] With the addition of a semi-automatic drop breech over the previously manual screw,[114] this breech modification increased the IS-2's rate of fire to 3-4 rounds per minute.[115]
The IS-2 proved to have surprisingly good anti-tank capabilities due to the D-25T's extremely heavy HE projectiles. Standard doctrine for purpose-built anti-tank guns of the period universally relied on small, dense solid projectiles propelled to high velocities, optimized for punching through armor. However, the 122mm HE shell would easily blow off the turret, driver sprocket and tread of the heaviest German tank even if it could not penetrate its armour[116][117]
The Western Allies were aware of the Panther and had access to technical details through the Soviets, but there was a difference in the American and British camps as to the significance of the tank. After taking two years to catch up with German tank design in Africa, the British were wary of falling behind yet again. They had developed the excellent 17-pounder anti-tank gun, but did not yet have a vehicle in service that could fit this large gun into its turret. For its part, the U.S. Army did not believe that the Panther would be a significant problem, and did not foresee their armoured forces having to fight pitched engagements against large numbers of Panthers. The Panther was not seen in combat by the Western Allies until early 1944 at Anzio in Italy, where Panthers were employed in small numbers. Until just before D-Day (6 June 1944), the Panther was thought to be another heavy tank that would not be built in large numbers.
Shortly before D-Day, Allied intelligence reported that large numbers of Panthers were being used in the panzer divisions, and an attempt was made to investigate Panther production. Using a statistical analysis of the serial numbers on the road wheels on two captured tanks, U.S. intelligence estimated Panther production for February 1944 to be 270 units, much greater than what had been anticipated.[Notes 3] This estimate was very accurate, especially compared to previous methods, as German records after the war showed production of Panthers for the month of February 1944 was 276. This indicated that the Panther would be encountered in much larger numbers than had previously been thought.[118] In the planning for the Battle of Normandy, the U.S. Army expected to face a handful of German heavy tanks alongside large numbers of Panzer IVs. At this point, it was too late to prepare to face the Panther. As it turned out, 38% of the German tanks in Normandy were Panthers, whose frontal armour could not be penetrated by the 75 mm guns of the US M4 Sherman.
The British were more astute in their recognition of the danger posed by the increasing armour strength of German tanks. Work on a more powerful anti-tank gun had started in 1941, and the tanks to use it in 1942. When these programmes were delayed, a stop-gap solution was found. The 17-pdr could through modifications be fitted to a Sherman, and orders for this Sherman Firefly were placed in 1943. By the time of the Normandy invasion, 340 Sherman Fireflies were available to the Commonwealth armoured divisions. The British lobbied for American production lines to be modified to produce Fireflies, but these suggestions were declined by the U.S. Army, in part due to the poor performance of British tank designs in North Africa.[119] There were also 200 interim Challenger tanks with the 17-pounder and other improved tank designs were under development. British and Commonwealth tank units in Normandy were initially equipped at the rate of one Firefly in a troop with three Shermans or Cromwells. This ratio increased until, by the end of the war, half of the British Shermans were Fireflies. The Comet with a gun similar to the 17-pounder had also replaced the 75 mm gun Sherman in some British units. The 17-pounder with APCBC shot was more or less equivalent in performance to the Panther's 75 mm gun, but superior with APDS shot.[120]
At the time, U.S. armour doctrine was dominated by the head of Army Ground Forces, Gen. Lesley McNair. An artilleryman by trade, he believed that tanks should concentrate on infantry support and exploitation roles and avoid enemy tanks, leaving them to be dealt with by the tank destroyer force, which was a mix of towed anti-tank guns and lightly armoured fighting vehicles with open top turrets with 3-inch (76.2 mm) (M10 tank destroyer), 76 mm (M18 Hellcat) or later, 90 mm (M36 tank destroyer) guns. This doctrine led to a lack of urgency in the U.S. Army to upgrade the armour and firepower of the M4 Sherman tank, which had previously done well against the most common German tanks – Panzer IIIs and Panzer IVs – in Africa and Italy. As with the Soviets, the German adoption of thicker armour and the 7.5 cm KwK 40 in their standard armoured fighting vehicles prompted the U.S. Army to develop the more powerful 76 mm version of the M4 Sherman tank in April 1944. Development of a heavier tank, the M26 Pershing, was delayed mainly by McNair's insistence on "battle need" and emphasis on producing only reliable, well-tested weapons, a reflection of America's 3,000 mi (4,800 km) supply line to Europe.[121]
An AGF (Armored Ground Forces) policy statement of November 1943 concluded the following:
The recommendation of a limited proportion of tanks carrying a 90mm gun is not concurred in for the following reasons: The M4 tank has been hailed widely as the best tank of the battlefield today. ... There appears to be no fear on the part of our forces of the German Mark VI (Tiger) tank. There can be no basis for the T26 tank other than the conception of a tank-vs.-tank duel-which is believed to be unsound and unnecessary. Both British and American battle experience has demonstrated that the antitank gun in suitable numbers is the master of the tank. ... There has been no indication that the 76mm antitank gun is inadequate against German Mark VI tank.[122]
U.S. awareness of the inadequacies of their tanks grew only slowly. All U.S. M4 Shermans that landed in Normandy in June 1944 had the 75 mm gun. The general purpose 75 mm M4 gun could not penetrate the Panther from the front at all, although it could penetrate various parts of the Panther from the side at ranges from 400 to 2,600 m (440 to 2,840 yd). The 76 mm gun could also not penetrate the front hull armour of the Panther, but could penetrate the Panther turret mantlet at very close range.[123] In August 1944, the HVAP (high velocity armour-piercing) 76 mm round was introduced to improve the performance of the 76 mm M4 Shermans. With a tungsten core, this round could still not penetrate the Panther glacis plate, but could punch through the Panther mantlet at 730 to 910 m (800 to 1,000 yd), instead of the usual 91 m (100 yd) for the normal 76 mm round. Tungsten production shortages meant that this round was always in short supply, with only a few available per tank, and some M4 Sherman units never received any.[124]
Whereas Sherman tanks used a high flash powder, making it easier for German tankers to spot them, German tanks used a low flash powder, making it harder for Allied crews to spot them.[119] Shermans, even though they were around 15 tons lighter than Panthers, had worse cross country mobility due to their narrower tracks. A US corporal stated:
I saw where some MkV tanks crossed a muddy field without sinking the tracks over five inches, where we in the M4 started across the same field the same day and bogged down.[125][page needed]
The 90 mm M36 tank destroyer was introduced in September 1944; the 90 mm round also proved to have difficulty penetrating the Panther's glacis plate, and it was not until an HVAP version of the round was developed that it could effectively penetrate it from combat range. It was very effective against the Panther's front turret and side.[126]
The high U.S. tank losses in the Battle of the Bulge against a force largely of Panther tanks brought about a clamour for better armour and firepower. At General Eisenhower's request, only 76 mm gun-armed M4 Shermans were shipped to Europe for the remainder of the war. Small numbers of the M26 Pershing were also rushed into combat in late February 1945.[127] A dramatic newsreel film was recorded by a U.S. Signal Corps cameraman of an M26 stalking and then blowing up a Panther in the city of Cologne, after the Panther had knocked out two M4 Shermans.[128]
The production of Panther tanks and other German tanks dropped off sharply after January 1945, and eight of the Panther regiments still on the Western Front were transferred to the Eastern Front in February 1945. The result was that, for the rest of the war during 1945, the greatest threats to the tanks of the Western Allies were no longer German tanks, but infantry anti-tank weapons, such as the Panzerschreck and Panzerfaust, infantry anti-tank guns, such as the ubiquitous 7.5 cm Pak 40, and tank destroyers, such as the Marder, StuG III, StuG IV, and Jagdpanzer. A German Army status report dated 15 March 1945 showed 117 Panthers left in the entire Western Front, of which only 49 were operational.[129]
This section needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (September 2009) (Learn how and when to remove this template message) |
The early impetus for upgrading the Panther came from the concern of Hitler and others that it lacked sufficient armour. Hitler had already insisted on an increase in its armour once, early in its design process in 1942. Discussions involving Hitler in January 1943 called for further increased armour; initially referred to as Panther 2 (it became the Panther II after April 1943). This upgrade increased the thickness of the glacis plate to 100 mm (3.9 in), the side armour to 60 mm (2.4 in), and the top armour to 30 mm (1.2 in). Production of the Panther 2 was slated to begin in September 1943.
On 10 February 1943, Dr. Wiebecke (chief design engineer for M.A.N.) suggested thoroughly redesigning the Panther II and incorporating Tiger components such as the steering gears, final drive, entire suspension and turret based on Eastern Front experience. Total weight would increase to more than 50 metric tons.[130] Another meeting on 17 February 1943 focused on sharing and standardizing parts between the Tiger II tank and the Panther II, such as the transmission, all-steel eighty centimeter diameter roadwheels (only overlapping and not interleaved as the original Schachtellaufwerk roadwheel design used) and running gear. Additional meetings in February began to outline the various components, including a suggestion to adopt the King Tiger's hard-hitting 8.8 cm KwK 43 L/71 gun, but it was ultimately decided to continue use of the production Panther's 7.5 cm KwK 42 L/70 gun.[131] In March 1943, MAN indicated that the first prototype would be completed by August 1943. A number of engines were under consideration, among them the new Maybach HL 234 fuel-injected engine (900 hp operated by an 8-speed hydraulic transmission) and the BMW 003 aviation turbojet-derived, GT 101 turboshaft powerplant, planned to be of some 1,150 shaft horsepower output and weighing only some 450 kg (992 lb) without its transmission, only some 38% of the weight of the Panther's standard Maybach HL230 V-12 gasoline fueled piston engine.
Thus, plans to replace the original Panther design with the Panther II were already underway before the first Panther had even seen combat. But from May to June 1943, work on the Panther II ceased as the focus was shifted to expanding production of the original Panther tank. It is not clear if there was ever an official cancellation – this may have been because the Panther II upgrade pathway was originally started at Hitler's insistence. The direction that the design was headed would not have been consistent with Germany's need for a mass-produced tank, which was the goal of the Reich Ministry of Armament and War Production.
One Panther II chassis was completed and eventually captured by the U.S.; it is now on display at the Patton Museum in Fort Knox. An Ausf G turret is mounted on this chassis.[132][133]
After the Panther II project died, a more limited upgrade of the Panther was planned, centred around a re-designed turret. The Ausf F variant was intended for production in April 1945, but the end of war ended these plans.
The earliest known redesign of the turret was dated 7 November 1943 and featured a narrow gun mantlet behind a 120 mm (4.7 in) thick turret front plate. Another design drawing by Rheinmetall dated 1 March 1944 reduced the width of the turret front even further; this was the Turm-Panther (Schmale Blende) (Panther with narrow gun mantlet).[134] Several experimental Schmaltürme (literally: "narrow turrets") were built in 1944 with modified versions of the production Panther's 7.5 cm KwK 42 L/70 standard gun, which were given the designation of KwK 44/1. A few were captured and shipped back to the U.S. and Britain. One badly damaged turret is on display at the Bovington Tank Museum. It had been used as a post-war range target until its historical significance was recognised.
The Schmalturm had a much narrower front face of 120 mm (4.7 in) armour sloped at 20 degrees; side turret armour was increased to 60 mm (2.4 in) from 45 mm (1.8 in); roof turret armour increased to 40 mm (1.6 in) from 16 mm (0.63 in); and a bell shaped gun mantlet similar to that of the Tiger II was used. This increased armour protection also had a slight weight saving due to the overall smaller size of the turret.[135]
The Panther Ausf F would have had the Schmalturm, with its better ballistic protection, and an extended front hull roof which was slightly thicker. The Ausf F's Schmalturm was to have a built-in stereoscopic rangefinder — using twin matching armored blisters, one on each turret side, much like the Americans' post-war M47 Patton tank — and lower weight than the original turrets. A number of Ausf F hulls were built at Daimler-Benz and Ruhrstahl-Hattingen steelworks; there is no evidence that any completed Ausf F saw service before the end of the war.
Proposals to equip the Schmalturm with the 8.8 cm KwK 43 L/71 were made from January to March 1945. These would have likely equipped future German tanks but none was built, as the war ended.[136]
The E series of experimental tanks — E-10, E-25, E-50, E-75, E-100 (the numbers designated their weight class) – was proposed to further streamline production with an even greater sharing of common parts and simplification of design. In this scheme, the Panther tank would have been replaced by the E-50. A Belleville washer-based, hull sidemount suspension system was proposed to replace the complex and costly dual torsion bar system. The Schmalturm would have been used, likely with a variant of the 8.8 cm L/71 gun.[137]
This section needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (August 2009) (Learn how and when to remove this template message) |
Although a technologically sophisticated vehicle, the Panther's design had a very limited influence on postwar tank development. The French postwar AMX 50 tank prototype was indirectly influenced by it through the Entwicklung series, but never entered series production. It is claimed that the Panther was arguably a forebear to the modern main battle tank.[139]
The Panther itself also saw some limited use outside the German military, both before and after 1945.
During the war, the Red Army employed a number of captured Panthers. These were repainted with prominent Soviet emblems and tactical markings to avoid friendly fire incidents.[140] Unlike captured Panzer IVs and StuGs, the Soviets generally only used Panthers and Tigers that had been captured intact and used them until they broke down, as they were too complex and difficult to transport for repair. Panzer IVs and StuGs, on the other hand, were so numerous in terms of spare parts and easy to repair that they could be used over a much longer period in combat conditions.
During March–April 1945, Bulgaria received 15 Panthers of various makes (D, A and G's) from captured and overhauled Soviet stocks; they only saw limited (training) service use. They were dug down, with automotive components removed, as pillboxes along the Bulgarian-Turkish border as early as the late 1940s. The final fate of these pillbox Panthers is unknown, but sources indicate that they were replaced and scrapped in the 1950s.
In May 1946, Romania received 13 Panther tanks from the USSR. They were initially used by the 1st Armoured Brigade, but in 1947 the equipment was ceded to the Soviet-organized "Tudor Vladimirescu Division", which was transformed from a volunteer infantry division into an armoured one. The Panther tank was officially known as T-V (T-5) in the army inventory. These tanks were in poor condition and remained in service until about 1950, by which time the Romanian Army had received T-34-85 tanks. All of the tanks were scrapped by 1954. The tanks were different models: Ausf A, Ausf D and Ausf G.[141] They were shown to the public in 1948, during the 1 May parade in Bucharest, painted with Romanian markings. Until 1950, the T-V (T-5) was the heaviest tank available to the Romanian Army.
During the Warsaw Uprising, the Polish Home Army captured and used two Panther tanks. One, nicknamed Magda, was used by Batalion Zośka's armored platoon under the command of Wacław Micuta to liberate the Gęsiówka concentration camp.
One captured vehicle (named "Cuckoo") also saw service with the British Coldstream Guards for some time.[142]
Germany sold Japan a single Panther along with a Tiger in September 1943; by the time it was ready in 1944, it was impossible to ship due to Allied naval interdiction.[143]
In 1946, Sweden sent a delegation to France to examine surviving specimens of German military vehicles. During their visit, the delegates found a few surviving Panthers and had one shipped to Sweden for further testing and evaluation, which continued until 1961. The tank is on display in the Deutsches Panzermuseum in Munster.[144]
After the war, France was able to recover enough operable vehicles and components to equip the French Army's 503e Régiment de Chars de Combat with a force of 50 Panthers from 1944 to 1947, in the 501st and 503rd Tank Regiments. In 1947, the French War Ministry wrote an evaluation of them entitled Le Panther 1947. These remained in service until they were replaced by French-built ARL 44 heavy tanks.[145][unreliable source?]
The last 'production' Panthers were produced at the factory by German staff just after the end of World War II under the supervision of the Royal Electrical and Mechanical Engineers (REME) using available components. 9 Panthers and 12 Jagdpanthers were produced and shipped back to Britain for post-war trials. A complete Panther and a complete Jagdpanther produced this way are now at the Bovington Tank Museum, Dorset, with brass plates on them, explaining their history.
Panther with full Schürzen spaced armour attached, intended to supplement the side armour above the large wheels.
|
|
All angles from horizontal.
This article uses material from the Wikipedia article "Panther tank", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted