powered by CADENAS

Social Share

Domestic rabbit (44400 views - Animals)

A domestic (or domesticated) rabbit (Oryctolagus), more commonly known as a pet rabbit, a bunny, or a bunny rabbit is any of the domesticated varieties of the European rabbit species. Rabbits were first domesticated in the Middle Ages as sources of food, fur, and wool, and later as pets. They may be considered a pocket pet depending on their size. A male rabbit is a buck, a female is a doe, and a young rabbit is a kit or kitten. Rabbits have been kept as pets in Western nations since the 19th century. Beginning in the 1980s, the idea of the domestic rabbit as a house companion, or house rabbit, was promoted. Rabbits are intelligent and can be litter box trained and may come when called, but they need exercise and can damage a house that is not "rabbit proof". Especially following the Easter season, unwanted rabbits end up in animal shelters. Because they have become invasive in Australia, pet rabbits are banned in Queensland.
Go to Article

Explanation by Hotspot Model

Domestic rabbit

Domestic rabbit

Domestic rabbit

Domestic rabbit
Domesticated
Scientific classification
Kingdom: Animalia
Phylum: Chordata
Class: Mammalia
Order: Lagomorpha
Family: Leporidae
Genus: Oryctolagus
Lilljeborg, 1873
Species: O. cuniculus
Binomial name
Oryctolagus cuniculus
(Linnaeus, 1758)
Synonyms

O. c. domesticus

A domestic (or domesticated) rabbit (Oryctolagus), more commonly known as a pet rabbit, a bunny, or a bunny rabbit is any of the domesticated varieties of the European rabbit species. Rabbits were first domesticated in the Middle Ages as sources of food, fur, and wool, and later as pets. They may be considered a pocket pet depending on their size. A male rabbit is a buck, a female is a doe, and a young rabbit is a kit or kitten.

Rabbits have been kept as pets in Western nations since the 19th century. Beginning in the 1980s, the idea of the domestic rabbit as a house companion, or house rabbit, was promoted. Rabbits are intelligent and can be litter box trained and may come when called, but they need exercise and can damage a house that is not "rabbit proof". Especially following the Easter season, unwanted rabbits end up in animal shelters.[1] Because they have become invasive in Australia, pet rabbits are banned in Queensland.[2]


History

Phoenician sailors visiting the coast of Spain c. 12th century BC, mistaking the European rabbit for a species from their homeland (the rock hyrax Procavia capensis), gave it the name i-shepan-ham (land or island of hyraxes).

Virgin & Child with Saint Catherine of Alexandria and a Rabbit
Titian (ca 1530)

A theory exists that a corruption of this name, used by the Romans, became the Latin name for the peninsula, Hispania – although this theory is somewhat controversial.[3] In Rome, rabbits were raised in large walled colonies.

The captivity of rabbits as a food source is recorded as early as the 1st century BC, when a Roman writer described the use of rabbit hutches, along with enclosures called leporaria (fr).[4] True domestication of rabbits may have begun in the Middle Ages, when they are thought to have been selectively bred as farm animals for meat and fiber. By the 16th century, several new breeds of different colors and sizes were being recorded.[citation needed]

In the 19th century, as animal fancy in general began to emerge, rabbit fanciers began to sponsor rabbit exhibitions and fairs in Western Europe and the United States. Breeds of various domesticated animals were created and modified for the added purpose of exhibition, a departure from the breeds that had been created solely for food, fur, or wool. The rabbit's emergence as a household pet began during the Victorian era.

Domestic rabbits have been popular in the United States since the late 19th century. What became known as the "Belgian Hare Boom" began with the importation of the first Belgian Hares from England in 1888 and, soon after, the founding of the American Belgian Hare Association, the first rabbit club in America. From 1898 to 1901, many thousands of Belgian Hares were imported to America.[5] Today, the Belgian Hare is one of the rarest breeds, with only 132 specimens found in the United States in a 2015 census.[6]

The American Rabbit Breeders Association (ARBA) was founded in 1910 and is the national authority on rabbit raising and rabbit breeds having a uniform Standard of Perfection, registration and judging system. The domestic rabbit continues to be popular as a show animal and pet. Many thousand rabbit shows occur each year and are sanctioned in Canada and the United States by the ARBA. Today, the domesticated rabbit is the third most popular mammalian pet in Britain after dogs and cats.

Rabbits have been, and continue to be, used in laboratory work such as the production of antibodies for vaccines and research of human male reproductive system toxicology. The Environmental Health Perspective, published by the National Institute of Health, states, "The rabbit [is] an extremely valuable model for studying the effects of chemicals or other stimuli on the male reproductive system." According to the Humane Society of the United States, rabbits are also used extensively in the study of bronchial asthma, stroke prevention treatments, cystic fibrosis, diabetes, and cancer. Animal rights activists have opposed animal experimentation for non-medical purposes, such as the testing of cosmetic and cleaning products, which has resulted in decreased use of rabbits in these areas.[citation needed]

Terminology

Male rabbits are called bucks; females are called does. An older term for an adult rabbit is coney, while rabbit once referred only to the young animals.[7] Another term for a young rabbit is bunny, though this term is often applied informally (especially by children) to rabbits generally, especially domestic ones. More recently, the term kit or kitten has been used to refer to a young rabbit. A young hare is called a leveret; this term is sometimes informally applied to a young rabbit as well. A group of rabbits is known as a "colony" or a "nest".[8]

Biology

Genetics

The study of rabbit genetics is of interest to fanciers, the fiber & fur industry, medical researchers, and the meat industry. Among rabbit fanciers, the genetics of rabbit health and diversity are paramount. The fiber & fur industry focuses on the genetics of coat color and hair properties. In the biomedical research community and the pharmaceutical industry, rabbit genetics are important in model organism research, antibody production, and toxicity testing. The meat industry relies on genetics for disease resistance, feed conversion ratios, and reproduction potential in rabbits.

The rabbit genome has been sequenced and is publicly available.[9] The mitochondrial DNA has also been sequenced.[10] In 2011, parts of the rabbit genome were re-sequenced in greater depth in order to expose variation within the genome.[11]

There are 11 color gene groups (or loci) in rabbits. A rabbit's coat has either two pigments (pheomelanin for yellow, and eumelanin for dark brown) or no pigment (for an albino rabbit). Clusters of color genes plus their modifiers control such aspects as coat patterns (e.g. Dutch or English markings), color hues and their intensity or dilution, and the location of color bands on the hair shaft (e.g., silvering).

Diet

As a refinement of the diet of the wild rabbit, the diet of the domestic rabbit is often a function of its purpose. Show rabbits eat for vibrant health, strong musculoskeletal systems, and—like rabbits intended for the fur trade—optimal coat production and condition. Rabbits intended for the meat trade eat for swift and efficient production of flesh, while rabbits in research settings have closely-controlled diets for specific goals. Nutritional needs of the domestic rabbit may also be focused on developing a physique that allows for the safe delivery of larger litters of healthy kits. Optimizing costs and producing feces that meet local waste regulations may also be factors.[12] The diet of a pet rabbit, too, is geared toward its purpose—as a healthy and long-lived companion.

Hay is an essential part of the diet of all rabbits and it is a major component of the commercial food pellets that are formulated for domestic rabbits and available in many areas. Pellets are typically fed to adult rabbits in limited quantities once or twice a day, to mimic their natural behavior and to prevent obesity. Most rabbit pellets are alfalfa-based for protein and fiber, with other grains completing the carbohydrate requirements. Minerals and vitamins are added during production to meet the nutritional requirements of the domestic rabbit. Along with pellets, many commercial rabbit raisers also feed one or more types of loose hay, for its freshness and important cellulose components. Alfalfa in particular is recommended for the growth needs of young rabbits.[13]

Digestion

Rabbits are hindgut fermenters and therefore have an enlarged cecum. This allows a rabbit to digest, via fermentation, what it otherwise would not be able to metabolically process.

After a rabbit ingests food, the food travels down the esophagus and through a small valve called the cardia. In rabbits, this valve is very well pronounced and makes the rabbit incapable of vomiting. The food enters the stomach after passing through the cardia. Food then moves to the stomach and small intestine where a majority of nutrient extraction and absorption takes place. Food then passes into the colon and eventually into the cecum. Peristaltic muscle contractions (waves of motion) help to separate fibrous and non-fibrous particles. The non-fibrous particles are then moved backwards up the colon, through the illeo-cecal valve, and into the cecum. Symbiotic bacteria in the cecum help to further digest the non-fibrous particles into a more metabolically manageable substance. After as little as three hours, a soft, fecal "pellet", called a cecotrope, is expelled from the rabbit's anus. The rabbit instinctively eats these grape-like pellets, without chewing, in exchange keeping the mucous coating intact. This coating protects the vitamin- and nutrient-rich bacteria from stomach acid, until it reaches the small intestine, where the nutrients from the cecotrope can be absorbed.[14][15]

The soft pellets contain a sufficiently large portion of nutrients that are critical to the rabbit's health. This soft fecal matter is rich in vitamin B and other nutrients. The process of coprophagy is important to the stability of a rabbit's digestive health because it is one important way that which a rabbit receives vitamin B in a form that is useful to its digestive wellness.[16] Occasionally, the rabbit may leave these pellets lying about its cage; this behavior is harmless and usually related to an ample food supply.

When caecal pellets are wet and runny (semi-liquid) and stick to the rabbit and surrounding objects they are called ontermittent soft cecotropes (ISCs). This is different from ordinary diarrhea and is usually caused by a diet too high in carbohydrates or too low in fiber. Soft fruit or salad items such as lettuce, cucumbers and tomatoes are possible causes.

Reproduction

Rabbits have a reputation as prolific breeders, and deservedly so, in part because rabbits reach breeding age quickly. To prevent unwanted offspring and to benefit the rabbit's health and behavior, rabbits may be spayed or neutered at sexual maturity: 4-5 months for small breeds (e.g., Mini Rex, Netherland Dwarf), 5-6 months for medium-sized breeds (e.g., Rex, New Zealand), and 6–7 months for large breeds (e.g., Flemish Giant). Bucks usually require more time to sexually mature than does, and they normally reach adult sperm counts at 6–7 months.

Rabbits, like all mammals, produce milk for their young. Female rabbits have six to eight nipples and produce milk for four weeks after birthing.[17] Rabbit milk is relatively high in fat, as a percentage by mass. While most species produce approximately 5% milk fat, rabbits produce 12%. The excerpted table below compares milk characteristics among mammals.[18]

Species Fat
%
Protein
%
Lactose
%
Ash
%
Total
Solids
%
Gray Seal  53.2      11.2       2.6    0.7    67.7
Polar Bear  31.0      10.2       0.5    1.2    42.9
Rabbit  12.2      10.4       1.8    2.0    26.4
Bison    1.7        4.8       5.7    .96    13.2
Donkey    1.2        1.7       6.9    .45    10.2

Health

Johann Daniel Meyer (1752)

A disease is rare when rabbits are raised in sanitary conditions and provided with adequate care. Rabbits have fragile bones, especially in their spines, and need support on the belly or bottom when they are picked up.

Spayed or neutered rabbits kept indoors with proper care may have a lifespan of 8 to 12 years, with mixed-breed rabbits typically living longer than purebred specimens, and dwarf breeds having longer average lifespans than larger breeds.[19] The world record for longest-lived rabbit is 18 years.[19]

Rabbits will gnaw on almost anything, including electrical cords (possibly leading to electrocution), potentially poisonous plants, and material like carpet and fabric that may cause life-threatening intestinal blockages, so areas to which they have access need to be rabbit-proofed.[20][21][22]

Spaying and neutering

Rabbit fancier organizations and veterinarians recommend that pet rabbits be spayed or neutered by a rabbit-experienced veterinarian.[23][24]:123 Health advantages of surgically altering a rabbit include increased longevity and (for females) a reduced risk of ovarian and uterine cancers or of endometritis.[24]:195–9[25][19] For both rabbit sexes, spaying or neutering reduces aggression toward other rabbits, as well as territorial marking (especially in males).[25][26][27] Rabbits are at high risk for complications from anesthesia and infection of the surgical site is another top concern.[28] Since un-altered animals are not as likely to form agreeable social bonds, spaying and neutering promotes less stressful interactions.

Vaccinations

In most jurisdictions, including the United States (except where required by local animal control ordinances), rabbits do not require vaccination. Vaccinations exist for both rabbit hemorrhagic disease and myxomatosis.[29] These vaccinations are usually given annually, two weeks apart. If there is an outbreak of myxomatosis locally, this vaccine can be administered every six months for extra protection.[30] Myxomatosis immunizations are not available in all countries, including Australia, due to fears that immunity will pass on to feral rabbits. However, they are recommended by some veterinarians as prophylactics, where they are legally available.[24]:182

Declawing

A rabbit cannot be declawed. Lacking pads on the bottoms of its feet, a rabbit requires its claws for balance. Removing its claws would render it unable to stand.[31][32]

Tonic immobility

Coping with stress is a key aspect of rabbit behavior, and this can be traced to part of the brain known as ventral tegmental area (VTA). Dopaminergic neurons in this part of the brain release the hormone dopamine, generalized as a "feel-good" hormone. In humans, dopamine is released through a variety of acts, including sexual activity, substance abuse, and even eating chocolate. However, in rabbits, it is released as part of a coping mechanism while in a heightened state of fear or stress, and has a calming effect. Dopamine has also been found in the rabbit's medial prefrontal cortex, the nucleus accumbens, and the amygdala.[33] Physiological and behavioral responses to human-induced tonic immobility (TI, sometimes termed "trancing" or "playing dead") have been found to be indicative of a fear-motivated stress state, confirming that the promotion of TI to try to increase a bond between rabbits and their owners—thinking the rabbits enjoy it—is misplaced.[34] However, some researchers conclude that inducing TI in rabbits is appropriate for certain procedures, as it holds less risk than anesthesia.[34]

Sore hocks

The formation of open sores on the rabbit's hocks, commonly called "sore hocks", is a problem that commonly afflicts mostly heavy-weight rabbits kept in cages with wire flooring[35] or soiled solid flooring. The problem is most prevalent in rex-furred rabbits and heavy-weight rabbits (9+ pounds in weight), as well as those with thin foot bristles.

The condition results when, over the course of time, the protective bristle-like fur on the rabbit's hocks thins down. Standing urine or other unsanitary cage conditions can exacerbate the problem by irritating the sensitive skin. The exposed skin in turn can result in tender areas or, in severe cases, open sores, which may then become infected and abscessed if not properly cared for.

Gastrointestinal stasis

Gastrointestinal stasis (GI stasis) is a serious and potentially fatal condition that occurs in some rabbits in which gut motility is severely reduced and possibly completely stopped. When untreated or improperly treated, GI stasis can be fatal in as little as 24 hours.

GI stasis is the condition of food not moving through the gut as quickly as normal. The gut contents may dehydrate and compact into a hard, immobile mass (impacted gut), blocking the digestive tract of the rabbit. Food in an immobile gut may also ferment, causing significant gas buildup and resultant gas pain for the rabbit.

The first noticeable symptom of GI stasis may be that the rabbit suddenly stops eating. Treatment frequently includes intravenous or subcutaneous fluid therapy (rehydration through injection of a balanced electrolyte solution), pain control, possible careful massage to promote gas expulsion and comfort, drugs to promote gut motility, and careful monitoring of all inputs and outputs. The rabbit's diet may also be changed as part of treatment, to include force-feeding to ensure adequate nutrition. Surgery to remove the blockage is not generally recommended and comes with a poor prognosis.[36]

Some rabbits are more prone to GI stasis than others. The causes of GI stasis are not completely understood, but common contributing factors are thought to include stress, reduced food intake, low fiber in the diet, dehydration, reduction in exercise or blockage caused by excess fur or carpet ingestion. Stress factors can include changes in housing, transportation, or medical procedures under anesthesia. As many of these factors may occur together (poor dental structure leading to decreased food intake, followed by a stressful veterinary dental procedure to correct the dental problem) establishing a root cause may be difficult.[37]

GI stasis is sometimes misdiagnosed as "hair balls" by veterinarians or rabbit keepers not familiar with the condition.[38][39] While fur is commonly found in the stomach following a fatal case of GI stasis, it is also found in healthy rabbits. Molting and chewing fur can be a predisposing factor in the occurrence of GI stasis, however, the primary cause is the change in motility of the gut.

Dental problems

Dental disease has several causes, namely genetics, inappropriate diet, injury to the jaw, infection, or cancer.

  • Malocclusion: Rabbit teeth are open-rooted and continue to grow throughout their lives. In some rabbits, the teeth are not properly aligned, a condition called malocclusion. Because of the misaligned nature of the rabbit's teeth, there is no normal wear to control the length to which the teeth grow. There are three main causes of malocclusion, most commonly genetic predisposition, injury, or bacterial infection. In the case of congenital malocclusion, treatment usually involves veterinary visits in which the teeth are treated with a dental burr (a procedure called crown reduction or, more commonly, teeth clipping) or, in some cases, permanently removed. In cases of simple malocclusion, a block of wood for the rabbit to chew on can rectify this problem.[citation needed]
  • Molar spurs: These are spurs that can dig into the rabbit's tongue and/or cheek causing pain. These should be filed down by an experienced exotic veterinarian specialised in rabbit care, using a dental burr, for example.
  • Osteoporosis: Rabbits, especially neutered females and those that are kept indoors without adequate natural sunlight, can suffer from osteoporosis, in which holes appear in the skull by X-Ray imaging. This reflects the general thinning of the bone, and teeth will start to become looser in the sockets, making it uncomfortable and painful for the animal to chew hay. The inability to properly chew hay can result in molar spurs, as described above, and weight loss, leading into a downward spiral if not treated promptly. This can be reversible and treatable. A veterinary formulated liquid calcium supplement[40] with vitamin D3 and magnesium can be given mixed with the rabbit's drinking water, once or twice per week, according to the veterinarian's instructions. The molar spurs should also be trimmed down by an experienced exotic veterinarian specialised in rabbit care, once per 1-2 months depending on the case.

Signs of dental difficulty include difficulty eating, weight loss and small stools and visibly overgrown teeth. However, there are many other causes of ptyalism, including pain due to other causes.[41]

Respiratory and conjunctival problems

An over-diagnosed ailment amongst rabbits is respiratory infection, known colloquially as "snuffles". Pasteurella, a bacterium, is usually misdiagnosed and this is known to be a factor in the overuse of antibiotics among rabbits.[42][full citation needed] A runny nose, for instance, can have several causes, among those being high temperature or humidity, extreme stress, environmental pollution (like perfume or incense), or a sinus infection. Options for treating this is removing the pollutant, lowering or raising the temperature accordingly, and medical treatment for sinus infections.[42] Pasteurella does live naturally in a rabbit's respiratory tract, and it can flourish out of control in some cases. In the rare event that happens, antibiotic treatment is necessary.

Sneezing can be a sign of environmental pollution (such as too much dust) or a food allergy.

Runny eyes and other conjunctival problems can be caused by dental disease or a blockage of the tear duct. Environmental pollution, corneal disease, entropion, distichiasis, or inflammation of the eyes are also causes. This is easy to diagnose as well as treat.[42]

Viral diseases

Rabbits are subject to infection by a variety of viruses. Some have had deadly and widespread impact.

Myxomatosis Trial
Wardang Island (Australia) 1938

Myxomatosis

Myxomatosis is a virulent threat to all rabbits but not to humans.[43] The intentional introduction of myxomatosis in rabbit-ravaged Australia killed an estimated 500 million feral rabbits between 1950 and 1952. The Australian government will not allow veterinarians to purchase and use the myxomatosis vaccine that would protect domestic rabbits, for fear that this immunity would be spread into the wild via escaped livestock and pets.[44] This potential consequence is also one motivation for the pet-rabbit ban in Queensland.[45]

In Australia, rabbits caged outdoors in areas with high numbers of mosquitoes are vulnerable to myxomatosis. In Europe, fleas are the carriers of myxomatosis. In some countries, annual vaccinations against myxomatosis are available.

Rabbit hemorrhagic disease (RHD)

Rabbit hemorrhagic disease (RHD), also known as viral hemorrhagic disease (VHD) or rabbit calicivirus disease (RCD),[46] is caused by a rabbit-specific calicivirus known as RHDV or RCV. Discovered in 1983, RHD is highly infectious and usually fatal. Initial signs of the disease may be limited to fever and lethargy, until significant internal organ damage results in labored breathing, squealing, bloody mucus, and eventual coma and death. Internally, the infection causes necrosis of the liver and damages other organs, especially the spleen, kidneys, and small intestine.

RHD, like myxomatosis, has been intentionally introduced to control feral rabbit populations in Australia and (illegally) in New Zealand, and RHD has, in some areas, escaped quarantine. The disease has killed tens of millions of rabbits in China (unintentionally) as well as Australia, with other epidemics reported in Bolivia, Mexico, South Korea, and continental Europe. Rabbit populations in New Zealand have bounced back after developing a genetic immunity to RHD, and the disease has, so far, had no effect on the genetically-divergent native wild rabbits and hares in the Americas.

In the United States, an October 2013 USDA document[47] stated:
RHD has been found in the United States as recently as 2010, and was detected in Canada in 2011. Thus far, outbreaks have been controlled quickly through quarantine, depopulation, disease tracing, and cleaning and disinfection; however, rabbit losses have been in the thousands. An RHD vaccine exists, but it is not recommended for use where the disease is not widespread in wildlife, as it may hide signs of disease and is not considered a practical response for such a rapidly spreading disease.

In the UK, reports of RHD (as recently as February 2018) have been submitted to the British Rabbit Council's online "Notice Board".[48] Vaccines for RHD are available—and mandatory—in the UK.

West Nile virus

West Nile virus is another threat to domestic as well as wild rabbits.[49] It is a fatal disease, and while vaccines are available for other species, there are none yet specifically indicated for rabbits.[50]

Wry neck & parasitic fungus

Wry neck (or head tilt) is a condition in rabbits that can be fatal, due to the resulting disorientation that causes the animal to stop eating and drinking.[citation needed] Inner ear infections or ear mites, as well as diseases or injuries affecting the brain (including stroke) can lead to wry neck. The most common cause, however, is a parasitic microscopic fungus called Encephalitozoon cuniculi (E. cuniculi). Note that: "despite approximately half of all pet rabbits carrying the infection, only a small proportion of these cases ever show any illness".[51] Some vets now recommend treating rabbits[clarification needed] against E. cuniculi.[citation needed] The usual drugs for treatment and prevention are the benzimidazole anthelmintics, particularly fenbendazole (also used as a deworming agent in other animal species). In the UK, fenbendazole (under the brand name Panacur Rabbit), is sold over-the-counter in oral paste form as a nine-day treatment. Fenbendazole is particularly recommended for rabbits kept in colonies and as a preventive before mixing new rabbits with each other.[51]

Fly strike

Fly strike, or blowfly strike, (Lucilia sericata) is a condition that occurs when flies (particularly bot flies) lay their eggs in a rabbit's damp or soiled fur, or in an open wound. Within 12 hours, the eggs hatch into the larval stage of the fly, known as maggots. Initially small but quickly growing to 15 millimetres (0.59 in) long, maggots can burrow into skin and feed on an animal's tissue, leading to shock and death. The most susceptible rabbits are those in unsanitary conditions, sedentary ones, and those unable to clean their excretory areas. Rabbits with diarrhea should be inspected for fly strike, especially during the summer months.[52] The topical treatment Rearguard® (from Novartis) is approved in the United Kingdom for 10-week-per-application prevention of fly strike.[53]

Breeds

Gemüsestilleben mit Häschen
by Johann Georg Seitz (1870)

There are currently 49 rabbit breeds recognized by the American Rabbit Breeders Association[54] and 106 recognized by the British Rabbit Council.[55] Many additional breeds of domestic rabbit are found throughout the world.[56] Selective breeding has produced rabbits ranging in size from dwarf to giant. Across the world, rabbits are raised as livestock (in cuniculture) for their meat, pelts, and wool, and also by fanciers and hobbyists as pets.

Rabbits have been selectively bred since ancient times to achieve certain desired characteristics.[56] Variations include size and body shape, coat type (including hair length and texture), coat color, ear carriage (erect or lop), and even ear length.[57] As with any animal, domesticated rabbits' temperaments vary in such factors as energy level and novelty seeking.

Most genetic defects in the domestic rabbit (such as dental problems in the Holland Lop breed) are due to recessive genes.[citation needed] Genetics are carefully tracked by fanciers who show rabbits, to breed out defects.

As pets

Rabbits have been kept as pets in Western nations since the 19th century, but because of the destructive history of feral rabbits in Australia, domestic rabbits are illegal as pets in Queensland.[58] Depending upon its size, a rabbit may be considered a type of pocket pet. Rabbits can bond with humans,[59] can learn to follow simple voice commands and to come when called,[24]:166 and are curious and playful.

Rabbits do not make good pets for small children because rabbits are fragile and easily injured by rough handling, can bite when hurt or frightened, and are easily frightened by loud noises and sudden motions.[60]

Rabbits are especially popular as pets in the United States during the Easter season, due to their association with the holiday. However, animal shelters that accept rabbits often complain that during the weeks and months following Easter, there is a rise in unwanted and neglected rabbits that were bought as Easter "gifts", especially for children.[61] Similar problems arise in rural areas after county fairs and the like, in jurisdictions where rabbits are legal prizes in fairground games.

Thus, there are many humane societies, animal shelters, and rescue groups that have rabbits available for pet adoption. Fancy rabbit breeds are often purchased from pet stores, private breeders, and fanciers.

House rabbits

A house rabbit sharing an apple

Rabbits may be kept as small house pets and "rabbit-proofed" spaces reduce the risks associated with their intrinsic need to chew.[20][21] Rabbits are easily litter box trained[62] and a rabbit that lives indoors may be less exposed to the dangers of predators, parasites, diseases, adverse weather, and pesticides.[20] Rabbits are often compatible with others of their kind, or with birds, chinchillas[citation needed], or guinea pigs, but opinion differs regarding the dangers of housing different species together.[63] Some people consider rabbits a pocket pet.

Keeping a rabbit as a house companion was popularised by Sandy Crook in her 1981 book Your French Lop.[citation needed] In 1983, at the American Family Pet Show in Anaheim, California (attended by 35,000), Crook presented her personal experiences living with an indoor rabbit as evidence of a human-rabbit bond.[64] In the late 1980s, it became more common to litter box train a rabbit and keep it indoors, after[citation needed] the publication of Marinell Harriman's House Rabbit Handbook: How to Live with an Urban Rabbit in 1985. (The book's fifth edition was published in 2013.)[65]

As the domestic descendants of wild prey animals, rabbits are alert, timid creatures that startle fairly easily, and many of their behaviors are triggered by the fight-or-flight response to perceived threats. According to the House Rabbit Society, the owner of a pet rabbit can use various behavioral approaches to gain the animal's trust and reduce aggression, though this can be a long and difficult process.[27]

In addition, there is evidence to suggest that young rabbits that occupy the periphery of the "litter huddle" obtain less milk from the mother and, as a result, have a lower weight. It has been suggested that this factor may contribute to behavioural differences in litter mates during adolescence. [66]

Advantages and disadvantages

The advantages of keeping rabbits as pets is that they are quiet, clean, smart, cute, and soft. They may react favorably to handling and petting depending on their personality and how they were raised. There are also many different sizes and characteristics available to a pet owner owing to a long history of breeding. Rabbits are friendly to each other and are often compatible with other pets. Rabbits are herbivores and their diet is relatively simple. Compared to other small animals, rabbits are robust creatures with strong hind legs (they can run fast) and powerful teeth. They have a "scruff" on the back of their neck, which can be used to pick them up.

The disadvantages of keeping rabbits as pets is that they may chew many things in the house. Male rabbits may mark their territory with a strong-smelling urine. Rabbits can bite under certain circumstances and they can also scratch. They can injure someone with their hind legs and rear claws if they jump out of someone's arms quickly. They have to be picked up and handled properly. They may leave poop around the house. Many rabbits may not be that friendly or interested in human beings. Male rabbits can be aggressive and territorial. Rabbits may not want to be touched. They will also do a high pitched scream when they are hurt or scared.

As livestock

Rabbits have been kept as livestock since ancient times for their meat, wool, and fur. In modern times, rabbits are also utilized in scientific research as laboratory animals.

Meat rabbits

Breeds such as the New Zealand and Californian are frequently utilized for meat in commercial rabbitries. These breeds have efficient metabolisms and grow quickly; they are ready for slaughter by approximately 14 to 16 weeks of age.

Rabbit fryers are rabbits that are between 70 and 90 days of age, and weighing between 3 and 5 lb (1 to 2 kg) live weight. Rabbit roasters are rabbits from 90 days to 6 months of age weighing between 5 and 8 lb (2 to 3.5 kg) live weight. Rabbit stewers are rabbits from 6 months on weighing over 8 lb.

Any type of rabbit can be slaughtered for meat, but those exhibiting the "commercial" body type are most commonly raised for meat purposes. Dark fryers (any other color but albino whites) are sometimes lower in price than albino fryers because of the slightly darker tinge of the fryer (purely pink carcasses are preferred by consumers) and because the dark hairs are easier to see than if there are residual white hairs on the carcass. There is no difference in skinability.

Wool rabbits

Rabbits such as the Angora, American Fuzzy Lop, and Jersey Wooly produce wool. However, since the American Fuzzy Lop and Jersey Wooly are both dwarf breeds, only the much larger Angora breeds such as the English Angora, Satin Angora, Giant Angora, and French Angoras are used for commercial wool production. Their long fur is sheared, combed, or plucked (gently pulling loose hairs from the body during molting) and then spun into yarn used to make a variety of products. Angora sweaters can be purchased in many clothing stores and is generally mixed with other types of wool. Rabbit wool, called Angora, is 2.5 times warmer than sheep's wool.[67]

Peaux de Lapin
"Rabbit skins"
by Edme Bouchardon (1737)

Fur rabbits

Rabbit breeds that were developed for their fur qualities include the Rex with its plush texture, the Satin with its lustrous color, and the Chinchilla for its exotic pattern. White rabbit fur may be dyed in an array of colors that aren't produced naturally. Rabbits in the fur industry are fed a diet focused for robust coat production and pelts are harvested after the rabbit reaches prime condition, which takes longer than in the meat industry. Rabbit fur is used in local and commercial textile industries throughout the world. China imports much of its rabbit fur from Scandinavia (80%) and some from North America (5%), according to the USDA Foreign Agricultural Service GAIN Report CH7607.[citation needed]

Laboratory rabbits

Rabbits have been and continue to be used in laboratory work such as production of antibodies for vaccines and research of human male reproductive system toxicology. In 1972, around 450,000 rabbits were used for experiments in the United States, decreasing to around 240 000 in 2006.[68] The Environmental Health Perspective, published by the National Institute of Health, states, "The rabbit [is] an extremely valuable model for studying the effects of chemicals or other stimuli on the male reproductive system."[69] According to the Humane Society of the United States, rabbits are also used extensively in the study of bronchial asthma, stroke prevention treatments, cystic fibrosis, diabetes, and cancer.

The New Zealand White is one of the most commonly used breeds for research and testing.

Animal rights activists generally oppose animal experimentation for all purposes, and rabbits are no exception.[improper synthesis?] The use of rabbits for the Draize test,[70] which is used for, amongst other things, testing cosmetics on animals, has been cited as an example of cruelty in animal research. Albino rabbits are typically used in the Draize tests because they have less tear flow than other animals, and the lack of eye pigment makes the effects easier to visualize.[71]

Housing

Rabbits can live outdoors in properly constructed, sheltered hutches, which provide protection from the elements in winter and keep rabbits cool in summer heat. To protect from predators, rabbit hutches are usually situated in a fenced yard, shed, barn, or other enclosed structure, which may also contain a larger pen for exercise.[72] Rabbits in such an environment can alternatively be allowed to roam the secured area freely, and simply be provided with an adapted doghouse for shelter. A more elaborate setup is an artificial warren.

Exhibition

Conformation shows

Judging at a rabbit show

Show rabbits are an increasingly popular activity. Showing rabbits helps to improve the vigor and physical behavior of each breed through competitive selection. County fairs are common venues through which rabbits are shown in the United States and many other countries. Rabbit clubs at local to national levels hold many shows each year. On any given weekend one may be able to find a show in most regions of the United States and the United Kingdom. Although only purebred animals are shown, a pedigree is not required to enter a rabbit in show sanctioned by the American Rabbit Breeders Association show but is required to register a rabbit with the ARBA.; a rabbit must be registered in order to receive a Grand Champion certificate.[73]

Children's clubs such as 4-H also include rabbit shows, usually in conjunction with county fairs. The ARBA holds an annual national convention which has as many as 25,000 animals competing for form all over the world. The national show moves to a different city each year. The ARBA also sponsors youth programs for families as well as underprivileged rural and inner-city children to learn responsible care and breeding of domestic rabbits.

Show jumping

Rabbit show jumping, a form of animal sport between rabbits, began in the 1970s and has since become popular in Europe, particularly Sweden and the United Kingdom. Any rabbit regardless of breed may participate in this kind of competition, as it is based on athletic skill.

See also



This article uses material from the Wikipedia article "Domestic rabbit", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Animals

3D,data,libary,model,catalog,rendering,skull,bone,animal,reptile,bird,insect,mammal,class,classification,order,family,species,genus