powered by CADENAS

Social Share

Lifting hook (8951 views - Tooling)

A lifting hook is a device for grabbing and lifting loads by means of a device such as a hoist or crane. A lifting hook is usually equipped with a safety latch to prevent the disengagement of the lifting wire rope sling, chain or rope to which the load is attached. A hook may have one or more built-in pulley sheaves as a block and tackle to multiply the lifting force.
Go to Article

Explanation by Hotspot Model

Lifting hook

Lifting hook

A lifting hook is a device for grabbing and lifting loads by means of a device such as a hoist or crane. A lifting hook is usually equipped with a safety latch to prevent the disengagement of the lifting wire rope sling, chain or rope to which the load is attached.

A hook may have one or more built-in pulley sheaves as a block and tackle to multiply the lifting force.

See also



This article uses material from the Wikipedia article "Lifting hook", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing