Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
A leg is a weight bearing and locomotive anatomical structure, usually having a columnar shape. During locomotion, legs function as "extensible struts".[1] The combination of movements at all joints can be modeled as a single, linear element capable of changing length and rotating about an omnidirectional "hip" joint.
As an anatomical animal structure it is used for locomotion. The distal end is often modified to distribute force (such as a foot). Most animals have an even number of legs.
As a component of furniture it is used for the economy of materials needed to provide the support for the useful surface, the table top or chair seat.
Many taxa are characterized by the number of legs:
A leg is a structure of gross anatomy, meaning that it is large enough to be seen unaided. The components depend on the animal. In humans and other mammals, a leg includes the bones, muscles, tendons, ligaments, blood vessels, nerves, and skin. In insects, the leg includes most of these things, except that insects have an exoskeleton that replaces the function of both the bones and the skin.
Sometimes the end of the leg, or foot, is considered part of the leg; other times it is considered separate. Similarly, the hip joint or other place where the leg attaches to the main body may be considered separate or part of the leg.
In tetrapod anatomy, leg is used to refer to the entire limb. In human medicine the precise definition refers[2][3][4] only to the segment between the knee and the ankle. This lower segment is also called the shank,[5][6] and the front (anterior) of the segment is called the shin or pretibia.
In bipedal tetrapods, the two lower limbs are referred to as the "legs" and the two upper limbs as "arms" or "wings" as the case may be.
A robotic leg is moved by an actuator, which is a type of motor for moving or controlling a mechanism or system. It is operated by a source of energy, usually in the form of an electric current, hydraulic fluid pressure or pneumatic pressure, and converts that energy into some kind of motion.
A prosthetic leg, a Prosthesis, is an artificial leg that is used to replace one that has been lost.
Wikimedia Commons has media related to Leg. |
This article uses material from the Wikipedia article "Leg", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted