Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Ransomware is a type of malicious software from cryptovirology that threatens to publish the victim's data or perpetually block access to it unless a ransom is paid. While some simple ransomware may lock the system in a way which is not difficult for a knowledgeable person to reverse, more advanced malware uses a technique called cryptoviral extortion, in which it encrypts the victim's files, making them inaccessible, and demands a ransom payment to decrypt them.[1][2][3][4] In a properly implemented cryptoviral extortion attack, recovering the files without the decryption key is an intractable problem – and difficult to trace digital currencies such as Ukash and Bitcoin are used for the ransoms, making tracing and prosecuting the perpetrators difficult.
Ransomware attacks are typically carried out using a Trojan that is disguised as a legitimate file that the user is tricked into downloading or opening when it arrives as an email attachment. However, one high-profile example, the "WannaCry worm", traveled automatically between computers without user interaction.
Starting from around 2012 the use of ransomware scams has grown internationally.[5][6][7] in June 2013, vendor McAfee released data showing that it had collected more than double the number of samples of ransomware that quarter than it had in the same quarter of the previous year.[8] CryptoLocker was particularly successful, procuring an estimated US $3 million before it was taken down by authorities,[9] and CryptoWall was estimated by the US Federal Bureau of Investigation (FBI) to have accrued over US $18m by June 2015.[10]
The concept of file encrypting ransomware was invented and implemented by Young and Yung at Columbia University and was presented at the 1996 IEEE Security & Privacy conference. It is called cryptoviral extortion and it was inspired by the fictional facehugger in the movie Alien.[11] Cryptoviral extortion is the following three-round protocol carried out between the attacker and the victim.[1]
The symmetric key is randomly generated and will not assist other victims. At no point is the attacker's private key exposed to victims and the victim need only send a very small ciphertext (the encrypted symmetric-cipher key) to the attacker.
Ransomware attacks are typically carried out using a Trojan, entering a system through, for example, a downloaded file or a vulnerability in a network service. The program then runs a payload, which locks the system in some fashion, or claims to lock the system but does not (e.g., a scareware program). Payloads may display a fake warning purportedly by an entity such as a law enforcement agency, falsely claiming that the system has been used for illegal activities, contains content such as pornography and "pirated" media.[12][13][14]
Some payloads consist simply of an application designed to lock or restrict the system until payment is made, typically by setting the Windows Shell to itself,[15] or even modifying the master boot record and/or partition table to prevent the operating system from booting until it is repaired.[16] The most sophisticated payloads encrypt files, with many using strong encryption to encrypt the victim's files in such a way that only the malware author has the needed decryption key.[1][17][18]
Payment is virtually always the goal, and the victim is coerced into paying for the ransomware to be removed—which may or may not actually occur—either by supplying a program that can decrypt the files, or by sending an unlock code that undoes the payload's changes. A key element in making ransomware work for the attacker is a convenient payment system that is hard to trace. A range of such payment methods have been used, including wire transfers, premium-rate text messages,[19] pre-paid voucher services such as Paysafecard,[5][20][21] and the digital currency Bitcoin.[22][23][24] A 2016 survey commissioned by Citrix claimed that larger businesses are holding bitcoin as contingency plans.[25]
The first known malware extortion attack, the "AIDS Trojan" written by Joseph Popp in 1989, had a design failure so severe it was not necessary to pay the extortionist at all. Its payload hid the files on the hard drive and encrypted only their names, and displayed a message claiming that the user's license to use a certain piece of software had expired. The user was asked to pay US$189 to "PC Cyborg Corporation" in order to obtain a repair tool even though the decryption key could be extracted from the code of the Trojan. The Trojan was also known as "PC Cyborg". Popp was declared mentally unfit to stand trial for his actions, but he promised to donate the profits from the malware to fund AIDS research.[26]
The idea of abusing anonymous cash systems to safely collect ransom from human kidnapping was introduced in 1992 by Sebastiaan von Solms and David Naccache.[27] This money collection method is a key feature of ransomware. In the von Solms-Naccache scenario a newspaper publication was used (since bitcoin ledgers did not exist at the time the paper was written).
The notion of using public key cryptography for data kidnapping attacks was introduced in 1996 by Adam L. Young and Moti Yung. Young and Yung critiqued the failed AIDS Information Trojan that relied on symmetric cryptography alone, the fatal flaw being that the decryption key could be extracted from the Trojan, and implemented an experimental proof-of-concept cryptovirus on a Macintosh SE/30 that used RSA and the Tiny Encryption Algorithm (TEA) to hybrid encrypt the victim's data. Since public key crypto is used, the cryptovirus only contains the encryption key. The attacker keeps the corresponding private decryption key private. Young and Yung's original experimental cryptovirus had the victim send the asymmetric ciphertext to the attacker who deciphers it and returns the symmetric decryption key it contains to the victim for a fee. Long before electronic money existed Young and Yung proposed that electronic money could be extorted through encryption as well, stating that "the virus writer can effectively hold all of the money ransom until half of it is given to him. Even if the e-money was previously encrypted by the user, it is of no use to the user if it gets encrypted by a cryptovirus".[1] They referred to these attacks as being "cryptoviral extortion", an overt attack that is part of a larger class of attacks in a field called cryptovirology, which encompasses both overt and covert attacks.[1] The cryptoviral extortion protocol was inspired by the forced-symbiotic relationship between H. R. Giger's facehugger and its host in the movie Alien.[1][11]
Examples of extortionate ransomware became prominent in May 2005.[28] By mid-2006, Trojans such as Gpcode, TROJ.RANSOM.A, Archiveus, Krotten, Cryzip, and MayArchive began utilizing more sophisticated RSA encryption schemes, with ever-increasing key-sizes. Gpcode.AG, which was detected in June 2006, was encrypted with a 660-bit RSA public key.[29] In June 2008, a variant known as Gpcode.AK was detected. Using a 1024-bit RSA key, it was believed large enough to be computationally infeasible to break without a concerted distributed effort.[30][31][32][33]
Encrypting ransomware returned to prominence in late 2013 with the propagation of CryptoLocker—using the Bitcoin digital currency platform to collect ransom money. In December 2013, ZDNet estimated based on Bitcoin transaction information that between 15 October and 18 December, the operators of CryptoLocker had procured about US$27 million from infected users.[34] The CryptoLocker technique was widely copied in the months following, including CryptoLocker 2.0 (though not to be related to CryptoLocker), CryptoDefense (which initially contained a major design flaw that stored the private key on the infected system in a user-retrievable location, due to its use of Windows' built-in encryption APIs),[23][35][36][37] and the August 2014 discovery of a Trojan specifically targeting network-attached storage devices produced by Synology.[38] In January 2015, it was reported that ransomware-styled attacks have occurred against individual websites via hacking, and through ransomware designed to target Linux-based web servers.[39][40][41]
The Microsoft Malware Protection Center identified a trend away from WSF files in favor of LNK files and PowerShell scripting.[42] These LNK shortcut files install Locky ransomware by automating infection operations rather than relying on traditional user downloads of WSF files—all of which is made possible by the universal PowerShell Windows application. Unfortunately, cyber criminals have been able to leverage PowerShell for their attacks for years. In a recent report, the application was found to be involved in nearly 40% of endpoint security incidents.[43] While attackers have been finding weaknesses in the Windows operating system for years, it’s clear that there’s something problematic with PowerShell scripting.[44]
Some ransomware strains have used proxies tied to Tor hidden services to connect to their command and control servers, increasing the difficulty of tracing the exact location of the criminals.[45][46] Furthermore, dark web vendors have increasingly started to offer the technology as a service.[46][47][48]
Symantec has classified ransomware to be the most dangerous cyber threat.[49]
In August 2010, Russian authorities arrested nine individuals connected to a ransomware Trojan known as WinLock. Unlike the previous Gpcode Trojan, WinLock did not use encryption. Instead, WinLock trivially restricted access to the system by displaying pornographic images, and asked users to send a premium-rate SMS (costing around US$10) to receive a code that could be used to unlock their machines. The scam hit numerous users across Russia and neighboring countries—reportedly earning the group over US$16 million.[14][50]
In 2011, a ransomware Trojan surfaced that imitated the Windows Product Activation notice, and informed users that a system's Windows installation had to be re-activated due to "[being a] victim of fraud". An online activation option was offered (like the actual Windows activation process), but was unavailable, requiring the user to call one of six international numbers to input a 6-digit code. While the malware claimed that this call would be free, it was routed through a rogue operator in a country with high international phone rates, who placed the call on hold, causing the user to incur large international long distance charges.[12]
In February 2013, a ransomware Trojan based on the Stamp.EK exploit kit surfaced; the malware was distributed via sites hosted on the project hosting services SourceForge and GitHub that claimed to offer "fake nude pics" of celebrities.[51] In July 2013, an OS X-specific ransomware Trojan surfaced, which displays a web page that accuses the user of downloading pornography. Unlike its Windows-based counterparts, it does not block the entire computer, but simply exploits the behavior of the web browser itself to frustrate attempts to close the page through normal means.[52]
In July 2013, a 21-year-old man from Virginia, whose computer coincidentally did contain pornographic photographs of underaged girls with whom he had conducted sexualized communications, turned himself in to police after receiving and being deceived by ransomware purporting to be an FBI message accusing him of possessing child pornography. An investigation discovered the incriminating files, and the man was charged with child sexual abuse and possession of child pornography.[53]
The converse of ransomware is a cryptovirology attack invented by Adam L. Young that threatens to publish stolen information from the victim's computer system rather than deny the victim access to it.[54] In a leakware attack, malware exfiltrates sensitive host data either to the attacker or alternatively, to remote instances of the malware, and the attacker threatens to publish the victim's data unless a ransom is paid. The attack was presented at West Point in 2003 and was summarized in the book Malicious Cryptography as follows, "The attack differs from the extortion attack in the following way. In the extortion attack, the victim is denied access to its own valuable information and has to pay to get it back, where in the attack that is presented here the victim retains access to the information but its disclosure is at the discretion of the computer virus".[55] The attack is rooted in game theory and was originally dubbed "non-zero sum games and survivable malware". The attack can yield monetary gain in cases where the malware acquires access to information that may damage the victim user or organization, e.g., reputational damage that could result from publishing proof that the attack itself was a success.
With the increased popularity of ransomware on PC platforms, ransomware targeting mobile operating systems has also proliferated. Typically, mobile ransomware payloads are blockers, as there is little incentive to encrypt data since it can be easily restored via online synchronization.[56] Mobile ransomware typically targets the Android platform, as it allows applications to be installed from third-party sources.[56][57] The payload is typically distributed as an APK file installed by an unsuspecting user; it may attempt to display a blocking message over top of all other applications,[57] while another used a form of clickjacking to cause the user to give it "device administrator" privileges to achieve deeper access to the system.[58]
Different tactics have been used on iOS devices, such as exploiting iCloud accounts and using the Find My iPhone system to lock access to the device.[59] On iOS 10.3, Apple patched a bug in the handling of JavaScript pop-up windows in Safari that had been exploited by ransomware websites.[60]
In 2012, a major ransomware Trojan known as Reveton began to spread. Based on the Citadel Trojan (which itself, is based on the Zeus Trojan), its payload displays a warning purportedly from a law enforcement agency claiming that the computer has been used for illegal activities, such as downloading unlicensed software or child pornography. Due to this behaviour, it is commonly referred to as the "Police Trojan".[61][62][63] The warning informs the user that to unlock their system, they would have to pay a fine using a voucher from an anonymous prepaid cash service such as Ukash or Paysafecard. To increase the illusion that the computer is being tracked by law enforcement, the screen also displays the computer's IP address, while some versions display footage from a victim's webcam to give the illusion that the user is being recorded.[5][64]
Reveton initially began spreading in various European countries in early 2012.[5] Variants were localized with templates branded with the logos of different law enforcement organizations based on the user's country; for example, variants used in the United Kingdom contained the branding of organizations such as the Metropolitan Police Service and the Police National E-Crime Unit. Another version contained the logo of the royalty collection society PRS for Music, which specifically accused the user of illegally downloading music.[65] In a statement warning the public about the malware, the Metropolitan Police clarified that they would never lock a computer in such a way as part of an investigation.[5][13]
In May 2012, Trend Micro threat researchers discovered templates for variations for the United States and Canada, suggesting that its authors may have been planning to target users in North America.[66] By August 2012, a new variant of Reveton began to spread in the United States, claiming to require the payment of a $200 fine to the FBI using a MoneyPak card.[6][7][64] In February 2013, a Russian citizen was arrested in Dubai by Spanish authorities for his connection to a crime ring that had been using Reveton; ten other individuals were arrested on money laundering charges.[67] In August 2014, Avast Software reported that it had found new variants of Reveton that also distribute password stealing malware as part of its payload.[68]
Encrypting ransomware reappeared in September 2013 with a Trojan known as CryptoLocker, which generated a 2048-bit RSA key pair and uploaded in turn to a command-and-control server, and used to encrypt files using a whitelist of specific file extensions. The malware threatened to delete the private key if a payment of Bitcoin or a pre-paid cash voucher was not made within 3 days of the infection. Due to the extremely large key size it uses, analysts and those affected by the Trojan considered CryptoLocker extremely difficult to repair.[22][69][70][71] Even after the deadline passed, the private key could still be obtained using an online tool, but the price would increase to 10 BTC—which cost approximately US$2300 as of November 2013.[72][73]
CryptoLocker was isolated by the seizure of the Gameover ZeuS botnet as part of Operation Tovar, as officially announced by the U.S. Department of Justice on 2 June 2014. The Department of Justice also publicly issued an indictment against the Russian hacker Evgeniy Bogachev for his alleged involvement in the botnet.[74][75] It was estimated that at least US$3 million was extorted with the malware before the shutdown.[9]
In September 2014, a wave of ransomware Trojans surfaced that first targeted users in Australia, under the names CryptoWall and CryptoLocker (which is, as with CryptoLocker 2.0, unrelated to the original CryptoLocker). The Trojans spread via fraudulent e-mails claiming to be failed parcel delivery notices from Australia Post; to evade detection by automatic e-mail scanners that follow all links on a page to scan for malware, this variant was designed to require users to visit a web page and enter a CAPTCHA code before the payload is actually downloaded, preventing such automated processes from being able to scan the payload. Symantec determined that these new variants, which it identified as CryptoLocker.F, were again, unrelated to the original CryptoLocker due to differences in their operation.[76][77] A notable victim of the Trojans was the Australian Broadcasting Corporation; live programming on its television news channel ABC News 24 was disrupted for half an hour and shifted to Melbourne studios due to a CryptoWall infection on computers at its Sydney studio.[78][79][80]
Another Trojan in this wave, TorrentLocker, initially contained a design flaw comparable to CryptoDefense; it used the same keystream for every infected computer, making the encryption trivial to overcome. However, this flaw was later fixed.[35] By late-November 2014, it was estimated that over 9,000 users had been infected by TorrentLocker in Australia alone, trailing only Turkey with 11,700 infections.[81]
Another major ransomware Trojan targeting Windows, CryptoWall, first appeared in 2014. One strain of CryptoWall was distributed as part of a malvertising campaign on the Zedo ad network in late-September 2014 that targeted several major websites; the ads redirected to rogue websites that used browser plugin exploits to download the payload. A Barracuda Networks researcher also noted that the payload was signed with a digital signature in an effort to appear trustworthy to security software.[82] CryptoWall 3.0 used a payload written in JavaScript as part of an email attachment, which downloads executables disguised as JPG images. To further evade detection, the malware creates new instances of explorer.exe and svchost.exe to communicate with its servers. When encrypting files, the malware also deletes volume shadow copies, and installs spyware that steals passwords and Bitcoin wallets.[83]
The FBI reported in June 2015 that nearly 1,000 victims had contacted the bureau's Internet Crime Complaint Center to report CryptoWall infections, and estimated losses of at least $18 million.[10]
The most recent version, CryptoWall 4.0, enhanced its code to avoid antivirus detection, and encrypts not only the data in files but also the file names.[84]
Fusob is one of the major mobile ransomware families. Between April 2015 and March 2016, about 56 percent of accounted mobile ransomware was Fusob.[85]
Like a typical mobile ransomware, it employs scare tactics to extort people to pay a ransom.[86] The program pretends to be an accusatory authority, demanding the victim to pay a fine from $100 to $200 USD or otherwise face a fictitious charge. Rather surprisingly, Fusob suggests using iTunes gift cards for payment. Also, a timer clicking down on the screen adds to the users’ anxiety as well.
In order to infect devices, Fusob masquerades as a pornographic video player. Thus, victims, thinking it is harmless, unwittingly download Fusob.[87]
When Fusob is installed, it first checks the language used in the device. If it uses Russian or certain Eastern European languages, Fusob does nothing. Otherwise, it proceeds on to lock the device and demand ransom. Among victims, about 40% of them are in Germany with the United Kingdom and the United States following with 14.5% and 11.4% respectively.
Fusob has lots in common with Small, which is another major family of mobile ransomware. They represented over 93% of mobile ransomwares between 2015 and 2016.
In May 2017, the WannaCry ransomware attack spread through the Internet, using an exploit vector named EternalBlue, which was leaked from the U.S. National Security Agency. The ransomware attack, unprecedented in scale,[88] infected more than 230,000 computers in over 150 countries,[89] using 20 different languages to demand money from users using Bitcoin cryptocurrency. WannaCrypt demanded US$300 per computer.[90] The attack affected Telefónica and several other large companies in Spain, as well as parts of the British National Health Service (NHS), where at least 16 hospitals had to turn away patients or cancel scheduled operations,[91] FedEx, Deutsche Bahn, Honda,[92] Renault, as well as the Russian Interior Ministry and Russian telecom MegaFon.[93] The attackers gave their victims a 7-day deadline from the day their computers got infected, after which the encrypted files would be deleted.[94]
Petya was first discovered in March 2016; unlike other forms of encrypting ransomware, the malware aimed to infect the master boot record, installing a payload which encrypts the file tables of the NTFS file system the next time that the infected system boots, blocking the system from booting into Windows at all until the ransom is paid. Check Point reported that despite what it believed to be an innovative evolution in ransomware design, it had resulted in relatively-fewer infections than other ransomware active around the same time frame.[95]
On June 27, 2017, a heavily modified version of Petya was used for a global cyberattack primarily targeting Ukraine. This version had been modified to propagate using the same EternalBlue exploit that was used by WannaCry. Due to another design change, it is also unable to actually unlock a system after the ransom is paid; this led to security analysts speculating that the attack was not meant to generate illicit profit, but to simply cause disruption.[96][97]
On October 24, 2017, some users in Russia and Ukraine reported a new ransomware attack, named "Bad Rabbit", which follows a similar pattern to WannaCry and Petya by encrypting the user's file tables and then demands a BitCoin payment to decrypt them. ESET believed the ransomware to have been distributed by a bogus update to Adobe Flash software.[98] Among agencies that were affected by the ransomware included Interfax, Odessa International Airport, Kiev Metro, and the Ministry of Infrastructure of Ukraine.[99] As it used corporate network structures to spread, the ransomware was also discovered in other countries, including Turkey, Germany, Poland, Japan, South Korea, and the United States.[100] Experts believed the ransomware attack was tied to the Petya attack in the Ukraine, though the only identity to the culprits are the names of characters from the Game of Thrones series embedded within the code.[100]
Security experts found that the ransomware did not use the EternalBlue exploit to spread, and a simple method to vaccinate an unaffected machine running older Windows versions was found by October 24, 2017.[101][102] Further, the sites that had been used to spread the bogus Flash updating have gone offline or removed the problematic files within a few days of its discovery, effectively killing off the spread of Bad Rabbit.[100]
As with other forms of malware, security software (antivirus software) might not detect a ransomware payload, or, especially in the case of encrypting payloads, only after encryption is under way or complete, particularly if a new version unknown to the protective software is distributed.[103] If an attack is suspected or detected in its early stages, it takes some time for encryption to take place; immediate removal of the malware (a relatively simple process) before it has completed would stop further damage to data, without salvaging any already lost.[104][105]
Security experts have suggested precautionary measures for dealing with ransomware. Using software or other security policies to block known payloads from launching will help to prevent infection, but will not protect against all attacks[22][106] Keeping "offline" backups of data stored in locations inaccessible from any potentially infected computer, such as external storage drives or devices that do not have any access to any network (including the Internet), prevents them from being accessed by the ransomware. Installing security updates issued by software vendors can mitigate the vulnerabilities leveraged by certain strains to propagate.[107][108][109][110][111] Other measures include cyber hygiene − exercising caution when opening e-mail attachments and links, network segmentation, and keeping critical computers isolated from networks.[112][113] Furthermore, to mitigate the spread of ransomware measures of infection control can be applied.[114] Such may include disconnecting infected machines from all networks, educational programs,[115] effective communication channels, malware surveillance[original research?] and ways of collective participation[114]
There are a number of tools intended specifically to decrypt files locked by ransomware, although successful recovery may not be possible.[2][116] If the same encryption key is used for all files, decryption tools use files for which there are both uncorrupted backups and encrypted copies (a known-plaintext attack in the jargon of cryptanalysis); recovery of the key, if it is possible, may take several days.[117] Free ransomware decryption tools can help decrypt files encrypted by the following forms of ransomware: AES_NI, Alcatraz Locker, Apocalypse, BadBlock, Bart, BTCWare, Crypt888, CryptoMix, CrySiS, EncrypTile, FindZip, Globe, Hidden Tear, Jigsaw, LambdaLocker, Legion, NoobCrypt, Stampado, SZFLocker, TeslaCrypt, XData.[118]
The publication of proof-of-concept attack code is common among academic researchers and vulnerability researchers. It teaches the nature of the threat, conveys the gravity of the issues, and enables countermeasures to be devised and put into place. However, lawmakers with the support of law-enforcement bodies are contemplating making the creation of ransomware illegal. In the state of Maryland the original draft of HB 340 made it a felony to create ransomware, punishable by up to 10 years in prison.[119] However, this provision was removed from the final version of the bill.[120] A minor in Japan was arrested for creating and distributing ransomware code.[121] Young and Yung have had the ANSI C source code to a ransomware cryptotrojan on-line, at cryptovirology.com, since 2005 as part of a cryptovirology book being written. The source code to the cryptotrojan is still live on the Internet and is associated with a draft of Chapter 2.[122]
This article uses material from the Wikipedia article "Ransomware", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D