powered by CADENAS

Social Share

Plasma torch (2419 views - Tooling)

A plasma torch (also known as a plasma arc, plasma gun, or plasma cutter, plasmatron) is a device for generating a directed flow of plasma. The plasma jet can be used for applications including plasma cutting, plasma arc welding, plasma spraying, and plasma gasification for waste disposal.
Go to Article

Explanation by Hotspot Model

Plasma torch

Plasma torch

A plasma torch (also known as a plasma arc, plasma gun, or plasma cutter, plasmatron) is a device for generating a directed flow of plasma.[1][2]

The plasma jet can be used for applications including plasma cutting, plasma arc welding, plasma spraying, and plasma gasification for waste disposal.[3]

Types of thermal plasma torches

Thermal plasmas are generated in plasma torches by direct current (DC), alternating current (AC), radio-frequency (RF) and other discharges. DC torches are the most commonly used and researched, because when compared to AC: “there is less flicker generation and noise, a more stable operation, better control, a minimum of two electrodes, lower electrode consumption, slightly lower refractory [heat] wear and lower power consumption”.[4]

Thermal plasma DC torches, non-transferred arc, based on hot cathode

In a DC torch, the electric arc is formed between the electrodes (which can be made of copper, tungsten, graphite, molybdenum, silver etc.), and the thermal plasma is formed from the continual input of carrier/working gas, projecting outward as a plasma jet/flame (as can be seen on the right). In DC torches, the carrier gas can be, for example, either oxygen, nitrogen, argon, helium, air, or hydrogen;[4] and although termed as such, it does not have to be a gas (thus, better termed a carrier fluid).

For example, a research plasma torch at the Institute of Plasma Physics (IPP) in Prague, Czech Republic, functions with an H2O vortex (as well as a small addition of argon to ignite the arc), and produces a high temperature/velocity plasma flame.[5] In fact, early studies of arc stabilization employed a water-vortex.[6] Overall, the electrode materials and carrier fluids have to be specifically matched to avoid excessive electrode corrosion or oxidation (and contamination of materials to be treated), while maintaining ample power and function.

Furthermore, the flow-rate of the carrier gas can be raised to promote a larger, more projecting plasma jet, provided that the arc current is sufficiently increased; and vice versa.

The plasma flame of a real plasma torch is a few inches long at most; it is to be distinguished from fictional long-range plasma weapons.

Transferred vs. non-transferred

It is important to note that there are two types of DC torches: non-transferred and transferred. In non-transferred DC torches, the electrodes are inside the body/housing of the torch itself (creating the arc there). Whereas in transferred—one electrode is outside (and is usually the conductive material to be treated), allowing the arc to form outside of the torch over a larger distance.

A benefit of transferred DC torches is that the plasma arc is formed outside the water-cooled body, preventing heat loss—as is the case with non-transferred torches, where their electrical-to-thermal efficiency can be as low as 50%, but the hot water can itself be utilized.[5] Furthermore, transferred DC torches can be used in a twin-torch setup, where one torch is cathodic and the other anodic, which has the earlier benefit of a regular transferred single-torch system, but allows their use with non-conductive materials, as there is no need for it to form the other electrode.[4] The electrodes of non-transferred torches are larger, because they suffer more wear by the plasma arc.

The quality of plasma produced is a function of density (pressure), temperature and torch power (the greater the better). With regards to the efficiency of the torch itself—this can vary among manufacturers and torch technology; though for example, Leal-Quirós reports that for Westinghouse Plasma Corp. torches “a thermal efficiency of 90% is easily possible; the efficiency represents the percentage of arc power that exits the torch and enters the process”.[7]

See also



This article uses material from the Wikipedia article "Plasma torch", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing