powered by CADENAS

Social Share

Injector (12280 views - Mechanical Engineering)

A steam injector is typically used to deliver cold water to a boiler against its own pressure using its own live or exhaust steam, replacing any mechanical pump. This was the purpose for which it was originally invented in 1858 by Henri Giffard. Its operation was from the start intriguing since it seemed paradoxical, almost like perpetual motion, but its operation was later explained using thermodynamics. Other types of injector may use other pressurised motive fluids such as air. Depending on the application, an injector can also take the form of an eductor-jet pump, a water eductor or an aspirator. An ejector operates on similar principles to create a vacuum feed connection for braking systems etc..
Go to Article

Explanation by Hotspot Model

Injector

Injector

A steam injector is typically used to deliver cold water to a boiler against its own pressure using its own live or exhaust steam, replacing any mechanical pump. This was the purpose for which it was originally invented in 1858 by Henri Giffard. Its operation was from the start intriguing since it seemed paradoxical, almost like perpetual motion, but its operation was later explained using thermodynamics.[1] Other types of injector may use other pressurised motive fluids such as air.

Depending on the application, an injector can also take the form of an eductor-jet pump, a water eductor or an aspirator. An ejector operates on similar principles to create a vacuum feed connection for braking systems etc..

History

The injector was invented by Henri Giffard for the steam locomotive[2] and patented in the United Kingdom by Messrs Sharp Stewart & Co. of Glasgow.

After some initial scepticism resulting from the unfamiliar and superficially paradoxical mode of operation, the injector was widely adopted as an alternative to mechanical pumps in steam locomotives.

Operation

The injector consists of a body containing a series of three or more "cones" containing nozzles along one axis.

It uses the Venturi effect of a converging-diverging nozzle on a steam jet to convert the pressure energy of the steam to velocity energy, reducing its pressure to below atmospheric which enables it to entrain a fluid (eg. water). After passing through the convergent "combining cone", the mixed fluid is fully condensed releasing the latent heat of evaporation of the steam which imparts extra velocity to the water. The condensate mixture then enters a divergent "delivery cone" which slows the jet, converting kinetic energy back into static pressure energy above the pressure of the boiler enabling its feed through a non-return valve.[3][4]

Most of the heat energy in the condensed steam is returned to the boiler, increasing the thermal efficiency of the process. Injectors are therefore typically over 98% energy-efficient overall; they are also simple compared to the many moving parts in a feed pump.

The motive fluid may be a liquid, steam or any other gas. The entrained suction fluid may be a gas, a liquid, a slurry, or a dust-laden gas stream.[5][6]

Key design parameters

Fluid feed rate and operating pressure range are the key parameters of an injector, and vacuum pressure and evacuation rate for an ejector.

Compression ratio and the entrainment ratio may also be defined:

The compression ratio of the injector, , is defined as ratio of the injector's outlet pressure to the inlet pressure of the suction fluid .

The entrainment ratio of the injector, , is defined as the amount (in kg/h) of suction fluid that can be entrained and compressed by a given amount (in kg/h) of motive fluid.

Lifting Properties

Other key properties of an injector include the fluid inlet pressure requirements i.e. whether it is lifting or non-lifting.

In a non-lifting injector, positive inlet fluid pressure is needed e.g. the cold water-input is fed by gravity.

The steam-cone minimal orifice diameter is kept larger than the combining cone minimal diameter.[7] The non-lifting Nathan 4000 injector used on the Southern Pacific 4294 could push 12,000 US gallons (45,000 L) per hour at 250 psi (17 bar).[8]

The lifting injector can operate with negative inlet fluid pressure i.e. fluid lying below the level of the injector. It differs from the non-lifting type mainly in the relative dimensions of the nozzles.[9]

Overflow

An overflow is required for excess steam or water to discharge, especially during starting; if the injector cannot initially overcome boiler pressure, the overflow allows the injector to continue to draw water and steam.

Check valve

There is at least one check valve (called a "clack valve" in locomotives because of the distinctive noise it makes[4]) between the exit of the injector and the boiler to prevent back flow, and usually a valve to prevent air being sucked in at the overflow.

Exhaust steam injector

Efficiency was further improved by the development of a multi-stage injector which is powered not by live steam from the boiler but by exhaust steam from the cylinders, thereby making use of the residual energy in the exhaust steam which would otherwise have gone to waste. However, an exhaust injector also cannot work when the locomotive is stationary; later exhaust injectors could use a supply of live steam if no exhaust steam was available.

Problems

Injectors can be troublesome under certain running conditions, when vibration caused the combined steam and water jet to "knock off". Originally the injector had to be restarted by careful manipulation of the steam and water controls, and the distraction caused by a malfunctioning injector was largely responsible for the 1913 Ais Gill rail accident. Later injectors were designed to automatically restart on sensing the collapse in vacuum from the steam jet, for example with a spring-loaded delivery cone.

Another common problem occurs when the incoming water is too warm and is less effective at condensing the steam in the combining cone. This can also occur if the metal body of the injector is too hot, e.g. from prolonged use.

Vacuum ejectors

An additional use for the injector technology is in vacuum ejectors in continuous train braking systems, which were made compulsory in the UK by the Regulation of Railways Act 1889. A vacuum ejector uses steam pressure to draw air out of the vacuum pipe and reservoirs of continuous train brake. Steam locomotives, with a ready source of steam, found ejector technology ideal with its rugged simplicity and lack of moving parts. A steam locomotive usually has two ejectors: a large ejector for releasing the brakes when stationary and a small ejector for maintaining the vacuum against leaks. The small ejector is sometimes replaced by a reciprocating pump driven from the crosshead because this is more economical of steam.

Vacuum brakes have been superseded by air brakes in modern trains, which use pumps, as diesel and electric locomotives no longer have a suitable working fluid for vacuum ejectors.

Earlier application of the principle

An empirical application of the principle was in widespread use on steam locomotives before its formal development as the injector, in the form of the arrangement of the blastpipe and chimney in the locomotive smokebox. The sketch on the right shows a cross section through a smokebox, rotated 90 degrees; it can be seen that the same components are present, albeit differently named, as in the generic diagram of an injector at the top of the article. Exhaust steam from the cylinders is directed through a nozzle on the end of the blastpipe, to reduce pressure inside the smokebox by entraining the flue gases from the boiler which are then ejected via the chimney. The effect is to increase the draught on the fire to a degree proportional to the rate of steam consumption, so that as more steam is used, more heat is generated from the fire and steam production is also increased. The effect was first noted by Richard Trevithick and subsequently developed empirically by the early locomotive engineers; Stephenson's Rocket made use of it, and this constitutes much of the reason for its notably improved performance in comparison with contemporary machines.

Modern uses

The use of injectors (or ejectors) in various industrial applications has become quite common due to their relative simplicity and adaptability. For example:

  • To inject chemicals into the boiler drums of small, stationary, low pressure boilers. In large, high-pressure modern boilers, usage of injectors for chemical dosing is not possible due to their limited outlet pressures.
  • In thermal power stations, they are used for the removal of the boiler bottom ash, the removal of fly ash from the hoppers of the electrostatic precipitators used to remove that ash from the boiler flue gas, and for drawing a vacuum pressure in steam turbine exhaust condensers.
  • Jet pumps have been used in boiling water nuclear reactors to circulate the coolant fluid.[10]
  • For use in producing a vacuum pressure in steam jet cooling systems.
  • For enhanced oil recovery processes in the oil & gas Industry.
  • For the bulk handling of grains or other granular or powdered materials.
  • The construction industry uses them for pumping turbid water and slurries.
  • Eductors are used in ships to pump residual ballast water, or cargo oil which cannot be removed using centrifugal pumps due to loss of suction head and may damage the centrifugal pump if run dry, which may be caused due to trim or list of the ship.
  • Eductors are used on-board ships to pump out bilges, since using centrifugal pump would not be feasible as the suction head may be lost frequently.
  • Some aircraft (mostly earlier designs) use an ejector attached to the fuselage to provide vacuum for gyroscopic instruments such as an attitude indicator (artificial horizon).
  • Eductors are used in aircraft fuel systems as transfer pumps; fluid flow from an engine-mounted mechanical pump can be delivered to a fuel tank-mounted eductor to transfer fuel from that tank.
  • Aspirators are vacuum pumps based on the same operating principle and are used in laboratories to create a partial vacuum and for medical use in suction of mucus or bodily fluids.
  • Water eductors are water pumps used for dredging silt and panning for gold, they're used because they can handle the highly abrasive mixtures quite well.
  • To create vacuum system in vacuum distillation unit (oil refinery)

Well pumps

Jet pumps are commonly used to extract water from water wells. The main pump, often a centrifugal pump, is powered and installed at ground level. Its discharge is split, with the greater part of the flow leaving the system, while a portion of the flow is returned to the jet pump installed below ground in the well. This recirculated part of the pumped fluid is used to power the jet. At the jet pump, the high-energy, low-mass returned flow drives more fluid from the well, becoming a low-energy, high-mass flow which is then piped to the inlet of the main pump.

The S type pump is useful for removing water from a well or container.

Shallow well pumps are those in which the jet assembly is attached directly to the main pump and are limited to a depth of approximately 5-8m to prevent cavitation.

Deep well pumps are those in which the jet is located at the bottom of the well. The maximum depth for deep well pumps is determined by the inside diameter of and the velocity through the jet. The major advantage of jet pumps for deep well installations is the ability to situate all mechanical parts (e.g., electric/petrol motor, rotating impellers) at the ground surface for easy maintenance. The advent of the electrical submersible pump has partly replaced the need for jet type well pumps, except for driven point wells or surface water intakes.

Multi-stage steam vacuum ejectors

In practice, for suction pressure below 100 mbar absolute, more than one ejector is used, usually with condensers between the ejector stages. Condensing of motive steam greatly improves ejector set efficiency; both barometric and shell-and-tube surface condensers are used.

In operation a two-stage system consists of a primary high-vacuum (HV) ejector and a secondary low-vacuum (LV) ejector. Initially the LV ejector is operated to pull vacuum down from the starting pressure to an intermediate pressure. Once this pressure is reached, the HV ejector is then operated in conjunction with the LV ejector to finally pull vacuum to the required pressure.

In operation a three-stage system consists of a primary booster, a secondary high-vacuum (HV) ejector, and a tertiary low-vacuum (LV) ejector. As per the two-stage system, initially the LV ejector is operated to pull vacuum down from the starting pressure to an intermediate pressure. Once this pressure is reached, the HV ejector is then operated in conjunction with the LV ejector to pull vacuum to the lower intermediate pressure. Finally the booster is operated (in conjunction with the HV & LV ejectors) to pull vacuum to the required pressure.

Construction materials

Injectors or ejectors are made of carbon steel, stainless steel, titanium, PTFE, carbon, and other materials.

See also



This article uses material from the Wikipedia article "Injector", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD