Licensed under Creative Commons Attribution-Share Alike 3.0 (User:Aka).
Chocolate most commonly comes in dark, milk, and white varieties, with cocoa solids contributing to the brown color. | |
Main ingredients | Chocolate liquor, cocoa butter for white chocolate, often with added sugar |
---|---|
Cookbook: Chocolate Media: Chocolate |
Chocolate /ˈtʃɒklɪt, -kəlɪt, -lət, ˈtʃɔːk-/ ( listen) is a typically sweet, usually brown food preparation of Theobroma cacao seeds, roasted and ground. It is made in the form of a liquid, paste, or in a block, or used as a flavoring ingredient in other foods. Cacao has been cultivated by many cultures for at least three millennia in Mesoamerica. The earliest evidence of use traces to the Olmecs (Mexico), with evidence of chocolate beverages dating back to 1900 BCE.[1] In fact, the majority of Mesoamerican people made chocolate beverages, including the Maya and Aztecs,[2] who made it into a beverage known as xocolātl Nahuatl pronunciation: [ʃoˈkolaːt͡ɬ], a Nahuatl word meaning "bitter water". The seeds of the cacao tree have an intense bitter taste and must be fermented to develop the flavor.
After fermentation, the beans are dried, cleaned, and roasted. The shell is removed to produce cacao nibs, which are then ground to cocoa mass, unadulterated chocolate in rough form. Once the cocoa mass is liquefied by heating, it is called chocolate liquor. The liquor also may be cooled and processed into its two components: cocoa solids and cocoa butter. Baking chocolate, also called bitter chocolate, contains cocoa solids and cocoa butter in varying proportions, without any added sugars. Much of the chocolate consumed today is in the form of sweet chocolate, a combination of cocoa solids, cocoa butter or added vegetable oils, and sugar. Milk chocolate is sweet chocolate that additionally contains milk powder or condensed milk. White chocolate contains cocoa butter, sugar, and milk, but no cocoa solids.
Cocoa solids are a source of flavonoids[3] and alkaloids, such as theobromine, phenethylamine and caffeine.[4] Chocolate also contains anandamide.[5]
Chocolate has become one of the most popular food types and flavors in the world, and a vast number of foodstuffs involving chocolate have been created, particularly desserts including cakes, pudding, mousse, chocolate brownies, and chocolate chip cookies. Many candies are filled with or coated with sweetened chocolate, and bars of solid chocolate and candy bars coated in chocolate are eaten as snacks. Gifts of chocolate molded into different shapes (e.g., eggs, hearts, coins) have become traditional on certain Western holidays, such as Easter, Valentine's Day, and Hanukkah. Chocolate is also used in cold and hot beverages such as chocolate milk and hot chocolate and in some alcoholic drinks, such as creme de cacao.
Although cocoa originated in the Americas, recent years have seen African nations assuming a leading role in producing cocoa. Since the 2000s, Western Africa produces almost two-thirds of the world's cocoa, with Ivory Coast growing almost half of that amount.
The word "chocolate" entered the English language from Spanish in about 1600.[6] The word entered Spanish from Nahuatl word chocolātl, the language of the Aztecs, but the exact etymology of the Nahuatl word is debated. One proposed etymology derives it from the word chicolatl, meaning "beaten drink", which may derive from the word for the frothing stick, chicoli.[7] The term "chocolate chip" was first used in 1940.[8] The term "chocolatier", for a chocolate confection maker, is attested from 1888.[8]
Chocolate has been prepared as a drink for nearly all of its history. For example, one vessel found at an Olmec archaeological site on the Gulf Coast of Veracruz, Mexico, dates chocolate's preparation by pre-Olmec peoples as early as 1750 BCE.[9] On the Pacific coast of Chiapas, Mexico, a Mokaya archaeological site provides evidence of cacao beverages dating even earlier, to 1900 BCE.[10][9] The residues and the kind of vessel in which they were found indicate the initial use of cacao was not simply as a beverage, but the white pulp around the cacao beans was likely used as a source of fermentable sugars for an alcoholic drink.[11]
An early Classic-period (460–480 AD) Mayan tomb from the site in Rio Azul had vessels with the Maya glyph for cacao on them with residue of a chocolate drink, suggests the Maya were drinking chocolate around 400 AD.[12] Documents in Maya hieroglyphs stated chocolate was used for ceremonial purposes, in addition to everyday life.[13] The Maya grew cacao trees in their backyards,[14] and used the cacao seeds the trees produced to make a frothy, bitter drink.[15]
By the 15th century, the Aztecs gained control of a large part of Mesoamerica and adopted cacao into their culture. They associated chocolate with Quetzalcoatl, who, according to one legend, was cast away by the other gods for sharing chocolate with humans,[16] and identified its extrication from the pod with the removal of the human heart in sacrifice.[17] In contrast to the Maya, who liked their chocolate warm, the Aztecs drank it cold, seasoning it with a broad variety of additives, including the petals of the Cymbopetalum penduliflorum tree, chile pepper, allspice, vanilla, and honey.
The Aztecs were not able to grow cacao themselves, as their home in the Mexican highlands was unsuitable for it, so chocolate was a luxury imported into the empire.[16] Those who lived in areas ruled by the Aztecs were required to offer cacao seeds in payment of the tax they deemed "tribute".[16] Cocoa beans were often used as currency.[18] For example, the Aztecs used a system in which one turkey cost 100 cacao beans and one fresh avocado was worth three beans.[19]
Until the 16th century, no European had ever heard of the popular drink from the Central American peoples.[16] Christopher Columbus and his son Ferdinand encountered the cacao bean on Columbus's fourth mission to the Americas on 15 August 1502, when he and his crew seized a large native canoe that proved to contain cacao beans among other goods for trade.[20] Spanish conquistador Hernán Cortés may have been the first European to encounter it, as the frothy drink was part of the after-dinner routine of Montezuma.[12][21] Jose de Acosta, a Spanish Jesuit missionary who lived in Peru and then Mexico in the later 16th century, wrote of its growing influence on the Spaniards:
Loathsome to such as are not acquainted with it, having a scum or froth that is very unpleasant taste. Yet it is a drink very much esteemed among the Indians, where with they feast noble men who pass through their country. The Spaniards, both men and women that are accustomed to the country are very greedy of this Chocolate. They say they make diverse sorts of it, some hot, some cold, and some temperate, and put therein much of that "chili"; yea, they make paste thereof, the which they say is good for the stomach and against the catarrh.[22]
While Columbus had taken cacao beans with him back to Spain,[20] chocolate made no impact until Spanish friars introduced it to the Spanish court.[16] After the Spanish conquest of the Aztecs, chocolate was imported to Europe. There, it quickly became a court favorite. It was still served as a beverage, but the Spanish added sugar, as well as honey, to counteract the natural bitterness.[23] Vanilla was also a popular additive, with pepper and other spices sometimes used to give the illusion of a more potent vanilla flavor. Unfortunately, these spices had the tendency to unsettle the European constitution; the Encyclopédie states, "The pleasant scent and sublime taste it imparts to chocolate have made it highly recommended; but a long experience having shown that it could potentially upset one's stomach," which is why chocolate without vanilla was sometimes referred to as "healthy chocolate."[24] By 1602, chocolate had made its way from Spain to Austria.[25] By 1662, Pope Alexander VII had declared that religious fasts were not broken by consuming chocolate drinks. Within about a hundred years, chocolate established a foothold throughout Europe.[16]
The new craze for chocolate brought with it a thriving slave market, as between the early 1600s and late 1800s, the laborious and slow processing of the cacao bean was manual.[16] Cacao plantations spread, as the English, Dutch, and French colonized and planted. With the depletion of Mesoamerican workers, largely to disease, cacao production was often the work of poor wage laborers and African slaves. Wind-powered and horse-drawn mills were used to speed production, augmenting human labor. Heating the working areas of the table-mill, an innovation that emerged in France in 1732, also assisted in extraction.[26]
New processes that sped the production of chocolate emerged early in the Industrial Revolution. In 1815, Dutch chemist Coenraad van Houten introduced alkaline salts to chocolate, which reduced its bitterness.[16] A few years thereafter, in 1828, he created a press to remove about half the natural fat (cocoa butter or cacao butter) from chocolate liquor, which made chocolate both cheaper to produce and more consistent in quality. This innovation introduced the modern era of chocolate.[20] Known as "Dutch cocoa", this machine-pressed chocolate was instrumental in the transformation of chocolate to its solid form when, in 1847, Joseph Fry learned to make chocolate moldable by adding back melted cacao butter.[23] Milk had sometimes been used as an addition to chocolate beverages since the mid-17th century, but in 1875 Daniel Peter invented milk chocolate by mixing a powdered milk developed by Henri Nestlé with the liquor.[16][20] In 1879, the texture and taste of chocolate was further improved when Rudolphe Lindt invented the conching machine.[28]
Besides Nestlé, a number of notable chocolate companies had their start in the late 19th and early 20th centuries. Rowntree's of York set up and began producing chocolate in 1862, after buying out the Tuke family business. Cadbury was manufacturing boxed chocolates in England by 1868.[16] In 1893, Milton S. Hershey purchased chocolate processing equipment at the World's Columbian Exposition in Chicago, and soon began the career of Hershey's chocolates with chocolate-coated caramels.
Several types of chocolate can be distinguished. Pure, unsweetened chocolate, often called "baking chocolate", contains primarily cocoa solids and cocoa butter in varying proportions. Much of the chocolate consumed today is in the form of sweet chocolate, which combines chocolate with sugar.
Milk chocolate is sweet chocolate that also contains milk powder or condensed milk. In the UK and Ireland, milk chocolate must contain a minimum of 20% total dry cocoa solids; in the rest of the European Union, the minimum is 25%.[29] "White chocolate" contains cocoa butter, sugar, and milk, but no cocoa solids. Chocolate contains alkaloids such as theobromine and phenethylamine, which have physiological effects in humans, but the presence of theobromine renders it toxic to some animals, such as dogs and cats.[30] Chocolate contains "brain cannabinoids" such as anandamide, N-oleoylethanolamine and N-linoleoylethanolamine.[5] Dark chocolate has been promoted for unproven health benefits.[31]
White chocolate, although similar in texture to that of milk and dark chocolate, does not contain any cocoa solids. Because of this, many countries do not consider white chocolate as chocolate at all.[32] Because it does not contain any cocoa solids, white chocolate does not contain any theobromine, so it can be consumed by animals.
Dark chocolate is produced by adding fat and sugar to the cacao mixture. The U.S. Food and Drug Administration calls this "sweet chocolate", and requires a 15% concentration of chocolate liquor. European rules specify a minimum of 35% cocoa solids.[29] Semisweet chocolate is a dark chocolate with a low sugar content. Bittersweet chocolate is chocolate liquor to which some sugar (typically a third), more cocoa butter, vanilla, and sometimes lecithin have been added. It has less sugar and more liquor than semisweet chocolate, but the two are interchangeable in baking.
Unsweetened chocolate is pure chocolate liquor, also known as bitter or baking chocolate. It is unadulterated chocolate: the pure, ground, roasted chocolate beans impart a strong, deep chocolate flavor. It is typically used in baking or other products to which sugar and other ingredients are added. Raw chocolate, often referred to as raw cacao, is always dark and a minimum of 75% cacao.
Poorly tempered chocolate may have whitish spots on the dark chocolate part, called chocolate bloom; it is an indication that sugar and/or fat has separated due to poor storage. It is not toxic and can be safely consumed.[33]
Roughly two-thirds of the entire world's cocoa is produced in West Africa, with 43% sourced from Ivory Coast,[34]As of 2007[update] where child labor is a common practice to obtain the product.[35][36] According to the World Cocoa Foundation, in 2007 some 50 million people around the world depended on cocoa as a source of livelihood.[37] >As of 2007[update] in the UK, most chocolatiers purchase their chocolate from them, to melt, mold and package to their own design.[38] According to the WCF's 2012 report, the Ivory Coast is the largest producer of cocoa in the world.[39] The two main jobs associated with creating chocolate candy are chocolate makers and chocolatiers. Chocolate makers use harvested cacao beans and other ingredients to produce couverture chocolate (covering). Chocolatiers use the finished couverture to make chocolate candies (bars, truffles, etc.).[40]
Production costs can be decreased by reducing cocoa solids content or by substituting cocoa butter with another fat. Cocoa growers object to allowing the resulting food to be called "chocolate", due to the risk of lower demand for their crops.[37]
The sequencing in 2010 of the genome of the cacao tree may allow yields to be improved.[41] Due to concerns about global warming effects on lowland climate in the narrow band of latitudes where cacao is grown (20 degrees north and south of the equator), the commercial company Mars, Incorporated and the University of California, Berkeley are conducting genomic research in 2017-18 to improve the survivability of cacao plants in hot climates.[42]
Chocolate is made from cocoa beans, the dried and fermented seeds of the cacao tree (Theobroma cacao), a small, 4–8 m tall (15–26 ft tall) evergreen tree native to the deep tropical region of the Americas. Recent genetic studies suggest the most common genotype of the plant originated in the Amazon basin and was gradually transported by humans throughout South and Central America. Early forms of another genotype have also been found in what is now Venezuela. The scientific name, Theobroma, means "food of the gods".[43] The fruit, called a cacao pod, is ovoid, 15–30 cm (6–12 in) long and 8–10 cm (3–4 in) wide, ripening yellow to orange, and weighing about 500 g (1.1 lb) when ripe.
Cacao trees are small, understory trees that need rich, well-drained soils. They naturally grow within 20° of either side of the equator because they need about 2000 mm of rainfall a year, and temperatures in the range of 21 to 32 °C (70 to 90 °F). Cacao trees cannot tolerate a temperature lower than 15 °C (59 °F).[44]
The three main varieties of cacao beans used in chocolate are criollo, forastero, and trinitario.
Representing only 5% of all cocoa beans grown As of 2008[update],[45] criollo is the rarest and most expensive cocoa on the market, and is native to Central America, the Caribbean islands and the northern tier of South American states.[46] The genetic purity of cocoas sold today as criollo is disputed, as most populations have been exposed to the genetic influence of other varieties.
Criollos are particularly difficult to grow, as they are vulnerable to a variety of environmental threats and produce low yields of cocoa per tree. The flavor of criollo is described as delicate yet complex, low in classic chocolate flavor, but rich in "secondary" notes of long duration.[47]
The most commonly grown bean is forastero,[45] a large group of wild and cultivated cacaos, most likely native to the Amazon basin. The African cocoa crop is entirely of the forastero variety. They are significantly hardier and of higher yield than criollo. The source of most chocolate marketed,[45] forastero cocoas are typically strong in classic "chocolate" flavor, but have a short duration and are unsupported by secondary flavors, producing "quite bland" chocolate.[45]
Trinitario is a natural hybrid of criollo and forastero. Trinitario originated in Trinidad after an introduction of forastero to the local criollo crop. Nearly all cacao produced over the past five decades is of the forastero or lower-grade trinitario varieties.[48]
Cacao pods are harvested by cutting them from the tree using a machete, or by knocking them off the tree using a stick. The beans with their surrounding pulp are removed from the pods and placed in piles or bins, allowing access to micro-organisms so fermentation of the pectin-containing material can begin. Yeasts produce ethanol, lactic acid bacteria produce lactic acid, and acetic acid bacteria produce acetic acid. The fermentation process, which takes up to seven days, also produces several flavor precursors, eventually resulting in the familiar chocolate taste.[49]
It is important to harvest the pods when they are fully ripe, because if the pod is unripe, the beans will have a low cocoa butter content, or sugars in the white pulp will be insufficient for fermentation, resulting in a weak flavor. After fermentation, the beans must be quickly dried to prevent mold growth. Climate and weather permitting, this is done by spreading the beans out in the sun from five to seven days.[50]
The dried beans are then transported to a chocolate manufacturing facility. The beans are cleaned (removing twigs, stones, and other debris), roasted, and graded. Next, the shell of each bean is removed to extract the nib. Finally, the nibs are ground and liquefied, resulting in pure chocolate in fluid form: chocolate liquor.[51] The liquor can be further processed into two components: cocoa solids and cocoa butter.[52]
Chocolate liquor is blended with the cocoa butter in varying quantities to make different types of chocolate or couvertures. The basic blends of ingredients for the various types of chocolate (in order of highest quantity of cocoa liquor first), are:
Usually, an emulsifying agent, such as soy lecithin, is added, though a few manufacturers prefer to exclude this ingredient for purity reasons and to remain GMO-free, sometimes at the cost of a perfectly smooth texture. Some manufacturers are now using PGPR, an artificial emulsifier derived from castor oil that allows them to reduce the amount of cocoa butter while maintaining the same mouthfeel.
The texture is also heavily influenced by processing, specifically conching (see below). The more expensive chocolate tends to be processed longer and thus have a smoother texture and mouthfeel, regardless of whether emulsifying agents are added.
Different manufacturers develop their own "signature" blends based on the above formulas, but varying proportions of the different constituents are used. The finest, plain dark chocolate couvertures contain at least 70% cocoa (both solids and butter), whereas milk chocolate usually contains up to 50%. High-quality white chocolate couvertures contain only about 35% cocoa butter.
Producers of high-quality, small-batch chocolate argue that mass production produces bad-quality chocolate.[45] Some mass-produced chocolate contains much less cocoa (as low as 7% in many cases), and fats other than cocoa butter. Vegetable oils and artificial vanilla flavor are often used in cheaper chocolate to mask poorly fermented and/or roasted beans.[45]
In 2007, the Chocolate Manufacturers Association in the United States, whose members include Hershey, Nestlé, and Archer Daniels Midland, lobbied the Food and Drug Administration (FDA) to change the legal definition of chocolate to let them substitute partially hydrogenated vegetable oils for cocoa butter, in addition to using artificial sweeteners and milk substitutes.[53] Currently, the FDA does not allow a product to be referred to as "chocolate" if the product contains any of these ingredients.[54][55]
In the EU a product can be sold as chocolate if it contains up to 5% vegetable oil, and must be labelled as "family milk chocolate" rather than "milk chocolate" if it contains 20% milk.[56]
According to Canadian Food and Drug Regulations,[57] a "chocolate product" is a food product that is sourced from at least one "cocoa product" and contains at least one of the following: "chocolate, bittersweet chocolate, semi-sweet chocolate, dark chocolate, sweet chocolate, milk chocolate, or white chocolate." A "cocoa product" is defined as a food product that is sourced from cocoa beans and contains "cocoa nibs, cocoa liquor, cocoa mass, unsweetened chocolate, bitter chocolate, chocolate liquor, cocoa, low-fat cocoa, cocoa powder, or low-fat cocoa powder."
The penultimate process is called conching. A conche is a container filled with metal beads, which act as grinders. The refined and blended chocolate mass is kept in a liquid state by frictional heat. Chocolate prior to conching has an uneven and gritty texture. The conching process produces cocoa and sugar particles smaller than the tongue can detect, hence the smooth feel in the mouth. The length of the conching process determines the final smoothness and quality of the chocolate. High-quality chocolate is conched for about 72 hours, and lesser grades about four to six hours. After the process is complete, the chocolate mass is stored in tanks heated to about 45 to 50 °C (113 to 122 °F) until final processing.[58]
The final process is called tempering. Uncontrolled crystallization of cocoa butter typically results in crystals of varying size, some or all large enough to be clearly seen with the naked eye. This causes the surface of the chocolate to appear mottled and matte, and causes the chocolate to crumble rather than snap when broken.[59][60] The uniform sheen and crisp bite of properly processed chocolate are the result of consistently small cocoa butter crystals produced by the tempering process.
The fats in cocoa butter can crystallize in six different forms (polymorphous crystallization).[59][61] The primary purpose of tempering is to assure that only the best form is present. The six different crystal forms have different properties.
Crystal | Melting temp. | Notes |
---|---|---|
I | 17 °C (63 °F) | Soft, crumbly, melts too easily |
II | 21 °C (70 °F) | Soft, crumbly, melts too easily |
III | 26 °C (79 °F) | Firm, poor snap, melts too easily |
IV | 28 °C (82 °F) | Firm, good snap, melts too easily |
V | 34 °C (93 °F) | Glossy, firm, best snap, melts near body temperature (37 °C) |
VI | 36 °C (97 °F) | Hard, takes weeks to form |
As a solid piece of chocolate, the cocoa butter fat particles are in a crystalline rigid structure that gives the chocolate its solid appearance. Once heated, the crystals of the polymorphic cocoa butter are able to break apart from the rigid structure and allow the chocolate to obtain a more fluid consistency as the temperature increases – the melting process. When the heat is removed, the cocoa butter crystals become rigid again and come closer together, allowing the chocolate to solidify.[62]
The temperature in which the crystals obtain enough energy to break apart from their rigid conformation would depend on the milk fat content in the chocolate and the shape of the fat molecules, as well as the form of the cocoa butter fat. Chocolate with a higher fat content will melt at a lower temperature.[63]
Making chocolate considered "good" is about forming as many type V crystals as possible. This provides the best appearance and texture and creates the most stable crystals, so the texture and appearance will not degrade over time. To accomplish this, the temperature is carefully manipulated during the crystallization.Generally, the chocolate is first heated to 45 °C (113 °F) to melt all six forms of crystals.[59][61] Next, the chocolate is cooled to about 27 °C (81 °F), which will allow crystal types IV and V to form. At this temperature, the chocolate is agitated to create many small crystal "seeds" which will serve as nuclei to create small crystals in the chocolate. The chocolate is then heated to about 31 °C (88 °F) to eliminate any type IV crystals, leaving just type V. After this point, any excessive heating of the chocolate will destroy the temper and this process will have to be repeated. However, other methods of chocolate tempering are used. The most common variant is introducing already tempered, solid "seed" chocolate. The temper of chocolate can be measured with a chocolate temper meter to ensure accuracy and consistency. A sample cup is filled with the chocolate and placed in the unit which then displays or prints the results.
Two classic ways of manually tempering chocolate are:
Chocolate tempering machines (or temperers) with computer controls can be used for producing consistently tempered chocolate. In particular continuous tempering machines are used in large volume applications. Various methods and apparatuses for continuous flow tempering have been described by Aasted, Sollich and Buhler, three manufacturers of commercial chocolate equipment, with a focus now on energy efficiency. In general, molten chocolate coming in at 40–50 °C is cooled in heat exchangers to crystallization temperates of about 26–30 °C, passed through a tempering column consisting of spinning plates to induce shear, then warmed slightly to re-melt undesirable crystal formations.[64][65]
Chocolate is very sensitive to temperature and humidity. Ideal storage temperatures are between 15 and 17 °C (59 and 63 °F), with a relative humidity of less than 50%. If refrigerated or frozen without containment, chocolate can absorb enough moisture to cause a whitish discoloration, the result of fat or sugar crystals rising to the surface. Various types of "blooming" effects can occur if chocolate is stored or served improperly.[66]
Chocolate bloom is caused by storage temperature fluctuating or exceeding 24 °C (75 °F), while sugar bloom is caused by temperature below 15 °C (59 °F) or excess humidity. To distinguish between different types of bloom, one can rub the surface of the chocolate lightly, and if the bloom disappears, it is fat bloom. Moving chocolate between temperature extremes, can result in an oily texture. Although visually unappealing, chocolate suffering from bloom is safe for consumption.[67][68][69] Bloom can be reversed by retempering the chocolate or using it for any use that requires melting the chocolate.[70]
Chocolate is generally stored away from other foods, as it can absorb different aromas. Ideally, chocolates are packed or wrapped, and placed in proper storage with the correct humidity and temperature. Additionally, chocolate is frequently stored in a dark place or protected from light by wrapping paper.
Nutritional value per 100 g (3.5 oz) | |
---|---|
Energy | 2,240 kJ (540 kcal) |
59.4 | |
Sugars | 51.5 |
Dietary fiber | 3.4 g |
29.7 | |
7.6 | |
Vitamins | |
Vitamin A | 195 IU |
Thiamine (B1) |
(9%) 0.1 mg |
Riboflavin (B2) |
(25%) 0.3 mg |
Niacin (B3) |
(3%) 0.4 mg |
Vitamin B6 |
(0%) 0.0 mg |
Folate (B9) |
(3%) 11 μg |
Vitamin B12 |
(29%) 0.7 μg |
Choline |
(9%) 46.1 mg |
Vitamin C |
(0%) 0 mg |
Vitamin E |
(3%) 0.5 mg |
Vitamin K |
(5%) 5.7 μg |
Minerals | |
Calcium |
(19%) 189 mg |
Iron |
(18%) 2.4 mg |
Magnesium |
(18%) 63 mg |
Manganese |
(24%) 0.5 mg |
Phosphorus |
(30%) 208 mg |
Potassium |
(8%) 372 mg |
Selenium |
(6%) 4.5 μg |
Sodium |
(5%) 79 mg |
Zinc |
(24%) 2.3 mg |
Other constituents | |
Water | 1.5 g |
Caffeine | 20 mg |
Cholesterol | 23 mg |
theobromine | 205 mg |
| |
| |
Percentages are roughly approximated using US recommendations for adults. Source: USDA Nutrient Database |
A 100 gram serving of milk chocolate supplies 540 calories. It is 59% carbohydrates (52% as sugar and 3% as dietary fiber), 30% fat and 8% protein (table). Approximately 65% of the fat in milk chocolate is saturated, composed mainly of palmitic acid and stearic acid, while the predominant unsaturated fat is oleic acid (table, see USDA reference for full report).
In 100 gram amounts, milk chocolate is an excellent source (> 19% of the Daily Value, DV) of riboflavin, vitamin B12 and the dietary minerals, manganese, phosphorus and zinc (table). Chocolate is a good source (10–19% DV) of calcium, magnesium and iron (table).
Chocolate may be a factor for heartburn in some people because one of its constituents, theobromine, may affect the oesophageal sphincter muscle, hence permitting stomach acidic contents to enter into the oesophagus.[71] Theobromine is also toxic to some animals unable to metabolize it (see theobromine poisoning).
Excessive consumption of large quantities of any energy-rich food, such as chocolate, without a corresponding increase in activity to expend the associated calories, can increase the risk of weight gain and possibly obesity.[71] Raw chocolate is high in cocoa butter, a fat which is removed during chocolate refining, then added back in varying proportions during the manufacturing process. Manufacturers may add other fats, sugars, and milk as well, all of which increase the caloric content of chocolate.[71]
Chocolate and cocoa contain moderate to high amounts of oxalate,[72][73] which may increase risk for kidney stones.[74] During cultivation and production, chocolate may absorb lead from the environment,[75] but the total amounts typically eaten are less than the tolerable daily limit for lead consumption, according to a World Health Organization report from 2010.[76] However, reports from 2014 indicate that "chocolate might be a significant source" of lead ingestion for children if consumption is high[77][78] and "one 10 g cube of dark chocolate may contain as much as 20% of the daily lead oral limit."[77]
A few studies have documented allergic reactions from chocolate in children.[71]
Chocolate and cocoa are under preliminary research to determine if consumption affects the risk of certain cardiovascular diseases[79] or cognitive abilities.[80]
Some manufacturers provide the percentage of chocolate in a finished chocolate confection as a label quoting percentage of "cocoa" or "cacao". It should be noted that this refers to the combined percentage of both cocoa solids and cocoa butter in the bar, not just the percentage of cocoa solids.[81] The Belgian AMBAO certification mark indicates that no non-cocoa vegetable fats have been used in making the chocolate.[82][83]
Chocolates that are organic[84] or fair trade certified[85] carry labels accordingly.
In the United States, some large chocolate manufacturers lobbied the federal government to permit confections containing cheaper hydrogenated vegetable oil in place of cocoa butter to be sold as "chocolate". In June 2007, as a response to consumer concern after the proposed change, the FDA reiterated "Cacao fat, as one of the signature characteristics of the product, will remain a principal component of standardized chocolate."[86]
The chocolate industry is a steadily growing, $50 billion-a-year worldwide business centered on the sale and consumption of chocolate. It is prevalent throughout most of the world.[87] Europe accounts for 45% of the world's chocolate revenue[88] and the US$20 billion.[89] Big Chocolate is the grouping of major international chocolate companies in Europe and the U.S. The U.S. companies, such as Mars and Hershey's alone, generate $13 billion a year in chocolate sales and account for two-thirds of U.S. production.[90] Despite the expanding reach of the chocolate industry internationally, cocoa farmers and labourers in the Ivory Coast are unaware of the uses of the beans. The high cost of chocolate in the Ivory Coast also means that it is inaccessible to the majority of the population, who are unaware of what it tastes like.[91]
Chocolate manufacturers produce a range of products from chocolate bars to fudge. Large manufacturers of chocolate products include Cadbury (the world's largest confectionery manufacturer), Ferrero, Guylian, The Hershey Company, Lindt & Sprüngli, Mars, Incorporated, Milka, Neuhaus and Suchard.
Guylian is best known for its chocolate sea shells; Cadbury for its Dairy Milk and Creme Egg. The Hershey Company, the largest chocolate manufacturer in North America, produces the Hershey Bar and Hershey's Kisses.[92] Mars Incorporated, a large privately owned U.S. corporation, produces Mars Bar, Milky Way, M&M's, Twix, and Snickers. Lindt is known for its truffle balls and gold foil-wrapped Easter bunnies.
Food conglomerates Nestlé SA and Kraft Foods both have chocolate brands. Nestlé acquired Rowntree's in 1988 and now markets chocolates under their own brand, including Smarties (a chocolate candy) and Kit Kat (a candy bar); Kraft Foods through its 1990 acquisition of Jacobs Suchard, now owns Milka and Suchard. In February 2010, Kraft also acquired British-based Cadbury.;[93] Fry's, Trebor Basset and the fair trade brand Green & Black's also belongs to the group.
The widespread use of children in cocoa production is controversial, not only for the concerns about child labor and exploitation, but also because up to 12,000 of the 200,000 children working in Côte d'Ivoire, the world's biggest producer of cocoa,[94] may be victims of trafficking or slavery.[95] Most attention on this subject has focused on West Africa, which collectively supplies 69 percent of the world's cocoa,[96] and Côte d'Ivoire in particular, which supplies 35 percent of the world's cocoa.[96] Thirty percent of children under age 15 in sub-Saharan Africa are child laborers, mostly in agricultural activities including cocoa farming.[97] It is estimated that more than 1.8 million children in West Africa are involved in growing cocoa.[98] Major chocolate producers, such as Nestlé, buy cocoa at commodities exchanges where Ivorian cocoa is mixed with other cocoa.[99]
In 2009, Salvation Army International Development (SAID) UK stated that 12,000 children have been trafficked on cocoa farms in the Ivory Coast of Africa, where half of the world's chocolate is made.[100] SAID UK states that it is these child slaves who are likely to be working in "harsh and abusive"[101] conditions for the production of chocolate,[100] and an increasing number of health-food[102] and anti-slavery[103] organisations are now highlighting and campaigning against the use of trafficking in the chocolate industry.
In the 2000s, some chocolate producers began to engage in fair trade initiatives, to address concerns about the marginalization of cocoa laborers in developing countries. Traditionally, Africa and other developing countries received low prices for their exported commodities such as cocoa, which caused poverty to abound. Fair trade seeks to establish a system of direct trade from developing countries to counteract this unfair system.[104] One solution for fair labor practices is for farmers to become part of an Agricultural cooperative. Cooperatives pay farmers a fair price for their cocoa so farmers have enough money for food, clothes, and school fees.[105] One of the main tenets of fair trade is that farmers receive a fair price, but this does not mean that the larger amount of money paid for fair trade cocoa goes directly to the farmers. The effectiveness of fair trade has been questioned. In a 2014 article, The Economist stated that workers on fair trade farms have a lower standard of living than on similar farms outside the fair trade system.[106]
Chocolate is sold in chocolate bars, which come in dark chocolate, milk chocolate and white chocolate varieties. Some bars that are mostly chocolate have other ingredients blended into the chocolate, such as nuts, raisins or crisped rice. Chocolate is used as an ingredient in a huge variety of candy bars, which typically contain various confectionary ingredients (e.g., nougat, wafers, caramel, nuts, etc.) which are coated in chocolate. Chocolate is used as a flavouring product in many desserts, such as chocolate cakes, chocolate brownies, chocolate mousse and chocolate chip cookies. Numerous types of candy and snacks contain chocolate, either as a filling (e.g., M&M's) or as a coating (e.g., chocolate-coated raisins or chocolate-coated peanuts). Some non-alcoholic beverages contain chocolate, such as chocolate milk, hot chocolate and chocolate milkshakes. Some alcoholic liqueurs are flavoured with chocolate, such as chocolate liqueur and creme de cacao. Chocolate is a popular flavour of ice cream and pudding, and chocolate sauce is a commonly added as a topping on ice cream sundaes.
Chocolate is associated with festivals such as Easter, when moulded chocolate rabbits and eggs are traditionally given in Christian communities, and Hanukkah, when chocolate coins are given in Jewish communities. Chocolate hearts and chocolate in heart-shaped boxes are popular on Valentine's Day and are often presented along with flowers and a greeting card. In 1868, Cadbury created Fancy Boxes – a decorated box of chocolates – in the shape of a heart for Valentine's Day.[27] Boxes of filled chocolates quickly became associated with the holiday.[27] Chocolate is an acceptable gift on other holidays and on occasions such as birthdays.
Many confectioners make holiday-specific chocolate candies. Chocolate Easter eggs or rabbits and Santa Claus figures are two examples. Such confections can be solid, hollow, or filled with sweets or fondant.
Chocolate has been the center of several successful book and film adaptations. In 1964, Roald Dahl published a children's novel titled Charlie and the Chocolate Factory. The novel centers on a poor boy named Charlie Bucket who takes a tour through the greatest chocolate factory in the world, owned by Willy Wonka. Two film adaptations of the novel were produced. The first was Willy Wonka & the Chocolate Factory, a 1971 film which later became a cult classic, and spawned the real world Willy Wonka Candy Company, which produces chocolate products to this day. Thirty-four years later, a second film adaptation was produced, titled Charlie and the Chocolate Factory. The 2005 film was very well received by critics[107] and was one of the highest-grossing films that year, earning over US$470,000,000 worldwide.[108] Charlie and the Chocolate Factory was also recognized at the 78th Academy Awards, where it was nominated for Best Costume Design for Gabriella Pesucci.[109]
Like Water for Chocolate (Como agua para chocolate), a 1989 love story by novelist Laura Esquivel, was adapted to film in 1992. The plot incorporates magical realism with Mexican cuisine, and the title is a double entendre in its native language, referring both to a recipe for hot chocolate and to an idiom that is a metaphor for sexual arousal. The film earned 11 Ariel Awards from the Academia Mexicana de Artes y Ciencias Cinematográficas, including Best Picture.
Chocolat, a 1999 novel by Joanne Harris, tells the story of Vianne Rocher, a young mother, whose confections change the lives of the townspeople. The 2000 film adaptation, Chocolat, also proved successful, grossing over US$150,000,000 worldwide,[110] and receiving Academy Award and Golden Globe nominations for Best Picture, Best Actress, and Best Original Score.[111][112]
This article uses material from the Wikipedia article "Chocolate", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
food,liquor,alcohol,drink,beverage,coke