powered by CADENAS

Social Share

Miter saw (3115 views - Tooling)

A miter saw (mitre in British English) is a saw used to make accurate crosscuts and miters in a workpiece by pulling a large backsaw or a mounted circular saw blade down onto a board in a quick motion. Both miter saws and abrasive cut off saws are commonly referred to as a chop saw.
Go to Article

Explanation by Hotspot Model

Miter saw

Miter saw

A miter saw (mitre in British English) is a saw used to make accurate crosscuts and miters in a workpiece by pulling a large backsaw or a mounted circular saw blade down onto a board in a quick motion. Both miter saws and abrasive cut off saws are commonly referred to as a chop saw.

Power miter saw

A power miter saw, also known as a chop saw or drop saw, is a power tool used to make a quick, accurate crosscut in a workpiece at a selected angle. Commonly used for cutting of molding and trim. Most miter saws are relatively small and portable, with common blade sizes ranging from eight to twelve inches.

The power miter saw was invented by Ed Niehaus, a tool designer for Rockwell, in 1964. The miter saw showcased several innovations still found today: radial arc spring action, blade braking and dust collection. Rockwell did not patent the design, leading to a large number of manufacturers and innovation improvements.[1]

The power miter saw makes cuts by pulling a spinning circular saw blade down onto a workpiece in a short, controlled motion. The workpiece is typically held against a fence, which provides a precise cutting angle between the plane of the blade and the plane of the longest workpiece edge. In standard position, this angle is fixed at 90°.

A primary distinguishing feature of the miter saw is the miter index that allows the angle of the blade to be changed relative to the fence.[2] While most miter saws enable precise one-degree incremental changes to the miter index, many also provide "stops" that allow the miter index to be quickly set to common angles (such as 15°, 22.5°, 30°, and 45°).

Types

There are several types of miter saws:[3][4]

  • Original miter box and saw - The original was a wood 3 sided box with 90° and 45° slots for guiding a hand saw into cutting miter cuts into the clamped lumber.
  • Standard miter saw - A power tool designed for straight cross cuts on you lumber at a range of angles (unlike a abrasive saw which can only cut 90 degrees to the board). Commonly used to create 45° degree straight cuts for framing.
  • Compound-miter saw - Compound adds the ability to rotate the blade head at a range of angles from the board allowing you to enter the wood at an angle other than 90 degrees. It creates a ramp angled cut into the side of the wood, allows for more complex cuts, and is commonly used in trim work for homes. A compound miter saw is also known as a single compound miter saw, meaning that the head only rotates when angled on one side, requiring the user to flip the board to get angle cuts in the other direction.
  • Dual compound-miter saw - Dual or double compound saws allow the head to rotate when angled on both the left and right hand sides. This is useful in decorative trim work where you don't have to flip the board to cut the mirror angle on the other side.
  • Sliding compound-miter saw - Sliding adds the radial arm saw feature of being able to move the saw head back and forth, thereby increasing the board size that can be cross cut. Without the sliding feature the cut can be made only by a straight pull down (like chop saws). With the sliding feature engaged, the user pulls the head forward, turns on the saw and pushes the blade back across the lumber.
  • Laser LED sliding dual compound miter-saw - The laser is a disc-shaped washer that attaches to the saw blade and shows where the blade will cut. The LED is a feature to light up the work area.

Features

Miter saws are dedicated cross cut saws; long rip cuts are not possible.

A laser guide provides a precise visual indication of where the cut will be positioned on the workpiece in the current configuration. Some models provide a single reference line for one side of the kerf, while others provide two lines to reflect the total kerf width. A blade guard is a cover for the teeth of the cutting blade. Most modern miter saws have self-retracting blade guards, which automatically retract when the saw is lowered onto a workpiece and re-cover the blade when the saw is raised. It is very dangerous to use the saw if these guards are removed or damaged. A dust bag connects directly to the saw, and helps to collect sawdust away from the workpiece during cutting. Optionally, many manufacturers sell adapters to connect an industrial vacuum cleaner in lieu of a bag to capture more of the dust and simplify disposal. Dust removal with these saws is notoriously poor. A safety clamp helps to lock a workpiece into position prior to making a cut. This is an especially important feature when cutting smaller workpieces (eight inches or smaller). The miter table is typically less than 24" in diameter.[5] Typically, the work needs to be supported on the far end to stabilize the piece while cutting.

Miter saws are inherently low-hazard as the work piece is held stationary against a fence while the saw head moves, making kick-back almost impossible, and normally allowing hands to be kept clear of the blade.[6] Also the saw head is usually drawn back, then lowered and fed forward through the material so that binding is unlikely.

Sliding compound miter saws are relatively portable, easy to set up, and robust enough to maintain accuracy even when moved around. Because they cut from above it is not necessary to adjust blade depth for different thicknesses of work piece and, like any bench machine, repeat cuts are very easy. Most saws have an adjustable scale plate for table swiveling, with positive stops at commonly used angles. Also, there are usually adjustable stops at 90 and 45 degrees for tilting the head, allowing easy and very accurate adjustment of the saw.[7]

Table swiveling in both directions is universal but most saws allow head tilting only in one direction (counter-clockwise), although some saws allow head tilting in both directions. Normally the work piece is held flat on the table and so table swiveling will produce a miter cut (blade vertical and angled across work piece), head rotation a bevel cut (blade angled from vertical and square across work piece), and in combination a compound cut.

One of the main disadvantages is relatively poor wood chip and dust extraction, as so much of the blade is exposed when cutting, especially in bevel cuts; consequently there is a tendency for chips to fly about.

Miter saw blades

Miter saws commonly come in 10" and 12" blade size configurations and are commonly made of carbon steel and may come with a coating to make the cut easier.

While the blade sizes are interchangeable with table saws, a miter blade is optimized for short cuts across the grain of the wood with little pull, where as table saws are optimized for long rip cuts with the grain and pulling the material into the blade.

Blades are marked with their number of teeth, kerf and hook angle. Teeth ranges vary from 24 to 100 teeth. The larger number of teeth the finer but slower the cut. The kerf is how much material is removed in making the cut. The standard being a 1/8" kerf with thinner options for working finer wood. The hook angle is how aggressively the blade will pull the material in. A low hook angle or even a negative hook angle is designed to cause little board movement during cutting of unclamped boards.

Teeth design comes in many variations: ATB (alternating top bevel), FTG (flat top grind) and TCG (triple chip grind) are the most common. Each design is optimized for a specific material and edge treatment.

An arbor bolt is the bolt that holds the blade to the miter saw. The diameter of the arbor bolt must match the blade hole size in order to properly secure the blade (12" blades commonly use 1" arbor holes and 10" blades favor 5/8"). Arbor bolts are reverse-threaded, meaning they have to be turned clockwise to be loosened. Many inexperienced users strip their arbor bolt as a result. The arbor bolt is designed so that the rotational spin of the saw blade is exerting a tightening pressure on the blade, to prevent the bolt working loose and the flying blade injuring the operator.

Development

Power miter saws have been available in various forms since the 1970s as specialized cross cut saws but with limited width of cut, especially compared to radial arm saws. Simple miter saws allowed the saw table to pivot allowing miters to be cut in one plane. Compound miter saws also provided saw head tilting allowing compound miters to be cut. Miter saws with abrasive cutting wheels are often used in metal work where they are known as "drop saws" or more commonly "chop saws".

In the late 1980s the sliding compound miter saw was introduced which combined all the best features of the compound miter saw with sliding tubes allowing the cutter head to traverse for a much wider cut. Since then it has become the primary cross cut saw for woodworking, largely supplanting the radial arm saw.

Manufacturers warn of possible electrocution when used near water or other related saws in close proximity.

See also



This article uses material from the Wikipedia article "Miter saw", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing