powered by CADENAS

Social Share

Pliers (6965 views - Tooling)

Pliers are a hand tool used to hold objects firmly, possibly developed from tongs used to handle hot metal in Bronze Age Europe. They are also useful for bending and compressing a wide range of materials. Generally, pliers consist of a pair of metal first-class levers joined at a fulcrum positioned closer to one end of the levers, creating short jaws on one side of the fulcrum, and longer handles on the other side. This arrangement creates a mechanical advantage, allowing the force of the hand's grip to be amplified and focused on an object with precision. The jaws can also be used to manipulate objects too small or unwieldy to be manipulated with the fingers. Pincers are a similar tool with a different type of head used for cutting and pulling, rather than squeezing. Tools designed for safely handling hot objects are usually called tongs. Special tools for making crimp connections in electrical and electronic applications are often called "crimping pliers"; each type of connection uses its own dedicated tool. There are many kinds of pliers made for various general and specific purposes.
Go to Article

Explanation by Hotspot Model

Pliers

Pliers

Pliers

Pliers are a hand tool used to hold objects firmly, possibly developed from tongs used to handle hot metal in Bronze Age Europe.[1] They are also useful for bending and compressing a wide range of materials. Generally, pliers consist of a pair of metal first-class levers joined at a fulcrum positioned closer to one end of the levers, creating short jaws on one side of the fulcrum, and longer handles on the other side.[1] This arrangement creates a mechanical advantage, allowing the force of the hand's grip to be amplified and focused on an object with precision. The jaws can also be used to manipulate objects too small or unwieldy to be manipulated with the fingers.

Pincers are a similar tool with a different type of head used for cutting and pulling, rather than squeezing. Tools designed for safely handling hot objects are usually called tongs. Special tools for making crimp connections in electrical and electronic applications are often called "crimping pliers"; each type of connection uses its own dedicated tool.

There are many kinds of pliers made for various general and specific purposes.

History

As pliers in the general sense are an ancient and simple invention, no single point in history, or inventor, can be credited. Early metal working processes from several millennia BCE would have required plier-like devices to handle hot materials in the process of smithing or casting. Development from wooden to bronze pliers would have probably happened sometime prior to 3000 BCE.[2] Among the oldest illustrations of pliers are those showing the Greek god Hephaestus in his forge.[3] The number of different designs of pliers grew with the invention of the different objects which they were used to handle: horseshoes, fasteners, wire, pipes, electrical, and electronic components.

Design

The basic design of pliers has changed little since their origins, with the pair of handles, the pivot (often formed by a rivet), and the head section with the gripping jaws or cutting edges forming the three elements.

The materials used to make pliers consist mainly of steel alloys with additives such as vanadium or chromium, to improve strength and prevent corrosion. The metal handles of pliers are often fitted with grips of other materials to ensure better handling; grips are usually insulated and additionally protect against electric shock. The jaws vary widely in size, from delicate needle-nose pliers to heavy jaws capable of exerting much pressure, and shape, from basic flat jaws to various specialized and often asymmetrical jaw configurations for specific manipulations. The surfaces are typically textured rather than smooth, to minimize slipping.

A plier-like tool designed for cutting wires is often called diagonal pliers. Some pliers for electrical work are fitted with wire-cutter blades either built into the jaws or on the handles just below the pivot.

Where it is necessary to avoid scratching or damaging the work piece, as for example in jewellery and musical instrument repair, pliers with a layer of softer material such as aluminium, brass, or plastic over the jaws are used.

Ergonomics

Much research has been undertaken to improve the design of pliers, to make them easier to use in often difficult circumstances (such as restricted spaces). The handles can be bent, for example, so that the load applied by the hand is aligned with the arm, rather than at an angle, so reducing muscle fatigue. It is especially important for factory workers who use pliers continuously, and prevents carpal tunnel syndrome.

Gallery

See also



This article uses material from the Wikipedia article "Pliers", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing