Licensed under Creative Commons Attribution-Share Alike 3.0 (I, Sailko).
A medal or medallion is a portable artistic object (objet d'art) belonging to the class known as numismatics, struck like a coin by dies on a durable metal flan or planchet of varying sizes and shapes though frequently found as the more common round piece of metal in bas relief of varying heights that has been sculpted, molded, cast, struck, stamped, or some way marked with an insignia, portrait, or other artistic rendering usually surrounded by a legend, i.e., an inscription. Medals having a rectangular shape, for example, are a special class known as plaquettes. Other irregular and non standard shapes or configurations abound including a wide variety of shapes of badges, crosses, stars, and so forth, sometimes attached to a ribbon or cord.
There are at least seven classes of medals. 1. Awards: A medal may be awarded to a person or organization as a form of recognition for sporting, military, scientific, cultural, academic, or various other achievements. Military awards and decorations are more precise terms for certain types of state decoration. Military decorations are often in shapes such as crosses or stars, but are still loosely called "medals", as in the star-shaped American Medal of Honor. 2. Commemoratives : Medals may also be created for sale to commemorate particular individuals or events, or as works of artistic expression in their own right. 3. Souvenirs: Medals are also made as souvenirs, similar to a commemorative, but more focused on a place or event like a State Fairs, Expositions, Museums, Historic sites, etc., and frequently found for sale within their respective souvenir shops. During the Renaissance, medals were sometimes commissioned for an individual, typically with their portrait, were often used as a form of diplomatic or personal gift, with no sense of being an award for the conduct of the recipient. 4. Religious : There are also devotional medals which may be worn for religious reasons. 5. Portraits : A medal produced to immortalize a person in their portrait sometimes with the caption in Latin Aetate to describe their age at the time of the portrait. 6. Artistic : Medals can be made purely as an art object. 7. Society Medals : Medals are very frequently made for societies used as a badge or token of membership.
An artist who creates medals or medallions is called a "medallist" (UK) or "medalist" (US).
Louis Forrer, Biographical Dictionary of Medallists (Spink & Sons, 1904-1930) is an eight volume reference in English listing medallists through history. Ulrich Thieme, Felix Becker, Allgemeines Lexicon der Bildenden Kùnstler von der Antike bis zur Gegenwart (Leipzig : 1907-1949) is a thirty six volume work in German that lists all artists without differentiating their specialty and medium like the Forrer work.
Medals have long been popular collectible items in the hobby called numismatics in a special class called either exonumia or militaria also known as Decorations.
In the proper use of the term, medallions are larger, starting at perhaps four inches across, and are, as such, usually too large to be worn very comfortably, though in colloquial use, "medallion" is often used to refer to a medal used as the pendant of a necklace (as in the medallion man fashion style of the 1960s and 1970s), or for other types of medals. Medallions may also be called "table medals" because they are too large to be worn and can only be displayed on a wall, table top, desk, or cabinet.
First attested in English in 1578, the word medal is derived from the Middle French médaille, itself from Italian medaglia, and ultimately from the post-classical Latin medalia, meaning a coin worth half a denarius. The word medallion (first attested in English in 1658) has the same ultimate derivation, but this time through the Italian medaglione, meaning "large medal". There are two theories as for the etymology of the word medalia: the first being that the Latin medalia itself is derived from the adjective medialis meaning "medial" or "middle";[1] the second being that medaglia comes from the Vulgar Latin metallea (moneta), meaning "metal (coin)" and that from Latin metallum,[2] which is the latinisation of the Greek μέταλλον (metallon), "a mine".[3][4][5][6]
The main or front surface of a medal is termed the obverse, and may contain a portrait, pictorial scene, or other image along with an inscription. The reverse, or back surface of the medal, is not always used and may be left blank or may contain a secondary design. It is not uncommon to find only an artistic rendering on the obverse, while all details and other information for the medal are inscribed on the reverse. The rim is found only occasionally employed to display an inscription such as a motto, privy mark, engraver symbol, assayer’s marking, or a series number.
Medals that are intended to be hung from a ribbon also include a small suspension piece at the crest with which to loop a suspension ring through. It is through the ring that a ribbon is run or folded so the medal may hang pendent. Medals pinned to the breast use only a small cut of ribbon that is attached to a top bar where the brooch pin is affixed. Top bars may be hidden under the ribbon so they are not visible, be a plain device from which the ribbon attaches, or may even be decorative to complement the design on the medal. Some top bars are elaborate and contain a whole design unto themselves.
Bronze has been the most common material employed for medals, due to its fair price range, durability, ease with which to work when casting, and the ample availability However, a wide range of other media have also been used. Rarer metals have been employed, such as silver, platinum, and gold, when wishing to add value beyond the mere artistic depiction, as well as base metals and alloys such as copper, brass, iron, aluminum, lead, zinc, nickel, and pewter. Medals that are made with inexpensive material might be gilded, silver-plated, chased, or finished in a variety of other ways to improve their appearance. Medals have also been made of rock, gemstone, ivory, glass, porcelain, terra cotta, coal, wood, paper, enamel, lacquerware, and plastics.
The first known instance of a medal being awarded comes from the historian Josephus who, writing long after the event, accounts that in the fourth century BCE, the High Priest Jonathan led the Hebrews in aid of Alexander the Great, and that in return for this, Alexander "...sent to Jonathan... honorary awards, as a golden button, which it is custom to give the king's kinsmen." Roman emperors used both military awards of medals, and political gifts of medallions that were like very large coins, usually in gold or silver, and die-struck like coins.[7] Both these and actual golden coins were often set as pieces of jewellery, worn by both sexes.
The bracteate is a type of thin gold medal, usually plain on the reverse, found in Northern Europe from the so-called "Dark Ages" or Migration Period. They often have suspension loops and were clearly intended to be worn on a chain as jewellery. They imitate, at a distance, Roman imperial coins and medallions, but have the heads of gods, animals, or other designs.[8] The Liudhard medalet, produced around AD 600 in Anglo-Saxon England, is an isolated example, known from a single copy, of a Christian medal, featuring an inscription naming Liudhard (or "Saint Letard"), the first priest among the Anglo-Saxons, and most likely presented to converts. The surviving example is mounted for wearing as jewellery.
In Europe, from the late Middle Ages on, it became common for sovereigns, nobles, and later, intellectuals to commission medals to be given simply as gifts to their political allies to either maintain or gain support of an influential person. The medals made be made in a range of metals, such as gold, silver-gilt, silver, bronze, and lead, depending on the status of the recipient. They were typically up to about three inches across, and usually featured the head of the donor on the obverse, surrounded by an inscription with their name and title, and their emblem on the reverse, with a learned motto inscribed round the edges. Such medals were not usually intended to be worn, although they might have been set as pendants on a chain. From the 16th century onward, medals were made, both by rulers for presentation and private enterprise for sale, to commemorate specific events, including military battles and victories, and from this grew the practice of awarding military medals specifically to combatants, though initially only a few of the much higher-ranking officers.
The medieval revival seems to have begun around 1400 with the extravagant French prince Jean, Duc de Berry, who commissioned a number of large classicising medals that were probably produced in very small numbers, or a unique cast. Only casts in bronze from the originals in precious metal survive, although it is known that at least some medals were also set with jewels, and these may well have been worn on a chain.[9] At the same period, the first known post-classical medal commemorating a victory was struck for Francesco Carrara (Novello) on the occasion of the capture of Padua in 1390. The Italian artist Pisanello, generally agreed to be the finest medallist of the Renaissance, began in 1438 with a medal, celebrating the unprecedented visit of the Byzantine Emperor John VIII Palaiologos to Italy. This was presumably a commercial venture, but his later medals were mostly commissioned for distribution as gifts by rulers or nobles. Like almost all early Renaissance medals, it was cast rather than die-struck. With each successive cast the medal became slightly smaller, and the numbers that could be produced were probably not large. A lead "proof" was probably often used. The association between medals and the classical revival began to take a rather different form, and the exchange of medals became associated with Renaissance Humanism. Princes would send humanist writers and scholars medals in recognition of their work, and the humanists began to make their own medals, normally in bronze, to send to their patrons and peers.[10] The fashion remained restricted to Italy until near the end of the 15th century, when it spread to other countries. By the 16th century, medals were increasingly produced by rulers or cities for propaganda purposes.[11] In 1550, a die-stamping machine, using steel dies, was introduced in Augsburg, Germany, and soon this process became standard. The artist now cut an intaglio die rather than modelling in relief.[12]
By the 16th century, the wearing of smaller medals on a chain was a persistent fashion for both sexes, and a variety of medals were produced commercially for the purpose, commemorating persons or events, or just with non-specific suitable sentiments. German artists had been producing high-quality medals from the beginning of the century, while the French and British were slower to produce fine work. However, by the late 17th century, most parts of Western Europe could produce fine work. Some medals were also collected, which continues to the present day. Official medals, from which specialized military awards descended, were increasingly produced, but the real growth in military medals did not come until the 19th century. Devotional medals also became very popular in Catholic countries. During the Reformation there had also been a vigorous tradition of Protestant medals, more polemical than devotional, which continued with the Geuzen medals produced in the Dutch Revolt.
Military decorations, service awards, and medals are often mistakenly confused with one another. Decoration is a term for awards which require specific acts of heroism or achievement (such as the British Victoria Cross or American Silver Star), whereas a service award or campaign medal is awarded for serving in a particular capacity in a particular geographical area and time frame (such as the Iraq Campaign Medal). In either case, an award or decoration may be presented as a medal.
The Roman Republic adopted an elaborate system of military awards that included medals called phalerae to be issued to soldiers and units for a variety of achievements. The practice was revived in the Early Modern period, and medals began to be worn on the chest as part of standard military uniform. The United States Continental Congress awarded the Fidelity Medallion as early as 1780, to three specified men for a particular incident, as a one-off award, which was characteristic of early military decorations. In 1782, the Badge of Military Merit was established, and mostly awarded to non-officers. The Légion d'honneur instituted by Napoleon I in 1802 had some of the characteristics of the old military orders, but was intended to be far more inclusive, and was awarded to rank and file soldiers for bravery or exceptional service. Other nations followed with decorations such as the British Army Gold Medal from 1810, though this only went to senior officers, and the Prussian Iron Cross from 1813. Medals were not awarded to all combatants in a war or battle until the 19th century, when the Waterloo Medal was the first British medal given to all present, at the Battle of Waterloo and all associated actions in 1815. By the middle of the 19th century, the number of awards used had greatly expanded in most countries to something near modern levels.
An order tends to be the most elaborate of military decorations, typically awarded for distinguished services to a nation or to the general betterment of humanity. Orders are distinguished from other forms of decoration in that they often imply membership in an organization or association of others that have received the same award. Two of the most well known and commonly awarded orders are the Légion d'honneur of France (military and civil) and the civil Order of the British Empire. The practice of conferring orders originates with the mediaeval fraternities of knighthood, some of which still exist and are still awarded. While most modern orders have no roots in knighthood, they still tend to carry over the terms of their historic counterparts, and terms such as knight, commander, officer, members, and so on are still commonly found as ranks. A military order may use a medal as its insignia, however, most tend to have a unique badge or a type of plaque specifically designed for an emblem.
The Medal of Honor is the highest military decoration awarded by the United States Government, and is an example of a decoration that is modeled as a military order, even though not expressly defining itself as one. It is bestowed on a member of the United States Armed Forces who distinguishes himself, "conspicuously by gallantry and intrepidity at the risk of his life above and beyond the call of duty while engaged in an action against an enemy of the United States."[13] Each of the three departments of the American armed forces has a unique picture displayed on a medal, which is in turn displayed upon a star-shaped heraldic badge. The medal of the U.S. Army depicts the head of Minerva, the U.S. Navy medal shows a scene of Minerva doing battle with Discord, and the U.S. Air Force depicts the Statue of Liberty upon its medal.
Military decorations, including medals and orders, are usually presented to the recipient in a formal ceremony. Medals are normally worn on more formal occasions and are suspended from a ribbon of the medal's colours on the left breast, while a corresponding ribbon bar is to be worn to common events where medals would be inappropriate or impractical to wear.
Medallion is a vague term, often used for larger, usually circular, medals worn as pendants round the neck. It is the correct term for such medals from the late Roman Empire, typically distributed by the emperor and bearing his image, but in later periods larger medals are still best termed just as medals.
Generally circular, table medals are issued for artistic, commemoration, or souvenir purposes, not for commerce, and are too large to be plausibly worn. Tokens and Table Medals of coin-like appearance are part of the Exonumia subcategory of Numismatics, while Orders, Decorations, and Medals are considered Militaria (military related). In the U.S. Military, modern medals are often referred to as challenge coins.
The Nobel Foundation, the organization awarding the prestigious Nobel Prize, presents each winner, "an assignment for the amount of the prize, a diploma, and a gold medal..." This example of a medal would be displayed on a table or in a cabinet, rather than be worn by the winner.
The Carnegie Hero Foundation is the issuer of a bravery medal, most commonly issued in the US, Canada, and the UK. This large bronze table medal features Andrew Carnegie's likeness on the obverse and the name of the awardee and citation engraved on the reverse. It is usually issued for lifesaving incidents.
Also related are plaques and plaquettes, which may be commemorative, but especially in the Renaissance and Mannerist periods were often made for purely decorative purposes, with often crowded scenes from religious, historical or mythological sources. While usually metal, table medals have been issued in wood, plastic, fibre, and other compositions. The US Government awards gold medals on important occasions, with bronze copies available for public sale.
Amongst the many fraternal organisations which wear ceremonial regalia, the use of medals is commonplace. In many prominent fraternal organisations, fraternal medals are known as jewels. Their purpose varies, and may include use as a badge of membership, an indication of rank, a symbol of office within the fraternity, or an indication of support having been given to a designated charitable cause (so-called charity jewels). Common secular fraternities using jewels (medals) in the English-speaking world include Freemasonry, the Orange Order, the Royal Antediluvian Order of Buffaloes, and the Oddfellows. There are also religious fraternal organisations attached to certain Christian denominations (for example, the Catenian Association), also using medals as jewels of their Orders. Many of these organisations advertise jewels (medals) for sale on their corporate websites.[14]
Fraternal jewels may be worn as military-style medals, on ribbons, from the left breast, or more prominently on collars or collarettes as part of the organisation's regalia. Historic examples of such medals and jewels may be found in many museums, particularly museums dedicated to fraternal organisations.[15]
There is extensive trade in fraternal jewels and medals, with societies and associations existing to promote such trade, and to encourage the sharing of resources,[16] and on-line resources available to support the hobby.[17]
Traditionally, medals are made of the following metals, in order of decreasing value[citation needed]:
Many medals were and are made in several different metals, either representing awards for different places in a competition, or standards or classes, as with the Olympic medals, or simply different price levels for medals made for sale or donation by the commissioner. Medals have historically been given as prizes in various types of competitive activities, especially athletics. The gold, silver and bronze Olympic medals for first, second and third places were first used at the 1904 Summer Olympics. At the 1896 event, silver was awarded to winners and bronze to runners-up, while at 1900 other prizes were given, not medals. The medals for the London 2012 Summer Olympics are the largest ever, reflecting a trend for increasing size in Olympic medals.
The first well-known great artist to create medals was the Italian painter Antonio Pisano, also known as Pisanello, who modelled and cast a number of portrait medals of princes and scholars in the 1440s. Many other artists followed his example, in places such as Italy, the Low Countries, Germany, and France. In the seventeenth century medals were extensively used to commemorate events and glorify rulers. In the eighteenth century prize medals became common. In the 19th century art medals exploded in popularity. In the early part of the aforementioned century, David d'Angers produced a great series of portrait medals of famous contemporaries and in the latter part of the century, Jules-Clément Chaplain and Louis-Oscar Roty were among many highly regarded medalists. The early twentieth century saw art medals flourish, particularly in France, Italy, and Belgium, while later in the century Czechoslovakia, Hungary, Poland, the USA, Canada, and England produced much high quality work. One such artist is the portrait medalist Christian Cardell Corbet. The Sanford Saltus medal is the most prestigious award for art medals in the USA.[citation needed]
1896 Colonial Exposition medal, by Louis-Oscar Roty. |
1900 Exposition Universelle medal, by Jules-Clément Chaplain. |
This article uses material from the Wikipedia article "Medal", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D, jewellery,jewelry