This article has multiple issues. Please help improve it or discuss these issues on the talk page. (Learn how and when to remove these template messages)
(Learn how and when to remove this template message)
|
A concrete mixer (often mistakenly called a cement mixer) is a device that homogeneously combines cement, aggregate such as sand or gravel, and water to form concrete. A typical concrete mixer uses a revolving drum to mix the components. For smaller volume works portable concrete mixers are often used so that the concrete can be made at the construction site, giving the workers ample time to use the concrete before it hardens. An alternative to a machine is mixing concrete by hand. This is usually done in a wheelbarrow; however, several companies have recently begun to sell modified tarps for this purpose.
The concrete mixer was invented by Columbus, Ohio industrialist Gebhardt Jaeger.[1]
Today's market increasingly requires consistent homogeneity and short mixing times for the industrial production of ready-mix concrete, and more so for precast/prestressed concrete. This has resulted in refinement of mixing technologies for concrete production. Different styles of stationary mixers have been developed, each with its own inherent strengths targeting different parts of the concrete production market. The most common mixers used today fall into 3 categories:
All the mixer styles have their own inherent strengths and weaknesses, and all three styles of mixers are used throughout the world to varying degrees of popularity.
Special concrete transport trucks (in–transit mixers) are made to transport and mix concrete up to the construction site. They can be charged with dry materials and water, with the mixing occurring during transport. They can also be loaded from a "central mix" plant, with this process the material has already been mixed prior to loading. The concrete mixing transport truck maintains the material's liquid state through agitation, or turning of the drum, until delivery. The interior of the drum on a concrete mixing truck is fitted with a spiral blade. In one rotational direction, the concrete is pushed deeper into the drum. This is the direction the drum is rotated while the concrete is being transported to the building site. This is known as "charging" the mixer. When the drum rotates in the other direction, the Archimedes' screw-type arrangement "discharges", or forces the concrete out of the drum. From there it may go onto chutes to guide the viscous concrete directly to the job site. If the truck cannot get close enough to the site to use the chutes, the concrete may be discharged into a concrete pump, connected to a flexible hose, or onto a conveyor belt which can be extended some distance (typically ten or more metres). A pump provides the means to move the material to precise locations, multi-floor buildings, and other distance prohibitive locations. Buckets suspended from cranes are also used to place the concrete. The drum is traditionally made of steel but on some newer trucks as a weight reduction measure, fibreglass has been used.
"Rear discharge" trucks require both a driver and a "chuteman" to guide the truck and chute back and forth to place concrete in the manner suitable to the contractor. Newer "front discharge" trucks have controls inside the cab of the truck to allow the driver to move the chute in all directions. The first front discharge mixer was designed and built by Royal W. Sims of Holladay, Utah, United States.
Concrete mixers are equipped with anywhere from two axles and up. Four, five and six axle trucks are the most common[citation needed] with the number being determined by the load and local legislation governing allowable loads on the road. These are necessary to distribute the load evenly and allow operation on weight restricted roads and to reduce wear and tear on normal roads. A two or three axle truck during the winter when road weight limits are reduced has no usable payload in many jurisdictions. Other areas may require expensive permits to operate. Additional axles other than those used for steering ("steers") or drivetrain ("drives") may be installed between the steers and drives or behind the drives. Mixers commonly will have multiple steering axles as well, which generally result in very large turning radii. To facilitate maneuvering the additional axles may be "lift axles" which allows them to be raised off the ground so that they do not scrub (get dragged sideways across the ground) on tight turns, or increase the vehicle's turning radius. Axles installed behind the drives are known as "tag axles" or "booster axles", and are often equipped to turn opposite to the steering axle to reduce scrubbing and automatically lift when the truck is put into a reverse gear.
Tractor trailer combination mixers where the mixer is installed on a trailer instead of a truck chassis are used in some jurisdictions, such as the province of Quebec where even 6 axle trucks would have trouble carrying a useful load.
Concrete mixers generally do not travel far from their plant, as the concrete begins to set as soon as it is in the truck. Many contractors require that the concrete be in place within 90 minutes after loading. If the truck breaks down or for some other reason the concrete hardens in the truck, workers may need to enter the barrel with jackhammers.[3]
Stephen Stepanian filed a patent application for the first truck mixer in 1916.[4] Trucks weigh 20,000 to 30,000 pounds (9,070 to 13,600 kg), and can carry roughly 40,000 pounds (18,100 kg) of concrete although many varying sizes of Mixer Truck are currently in use. The most common truck capacity is 8 cubic yards (6.1 m3).
Most concrete mixers in the UK are limited to a speed of 56 miles per hour (90 km/h).
A variant of standard concrete transportation is the concrete or cement mixing trailer. These small versions of a transit-mix truck are used to supply short loads of concrete. These cart-away style trailers have a concrete mixing drum with a capacity of between 1 and 1.75 cubic yards (0.76 and 1.34 m3). Cart-aways are usually pulled behind a pick-up truck and batched from smaller batching systems. The mixing trailer system is popular with rental yards and building material locations, who use them to supply ready-mix to their regular customer base.
Metered concrete trucks or volumetric mobile mixers are trucks that contain concrete ingredient materials and water to be mixed on the truck at the job site to make and deliver concrete according to the amount needed.[5]
For smaller jobs, such as residential repairs, renovations, or hobbyist-scale projects, many cubic yards of concrete are usually not required. Bagged cement is readily available in small-batch sizes, and aggregate and water are easily obtained in small quantities for the small work site. To service this small-batch concrete market, there are many types of small portable concrete mixers available
A typical portable concrete mixer uses a small revolving drum to mix the components. For smaller jobs the concrete made at the construction site has no time lost in transport, giving the workers ample time to use the concrete before it hardens.
Portable concrete mixers may be powered by a gasoline engine, although it is more common that they are powered by electric motors using standard mains current.
These concrete mixers are further divided based on their loading mechanism. Cement, sand and other aggregates are loaded in a hydraulically operated hopper and then poured in the mixing drum for final mixing and then can be unloaded by tilting the drum. While in Hand Feed Concrete Mixers, cement, sand and other aggregates are directly added to the mixing drum manually. These both type of concrete mixers are highly popular and used in regular construction activities in Africa, some Middle Eastern Countries and in the Indian subcontinent.
Amran Self Loading Concrete Mixers are unique machines designed to batch, mix and transport concrete. These mixers consist of a rotating drum mounted on an operator-driven cab-mounted chassis frame fitted with a loading bucket.
The operator of the Self Loading Concrete Mixer batches and introduces the ingredients required for mixing concrete viz., cement, stone aggregates etc., into the drum using the loading bucket. The drum is usually of reversible type, tilt type or a combination of both. A predetermined volume of water is discharged to the drum via a water dispensing unit. The mixture is rotated at mixing speeds within the drum until concrete discharge via a fitted chute.Self-loading concrete mixers are suited for construction sites where Concrete batching plants are unavailable, underfoot conditions are not suited for Concrete transit mixer trucks or labor availability is scarce or constrained. Applications include urban and rural construction, concrete pavement maintenance, bridge and tunnel construction, township-level highways construction, foundation construction, national defense facilities, construction of high-speed railway etc.
Operating concrete mixers correctly is one of the biggest safety issues in construction zones. Data shows that workers whose tasks are related to concrete processing number more than 250,000 currently and over 10 percent of those workers, 28,000, experienced a job-related injury or illness and 42 died in just one year.[6][7][8]
This article uses material from the Wikipedia article "Concrete mixer", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD