Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
A downhill bike (also known as a downhill mountain bike) is a full suspension bicycle designed for downhill cycling on particularly steep, rocky trails. Unlike a typical mountain bike, durability and stability are the most important design features, compared to lighter, more versatile cross-country bikes. Downhill bikes are primarily intended for high speed descent, and downhill riders will usually push, or shuttle via chairlifts or motorized vehicles, to the trailhead.[1] Downhill bikes share similarities with freeride bikes due to their large strong frames and increased travel.[1]
These bikes will also have very slack head tube angles (66 degrees or less),[2] long wheelbases (over 45 inches or 1,143 mm),[2] and will accommodate the use of up to 3-inch (76.2 mm) width knobbed tires. Downhill frames are also overbuilt to handle the stress of riding over rocky terrain, drops, and jumps. Bike weights have been typically over 34 lb (15.4 kg), but modern downhill bikes have broken the 30 lb (13.6 kg) weight barrier (with some custom builds on carbon frames weighing between 27-29 pounds) Some newer (2014/5) downhill bikes can be built to weigh under 30 lb (13.6 kg), such as the Trek Session 9.9 or Kona Supreme Operator.
Adjustable head tube angles are also available to adapt the bike to the owner's preferred style of riding.[3]
Will typically have 7–10 inches (178–254 mm) of rear suspension travel, and be designed around a 7–8-inch (178–203 mm) suspension fork.[2] The suspension sag is also much higher than cross-country bikes (25%-50% of total travel vs. 10%-20%) for a more supple ride at higher speeds.
Other innovations include the use of OnePointFive head tube standard, which uses a 1.5 in (38 mm) wide steerer tube, instead of the more conventional 1.125 in (29 mm) diameter, for added stiffness and strength.[4] Most downhill bikes use dual crown forks which allow longer travel at the front(usually 203 mm or 8 in and increased stiffness that a single crown fork cannot offer. Drawbacks though, are increased weight and reduced turning circle.
Downhill bikes usually have hydraulic disc brakes, and the discs may be 200 mm or larger.[5]
Downhill bikes usually have a chain guide to prevent accidental chain deraillment. Some manufacturers are experimenting with internal gearboxes for improved reliability.
Downhill bikes have very thick and big tires in order not to lose traction in bad terrain, often they are 650b
Downhill bikes are typically made of aluminum alloys or carbon fiber.
This article uses material from the Wikipedia article "Downhill bike", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht