Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article does not cite any sources. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (September 2008) (Learn how and when to remove this template message) |
A papasan chair (also called a bowl chair or moon chair) is a large rounded bowl-shaped chair with an adjustable angle similar to that of a futon. The bowl rests in an upright frame traditionally made of rattan, but also sometimes made of sturdy wicker or wood. The papasan chair gained popularity when American World War II servicemembers brought them home from Asia, where they had been used in the Philippines and Japan for centuries.[1]
The cushion of the chair is typically thick velveteen material filled with cotton fluff. In traditional papasans, the cushion can be removed and used outside of the sturdy frame, although it is hand-wash only.
The mamasan chair is a double-seating version, and was introduced to the western world in the 1950s. Prior to that it was in use in far eastern Asia, particularly in Indonesia, Thailand and Japan. It can also be called as double papasan chair which is widely used.
Papasan chairs are typically 35–60 inches wide and 35 inches deep.
|title=
(help)
This article about furniture or furnishing is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "Papasan chair", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, BIM Object, BIM component, BIM library, BIM family, BIM catalog, GIS, Advanced Steel, AutoCAD MEP, linear, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, BIM family creation, 3D, Download, MEP BIM product library