powered by CADENAS

Social Share

Notebook (10893 views - Basics)

A notebook (notepad, writing pad, drawing pad, legal pad) is a small book or binder of paper pages, often ruled, used for purposes such as recording notes or memoranda, writing, drawing or scrapbooking.
Go to Article

Explanation by Hotspot Model

Notebook

Notebook

Notebook

Licensed under Creative Commons Attribution 2.0 (L.Marie).

A notebook (notepad, writing pad, drawing pad, legal pad) is a small book or binder of paper pages, often ruled, used for purposes such as recording notes or memoranda, writing, drawing or scrapbooking.[1][2][3][4]

Legal pad

According to a legend, Thomas W. Holley of Holyoke, Massachusetts, invented the legal pad around the year 1888 when he innovated the idea to collect all the sortings, various sort of substandard paper scraps from various factories, and stitch them together in order to sell them as pads at an affordable and fair price. In about 1900, the latter then evolved into the modern legal pad when a local judge requested for a margin to be drawn on the left side of the paper. This was the first legal pad.[5]

In 1902, J.A. Birchall of Birchalls, a Launceston, Tasmania-based stationery shop, decided that the cumbersome method of selling writing paper in folded stacks of "quires" (four sheets of paper or parchment folded to form eight leaves) was inefficient. As a solution, he glued together a stack of halved sheets of paper, supported by a sheet of cardboard, creating what he called the "Silver City Writing Tablet".[6][7]

The only technical requirement for this type of stationery to be considered a true "legal pad" is that it must have margins of 1.25 inches (3.17 centimeters) from the left edge of legal pad. Here, the margin, also known as down lines,[8] is room used to write notes or comments. Legal pads usually have a gum binding at the top as opposed to a spiral or stitched binding.

Binding and cover

Principal types of binding are padding, perfect, spiral, comb, sewn, clasp, disc, and pressure, some of which can be combined. Binding methods can affect whether a notebook can lie flat when open and whether the pages are likely to remain attached. The cover material is usually distinct from the writing surface material, more durable, more decorative, and more firmly attached. It also is stiffer than the pages, even taken together. Cover materials should not contribute to damage or discomfort.

It is frequently cheaper to purchase notebooks that are spiral-bound, meaning that a spiral of wire is looped through large perforations at the top or side of the page. Other bound notebooks are available that use glue to hold the pages together; this process is "padding".[9] Today, it is common for pages in such notebooks to include a thin line of perforations that make it easier to tear out the page. Spiral-bound pages can be torn out, but frequently leave thin scraggly strips from the small amount of paper that is within the spiral, as well as an uneven rip along the top of the torn-out page. Hard-bound notebooks include a sewn spine, and the pages are not easily removed. Some styles of sewn bindings allow pages to open flat, while others cause the pages to drape.

Variations of notebooks that allow pages to be added, removed, and replaced are bound by rings, rods, or discs. In each of these systems, the pages are modified with perforations that facilitate the specific binding mechanism's ability to secure them. Ring-bound and rod-bound notebooks secure their contents by threading perforated pages around straight or curved prongs. In the open position, the pages can be removed and rearranged. In the closed position, the pages are kept in order. Disc-bound notebooks remove the open or closed operation by modifying the pages themselves. A page perforated for a disc-bound binding system contains a row of teeth along the side edge of the page that grip onto the outside raised perimeter of individual discs.

Preprinting

Notebooks used for drawing and scrapbooking are usually blank. Notebooks for writing usually have some kind of printing on the writing material, if only lines to align writing or facilitate certain kinds of drawing. Inventor's notebooks have page numbers preprinted to support priority claims. They may be considered as grey literature. Many notebooks have graphic decorations. Personal organizers can have various kinds of preprinted pages.

Uses

Artists often use large notebooks, which include wide spaces of blank paper appropriate for drawing. Lawyers use rather large notebooks known as legal pads that contain lined paper (often yellow) and are appropriate for use on tables and desks. These horizontal lines or "rules" are sometimes classified according to their space apart with "wide rule" the farthest, "college rule" closer, "legal rule" slightly closer and "narrow rule" closest, allowing more lines of text per page. When sewn into a pasteboard backing, these may be called composition books, or in smaller signatures may be called "blue books" or exam books and used for essay exams.

In contrast, journalists prefer small, hand-held notebooks for portability (reporters' notebooks), and sometimes use shorthand when taking notes. Scientists and other researchers use lab notebooks to document their experiments. The pages in lab notebooks are sometimes graph paper to plot data. Police officers are required to write notes on what they observe, using a police notebook. Land surveyors commonly record field notes in durable, hard-bound notebooks called "field books."

Coloring enthusiasts use coloring notebooks for stress relief. The pages in coloring notebooks contain different adult coloring pages.[10] Students take notes in notebooks, and studies suggest that the act of writing (as opposed to typing) improves learning.[11]

Notebook pages can be recycled via standard paper recycling. Recycled notebooks are available, differing in recycled percentage and paper quality.

Electronic successors

Since the late 20th century, many attempts have been made to integrate the simplicity of a notebook with the editing, searching, and communication capacities of computers through the development of note taking software. Laptop computers began to be called notebooks when they reached a small size in the 1990s, but they did not have any special note-taking ability. Personal digital assistants (PDAs) came next, integrating small liquid crystal displays with a touch-sensitive layer to input graphics and written text. Tablet PCs are larger and provide more writing and navigation space.

Digital paper combines the simplicity of a traditional pen and notebook with digital storage and interactivity. By printing an invisible dot pattern on the notebook paper and using a pen with a built in infrared camera the written text can be transferred to a laptop, mobile phone or backoffice for storage and processing.

See also



This article uses material from the Wikipedia article "Notebook", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Basics

3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted