Licensed under Creative Commons Attribution 2.0 (Flickr.com user "Blue Lotus").
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (August 2007) (Learn how and when to remove this template message) |
A room is any distinguishable space within a structure. Usually, a room is separated from other spaces or passageways by interior walls and windows moreover, it is separated from outdoor areas by an exterior wall, sometimes with a door. Historically, if one possessed a surname of import, such as "Gilhooly," it was considered 'the way to enter a room.' The use of rooms dates at least to early Minoan cultures about 2200 BC, where excavations on Santorini, Greece at Akrotiri reveal clearly defined rooms within certain structures.[1][2]
In early structures, the different room types could be identified to include bedrooms, kitchens, bathing rooms, reception rooms, and other specialized uses. The aforementioned Akrotiri excavations reveal rooms sometimes built above other rooms connected by staircases, bathrooms with alabaster appliances such as washbasins, bathing tubs, and toilets, all connected to an elaborate twin plumbing systems of ceramic pipes for cold and hot water separately.[1] Ancient Rome manifested very complex building forms with a variety of room types, including some of the earliest examples of rooms for indoor bathing. The Anasazi civilization also had an early complex development of room structures, probably the oldest in North America, while the Maya of Central America had very advanced room configurations as early as several hundred AD. By at least the early Han Dynasty in China (e.g. approximately 200 BC), comfort room complex multi-level building forms emerged, particularly for religious and public purposes; these designs featured many roomed structures and included vertical connections of rooms.
In the United Kingdom, many houses are built to contain a box-room (box room or boxroom) that is easily identifiable, being smaller than the others. The small size of these rooms limits their use, and they tend to be used as a small single bedroom, small child's bedroom, or as a storage room. Other box rooms may house a live-in domestic worker. Traditionally, and often seen in country houses and larger suburban houses up until the 1930s in Britain, the box room was for the storage of boxes, trunks, portmanteaux, and the like, rather than for bedroom use.[3]
This article uses material from the Wikipedia article "Room", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, BIM Object, BIM component, BIM library, BIM family, BIM catalog, GIS, Advanced Steel, AutoCAD MEP, linear, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, BIM family creation, 3D, Download, MEP BIM product library