powered by CADENAS

Social Share

Ford Mustang (18519 views - Cars & Motorbikes & Trucks)

The Ford Mustang is an American car manufactured by Ford. It was originally based on the platform of the second generation North American Ford Falcon, a compact car. The original 1962 Ford Mustang I two-seater concept car had evolved into the 1963 Mustang II four-seater concept car which Ford used to pretest how the public would take interest in the first production Mustang. The 1963 Mustang II concept car was designed with a variation of the production model's front and rear ends with a roof that was 2.7 inches shorter. Introduced early on April 17, 1964 (16 days after the Plymouth Barracuda), and thus dubbed as a "1964½" by Mustang fans, the 1965 Mustang was the automaker's most successful launch since the Model A. The Mustang has undergone several transformations to its current sixth generation. The Mustang created the "pony car" class of American muscle cars, affordable sporty coupes with long hoods and short rear decks, and gave rise to competitors such as the Chevrolet Camaro, Pontiac Firebird, AMC Javelin, Chrysler's revamped Plymouth Barracuda, and the second generation Dodge Challenger. The Mustang is also credited for inspiring the designs of coupés such as the Toyota Celica and Ford Capri, which were imported to the United States.
Go to Article

Explanation by Hotspot Model

Ford Mustang

Ford Mustang

Ford Mustang
2018 Ford Mustang facelift
Overview
Manufacturer Ford
Production March 1964 – present
Model years 1965–present
Designer John Najjar
Philip T. Clark
Joe Oros
Body and chassis
Class Pony car
Muscle car
Body style
Layout FR layout

The Ford Mustang is an American car manufactured by Ford. It was originally based on the platform of the second generation North American Ford Falcon, a compact car.[1] The original 1962 Ford Mustang I two-seater concept car had evolved into the 1963 Mustang II four-seater concept car which Ford used to pretest how the public would take interest in the first production Mustang. The 1963 Mustang II concept car was designed with a variation of the production model's front and rear ends with a roof that was 2.7 inches shorter.[2] Introduced early on April 17, 1964[3] (16 days after the Plymouth Barracuda), and thus dubbed as a "1964½" by Mustang fans, the 1965 Mustang was the automaker's most successful launch since the Model A.[4] The Mustang has undergone several transformations to its current sixth generation.

The Mustang created the "pony car" class of American muscle cars, affordable sporty coupes with long hoods and short rear decks[5], and gave rise to competitors such as the Chevrolet Camaro,[6] Pontiac Firebird, AMC Javelin,[7] Chrysler's revamped Plymouth Barracuda, and the second generation Dodge Challenger.[8] The Mustang is also credited for inspiring the designs of coupés such as the Toyota Celica and Ford Capri, which were imported to the United States.

Background

The Ford Mustang was brought out five months before the normal start of the 1965 production year. The early production versions are often referred to as "1964½ models" but all Mustangs were advertised, VIN coded and titled by Ford as 1965 models, though minor design updates for fall 1965 contribute to tracking 1964½ production data separately from 1965 data (see data below).[9] with production beginning in Dearborn, Michigan on March 9, 1964;[10] the new car was introduced to the public on April 17, 1964[11] at the New York World's Fair.[12]

Executive stylist John Najjar, who was a fan of the World War II P-51 Mustang fighter plane, is credited by Ford to have suggested the name.[13][14] Najjar co-designed the first prototype of the Ford Mustang known as Ford Mustang I in 1961, working jointly with fellow Ford stylist Philip T. Clark.[15] The Mustang I made its formal debut at the United States Grand Prix in Watkins Glen, New York on October 7, 1962, where test driver and contemporary Formula One race driver Dan Gurney lapped the track in a demonstration using the second "race" prototype. His lap times were only slightly off the pace of the F1 race cars.

An alternative view was that Robert J. Eggert, Ford Division market research manager, first suggested the Mustang name. Eggert, a breeder of quarterhorses, received a birthday present from his wife of the book, The Mustangs by J. Frank Dobie in 1960. Later, the book's title gave him the idea of adding the "Mustang" name for Ford's new concept car. The designer preferred Cougar (early styling bucks can be seen wearing a Cougar grille emblem) or Torino (an advertising campaign using the Torino name was actually prepared), while Henry Ford II wanted T-bird II.[16] As the person responsible for Ford's research on potential names, Eggert added "Mustang" to the list to be tested by focus groups; "Mustang," by a wide margin, came out on top under the heading: "Suitability as Name for the Special Car."[17][18] The name could not be used in Germany,[16] however, because it was owned by Krupp, which had manufactured trucks between 1951 and 1964 with the name Mustang. Ford refused to buy the name for about US$10,000 from Krupp at the time. Kreidler, a manufacturer of mopeds, also used the name, so Mustang was sold in Germany as the "T-5" until December 1978.

Mustangs grew larger and heavier with each model year until, in response to the 1971–1973 models, Ford returned the car to its original size and concept for 1974. It has since seen several platform generations and designs. Although some other pony cars have seen a revival, the Mustang is the only original model to remain in uninterrupted production over five decades of development and revision.[19]

First generation (1965–1973)

Lee Iacocca's assistant general manager and chief engineer, Donald N. Frey was the head engineer for the T-5 project—supervising the overall development of the car in a record 18 months[21]—while Iacocca himself championed the project as Ford Division general manager. The T-5 prototype was a two-seat, mid-mounted engine roadster. This vehicle employed the German Ford Taunus V4 engine.

It was claimed that the decision to abandon the two-seat design was in part due to the increase in sales the Thunderbird had seen when enlarged from a two-seater to a 2+2 in 1958.[citation needed] Thus, a four-seat car with full space for the front bucket seats, as originally planned, and a rear bench seat with significantly less space than was common at the time, were standard. A "Fastback 2+2", first manufactured on August 17, 1964, enclosed the trunk space under a sweeping exterior line similar to the second series Corvette Sting Ray and European sports cars such as the Jaguar E-Type coupe.

Favorable publicity articles appeared in 2,600 newspapers the next morning, the day the car was "officially" revealed.[22][23] A Mustang convertible also appeared in the James Bond film Goldfinger in September 1964.[24]

Price and sales

To achieve an advertised list price of US$2,368, the Mustang was based heavily on familiar yet simple components, many of which were already in production for other Ford models.[25] Many (if not most) of the interior, chassis, suspension, and drivetrain components were derived from those used on Ford's Falcon and Fairlane. This use of common components also shortened the learning curve for assembly and repair workers, while at the same time allowing dealers to pick up the Mustang without also having to invest in additional spare parts inventory to support the new car line. Original sales forecasts projected less than 100,000 units for the first year.[26] This mark was surpassed in three months from rollout.[3] Another 318,000 would be sold during the model year (a record),[3] and in its first eighteen months, more than one million Mustangs were built.[26]

Upgrades

Several changes were made at the traditional opening of the new model year (beginning August 1964), including the addition of back-up lights on some models, the introduction of alternators to replace generators, an upgrade of the six-cylinder engine from 170 to 200 cu in (2.8 to 3.3 l) with an increase from 101 to 120 hp (75 to 89 kW), and an upgrade of the V8 engine from 260 to 289 cu in (4.3 to 4.7 l) with an increase from 164 to 210 hp (122 to 157 kW). The rush into production included some unusual quirks, such as the horn ring bearing the 'Ford Falcon' logo covered by a trim ring with a 'Ford Mustang' logo. These characteristics made enough difference to warrant designation of the 121,538 early versions as "1964½" Mustangs, a distinction that has endured with purists.[27]

Ford's designers began drawing up larger versions even as the original was achieving sales success, and while "Iacocca later complained about the Mustang's growth, he did oversee the 1967 redesign."[28] From 1967 until 1973, the Mustang got bigger but not necessarily more powerful.[29] The Mustang was facelifted, giving the Mustang a more massive look overall and allowing a big block engine to be offered for the first time. Front and rear end styling was more pronounced, and the "twin cove" instrument panel offered a thicker crash pad, and larger gauges. Hardtop, fastback and convertible body styles continued as before. Around this time, the Mustang was paired with a Mercury variant, called the Cougar, which used its own styling cues, such as a "cougar's head" logo and hidden quad headlamps. New safety regulations by the U.S. National Highway Traffic Safety Administration (NHTSA) for 1967 included an energy-absorbing steering column and wheel, 4-way emergency flashers, a dual-circuit hydraulic braking system, and softer interior knobs. The 1968 models received revised side scoops, steering wheel, and gasoline caps. Side marker lights were also added that year, and cars built after January 1, 1968 included shoulder belts for both front seats on coupes. The 1968 models also introduced a new 302 cu in (4.9 L) V8 engine, designed with Federal emissions regulations in mind.

The 1969 restyle "added more heft to the body as width and length again increased. Weight went up markedly too."[28] Due to the larger body and revised front end styling, the 1969 models (but less so in 1970) had a notable aggressive stance. The 1969 models featured "quad headlamps" which disappeared to make way for a wider grille and a return to standard headlamps in the 1970 models. This switch back to standard headlamps was an attempt to tame the aggressive styling of the 1969 model, which some felt was too extreme and hurt sales, but 1969 production exceeded the 1970 total.[30]

Models

Starting in 1969, to aid sales and continue the winning formula of the Mustang, a variety of new performance and decorative options became available, including functional (and non-functional) air scoops, cable and pin hood tie downs, and both wing and chin spoilers. Additionally, a variety of performance packages were introduced that included the Mach 1, the Boss 302, and Boss 429. The two Boss models were to homologate the engines for racing. The 1969 Mustang was the last year for the GT option (although it did return on the 3rd Generation Mustang for the 1982 Model Year). A fourth model available only as a hardtop, the Grande, saw success starting in 1969 with its soft ride, "luxurious" trim, 55 pounds (24.9 kg) of extra sound deadening, and simulated wood trim.

Downfall

Developed under the watch of Semon "Bunkie" Knudsen, the Mustang evolved "from speed and power" to the growing consumer demand for bigger and heavier "luxury" type designs.[31] "The result were the styling misadventures of 1971–73 ... The Mustang grew fat and lazy,"[31] "Ford was out of the go-fast business almost entirely by 1971."[32] "This was the last major restyling of the first-generation Mustang."[33] "The cars grew in every dimension except height, and they gained about 800 pounds (363 kg)."[33] "The restyling also sought to create the illusion that the cars were even larger."[33] The 1971 Mustang was nearly 3 inches (76 mm) wider than the 1970, its front and rear track was also widened by 3 inches (76 mm), and its size was most evident in the SportsRoof models with its nearly flat rear roofline[34] and cramped interior with poor visibility for the driver.[35] Performance decreased with sales continuing to decrease[36] as consumers switched to the smaller Pintos and Mavericks. A displeased Iacocca summed up later: "The Mustang market never left us, we left it."[37]

Second generation (1974–1978)

Lee Iacocca, who had been one of the forces behind the original Mustang, became President of Ford Motor Company in 1970 and ordered a smaller, more fuel-efficient Mustang for 1974. Initially it was to be based on the Ford Maverick, but ultimately was based on the Ford Pinto subcompact.

The new model, called the "Mustang II", was introduced two months before the first 1973 oil crisis, and its reduced size allowed it to compete against imported sports coupés such as the Japanese Toyota Celica and the European Ford Capri[citation needed] (then Ford-built in Germany and Britain, sold in U.S. by Mercury as a captive import car). First-year sales were 385,993 cars, compared with the original Mustang's twelve-month sales record of 418,812.[38] Ultimately, the Mustang II would be an early example of downsizing that would take place among Detroit's Big Three later in the decade.

Iacocca wanted the new car, which returned the Mustang to its 1964 predecessor in size, shape, and overall styling,[39] to be finished to a high standard, saying it should be "a little jewel."[40] Not only was it smaller than the original car, but it was also heavier, owing to the addition of equipment needed to meet new U.S. emission and safety regulations. Performance was reduced, and despite the car's new handling and engineering features the galloping mustang emblem "became a less muscular steed that seemed to be cantering.[41]

Engines for the 1974 models included the venerable 2.3 L I-4 from the Pinto and the 2.8 L Cologne V6 from the Mercury Capri. The 1975 model year reintroduced 302 cu in (4.9 L) Windsor V8 that was only available with the C-4 automatic transmission, power brakes, and power steering. This continued through production end in 1978. Other transmissions were the RAD 4-speed with unique gearing for all three engines, and the C-3 automatic behind the 2.3 L and 2.8 L. The 5.0 L designation was not applied until the 1978 King Cobra model. All 302 equipped Mustang II's, except the King Cobra received an updated version of the classic Ford "V8" emblem on each front fender.

The car was available in coupé and hatchback versions, including a "luxury" Ghia model designed by Ford's recently acquired Ghia of Italy. The coupe was marketed as the "Hardtop" but in fact had a thin "B" pillar and rear quarter windows that did not roll down. All Mustangs in this generation did feature frameless door glass, however. The "Ghia" featured a thickly padded vinyl roof and smaller rear quarter windows, giving a more formal look. 1974 models were: Hardtop, Hatchback, Mach 1 and Ghia. Changes introduced for 1975 included availability of an "MPG" model which had a different rear axle ratio for better fuel economy. 1976 added the "Stallion" trim package. The Mach 1 remained through the life cycle 1974-1978. Other changes in appearance and performance came with a "Cobra II" version in 1976–1978 and a "King Cobra" in 1978 of which 4,972 (approx) were built. 1977-1978 hatchback models, in all trim levels was also now available with the very popular T-top roof option, which included a leatherette storage bag that clipped to the top of the spare tire hump.

Third generation (1979–1993)

The 1979 Mustang was based on the longer Fox platform (initially developed for the 1978 Ford Fairmont and Mercury Zephyr). The interior was engineered to accommodate four people in comfort despite a smaller rear seat. The larger body meant the interior offered more space for four passengers, especially in the back seat, as well as a larger capacity trunk and a bigger engine bay. Two trim levels were available and included the base model and the more luxurious Ghia model. Body styles included a coupé (or notchback), hatchback, and convertible. Available trim levels included L, GL, GLX, LX, GT (1982-1993), GTS, Turbo GT (1983–84), GT-350 (1984), SVO (1984–86), Cobra (1979–81,1993), Cobra R (1993), and Ghia (1979–81). From 1979 to 1986, the Mustang's Mercury counterpart was called the Capri, again using its own styling cues. Handling was upgraded with a new rack-and-pinion steering system.

The third generation Mustang had two different front end styles. From 1979 to 1986 the car had an angled back front clip and four headlights, known by enthusiasts as "Four Eyes," the same front end styling that was also used on the Chevrolet Camaro from 1982 until 1992. Then in the 1987 to 1993 model years, the front clip had a rounded-off shape known as the "aero" style with flush composite headlamps. Also in 1986, engines featured EFI (electronic fuel injection) instead of carburetors. Other changes for the 1986 models included an upgraded 8.8-inch (224 mm) rear-end with four shock absorbers.

In addition to the base & Ghia trim levels, a Cobra appearance package also made its debut and would continue through both the 1980 & 1981 model years. The all-new 1979 Cobra (17,579 produced) featured black trim and grille area, chrome door handles, stainless steel lock sets & antenna, aluminum roof drip rail, body colored sail panels, black lower body-side paint, colored coordinated dual pinstripes in the wraparound body-side moldings and bumper grooves, an optional snake decal for the hood and Cobra lettering on the doors. There was no rear spoiler on the 1979 models (except on the mid year introduction of the Indianapolis Pace Cars). The 1980 Cobra (5,550 produced) and the 1981 Cobras (1,821 produced) had a makeover in the appearance department as a new front bumper and air dam (complete with fog lights), full length cowl type hood scoop, and rear spoiler were added (all carried over from the 1979 Indy Pace Car). Also included in the '80/'81 Cobra package were colorful body length decals, COBRA hood decal, COBRA side window decals, and a COBRA decal on the rear spoiler. All trim was now "Blacked out", including the door handles, keylocks, antenna, and sail panels.

On May 27, 1979, the all-new Mustang was chosen as the Official Pace Car of the Indianapolis 500. Ford commemorated this event with a mid-year addition "Indy 500" Pace Car model (10,478 produced). The two-tone Pewter and Black colors were complimented with Orange and Red graphics. The front end featured a unique front air dam with fog lights, and a full length cowl type hood scoop, while the rear end got the new for '79 rear spoiler (all of these additions carried over to both the '80 & '81 Cobra). The black interior featured Recaro seats with patterned Black and White inserts. Available were the 2.3 L Turbo with mandatory four-speed manual transmission or the 5.0 L V8 with either an overdrive 4-speed manual or three-speed automatic transmission. The production cars included a sunroof. However, the three actual pace cars were fitted with a T-roof by Cars & Concepts of Brighton, MI. The T-roof option would not become an available option until the 1981 model year.[42]

In 1982, the Cobra model was dropped in favor of the Mustang GT, which returned after 13 years. The new GT featured a re-engineered 157 hp (117 kW; 159 PS) 302 cu in (4.9 L) "5.0 L" engine with new valves, a more aggressive cam (from a 1973 351W Torino application), a larger twin-barrel carburetor, and a revised firing order, as well as a better breathing intake and exhaust system. The GT included the front air dam with fog lamps and the rear spoiler from the '79 Pace Car and the 1980 & 1981 Cobras. However, the full length hood scoop from those models did not carry over and the smaller 1979 Cobra hood scoop made its return on the GT. Only four colors were offered on the GT model and they consisted of Dark Red, Bright Red, Silver, and Black. As in many previous years, the 5.0 engine was not tied only to the performance flagship GT. It was available on lower trims, and also formed the basis for the "SSP" (Special Service Package) cars that were used by government and police law enforcement, and were almost exclusively ordered in the 2-door sedan bodystyle. The 4.2 Liter V8 was available for the last time on all Mustang models and only with an automatic transmission. Trim levels were also revised to now include the L (base), GL, and GLX under the GT model.

Engines for the 1979-1982 models included the 88 hp (66 kW) 2.3 L Pinto inline-four, 109 hp (81 kW) 2.8 L Cologne V6 (made by Ford of Germany), and the 140 hp (104 kW) 302 cu in (4.9 L) Windsor V8; which was marketed as a 5.0 L engine and front fenders badged as such. All were carried over from the Mustang II line. Shortly after the model year started a 85 hp (63 kW) 3.3 L straight-six engine was available. Supplies of the 2.8 L V6 proved inadequate leading to it being discontinued in late 1979. A new 132 hp (98 kW) 2.3 L turbo four-cylinder, debuted that offered similar horsepower to the V8. The automaker had plans this engine would usher in a new era in performance. The 2.3 and 2.3 Turbo, as well as the V8 models could also be optioned with the newly developed TRX handling suspension that included Michelin 390 mm tires and specific metric wheels.

Following the second oil crisis in 1979, the 302 cu in (4.9 L) "5.0 L" engine was dropped in favor of a new 255 cu in (4.2 L) V8 due to its better fuel economy. It was the only V8 offered in 1980 and 1981. Basically a sleeved down 302, the 4.2 L V8 had restrictive heads and produced 120 hp (89 kW), the lowest power ever for a Mustang V8. The 4.2 L was mated only with the three-speed automatic transmission. This meant the 2.3 L Turbo 4 was the sole "performance" engine. The Turbo 4 was plagued with reliability issues from its release. Inadequate lubrication led to premature turbo failure and some engines caught fire. It was listed as an option through 1981, but dropped for 1982, although it was still available in Canada. This engine would return in the new-for-1983 Turbo GT. The "Traction-Lok" limited slip differential was available for the first time in 1981, with all engine combinations. A five-speed manual option arrived late during the 1980 model year, originally only in the 2.3-liter four-cylinder engines.[43] New for 1981 was an optional Traction-Lok rear axle (all engines), and a T-bar roof.[43]

In response to poor sales and escalating fuel prices during the early 1980s, a new Mustang was in development. It was to be a variant of the Mazda MX-6 assembled at AutoAlliance International in Flat Rock, Michigan. Enthusiasts wrote to Ford objecting to the proposed change to a front-wheel drive, Japanese-designed Mustang without a V8 option. The result was a major facelift of the existing Mustang in 1987, while the MX-6 variant had a last minute name change from Mustang to Probe and released as a 1989 model.

Fourth generation (1994–2004)

In November 1993, the Mustang debuted its first major redesign in fifteen years. Code-named "SN-95" by the automaker, it was based on an updated version of the rear-wheel drive Fox platform called "Fox-4." The new styling by Patrick Schiavone incorporated several styling cues from earlier Mustangs.[44] For the first time since its introduction 1964, a notchback coupe model was unavailable.

The base model came with a 3.8 OHV V6 (232 cid) engine rated at 145 bhp (108 kW) in 1994 and 1995, or 150 bhp (110 kW) (1996–1998), and was mated to a standard 5-speed manual transmission or optional 4-speed automatic. Though initially used in the 1994 and 1995 Mustang GTS, GT and Cobra, Ford retired the 302 cid pushrod small-block V8 after nearly 30 years of use, replacing it with the newer Modular 4.6 L (281 cid) SOHC V8 in the 1996 Mustang GT. The 4.6 L V8 was initially rated at 215 bhp (160 kW), 1996–1997, but was later increased to 225 bhp (168 kW) in 1998.[45]

For 1999, the Mustang was reskinned with Ford's New Edge styling theme with sharper contours, larger wheel arches, and creases in its bodywork, but its basic proportions, interior design, and chassis remained the same as the previous model. The Mustang's powertrains were carried over for 1999, but benefited from new improvements. The standard 3.8 L V6 had a new split-port induction system, and was rated at 190 bhp (140 kW) 1999–2000, while the Mustang GT's 4.6 L V8 saw an increase in output to 260 bhp (190 kW) (1999–2004), due to a new head design and other enhancements. In 2001, the 3.8 L was increased to 193 bhp.[46] In 2004, a 3.9L variant of the Essex engine replaced the standard 3.8L mid year with an increase of 3 ft⋅lb (4 N⋅m) of torque as well as NVH improvements. There were also three alternate models offered in this generation: the 2001 Bullitt, the 2003 and 2004 Mach 1, as well as the 320 bhp (240 kW) 1999 and 2001,[47][48] and 390 bhp (290 kW) 2003 and 2004[49] Cobra.

Ford Australia

This generation was sold in Australia between 2001 and 2002, to compete against the Holden Monaro (which eventually became the basis for the reborn Pontiac GTO). Due to the fact that the Mustang was never designed for right-hand-drive, Ford Australia contracted Tickford Vehicle Engineering to convert 250 Mustangs and modify them to meet Australian Design Rules,[50] at a cost of A$4,000,000.[51] Sales did not meet expectations, including due to a very high selling price.[52] In total, just 377 Mustangs were sold in Australia between 2001-2003.[53] For promotional purposes, Ford Racing Australia also built a Mustang V10 convertible, which was powered by a Ford Modular 6.8-Litre V10 engine from the American F truck series but fitted with an Australian-made Sprintex supercharger.[54]

Fifth generation (2005–2014)

Ford introduced a redesigned 2005 model year Mustang at the 2004 North American International Auto Show, codenamed "S-197," that was based on the new D2C platform. Developed under the direction of Chief Engineer Hau Thai-Tang, a veteran engineer for Ford's IndyCar program under Mario Andretti, and exterior styling designer Sid Ramnarace,[55] the fifth-generation Mustang's styling echoes the fastback Mustang models of the late-1960s. Ford's senior vice president of design, J Mays, called it "retro-futurism." The fifth-generation Mustang was manufactured at the Flat Rock Assembly Plant in Flat Rock, Michigan.

For the 2005 to 2010 production years, the base model was powered by a 210 hp (157 kW; 213 PS) cast-iron block 4.0 L SOHC V6, while the GT used an aluminum block 4.6 L SOHC 3-valve Modular V8 with variable camshaft timing (VCT) that produced 300 hp (224 kW; 304 PS). Base models had a Tremec T5 5-speed manual transmission with Ford's 5R55S 5-speed automatic being optional. Automatic GTs also featured this, but manual GTs had the Tremec TR-3650 5-speed.[56]

The 2010 model year Mustang was released in the spring of 2009 with a redesigned exterior — which included sequential LED taillights — and a reduced drag coefficient of 4% on base models and 7% on GT models.[57] The engine for base Mustangs remained unchanged, while GTs 4.6 L V8 was revised resulting in 315 hp (235 kW; 319 PS) at 6000 rpm and 325 lb⋅ft (441 N⋅m) of torque at 4255 rpm.[58] Other mechanical features included new spring rates and dampers, traction and stability control system standard on all models, and new wheel sizes.

Engines were revised for 2011, and transmission options included the Getrag-Ford MT82 6-speed manual or the 6R80 6-speed automatic based on the ZF 6HP26 transmission licensed for production by Ford. Electric power steering replaced the conventional hydraulic version. A new 3.72 L (227 cu. in.) aluminum block V6 engine weighed 40 lb (18 kg) less than the previous version. With 24 valves and Twin Independent Variable Cam Timing (TiVCT), it produced 305 hp (227 kW; 309 PS) and 280 lb⋅ft (380 N⋅m) of torque. The 3.7 L engine came with a new dual exhaust; gasoline mileage increased to 19 city/31 highway mpg.[2]. GT models included a 32-valve 5.0 L engine (4951cc or 302.13 cu. in.) (also referred to as the "Coyote".) producing 412 hp and 390 ft-lbs of torque. Brembo brakes are optional along with 19-inch wheels and performance tires.[59]

The Shelby GT500's 5.4 L supercharged V8 block was made of aluminum making it 102 lb (46 kg) lighter than the iron units in previous years. It was rated at 550 hp (410 kW; 558 PS) and 510 lb⋅ft (690 N⋅m) of torque.[60]

For 2012, a new Mustang Boss 302 version was introduced. The engine had 444 hp (331 kW; 450 PS) and 380 lb⋅ft (520 N⋅m) of torque. A "Laguna Seca" edition was also available, which offered additional body bracing, the replacement of the rear seat with a steel 'X-brace' for stiffening, and other powertrain and handling enhancements.

In the second quarter of 2012, Ford launched an update to the Mustang line as an early 2013 model. The Shelby GT500 has a new 5.8 L supercharged V8 producing 662 hp (494 kW; 671 PS). Shelby and Boss engines came with a six-speed manual transmission. The GT and V6 models revised styling incorporated the grille and air intakes from the 2010–2012 GT500. The decklid received a black cosmetic panel on all trim levels. The GT's 5.0 liter V8 gained eight horsepower from 412 hp (307 kW; 418 PS) to 420 hp (313 kW; 426 PS).

Sixth generation (2015–present)

The sixth generation Mustang was unveiled on December 5, 2013, in Dearborn, Michigan; New York, New York; Los Angeles, California; Barcelona, Spain; Shanghai, China; and Sydney, Australia.[61] The internal project codename is S-550.[citation needed]

Changes include widened body by 1.5 inches, 1.4 inches lower body, trapezoidal grille, and a 2.75-inch lower decklid, as well as new colors. The passenger volume is increased to 84.5 cubic feet, and three engine options are available: a newly developed 2.3 L EcoBoost 310 hp four-cylinder introduced to reach high tariff global markets like China,[62] 3.7 L 300 hp V6,[63] or 5.0 L Coyote 435 hp V8, with either a Getrag six-speed manual or six-speed automatic transmission with paddle shifters. [64][65][66]

A new independent rear suspension (IRS) system was developed specifically for the new model.[67] It also became the first version factory designed as a right hand drive export model to be sold overseas through Ford new car dealerships in right hand drive markets.[citation needed] During this model year, left hand drive versions were expanded to new export markets.[citation needed]

In February 2015, the Mustang earned a 5-star rating from the National Highway Traffic Safety Administration (NHTSA) for front, side, and rollover crash protection.[68]

In May 2015, Ford issued a recall involving 19,486 of the 2015 Ford Mustang with the 2.3 L EcoBoost turbocharged four-cylinder engine with a production date between February 14, 2014, and February 10, 2015 that were built at the Flat Rock Assembly Plant. As of June 2015, 1 million Mustangs (between 2005-2011) and GTs (between 2005-2006) were affected by a recall of airbags made by Takata Corporation. This was after Takata announced that it was recalling 33.8 million vehicles in the U.S. for airbags that could explode and send metal pieces flying at drivers and passengers.[69]

Euro NCAP Crash-tested the LHD (Left Hand Drive) European version of the 2017 Mustang recently, the car got two stars only due to the lack of auto safety features such as lane assist and auto braking. Otherwise the Mustang did average to good in the other areas of the test".[70][71]

The 2018 model year Mustang is set to be released in the third quarter of 2017 in North America and by 2018 globally. It will have a minor redesign to the exterior. The 2018 Ford Mustang engine line up sees changes from the previous years. The 3.7L V6 has been dropped and the 2.3L 4 cyl. Ecoboost now serves as the base engine for the Mustang. The 5.0L V8 sees a power increase to 460HP and 420 lb.-ft. of torque. The automatic transmission in both engines is now a ten-speed that was co-developed by Ford and GM.[citation needed]

Racing

The Mustang made its first public appearance on a racetrack as pace car for the 1964 Indianapolis 500.[13]

The same year, Mustangs won first and second in class at the Tour de France international rally.

In 1969, modified versions of the 428 Mach 1, Boss 429 and Boss 302 took 295 United States Auto Club-certified records at Bonneville Salt Flats. The outing included a 24-hour run on a 10-mile (16 km) course at an average speed of 157 mph (253 km/h). Drivers were Mickey Thompson, Danny Ongais, Ray Brock, and Bob Ottum.[13]

Drag racing

The car's American competition debut, also in 1964, was in drag racing, where private individuals and dealer-sponsored teams campaigned Mustangs powered by 427 cu in (7.0 L) V8s.

In late 1964, Ford contracted Holman & Moody to prepare ten 427-powered Mustangs to contest the National Hot Rod Association's (NHRA) A/Factory Experimental class in the 1965 drag racing season. Five of these special Mustangs made their competition debut at the 1965 NHRA Winternationals, where they qualified in the Factory Stock Eliminator class. The car driven by Bill Lawton won the class.[72]

A decade later Bob Glidden won the Mustang's first NHRA Pro Stock title.

Rickie Smith's Motorcraft Mustang won the International Hot Rod Association Pro Stock world championship.

In 2002 John Force broke his own NHRA drag racing record by winning his 12th national championship in his Ford Mustang Funny Car, Force beat that record again in 2006, becoming the first-ever 14-time champion, driving a Mustang.[13]

Sports car racing

Early Mustangs also proved successful in road racing. The GT 350 R, the race version of the Shelby GT 350, won five of the Sports Car Club of America's (SCCA) six divisions in 1965. Drivers were Jerry Titus, Bob Johnson and Mark Donohue, and Titus won the (SCCA) B-Production national championship. GT 350s won the B-Production title again in 1966 and 1967. They also won the 1966 manufacturers' championship in the inaugural SCCA Trans-Am series, and repeated the win the following year.[13]

In 1970, Mustang won the SCCA series manufacturers' championship again, with Parnelli Jones and George Follmer driving for car owner/builder Bud Moore and crew chief Lanky Foushee. Jones won the "unofficial" drivers' title.

In 1975 Ron Smaldone's Mustang became the first-ever American car to win the Showroom Stock national championship in SCCA road racing.

Mustangs competed in the IMSA GTO class, with wins in 1984 and 1985. In 1985 John Jones won the 1985 GTO drivers' championship; Wally Dallenbach Jr., John Jones and Doc Bundy won the GTO class at the Daytona 24 Hours; and Ford won its first manufacturers' championship in road racing since 1970. Three class wins went to Lynn St. James, the first woman to win in the series.

1986 brought eight more GTO wins and another manufacturers' title. Scott Pruett won the drivers' championship. The GT Endurance Championship also went to Ford.

In 1987 Saleen Autosport Mustangs driven by Steve Saleen and Rick Titus won the SCCA Escort Endurance SSGT championship, and in International Motor Sports Association (IMSA) racing a Mustang again won the GTO class in the Daytona 24 Hours. In 1989, the Mustang won Ford its first Trans-Am manufacturers' title since 1970, with Dorsey Schroeder winning the drivers' championship.[73]

In 1997, Tommy Kendall's Roush-prepared Mustang won a record 11 consecutive races in Trans-Am to secure his third straight driver's championship.

Mustangs compete in the SCCA World Challenge, with Brandon Davis won the 2009 GT driver's championship. Mustangs competed in the now-defunct Grand-Am Road Racing Ford Racing Mustang Challenge for the Miller Cup series.

Ford won championships in the Grand-Am Road Racing Continental Tire Sports Car Challenge for the 2005, 2008, and 2009 seasons with the Mustang FR500C and GT models. In 2004, Ford Racing retained Multimatic Motorsports to design, engineer, build and race the Mustang FR500C turn-key race car. In 2005, Scott Maxwell and David Empringham took the driver's title. In 2010, the next generation Mustang race car was known as the Boss 302R. It took its maiden victory at Barber Motorsports Park in early 2011, with drivers Scott Maxwell and Joe Foster. In 2016, Multimatic Motorsports won the IMSA CTSCC drivers' and manufacturers' titles with the S550-based Shelby GT350R-C, driven by Scott Maxwell and Billy Johnson.[74]

In 2012, Jack Roush won the Continental Tire Sports Car Challenge race at the Daytona International Speedway opening race of the 50th Anniversary Rolex 24 At Daytona weekend in a Mustang Boss 302R.[75]

Stock car racing

Dick Trickle won 67 short-track oval feature races in 1972, a national record for wins in a single season.

In 2010 the Ford Mustang became Ford's Car of Tomorrow for the NASCAR Nationwide Series with full-time racing of the Mustang beginning in 2011. This opened a new chapter in both the Mustang's history and Ford's history. NASCAR insiders expect to see Mustang racing in NASCAR Sprint Cup by 2014 (the model's 50th anniversary). The NASCAR vehicles are not based on production models, but are a silhouette racing car with decals that give them a superficial resemblance to road cars. Carl Edwards won the first-ever race with a NASCAR-prepped Mustang on April 8, 2011 at the Texas Motor Speedway.

Ford Mustangs also race in the NASCAR Xfinity Series since 2010.

Drifting

Mustangs have competed at the Formula Drift and D1 Grand Prix series, most notably by American driver Vaughn Gittin Jr.

Europe

Ford Mustangs compete in the FIA GT3 European Championship, and compete in the GT4 European Cup and other sports car races such as the 24 Hours of Spa. The Marc VDS Racing Team was developing the GT3 spec Mustang since 2010.[76]

Awards

The 1965 Mustang won the Tiffany Gold Medal for excellence in American design, the first automobile ever to do so.

The Mustang was on the Car and Driver Ten Best list in 1983, 1987, 1988, 2005, 2006, 2011, and 2016. It won the Motor Trend Car of the Year award in 1974 and 1994.

Sales

Model Year US sales
 
 
 
 
1964½ 121,538
1965 559,451[77]
1966 607,568[78]
1967 472,121[79]
1968 317,404[80]
1969 299,824[81]
Model Year US sales
1970 191,239
1971 151,484
1972 125,813
1973 134,817
1974 385,993
1975 188,575
1976 187,567
1977 153,173
1978 192,410
1979 369,936
Model Year US sales
1980 271,322
1981 182,552
1982 130,418
1983 120,873
1984 141,480
1985 156,514
1986 224,410
1987 169,772
1988 211,225
1989 209,769
Model Year US sales
1990 128,189
1991 98,737
1992 79,280
1993 114,335
1994 123,198
1995 136,962[82]
1996 122,674
1997 116,610
1998 144,732
1999 166,915[83]
Model Year US sales
2000 202,990
2001 169,198[84]
2002 138,356[85]
2003 140,350
2004 129,858[86]
2005 160,975
2006 166,530[87]
2007 134,626
2008 91,251[88]
2009 66,623[89]
Model Year US sales
2010 73,716[90]
2011 70,438[91]
2012 82,995[92]
2013 77,186[93]
2014 82,635[94]
2015 122,349[95]
2016 105,932[95]
 
 
 

National Mustang Museum

In May 2016, the National Mustang Museum was announced, with an expected opening in Concord, North Carolina in summer 2017. The decision to locate somewhere in Concord was a result of the success of the 2014 Mustang 50th anniversary celebration at Charlotte Motor Speedway in Concord, with over 4,000 Mustangs registered and an estimated economic impact of US$8,300,000.[96]

In popular culture

The Ford Mustang has been featured in numerous media. Effective product placement allowed the car to reach "celebrity status in the 1960s."[97] In particular, "movie glamour" assisted in establishing a positive association with the Mustang.[98] The following are a few notable cases where embedded marketing influenced the sales or other tangible aspect of the vehicle:

  • The 1964 movie Goldfinger, was the Ford Mustang's first appearance in a feature film and timed with the car's introduction in the US marketplace.[99]
  • The song "Mustang Sally", recorded by Wilson Pickett in 1966, is about a man who buys a Mustang for his ungrateful girlfriend. It has been described by one cultural historian as "free advertising for the Ford Motor Company."[100]
  • The TV series The F.B.I. was sponsored by Ford Motor Company and Efrem Zimbalist Jr. drove new Mustang convertibles during the first four seasons (1965-1969) and viewers can see how the Mustang evolved into a muscle car.[101]

See also



This article uses material from the Wikipedia article "Ford Mustang", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks

Car, Truck,MotorBike, Bicycle, Engine, Racer