Licensed under Creative Commons Attribution-Share Alike 4.0 (Luca Aless).
Pisa Cathedral Primatial Metropolitan Cathedral of the Assumption of Mary | |
---|---|
Il Duomo di Santa Maria Assunta | |
Pisa Cathedral | |
Tuscany_type:landmark 43°43′24″N 10°23′45″E / 43.723281°N 10.395845°E / 43.723281; 10.395845Coordinates: Tuscany_type:landmark 43°43′24″N 10°23′45″E / 43.723281°N 10.395845°E / 43.723281; 10.395845 | |
Location | Pisa |
Country | Italy |
Denomination | Catholicism of the Roman rite |
Website | Official website |
History | |
Consecrated | 26 September 1118 (1118-09-26) |
Architecture | |
Architect(s) | Buscheto and Rainaldo |
Style | Pisan Romanesque |
Groundbreaking | 1063 |
Completed | 1092 |
Administration | |
Archdiocese | Pisa |
Pisa Cathedral (Italian: Cattedrale Metropolitana Primaziale di Santa Maria Assunta; Duomo di Pisa) is a medieval Roman Catholic cathedral dedicated to the Assumption of the Virgin Mary, in the Piazza dei Miracoli in Pisa, Italy. It is a notable example of Romanesque architecture, in particular the style known as Pisan Romanesque.[1] It is the seat of the Archbishop of Pisa.
Construction on the cathedral began in 1063 (1064 according to the Pisan calendar of the time) by the architect Buscheto, and expenses were paid using the spoils received fighting against the Muslims in Sicily in 1063.[2] It includes various stylistic elements: classical, Lombard-Emilian, Byzantine, and Islamic, drawing upon the international presence of Pisan merchants at that time. In the same year, St. Mark's Basilica began its reconstruction in Venice, evidence of a strong rivalry between the two maritime republics to see which could create the most beautiful and luxurious place of worship.
The church was erected outside Pisa's high middle age-era walls, to show that Pisa that was so powerful, it had no fear of being attacked.[citation needed] The chosen area had already been used in the Lombard era as a necropolis and at the beginning of the 11th century a church had been erected here, but never finished, that was to be named Santa Maria.[citation needed] Buscheto's grand new church, was initially called Santa Maria Maggiore until it was officially named Santa Maria Assunta.[citation needed]
In 1092 the cathedral was declared a primatial church, archbishop Dagobert having been given the title of Primate by Pope Urban II. The cathedral was consecrated in 1118 by Pope Gelasius II, who belonged to the Caetani family which was powerful both in Pisa and in Rome.
In the early 12th century the cathedral was enlarged under the direction of architect Rainaldo, who increased the length of the nave by adding three bays consistent with the original style of Buscheto, enlarged the transept, and planned a new facade which was completed by workers under the direction of the sculptors Guglielmo and Biduino.[3] The exact date of the work is unclear: according to some [who?] the work was done right after the death of Buscheto about the year 1100, though others [who?] say it was done closer to 1140. In any case, work was finished in 1180, as documented by the date written on the bronze knockers made by Bonanno Pisano found on the main door.
The structure's present appearance is the result of numerous restoration campaigns that were carried out in different eras. The first radical interventions occurred after the fire of 1595, following which the roof was replaced and sculptors from the workshop of Giambologna, among whom were Gasparo Mola and Pietro Tacca, created the three bronze doors of the facade. In the early 18th century began the redecoration of the inside walls of the cathedral with large paintings, the "quadroni", depicting stories of the blesseds and saints of Pisa. These works were made by the principal artists of the era, and a group of citizens arranged for the special financing of the project. Successive interventions occurred in the 19th century and included both internal and external modifications; among the latter was the removal of the original facade statues (presently in the cathedral museum) and their replacement with copies.
Other notable interventions include: the dismantling of Giovanni Pisano's pulpit between 1599 and 1601 that only in 1926 was reassembled and returned to the cathedral (with some original pieces missing, including the staircase); and the dismantling of the monument to Henry VII made by Lupo di Francesco that was found in front of the door of San Ranieri and later substituted by a simpler, symbolic version.
The original building plan was a Greek cross with a grand cupola at the crossing, but today the plan is a Latin cross with a central nave flanked by two side aisles on each side, with the apse and transepts having three naves. The inside offers a spatial effect similar to that of the great mosques thanks to the use of raised lancet arches, the alternating layers of black and white marble, and the elliptical dome, inspired by the Moors. The presence of two raised matronea in the nave, with their solid, monolithic columns of granite, is a clear sign of Byzantine influence. Buscheto welcomed Islamic and Armenian influence.[4]
The rich exterior decoration contains multicolored marble, mosaic, and numerous bronze objects from the spoils of war, among which is the griffin which was taken in Palermo in 1061 and later placed on the eastern part of the roof. In the early 19th century the original sculpture, which can now be seen in the cathedral museum, was removed from the roof and replaced with a copy. The high arches show Islamic and southern Italian influence. The blind arches with lozenge shapes recall similar structures in Armenia. The facade of grey and white marble, decorated with colored marble inserts, was built by Master Rainaldo. Above the three doorways are four levels of loggia divided by cornices with marble intarsia, behind which open single, double, and triple windows.
The heavy bronze doors of the facade were made by different Florentine artists in the 17th century. Contrary to what might be thought, from the beginning the faithful entered the cathedral through the door of Saint Rainerius, found in the transept of the same name, which faces the bell tower. This was because the nobles of the city, who approached the cathedral by via Santa Maria, would find themselves precisely at this entrance. This door was cast about 1180 by Bonanno Pisano, and it is the only door not destroyed by the fire of 1595 that heavily damaged the cathedral.
The door of Saint Rainerius is decorated with 24 bronze relief sculptures showing stories of the New Testament. This door is one of the first produced in Italy during the Middle Ages, after the importation of numerous examples from Constantinople (to Amalfi, Salerno, Rome, Montecassino, Venice, etc.), and a completely western sensibility, detached from the Byzantine tradition, can be admired. Above the doors are four open galleries, with, at the top, the Madonna and Child and, in the angles, the four evangelists. The tomb of Buscheto is found to the left of the north door of the facade.
The interior, subdivided at the front into a central nave flanked by two side aisles on either side and with the transept and apse in three naves, is covered with white and black marble, with monolithic grey marble columns having corinthian capitals. It has a wooden 17th-century coffered ceiling, painted and decorated with gold leaf, made by Domenico and Bartolomeo Atticciati; it bears the Medici coat of arms. Presumably the earlier ceiling was a structure with wooden trusses.
The inside of the dome, found where the central nave and the transepts cross, is decorated using a rare painting technique called encaustic[5][6] and depicts the Virgin in glory with saints by the Pisan artists Orazio and Girolamo Riminaldi (1627-1631). Restoration of the dome began in 2015 and is expected to conclude in 2018.
The granite Corinthian columns between the nave and the apse come from the mosque of Palermo, and are Pisan spoils retained in 1063 after a successful joint attack with the Normans on the Muslims in that city.
The large mosaic in the apse of Christ enthroned between the Virgin and Saint John is famous for the face of Saint John, painted by Cimabue in 1302, which miraculously survived the fire of 1595. This is the last work painted by Cimabue and the only work of his for which we have certified documentation. The work evokes the mosaics of the Byzantine and Norman churches found in Cefalù and Monreale in Sicily. The mosaic, in large part made by Francesco da Pisa, was brought to completion by Vincino da Pistoia with the Madonna on the left side (1320).
Among the medieval works that avoided destruction during the fire of 1595 are the fresco of the Madonna with Child in the triumphal arch by the Pisan artist Maestro di San Torpè, as well as the cosmati pavement, work rarely found outside of Lazio. It was made using inlaid marble to create geometric patters (mid-12th century). Other fresco fragments from the late medieval period have survived, among which is Saint Jerome on one of the four central pylons, as well as Saint John the Bapstist, a Crucifixion, and Saints Cosmas and Damian on one of the pylons near the entrance, partially hidden by the entry way.
The pulpit, a masterpiece made by Giovanni Pisano (1302-1310), survived the fire but was dismantled during the work of restoration and was not reassembled until 1926. With its intricate architecture and its complex sculptural decoration the work presents one of the most sweeping narratives of the 13th-century imagination which reflects the religious renewal and fervor of the era. On the slightly curved panels are sculpted with an expressive language the episodes of the life of Christ. The structure is polygonal (exactly as seen in the analogous works in the Baptistery of Pisa, in the Siena Cathedral Pulpit, and in the church of Saint Andrew); but this is the first example in a work of this type in which the panels are slightly curved. Other original features include:
For these qualities united to the skillful narrative art of the nine scenes the pulpit is generally considered [by whom?] to be a masterpiece, but more broadly it is considered a masterpiece of Italian gothic sculpture. This pulpit substituted the previous one made by Guglielmo (1157-1162) that was sent to the Cagliari Cathedral. Given the lack of documentation prior to its dismantling, the pulpit was placed in a location different from its original spot, and without doubt, its parts are not in their original positions either. It is unknown if the original work possessed a marble staircase.
The church also houses the relics of Saint Rainerius, patron saint of Pisa, and the fragmentary tomb of Henry VII, Holy Roman Emperor, who died at Buonconvento while holding Florence, in vain, under siege. The tomb, sculpted by Tino da Camaino between 1313-1315, was also dismantled then reconstructed and today sits in the right transept, while its original position was in the center of the apse as a sign of the city's ghibbeline adherence. Moved several times for political reasons, it eventually was separated into many parts (some inside the church, some on the facade, others in the Camposanto, and yet others in the cathedral museum).
The 27 paintings that cover the galleries behind the main altar, depicting stories of the Old Testament and stories of the life of Christ, were made between the 16th and 17th centuries mostly by Tuscan artists, among whom are Andrea del Sarto (three works: Saint Agnes, Saints Catherine and Margaret, and Saints Peter and John the Baptist) il Sodoma, and Domenico Beccafumi (Stories of Moses and the Evagelists).
Numerous and prestigious are the sacred furnishings of the church, including the bronze crucifix found on the main altar, and the angel candleholders placed at the ends of the rich marble transenna, made by Giambologna, as well as the large ciborium in silver designed by Giovanni Battista Foggini (1678–86) on the altar of the Blessed Sacrament chapel. On the numerous side altars are located 16th and 17th century paintings. Among these works are the Our Lady of Graces with saints, by the Florentine Mannerist Andrea del Sarto, and the Madonna enthroned with saints in the right transept, by Perin del Vaga, a student of Raphael, both finished by Giovanni Antonio Sogliani. In the Baroque style are: the Disputa del Sacramento by the Sienese painter Francesco Vanni, and the Cross with saints by Genoan Giovanni Battista Paggi. Particularly well-loved is the 13th century image of the Madonna col Bambino, also called the Madonna under the organ, attributed to Berlinghiero Berlinghieri of Volterra.
The cathedral, like the leaning bell tower, is sinking perceptibly into the ground, and a few indications of this instability are visible. For example, the difference in the floor levels of the original nave of Buscheto and the bays which were added later by Rainaldo .
The cathedral's original gràdule, constructed by Giovanni Pisano and dating from the late 13th century, were replaced in 1865 by the present parvise. These marble panels, decorated with carved animal figures and faces, were used to create a low wall which was placed close to the outer perimeter of the cathedral and which created an enclosure that provided space for the numerous sarcophagi from the Roman period. During the Middle Ages, these panels were reused for burials of nobles (among them Beatrice of Lorraine) and other well known persons. Some fragments are still visible in the cathedral museum, while the sarcophagi were all moved inside the fence of the Camposanto.
Inside the cathedral are found the Serassi organ made between 1831-1835, as well as an organ made in 1977 by the company Mascioni of Cuvio.
The three artists listed above are buried in the cathedral.
|access-date=
requires |url=
(help)
This article uses material from the Wikipedia article "Pisa Cathedral", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D - 3D Model - 3D CAD - 3D Building - 3D monument - 3D Map - 3D City - 3D GIS - LIDAR - CityGML - Paris London Berlin Rome Sydney Barcelona Vienna Wien Budapest Madrid London