Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Nevit Dilmen).
The tangram (Chinese: 七巧板; pinyin: qīqiǎobǎn; literally: "seven boards of skill") is a dissection puzzle consisting of seven flat shapes, called tans, which are put together to form shapes. The objective of the puzzle is to form a specific shape (given only an outline or silhouette) using all seven pieces, which may not overlap. It is reputed to have been invented in China during the Song Dynasty,[1] and then carried over to Europe by trading ships in the early 19th century. It became very popular in Europe for a time then, and then again during World War I. It is one of the most popular dissection puzzles in the world.[2][3] A Chinese psychologist has termed the tangram "the earliest psychological test in the world", albeit one made for entertainment rather than for analysis.[1]
The origin of the word 'tangram' is unclear. The '-gram' element is apparently from Greek γράμμα ('written character, letter, that which is drawn'). The 'tan-' element is variously conjectured to be Chinese t'an 'to extend' or Cantonese t'ang 'Chinese'.[4]
The tangram had already been around in China for a long time when it was first brought to America by Captain M. Donnaldson, on his ship, Trader, in 1815. When it docked in Canton, the captain was given a pair of Sang-Hsia-koi's (author) Tangram books from 1815.[5] They were then brought with the ship to Philadelphia, where it docked in February 1816. The first Tangram book to be published in America was based on the pair brought by Donnaldson.
The puzzle was originally popularized by The Eighth Book Of Tan, a fictitious history of Tangram, which claimed that the game was invented 4,000 years prior by a god named Tan. The book included 700 shapes, some of which are possible to solve.[6]The puzzle eventually reached England, where it became very fashionable.[5] The craze quickly spread to other European countries.[5] This was mostly due to a pair of British Tangram books, The Fashionable Chinese Puzzle, and the accompanying solution book, Key.[7] Soon, tangram sets were being exported in great number from China, made of various materials, from glass, to wood, to tortoise shell.[8]
Many of these unusual and exquisite tangram sets made their way to Denmark. Danish interest in tangrams skyrocketed around 1818, when two books on the puzzle were published, to much enthusiasm.[9] The first of these was Mandarinen (About the Chinese Game). This was written by a student at Copenhagen University, which was a non-fictional work about the history and popularity of tangrams. The second, Det nye chinesiske Gaadespil (The new Chinese Puzzle Game), consisted of 339 puzzles copied from The Eighth Book of Tan, as well as one original.[9]
One contributing factor in the popularity of the game in Europe was that although the Catholic Church forbade many forms of recreation on the sabbath, they made no objection to puzzle games such as the tangram.[10]
Tangrams were first introduced to the German public by industrialist Friedrich Adolf Richter around 1891.[11] The sets were made out of stone or false earthenware,[12] and marketed under the name "The Anchor Puzzle".[11]
More internationally, the First World War saw a great resurgence of interest in Tangrams, on the homefront and trenches of both sides. During this time, it occasionally went under the name of "The Sphinx" an alternative title for the "Anchor Puzzle" sets.[13][14]
A tangram paradox is a dissection fallacy: Two figures composed with the same set of pieces, one of which seems to be a proper subset of the other.[15] One famous paradox is that of the two monks, attributed to Dudeney, which consists of two similar shapes, one with and the other missing a foot.[16] In reality, the area of the foot is compensated for in the second figure by a subtly larger body. Another tangram paradox is proposed by Sam Loyd in The 8th Book of Tan:[17]
The seventh and eighth figures represent the mysterious square, built with seven pieces: then with a corner clipped off, and still the same seven pieces employed.[18]
The two monks paradox – two similar shapes but one missing a foot.
The Magic Dice Cup tangram paradox – from Sam Loyd’s book The Eighth Book of Tan' (1903). Each of these cups was composed using the same seven geometric shapes. But the first cup is whole, and the others contain vacancies of different sizes. (Notice that the one on the left is slightly shorter than the other two. The one in the middle is ever-so-slightly wider than the one on the right, and the one on the left is narrower still.)[19]
Clipped square tangram paradox – from Sam Loyd’s book The Eighth Book of Tan (1903).
Over 6500 different tangram problems have been created from 19th century texts alone, and the current number is ever-growing.[20] Fu Traing Wang and Chuan-Chin Hsiung proved in 1942 that there are only thirteen convex tangram configurations (config segment drawn between any two points on the configuration's edge always pass through the configuration's interior, i.e., configurations with no recesses in the outline).[21][22]
Choosing a unit of measurement so that the seven pieces can be assembled to form a square of side one unit and having area one square unit, the seven pieces are:
Of these seven pieces, the parallelogram is unique in that it has no reflection symmetry but only rotational symmetry, and so its mirror image can be obtained only by flipping it over. Thus, it is the only piece that may need to be flipped when forming certain shapes.
This article uses material from the Wikipedia article "Tangram", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,model,playground,board games,computer,strategy,thinktank