An air pump is a device for pushing air. Examples include a bicycle pump, pumps that are used to aerate an aquarium or a pond via an airstone; a gas compressor used to power a pneumatic tool, air horn or pipe organ; a bellows used to encourage a fire; a vacuum cleaner and a vacuum pump.
Pumps and compressors use very similar mechanisms, and basically perform the same action, but in different fluid regimes. At some point there is a crossover point in terminology, but here are some stereotypes:
• Compressors operate on compressible fluids, typically gases. Pumps operate on fluids, typically liquids, approximated as incompressible.
• Compressors are intended to develop a very high pressure rise against a closed system; pumps are designed to develop relatively little pressure against a free-flowing system with minimal backpressure.
• Pumps are often used in continuous-flow operation, while many lower-end compressors must have intermittent duty cycles.
• Compressors usually have a feedback sensor to shut off when they reach a desired pressure; pumps have a fixed design and operate freely across their performance curve as conditions change
In 1649, Otto von Guericke invented the spool vacuum air pump. This pump was called air pump in 19th century lexicons.[1]
The first effective air pump constructed in England for scientific purposes was made in 1658 by Robert Hooke for Robert Boyle.[2]
This engineering-related article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "Air pump", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD