Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Brand | Razer Inc. |
---|---|
Slogan | Watch, Listen, Play[1] |
First released | November 15, 2017; 9 days ago (2017-11-15) |
Availability by country |
November 15, 2017
|
Predecessor | Nextbit Robin (indirect) |
Type | Phablet |
Form factor | Slate |
Dimensions |
158.5 mm (6.24 in) H 77.7 mm (3.06 in) W 8 mm (0.31 in) D |
Weight | 197 g (6.9 oz) |
Operating system | Android 7.1 "Nougat" |
System on chip | Qualcomm Snapdragon 835 |
CPU | Octa-core (4x2.35 GHz & 4x1.9 GHz) Kryo |
GPU | Adreno 540 |
Memory | 8 GB LPDDR4X RAM |
Storage | 64 GB |
Removable storage | microSD, up to 2 TB[1] |
Battery | 4,000 mAh Li-ion |
Data inputs |
|
Display | 5.7 in (140 mm) IPS LCD, 2560x1440 resolution, 515 ppi, DCI-P3 wide color gamut, 120 Hz refresh rate |
Rear camera | Dual 12 MP + 12 MP (f/1.75, PDAF & f/2.6, PDAF), 2x optical zoom, dual-LED flash |
Front camera | 8 MP, autofocus |
Sound | Dolby Atmos stereo speakers (front-facing) |
Connectivity | 3G, 4G VoLTE, Bluetooth 4.2, NFC, WiFi 802.11a/b/g/n/ac, GPS & GLONASS, USB-C[2] |
Website |
www |
The Razer Phone is an Android smartphone designed and developed by Razer Inc. It went on sale on 15 November 2017.[3]
Razer has designed the Phone mainly for gamers, although reviewers have noted that it is also great for everyday use.[4]
As a result of the acquistion of Nextbit in January 2017,[5] Razer started developing its own phone. The Razer Phone, therefore, is very similar in design to the Nextbit Robin. Its fingerprint scanner and front camera's positioning is the same, and both phones have large bezels, although the Razer Phone is made of aluminum, unlike the plastic Robin.
The Razer Phone's back is a slab of black aluminum with a chrome Razer logo. A special edition Phone is also to be released in limited quantity, that will have a green Razer logo.[3] The front glass is protected by Corning Gorilla Glass 3,[6] and the power and volume buttons are made of plastic.
It is powered by the Qualcomm Snapdragon 835, coupled with 8 GB LPDDR4X RAM and 64 GB internal storage. The internal storage is expandable by a microSD card.[7]
The display is a 5.7" 1440p IPS LCD panel with a 16:9 aspect ratio. Its highlighted feature is an "UltraMotion" 120 Hz display refresh rate, similar to Apple's second-generation iPad Pro.[7]
The Phone comes with two 12 MP cameras on the back, out of which, one is a wide-angle lens, and the other a telephoto. The wide-angle lens features an f/1.75 aperture, while the telephoto lens offers f/2.6 aperture.[7]
It has the market-standard USB-C charging port[2] for its large 4,000 mAh battery capable of fast charging using Qualcomm Quick Charge 4+. It also has a 24W fast charger included in the box, but does not have a 3.5 mm headphone jack.[7]
The sound is provided by Dolby Atmos, and comes with THX certified sound.[8]
The Phone runs Android 7.1 "Nougat" using the nearly stock OS and it uses Nova Launcher Prime as the launcher. Razer has promised an update to Android 8.0 "Oreo" in Q1 2018.[3]
This article uses material from the Wikipedia article "Razer Phone", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced