Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 2.5 (Randal J. (RJFerret)).
This article contains special characters. Without proper rendering support, you may see question marks, boxes, or other symbols. |
A wheel is a circular component that is intended to rotate on an axle bearing. The wheel is one of the key components of the wheel and axle which is one of the six simple machines. Wheels, in conjunction with axles, allow heavy objects to be moved easily facilitating movement or transportation while supporting a load, or performing labor in machines. Wheels are also used for other purposes, such as a ship's wheel, steering wheel, potter's wheel and flywheel.
Common examples are found in transport applications. A wheel greatly reduces friction by facilitating motion by rolling together with the use of axles. In order for wheels to rotate, a moment needs to be applied to the wheel about its axis, either by way of gravity or by the application of another external force or torque.
The English word wheel comes from the Old English word hweol, hweogol, from Proto-Germanic *hwehwlan, *hwegwlan, from Proto-Indo-European *kwekwlo-,[1] an extended form of the root *kwel- "to revolve, move around". Cognates within Indo-European include Icelandic hjól "wheel, tyre", Greek κύκλος kúklos, and Sanskrit chakra, the latter both meaning "circle" or "wheel".[2]
The invention of the wheel falls into the late Neolithic, and may be seen in conjunction with other technological advances that gave rise to the early Bronze Age. Note that this implies the passage of several wheel-less millennia even after the invention of agriculture and of pottery, during the Aceramic Neolithic (15713 BCE).
The Halaf culture of 6500–5100 BCE is sometimes credited with the earliest depiction of a wheeled vehicle, but this is doubtful as there is no evidence of Halafians using either wheeled vehicles or even pottery wheels.[3]
Precursors of wheels, known as "tournettes" or "slow wheels", were known in the Middle East by the 5th millennium BCE (one of the earliest examples was discovered at Tepe Pardis, Iran, and dated to 5200–4700 BCE). These were made of stone or clay and secured to the ground with a peg in the center, but required significant effort to turn. True (freely-spinning) potter's wheels were apparently in use in Mesopotamia by 3500 BCE and possibly as early as 4000 BCE,[4] and the oldest surviving example, which was found in Ur (modern day Iraq), dates to approximately 3100 BCE.[5]
The first evidence of wheeled vehicles appears in the second half of the 4th millennium BCE, near-simultaneously in Mesopotamia (Sumerian civilization), the Northern Caucasus (Maykop culture) and Central Europe (Cucuteni-Trypillian culture), so the question of which culture originally invented the wheeled vehicle is still unsolved.
The earliest well-dated depiction of a wheeled vehicle (here a wagon — four wheels, two axles) is on the Bronocice pot, a c. 3500 – 3350 BCE clay pot excavated in a Funnelbeaker culture settlement in southern Poland.[6]
The oldest securely dated real wheel-axle combination, that from Stare Gmajne near Ljubljana in Slovenia (Ljubljana Marshes Wooden Wheel) is now dated within two standard deviations to 3340–3030 BCE, the axle to 3360–3045 BCE.[7]
Two types of early Neolithic European wheel and axle are known; a circumalpine type of wagon construction (the wheel and axle rotate together, as in Ljubljana Marshes Wheel), and that of the Baden culture in Hungary (axle does not rotate). They both are dated to c. 3200–3000 BCE.[8]
In China, the wheel was certainly present with the adoption of the chariot in c. 1200 BCE,[9] although Barbieri-Low[10] argues for earlier Chinese wheeled vehicles, c. 2000 BC.
In Britain, a large wooden wheel, measuring about 1 m (3.3 ft) in diameter, was uncovered at the Must Farm site in East Anglia in 2016. The specimen, dating from 1,100–800 years BCE, represents the most complete and earliest of its type found in Britain. The wheel's hub is also present. A horse's spine found nearby suggests the wheel may have been part of a horse-drawn cart. The wheel was found in a settlement built on stilts over wetland, indicating that the settlement had some sort of link to dry land.[11]
Although they did not develop the wheel proper, the Olmec and certain other American cultures seem to have approached it, as wheel-like worked stones have been found on objects identified as children's toys dating to about 1500 BC.[12] It is thought that the primary obstacle to large-scale development of the wheel in the Americas was the absence of domesticated large animals which could be used to pull wheeled carriages.[13] The closest relative of cattle present in Americas in pre-Columbian times, the American Bison, is difficult to domesticate and was never domesticated by Native Americans; several horse species existed until about 12,000 years ago, but ultimately became extinct.[14] The only large animal that was domesticated in the Western hemisphere, the llama, did not spread far beyond the Andes by the time of the arrival of Columbus.
Nubians from after about 400 BCE used wheels for spinning pottery and as water wheels.[15] It is thought that Nubian waterwheels may have been ox-driven.[16] It is also known that Nubians used horse-drawn chariots imported from Egypt.[17]
The wheel was barely used, with the exception of Ethiopia and Somalia, in Sub-Saharan Africa well into the 19th century but this changed with the arrival of the Europeans.[18][19]
Early wheels were simple wooden disks with a hole for the axle. Some of the earliest wheels were made from horizontal slices of tree trunks. Because of the uneven structure of wood, a wheel made from a horizontal slice of a tree trunk will tend to be inferior to one made from rounded pieces of longitudinal boards.
The spoked wheel was invented more recently, and allowed the construction of lighter and swifter vehicles. In the Harappan civilization of the Indus Valley and Northwestern India, we find toy-cart wheels made of clay with lines which have been interpreted as spokes painted or in relief,[20] and a symbol interpreted as a spoked wheel in the script of the seals,[21] already in the second half of the 3rd millennium BCE. The earliest known examples of wooden spoked wheels are in the context of the Andronovo culture, dating to c. 2000 BCE. Soon after this, horse cultures of the Caucasus region used horse-drawn spoked-wheel war chariots for the greater part of three centuries. They moved deep into the Greek peninsula where they joined with the existing Mediterranean peoples to give rise, eventually, to classical Greece after the breaking of Minoan dominance and consolidations led by pre-classical Sparta and Athens. Celtic chariots introduced an iron rim around the wheel in the 1st millennium BCE.
The spoked wheel was in continued use without major modification until the 1870s, when wire-spoked wheels and pneumatic tires were invented.[22] The wire spokes are under tension, not compression, making it possible for the wheel to be both stiff and light. Early radially-spoked wire wheels gave rise to tangentially-spoked wire wheels, which were widely used on cars into the late 20th century. Cast alloy wheels are now more commonly used; forged alloy wheels are used when weight is critical.
The invention of the wheel has also been important for technology in general, important applications including the water wheel, the cogwheel (see also antikythera mechanism), the spinning wheel, and the astrolabe or torquetum. More modern descendants of the wheel include the propeller, the jet engine, the flywheel (gyroscope) and the turbine.
The low resistance to motion (compared to dragging) is explained as follows (refer to friction):
Bearings are used to help reduce friction at the interface. In the simplest and oldest case the bearing is just a round hole through which the axle passes (a "plain bearing").
Example:
Additional energy is lost from the wheel-to-road interface. This is termed rolling resistance which is predominantly a deformation loss. This energy is also lowered by the use of a wheel (in comparison to dragging) because the net force on the contact point between the road and the wheel is almost perpendicular to the ground, and hence, generates an almost zero net work. This depends on the nature of the ground, of the material of the wheel, its inflation in the case of a tire, the net torque exerted by the eventual engine, and many other factors.
A wheel can also offer advantages in traversing irregular surfaces if the wheel radius is sufficiently large compared to the irregularities.
The wheel alone is not a machine, but when attached to an axle in conjunction with bearing, it forms the wheel and axle, one of the simple machines. A driven wheel is an example of a wheel and axle. Note that wheels pre-date driven wheels by about 6000 years, themselves an evolution of using round logs as rollers to move a heavy load—a practice going back in pre-history so far, it has not been dated.
The rim is the "outer edge of a wheel, holding the tire."[23] It makes up the outer circular design of the wheel on which the inside edge of the tire is mounted on vehicles such as automobiles. For example, on a bicycle wheel the rim is a large hoop attached to the outer ends of the spokes of the wheel that holds the tire and tube.
In the 1st millennium BCE an iron rim was introduced around the wooden wheels of chariots.
The hub is the center of the wheel, and typically houses a bearing, and is where the spokes meet.
A hubless wheel (also known as a rim-rider or centerless wheel) is a type of wheel with no center hub. More specifically, the hub is actually almost as big as the wheel itself. The axle is hollow, following the wheel at very close tolerances.
A spoke is one of some number of rods radiating from the center of a wheel (the hub where the axle connects), connecting the hub with the round traction surface. The term originally referred to portions of a log which had been split lengthwise into four or six sections. The radial members of a wagon wheel were made by carving a spoke (from a log) into their finished shape. A spokeshave is a tool originally developed for this purpose. Eventually, the term spoke was more commonly applied to the finished product of the wheelwright's work, than to the materials used.
The rims of wire wheels (or "wire spoked wheels") are connected to their hubs by wire spokes. Although these wires are generally stiffer than a typical wire rope, they function mechanically the same as tensioned flexible wires, keeping the rim true while supporting applied loads.
Wire wheels are used on most bicycles and still used on many motorcycles. They were invented by aeronautical engineer George Cayley and first used in bicycles by James Starley. A process of assembling wire wheels is described as wheelbuilding.
A tire (in American English and Canadian English) or tyre (in some Commonwealth Nations such as UK, India, South Africa and Australia) is a ring-shaped covering that fits around a wheel rim to protect it and enable better vehicle performance by providing a flexible cushion that absorbs shock while keeping the wheel in close contact with the ground. The word itself may be derived from the word "tie," which refers to the outer steel ring part of a wooden cart wheel that ties the wood segments together (see Etymology below).
The fundamental materials of modern tires are synthetic rubber, natural rubber, fabric and wire, along with other compound chemicals. They consist of a tread and a body. The tread provides traction while the body ensures support. Before rubber was invented, the first versions of tires were simply bands of metal that fitted around wooden wheels to prevent wear and tear. Today, the vast majority of tires are pneumatic inflatable structures, comprising a doughnut-shaped body of cords and wires encased in rubber and generally filled with compressed air to form an inflatable cushion. Pneumatic tires are used on many types of vehicles, such as cars, bicycles, motorcycles, trucks, earthmovers, and aircraft.
A trywheel is an arrangement of three wheels mounted on a y-shaped frame for the purpose of passing over stairs or rough ground. These may be driven by external force or integral motors.[citation needed]
To the 21st century observer, a wheel appears to be a fairly simple thing, but there have been many attempts to improve, and patent the wheel.
Inventors include:
In many cases, the idea was to create a resilient wheel. This function is now provided by what's known as the pneumatic tyre.
While wheels are very widely used for ground transport, there are alternatives, some of which are suitable for terrain where wheels are ineffective. Alternative methods for ground transport without wheels include:
A recent invention is the so-called Liddiard Wheel, which claims to be a superior omnidirectional wheel.[28][29]
The wheel has also become a strong cultural and spiritual metaphor for a cycle or regular repetition (see chakra, reincarnation, Yin and Yang among others). As such and because of the difficult terrain, wheeled vehicles were forbidden in old Tibet. The wheel in ancient China is seen as a symbol of health and strength and utilized by some villages as a tool to predict future health and success. The diameter of the wheel is indicator of one's future health.
The winged wheel is a symbol of progress, seen in many contexts including the coat of arms of Panama, the logo of the Ohio State Highway Patrol and the State Railway of Thailand. The wheel is also the prominent figure on the flag of India. The wheel in this case represents law (dharma). It also appears in the flag of the Romani people, hinting to their nomadic history and their Indian origins.
The introduction of spoked (chariot) wheels in the Middle Bronze Age appears to have carried somewhat of a prestige. The sun cross appears to have a significance in Bronze Age religion, replacing the earlier concept of a Solar barge with the more 'modern' and technologically advanced solar chariot. The wheel was also a solar symbol for the Ancient Egyptians.[30]This article uses material from the Wikipedia article "Wheel", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht