powered by CADENAS

Social Share

Drinking fountain (2565 views - Transportation - Air Water Earth)

A drinking fountain, also called a bubbler (generic trademark) or water fountain, is a fountain designed to provide drinking water. It consists of a basin with either continuously running water or a tap. The drinker bends down to the stream of water and swallows water directly from the stream. Modern indoor drinking fountains may incorporate filters to remove impurities from the water and chillers to lower its temperature. Drinking fountains are usually found in public places, like schools, rest areas, libraries, and grocery stores. Many jurisdictions require drinking fountains to be wheelchair accessible (by sticking out horizontally from the wall), and to include an additional unit of a lower height for children and short adults. The design that this replaced often had one spout atop a refrigeration unit. Use of the words water fountain and drinking fountain vary across regional dialects of English.
Go to Article

Explanation by Hotspot Model

Drinking fountain

Drinking fountain

A drinking fountain, also called a bubbler (generic trademark) or water fountain, is a fountain designed to provide drinking water. It consists of a basin with either continuously running water or a tap. The drinker bends down to the stream of water and swallows water directly from the stream. Modern indoor drinking fountains may incorporate filters to remove impurities from the water and chillers to lower its temperature. Drinking fountains are usually found in public places, like schools, rest areas, libraries, and grocery stores. Many jurisdictions require drinking fountains to be wheelchair accessible (by sticking out horizontally from the wall), and to include an additional unit of a lower height for children and short adults. The design that this replaced often had one spout atop a refrigeration unit.

Use of the words water fountain and drinking fountain vary across regional dialects of English.

History

In mid-19th century London, water provision from private water companies was generally inadequate for the rapidly growing population and was often contaminated. Legislation in the mid nineteenth century formed the Metropolitan Commission of Sewers, made water filtration compulsory, and moved water intakes on the Thames above the sewage outlets. In this context, the public drinking fountain movement began. It built the first public baths and public drinking fountains.[1]

Combined drinking fountain for people, horses and dogs, Toronto, Canada, 1899

In London, the Metropolitan Free Drinking Fountain Association was established in 1859. The first fountain was built on Holborn Hill on the railings of the church of St Sepulchre-without-Newgate on Snow Hill, paid for by Samuel Gurney, and opened on 21 April 1859.[2] The fountain became immediately popular, used by 7,000 people a day. In the next six years 85 fountains were built, with much of the funding coming directly from the association. The movement soon became associated with the temperance movement as they provided a substitute for alcohol and were purposely positioned outside public houses.[1]

In the United States, drinking fountains were built beginning in 1889 by the then-small Kohler Water Works (now Kohler Company) in Kohler, Wisconsin, a company already established as a faucet producer.[citation needed] The original 'Bubbler' shot water one inch straight into the air, creating a bubbling texture, and the excess water ran back down over the sides of the nozzle. Several years later the Bubbler adopted the more sanitary arc projection, which also allowed the user to drink more easily from it. At the start of the 20th century, it was discovered that the original vertical design was related to the spread of many contagious diseases.[3]

Cleanliness

In recent studies, it has been found that some drinking fountains have been contaminated with pathogens such as bacteria. In one study, a virus commonly known to cause diarrhea in young children known as the rotavirus has been found on drinking fountains in child day care facilities.[4] Due to cases in the past where children have fallen ill due to coliform bacteria poisoning, many governments have placed strict regulations on drinking fountain designs. The vertical spout design[clarification needed] is now illegal in most US jurisdictions.[citation needed] Some governments even require water spouts to be as long as four inches to meet health standards.[3] It is also recommended for young children to allow drinking fountains to run before drinking, as the water may also be contaminated with lead. This is especially common in older buildings with obsolete plumbing.[5]

Terminology

The term bubbler is used in some regional dialects of the United States and in Australia.[6] A survey of US dialects undertaken between 2002 and 2004 found the word bubbler is commonly used in southern and eastern Wisconsin and in Massachusetts and Rhode Island. The phrase drinking fountain was common in the rest of the inland north and in the west, while water fountain dominated other parts of the country.[7]

The term bubbler is sometimes used in the Portland, Oregon, region where in the late 1800s former Wisconsin resident Simon Benson installed 20 fountains, which are now known in the Portland area as "Benson Bubblers".[8]

Outdoors

Frost-resistant drinking fountains are used outdoors in cold climates and keep the control mechanisms below the frostline resulting in a delay for when water comes out.[9]

Gallery

See also



This article uses material from the Wikipedia article "Drinking fountain", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht