powered by CADENAS

Social Share

Amazon

Angle bracket (10524 views - Mechanical Engineering)

A bracket is a tall punctuation mark typically used in matched pairs within text, to set apart or interject other text. The matched pair may be described as opening and closing, or left and right symbols. Forms include round (also called "parentheses"), square, curly (also called "braces"), and angle brackets (also called "chevrons"); and various other pairs of symbols. In addition to referring to the class of all types of brackets, the unqualified word bracket is most commonly used to refer to a specific type of bracket: in modern American usage this is usually the square bracket and in modern British usage this is usually the round bracket.
Go to Article

Explanation by Hotspot Model

Angle bracket

Angle bracket

[ ] { } ( ) ⟨ ⟩
Brackets
( ) { } ⟨ ⟩
Round brackets or parentheses Curly brackets or braces Angle brackets or chevrons
Punctuation
apostrophe  '
brackets [ ]  ( )  { }  ⟨ ⟩
colon :
comma ,  ،  
dash ‒  –  —  ―
ellipsis  ...      
exclamation mark !
full stop, period .
guillemets ‹ ›  « »
hyphen
hyphen-minus -
question mark ?
quotation marks ‘ ’  “ ”  ' '  " "
semicolon ;
slash, stroke, solidus /  
Word dividers
interpunct ·
space     
General typography
ampersand &
asterisk *
at sign @
backslash \
bullet
caret ^
dagger † ‡
degree °
ditto mark
inverted exclamation mark ¡
inverted question mark ¿
komejirushi, kome, reference mark
number sign, pound, hash, octothorpe #
numero sign
obelus ÷
multiplication sign ×
ordinal indicator º ª
percent, per mil % ‰
plus and minus + −
equals sign =
basis point
pilcrow
prime    
section sign §
tilde ~
underscore, understrike _
vertical bar, pipe, broken bar |    ¦
Intellectual property
copyright ©
sound-recording copyright
registered trademark ®
service mark
trademark
Currency
currency sign ¤

؋฿¢$֏ƒ£元 圆 圓 ¥ 円

Uncommon typography
asterism
hedera
index, fist
interrobang
irony punctuation
lozenge
tie
Related
In other scripts

A bracket is a tall punctuation mark typically used in matched pairs within text, to set apart or interject other text. The matched pair may be described as opening and closing,[1] or left and right symbols.

Forms include round (also called "parentheses"), square, curly (also called "braces"), and angle brackets (also called "chevrons"); and various other pairs of symbols.

In addition to referring to the class of all types of brackets, the unqualified word bracket is most commonly used to refer to a specific type of bracket: in modern American usage this is usually the square bracket and in modern British usage this is usually the round bracket.

History

Chevrons (< >) were the earliest type of bracket to appear in written English. Desiderius Erasmus coined the term lunula to refer to the rounded parentheses (), recalling the shape of the crescent moon.[2]

Names for various bracket symbols

Some of the following names are regional or contextual.

  • ( ) – parentheses, brackets (UK, Canada, New Zealand, South Africa and Australia), parens, round brackets, soft brackets, first brackets or circle brackets
  • [ ] – square brackets, closed brackets, hard brackets, second brackets, crotchets,[3] or brackets (US)
  • { } – braces are "two connecting marks used in printing"; and in music "to connect staves to be performed at the same time"[4] (UK and US), French brackets, curly brackets, definite brackets, swirly brackets, curly braces, birdie brackets, Scottish brackets, squirrelly brackets, gullwings, seagulls, squiggly brackets, twirly brackets, Tuborg brackets (DK), accolades (NL), pointy brackets, third brackets, fancy brackets, M Brace.
  • ⟨ ⟩ – pointy brackets, angle brackets, triangular brackets, diamond brackets, tuples, or chevrons
  • < > – inequality signs, pointy brackets, or brackets. Sometimes referred to as angle brackets, in such cases as HTML markup. Occasionally known as broken brackets or brokets.[5]
  • ⸤ ⸥; 「 」 – corner brackets
  • ⟦ ⟧ – double square brackets, white square brackets
  • 〔 〕 – tortoise shell brackets
  • Guillemets, ‹ › and « », are sometimes referred to as chevrons or [double] angle brackets.[1]

Typography

The characters ‹ › and « », known as guillemets or angular quote brackets, are actually quotation mark glyphs used in several European languages.[6] Which one of each pair is the opening quote mark and which is the closing quote varies between languages.

Similarly, the corner-brackets 「 」 are quotation marks used in East Asian languages (see Quotation mark § Chinese, Japanese and Korean quotation marks).

In English, typographers generally prefer to not set brackets in italics, even when the enclosed text is italic.[7] However, in other languages like German, if brackets enclose text in italics, they are usually set in italics too.[8]

Types and uses

Parentheses

Parentheses /pəˈrɛnθɪsz/ (singular, parenthesis /pəˈrɛnθɪsɪs/) (also called simply brackets, or round brackets, curved brackets, oval brackets, stalls or, colloquially, parens /pəˈrɛnz/) contain material that serves to clarify (in the manner of a gloss) or is aside from the main point.[9] A milder effect may be obtained by using a pair of commas as the delimiter, though if the sentence contains commas for other purposes, visual confusion may result.

In American usage, parentheses are usually considered separate from other brackets, and calling them "brackets" is unusual.

Parentheses may be used in formal writing to add supplementary information, such as "Sen. John McCain (R-Arizona) spoke at length". They can also indicate shorthand for "either singular or plural" for nouns, e. g. "the claim(s)". It can also be used for gender neutral language, especially in languages with grammatical gender, e. g. "(s)he agreed with his (her) physician".[10]

Parenthetical phrases have been used extensively in informal writing and stream of consciousness literature. Examples include the southern American author William Faulkner (see Absalom, Absalom! and the Quentin section of The Sound and the Fury) as well as poet E. E. Cummings.

Parentheses have historically been used where the dash is currently used in alternatives, such as "parenthesis)(parentheses". Examples of this usage can be seen in editions of Fowler's.

Parentheses may be nested (generally with one set (such as this) inside another set). This is not commonly used in formal writing (though sometimes other brackets [especially square brackets] will be used for one or more inner set of parentheses [in other words, secondary {or even tertiary} phrases can be found within the main parenthetical sentence]).[11]

Any punctuation inside parentheses or other brackets is independent of the rest of the text: "Mrs. Pennyfarthing (What? Yes, that was her name!) was my landlady." In this usage, the explanatory text in the parentheses is a parenthesis. (Parenthesized text is usually short and within a single sentence. Where several sentences of supplemental material are used in parentheses the final full stop would be within the parentheses, or simply omitted. Again, the parenthesis implies that the meaning and flow of the text is supplemental to the rest of the text and the whole would be unchanged were the parenthesized sentences removed.)

Parentheses are included in the syntaxes of many computer programming languages. Typically needed to denote an argument; to tell the compiler what data type the Method/Function needs to look for first in order to initialise. In some cases, such as in LISP, parentheses are a fundamental construct of the language.

Parentheses in mathematics signify a different precedence of operators. For example: in algebraic order of operations, 2 + 3 × 4 equals 14, since the multiplication is done before the addition. However, (2 + 3) × 4 equals 20, because the parentheses override normal precedence, causing the addition to be done first. Some authors follow the convention in mathematical equations that, when parentheses have one level of nesting, the inner pair are parentheses and the outer pair are square brackets. Example:

A related convention is that when parentheses have two levels of nesting, curly brackets (braces) are the outermost pair. Following this convention, when more than three levels of nesting are needed, often a cycle of parentheses, square brackets, and curly brackets will continue. This helps to distinguish between one such level and the next.[12]

Parentheses are also used to set apart the arguments in mathematical functions. For example, f(x) is the function f applied to the variable x. In coordinate systems parentheses are used to denote a set of coordinates; so in the Cartesian coordinate system (4, 7) may represent the point located at 4 on the x-axis and 7 on the y-axis.

Parentheses may also be used to represent a binomial coefficient, and in chemistry to denote a polyatomic ion.

Since 2014, antisemites have used triple parentheses around the names of people to denote them as Jewish.[13]

Unpaired parenthesis

Lowercase latin letters used as indexes, rather than bullets or numbers, followed by unpaired parenthesis, are used in ordered lists especially in:

  1. educational testing,
  2. technical writing and diagrams,
  3. market research, and
  4. elections

In more formal usage, "parenthesis" may refer to the entire bracketed text, not just to the punctuation marks used (so all the text in this set of round brackets may be said to be "a parenthesis", "a parenthetical", or "a parenthetical phrase").[14]

Square brackets

Usage in journalism

Square brackets—also called crotchets or simply brackets (US)—are mainly used to insert explanatory material or to mark where a passage was omitted from an original material by someone other than the original author, or to mark modifications in quotations.[15]

A bracketed ellipsis, […], is often used to indicate omitted material: "I'd like to thank [several unimportant people] for their tolerance [...]"[16] Bracketed comments inserted into a quote indicate when the original has been modified for clarity: "I appreciate it [the honor], but I must refuse", and "the future of psionics [see definition] is in doubt". Or one can quote the original statement "I hate to do laundry" with a (sometimes grammatical) modification inserted: He "hate[s] to do laundry".

Additionally, a small letter can be replaced by a capital one, when the beginning of the original text is omitted for succinctness, for example, when referring to a verbose original: "To the extent that policymakers and elite opinion in general have made use of economic analysis at all, they have, as the saying goes, done so the way a drunkard uses a lamppost: for support, not illumination", it can be quoted succinctly as: "[P]olicymakers […] made use of economic analysis […] the way a drunkard uses a lamppost: for support, not illumination." When nested parentheses are needed, brackets are used as a substitute for the inner pair of parentheses within the outer pair.[17] When deeper levels of nesting are needed, convention is to alternate between parentheses and brackets at each level.

Alternatively, empty square brackets can also indicate omitted material, usually single letter only. The original "Reading is also a process and it also changes you." can be rewritten in a quote as: It has been suggested that reading can "also change[] you".

The bracketed expression "[sic]" is used after a quote or reprinted text to indicate the passage appears exactly as in the original source, where it may otherwise appear that a mistake has been made in reproduction.

In translated works, brackets are used to signify the same word or phrase in the original language to avoid ambiguity.[18] For example: He is trained in the way of the open hand [karate].

Usage in proofreading

Brackets (called move-left symbols or move right symbols) are added to the sides of text in proofreading to indicate changes in indentation:

Move left [To Fate I sue, of other means bereft, the only refuge for the wretched left.
Center ]Paradise Lost[
Move up

Usage in scientific fields

Brackets are used in mathematics in a variety of notations, including standard notations for intervals, commutators, the floor function, the Lie bracket, equivalence classes, the Iverson bracket, and matrices. Square brackets may also represent intervals; ]0, 5[ for example, is the interval between 0 and 5, not including 0 or 5 (sometimes written (0,5)).

Brackets can also be used in chemistry to represent the concentration of a chemical substance or to denote distributed charge in a complex ion.

Brackets are used in many computer programming languages, especially those derived or inspired by the C language, to indicate array indexing operators. In this context, the opening bracket is often pronounced as "sub", indicating a subscript.

Other uses

In linguistics, phonetic transcriptions are generally enclosed within brackets,[19] often using the International Phonetic Alphabet, whereas phonemic transcriptions typically use paired slashes. Pipes (| |) are often used to indicate a morphophonemic rather than phonemic representation. Other conventions are double slashes (// //), double pipes (|| ||) and curly brackets ({ }). In lexicography, square brackets usually surround the section of a dictionary entry which contains the etymology of the word the entry defines.

Brackets are used to denote parts of the text that need to be checked when preparing drafts prior to finalizing a document. They often denote points that have not yet been agreed to in legal drafts and the year in which a report was made for certain case law decisions.

Curly brackets

Curly brackets- { } —also called braces in the US (or, colloquially, squiggly brackets)—are used in specialized ways in poetry and music (to mark repeats or joined lines). The musical terms for this mark joining staves are accolade and "brace", and connect two or more lines of music that are played simultaneously.[20] In mathematics they delimit sets, and in writing, they may be used similarly, "Select your animal {goat, sheep, cow, horse} and follow me". In many programming languages, they enclose groups of statements. Such languages (C being one of the best-known examples) are therefore called curly bracket languages.[21]

In classical mechanics, curly brackets are often also used to denote the Poisson bracket between two quantities.

Angle brackets

Chevrons ⟨ ⟩, similar to the commonly used less-than (<) and greater-than symbol (>), are often used to enclose highlighted material.

In physical sciences, chevrons are used to denote an average over time or over another continuous parameter. For example,

The inner product of two vectors is commonly written as a,b, but the notation (a,b) is also used.

In mathematical physics, especially quantum mechanics, it is common to write the inner product between elements as a|b, as a short version of a|·|b, or a|Ô|b, where Ô is an operator. This is known as Dirac notation or bra–ket notation.

In set theory, chevrons or parentheses are used to denote ordered pairs and other tuples, whereas curly brackets are used for unordered sets.

In linguistics, chevrons indicate graphemes (i.e., written letters) or orthography, as in "The English word /kæt/ is spelled ⟨cat⟩."[22][23][24]

In epigraphy, they may be used for mechanical transliterations of a text into the Latin script.[23]

In textual criticism, and hence in many editions of pre-modern works, chevrons denote sections of the text which are illegible or otherwise lost; the editor will often insert their own reconstruction where possible within them.[24]

Chevrons are infrequently used to denote words that are thought instead of spoken, such as:

⟨ What an unusual flower! ⟩

The mathematical or logical symbols for greater-than (>) and less-than (<) are inequality symbols; when either symbol is bisected by a vertical line, it represents "not greater than" or "not less than," respectively. These symbols are not punctuation marks when used, as intended, to represent an inequality. However, as true chevrons are not present on computer keyboards, the available less-than and greater-than symbols are often used instead. They are loosely referred to as angle[d] brackets or chevrons in this case.[citation needed]

Single and double pairs of comparison operators (<<, >>) (meaning much smaller than and much greater than) are sometimes used instead of guillemets («, ») (used as quotation marks in many languages) when the proper characters are not available.

In comic books, chevrons are often used to mark dialogue that has been translated notionally from another language; in other words, if a character is speaking another language, instead of writing in the other language and providing a translation, one writes the translated text within chevrons. Of course, since no foreign language is actually written, this is only notionally translated.[citation needed]

Chevron-like symbols are part of standard Chinese, and Korean punctuation, where they generally enclose the titles of books: ︿ and ﹀ or ︽ and ︾ for traditional vertical printing, and 〈 and 〉 or 《 and 》 for horizontal printing. See also non-English usage of quotation marks.

In continuum mechanics, chevrons may be used as Macaulay brackets.

In East Asian punctuation, angle brackets are used as quotation marks.

Lenticular brackets

Some East Asian languages use lenticular brackets 【 】, a combination of square brackets and parentheses called 方頭括號 fāngtóu guāhào in Chinese and すみ付き sumitsuki in Japanese. They are used for inference[clarification needed] in Chinese and used in titles and headings in Japanese.

Floor and ceiling corners

The floor corner brackets ⌊ and ⌋, the ceiling corner brackets ⌈ and ⌉ are used to denote the integer floor and ceiling functions.

Quine corners and half brackets

The Quine corners ⌜ and ⌝ have at least two uses in mathematical logic: either as quasi-quotation, a generalization of quotation marks, or to denote the Gödel number of the enclosed expression.

Half brackets are used in English to mark added text, such as in translations: "Bill saw ⸤her⸥".

In editions of papyrological texts, half brackets, ⸤ and ⸥ or ⸢ and ⸣, enclose text which is lacking in the papyrus due to damage, but can be restored by virtue of another source, such as an ancient quotation of the text transmitted by the papyrus.[25] For example, Callimachus Iambus 1.2 reads: ἐκ τῶν ὅκου βοῦν κολλύ⸤βου π⸥ιπρήσκουσιν. A hole in the papyrus has obliterated βου π, but these letters are supplied by an ancient commentary on the poem. Second intermittent sources can be between ⸢ and ⸣. Quine corners are sometimes used instead of half brackets.[26]

Double brackets

Double brackets (or white square brackets), ⟦ ⟧, are used to indicate the semantic evaluation function in formal semantics for natural language and denotational semantics for programming languages.[27][28] The brackets stand for a function that maps a linguistic expression to its “denotation” or semantic value. Double brackets may also refer to the mathematical floor function.

Brackets with quills

Known as "spike parentheses" (Swedish: piggparenteser) ⁅ and ⁆ are used in Swedish dictionaries.[29]

Specific uses

Computing

The various bracket characters are frequently used in many programming languages as operators or for other syntax markup. For instance, in C-like languages, { and } are often used to delimit a code block, and the parameters of method calls are generally enclosed by ( and ).

In C, C++, Java and other C-derived languages—as well as in Scheme-influenced languages that have adopted C/Java syntax, such as JavaScript—the "{}" symbols are referred to as "braces" or "curly braces" and never as brackets. Since the term "brace" is documented in the definitive programming specifications for these languages, it is preferable to use the correct term brace so there is no confusion between the brace (used to denote compound statements) and the bracket, used to denote other concepts, such as array indices.[30][31]

Mathematics

In addition to the use of parentheses to specify the order of operations, both parentheses and brackets are used to denote an interval, also referred to as a half-open range. The notation [a,c) is used to indicate an interval from a to c that is inclusive of a but exclusive of c. That is, [5, 12) would be the set of all real numbers between 5 and 12, including 5 but not 12. The numbers may come as close as they like to 12, including 11.999 and so forth (with any finite number of 9s), but 12.0 is not included. In some European countries, the notation [5, 12[ is also used for this. The endpoint adjoining the bracket is known as closed, whereas the endpoint adjoining the parenthesis is known as open. If both types of brackets are the same, the entire interval may be referred to as closed or open as appropriate. Whenever +∞ or −∞ is used as an endpoint, it is normally considered open and adjoined to a parenthesis. See Interval (mathematics) for a more complete treatment.

In quantum mechanics, chevrons are also used as part of Dirac's formalism, bra–ket notation, to note vectors from the dual spaces of the Bra ⟨A| and the Ket |B⟩. Mathematicians will also commonly write ⟨a, b⟩ for the inner product of two vectors. In statistical mechanics, chevrons denote ensemble or time average. Chevrons are used in group theory to write group presentations, and to denote the subgroup generated by a collection of elements. Note that obtuse angled chevrons are not always (and even not by all users) distinguished from a pair of less-than and greater-than signs <>, which are sometimes used as a typographic approximation of chevrons.

In group theory and ring theory, brackets denote the commutator. In group theory, the commutator [g, h] is commonly defined as g −1h −1gh. In ring theory, the commutator [a, b] is defined as abba. Furthermore, in ring theory, braces denote the anticommutator where {a, b} is defined as ab + ba. The bracket is also used to denote the Lie derivative, or more generally the Lie bracket in any Lie algebra.

Various notations, like the vinculum have a similar effect to brackets in specifying order of operations, or otherwise grouping several characters together for a common purpose.

In the Z formal specification language, braces define a set and chevrons define a sequence.

Accounting

Traditionally in accounting, contra amounts are placed in parentheses. A debit balance account in a series of credit balances will have brackets and vice versa.

Law

Brackets are used in some countries in the citation of law reports to identify parallel citations to non-official reporters. For example: Chronicle Pub. Co. v. Superior Court, (1998) 54 Cal.2d 548, [7 Cal.Rptr. 109]. In some other countries (such as England and Wales), square brackets are used to indicate that the year is part of the citation and parentheses are used to indicate the year the judgment was given. For example, National Coal Board v England [1954] AC 403, is in the 1954 volume of the Appeal Cases reports although the decision may have been given in 1953 or earlier, whereas (1954) 98 Sol Jo 176 reports a decision from 1954, in volume 98 of the Solicitor's Journal which may be published in 1955 or later.

When quoted material is in any way altered, the alterations are enclosed in brackets within the quotation. For example: Plaintiff asserts his cause is just, stating, "[m]y causes is [sic] just." Although in the original quoted sentence the word "my" was capitalized, it has been modified in the quotation and the change signalled with brackets. Similarly, where the quotation contained a grammatical error, the quoting author signalled that the error was in the original with "[sic]" (Latin for 'thus'). (California Style Manual, section 4:59 (4th ed.))

Sports

Tournament brackets, the diagrammatic representation of the series of games played during a tournament usually leading to a single winner, are so named for their resemblance to brackets or braces.

Encoding in digital media

Representations of various kinds of brackets in Unicode and HTML are given below.

Usage Unicode SGML/HTML/XML entities Sample
General purpose[32] U+0028 Left parenthesis &#40; &lparen; (parentheses)
U+0029 Right parenthesis &#41; &rparen;
U+005B Left square bracket &#91; [sic]
U+005D Right square bracket &#93;
Technical/mathematical
(common)[32]
U+003C Less-than sign &#60; &lt; <HTML>
U+003E Greater-than sign &#62; &gt;
U+007B Left curly bracket &#123; {round, square, curly}
U+007D Right curly bracket &#125;
Quotation
(Western texts)[33][34]
U+00AB Left-pointing double angle quotation mark &#171; « French quote »
U+00BB Right-pointing double angle quotation mark &#187;
U+2039 Single left-pointing angle quotation mark &#8249; ‹ x ›
U+203A Single right-pointing angle quotation mark &#8250;
U+201C Left double quotation mark &#8220; “English quote”
U+201D Right double quotation mark &#8221;
U+2018 Left single quotation mark &#8216; ‘English quote’
U+2019 Right single quotation mark &#8217;
U+201A Single low-9 quotation mark &#8218; &sbquo; ‚German quote‘ or ‚Polish quote’
U+201E Double low-9 quotation mark &#8222; &bdquo; „German quote“ or „Polish quote”
Floor and ceiling functions[26] U+2308 Left ceiling &#8968; ceiling
U+2309 Right ceiling &#8969;
U+230A Left floor &#8970; floor
U+230B Right floor &#8971;
Quine corners[26] U+231C Top left corner &#8988; quasi-quotation
editorial notation
U+231D Top right corner &#8989;
U+231E Bottom left corner &#8990; editorial notation
U+231F Bottom right corner &#8991;
Technical/mathematical
(specialized)[26][35][36][37]
U+207D Superscript left parenthesis &#8317; X⁽²⁾
U+207E Superscript right parenthesis &#8318;
U+208D Subscript left parenthesis &#8333; X₍₂₎
U+208E Subscript right parenthesis &#8334;
U+239B Left parenthesis upper hook &#9115;


large parentheses

U+239C Left parenthesis extension &#9116;
U+239D Left parenthesis lower hook &#9117;
U+239E Right parenthesis upper hook &#9118;
U+239F Right parenthesis extension &#9119;
U+23A0 Right parenthesis lower hook &#9120;
U+23A1 Left square bracket upper corner &#9121;


large square brackets

U+23A2 Left square bracket extension &#9122;
U+23A3 Left square bracket lower corner &#9123;
U+23A4 Right square bracket upper corner &#9124;
U+23A5 Right square bracket extension &#9125;
U+23A6 Right square bracket lower corner &#9126;
U+23A7 Left curly bracket upper hook &#9127;


large curly brackets

U+23A8 Left curly bracket middle piece &#9128;
U+23A9 Left curly bracket lower hook &#9129;
U+23AB Right curly bracket upper hook &#9131;
U+23AC Right curly bracket middle piece &#9132;
U+23AD Right curly bracket lower hook &#9133;
U+23AA Curly bracket extension &#9130;
U+23B0 Upper left or lower right curly bracket section &#9136; ⎰            ⎱
⎱            ⎰
U+23B1 Upper right or lower left curly bracket section &#9137;
U+23B4 Top square bracket &#9140;
horizontal square brackets
U+23B5 Bottom square bracket &#9141;
U+23B6 Bottom square bracket over top square bracket &#9142;
t e r m i n a l
e m u l a t i o n
U+23B8 Left vertical box line &#9144; ⎸boxed text⎹
U+23B9 Right vertical box line &#9145;
U+23DC Top parenthesis &#9180;
horizontal parentheses
U+23DD Bottom parenthesis &#9181;
U+23DE Top curly bracket &#9182;
horizontal curly brackets
U+23DF Bottom curly bracket &#9183;
U+23E0 Top tortoise shell bracket &#9184;
tortoise shell brackets
U+23E1 Bottom tortoise shell bracket &#9185;
U+27C5 Left s-shaped bag delimiter &#10181; ⟅…⟆
U+27C6 Right s-shaped bag delimiter &#10182;
U+27D3 Lower right corner with dot &#10195; ⟓pullback…pushout⟔
U+27D4 Upper left corner with dot &#10196;
U+27E6 Mathematical left white square bracket &#10214; ⟦white square brackets⟧
U+27E7 Mathematical right white square bracket &#10215;
U+27E8 Mathematical left angle bracket &#10216; &lang;[e 1] a, b
U+27E9 Mathematical right angle bracket &#10217; &rang;[e 1]
U+27EA Mathematical left double angle bracket &#10218; A, B
U+27EB Mathematical right double angle bracket &#10219;
U+27EC Mathematical left white tortoise shell bracket &#10220; ⟬white tortoise shell brackets⟭
U+27ED Mathematical right white tortoise shell bracket &#10221;
U+27EE Mathematical left flattened parenthesis &#10222; ⟮flattened parentheses⟯
U+27EF Mathematical right flattened parenthesis &#10223;
U+2983 Left white curly bracket &#10627; ⦃white curly brackets⦄
U+2984 Right white curly bracket &#10628;
U+2985 Left white parenthesis &#10629; ⦅white/double parentheses⦆
U+2986 Right white parenthesis &#10630;
U+2987 Z notation left image bracket &#10631; RS
U+2988 Z notation right image bracket &#10632;
U+2989 Z notation left binding bracket &#10633; AB
U+298A Z notation right binding bracket &#10634;
U+298B Left square bracket with underbar &#10635; ⦋underlined square brackets⦌
U+298C Right square bracket with underbar &#10636;
U+298D Left square bracket with tick in top corner &#10637; ⦍ticked square brackets⦐
U+2990 Right square bracket with tick in top corner &#10640;
U+298E Right square bracket with tick in bottom corner &#10638; ⦏ticked square brackets⦎
U+298F Left square bracket with tick in bottom corner &#10639;
U+2991 Left angle bracket with dot &#10641; ⦑dotted angle brackets⦒
U+2992 Right angle bracket with dot &#10642;
U+2993 Left arc less-than bracket &#10643; inequality sign brackets⦔
U+2994 Right arc greater-than bracket &#10644;
U+2995 Double left arc greater-than bracket &#10645; ⦕inequality sign brackets⦖
U+2996 Double right arc less-than bracket &#10646;
U+2997 Left black tortoise shell bracket &#10647; ⦗black tortoise shell brackets⦘
U+2998 Right black tortoise shell bracket &#10648;
U+29D8 Left wiggly fence &#10712; ⧘…⧙
U+29D9 Right wiggly fence &#10713;
U+29DA Left double wiggly fence &#10714; ⧚…⧛
U+29DB Right double wiggly fence &#10715;
U+29FC Left-pointing curved angle bracket &#10748; ⧼…⧽
U+29FD Right-pointing curved angle bracket &#10749;
Half brackets[38] U+2E22 Top left half bracket &#11810; editorial notation
U+2E23 Top right half bracket &#11811;
U+2E24 Bottom left half bracket &#11812; editorial notation
U+2E25 Bottom right half bracket &#11813;
Dingbats[39] U+2768 Medium left parenthesis ornament &#10088; ❨medium parenthesis ornament❩
U+2769 Medium right parenthesis ornament &#10089;
U+276A Medium flattened left parenthesis ornament &#10090; ❪medium flattened parenthesis ornament❫
U+276B Medium flattened right parenthesis ornament &#10091;
U+276C Medium left-pointing angle bracket ornament &#10092; ❬medium angle bracket ornament❭
U+276D Medium right-pointing angle bracket ornament &#10093;
U+2770 Heavy left-pointing angle bracket ornament &#10096; ❰heavy angle bracket ornament❱
U+2771 Heavy right-pointing angle bracket ornament &#10097;
U+276E Heavy left-pointing angle quotation mark ornament &#10094; ❮heavy angle quotation ornament❯
U+276F Heavy right-pointing angle quotation mark ornament &#10095;
U+2772 Light left tortoise shell bracket ornament &#10098; ❲light tortoise shell bracket ornament❳
U+2773 Light right tortoise shell bracket ornament &#10099;
U+2774 Medium left curly bracket ornament &#10100; ❴medium curly bracket ornament❵
U+2775 Medium right curly bracket ornament &#10101;
Arabic[40] U+FD3E Ornate left parenthesis &#64830; ﴿العربية﴾‎
U+FD3F Ornate right parenthesis &#64831;
N'Ko[38] U+2E1C Left low paraphrase bracket &#11804; ⸜ߒߞߏ⸝
U+2E1D Right low paraphrase bracket &#11805;
Ogham[41] U+169B Ogham feather mark &#5787; ᚛ᚑᚌᚐᚋ᚜
U+169C Ogham reversed feather mark &#5788;
Old Hungarian U+2E42 Double low-reversed-9 quotation mark &#11842;
Tibetan[42] U+0F3A Tibetan mark gug rtags gyon &#3898; ༺དབུ་ཅན་༻
U+0F3B Tibetan mark gug rtags gyas &#3899;
U+0F3C Tibetan mark ang khang gyon &#3900; ༼༡༢༣༽
U+0F3D Tibetan mark ang khang gyas &#3901;
New Testament editorial marks[38] U+2E02 Left substitution bracket &#11778; ⸂…⸃
U+2E03 Right substitution bracket &#11779;
U+2E04 Left dotted substitution bracket &#11780; ⸄…⸅
U+2E05 Right dotted substitution bracket &#11781;
U+2E09 Left transposition bracket &#11785; ⸉…⸊
U+2E0A Right transposition bracket &#11786;
U+2E0C Left raised omission bracket &#11788; ⸌…⸍
U+2E0D Right raised omission bracket &#11789;
Medieval studies[34][38] U+2045 Left square bracket with quill &#8261; ⁅…⁆
U+2046 Right square bracket with quill &#8262;
U+2E26 Left sideways u bracket &#11814; ⸦crux⸧
U+2E27 Right sideways u bracket &#11815;
U+2E28 Left double parenthesis &#11816; ⸨…⸩
U+2E29 Right double parenthesis &#11817;
Quotation
(East-Asian texts)[43]
U+3014 Left tortoise shell bracket &#12308; 〔…〕
U+3015 Right tortoise shell bracket &#12309;
U+3016 Left white lenticular bracket &#12310; 〖…〗
U+3017 Right white lenticular bracket &#12311;
U+3018 Left white tortoise shell bracket &#12312; 〘…〙
U+3019 Right white tortoise shell bracket &#12313;
U+301A Left white square bracket &#12314; 〚…〛
U+301B Right white square bracket &#12315;
U+301D Reversed double prime quotation mark &#12317; 〝…〞
U+301E Double prime quotation mark &#12318;[e 2]
Quotation
(halfwidth East-Asian texts)[26][44]
U+2329 Left-pointing angle bracket &#9001; &lang;[e 1] 〈deprecated〉
U+232A Right-pointing angle bracket &#9002; &rang;[e 1]
U+FF62 Halfwidth left corner bracket &#65378; 「カタカナ」
U+FF63 Halfwidth right corner bracket &#65379;
Quotation
(fullwidth East-Asian texts)[43]
U+3008 Left angle bracket &#12296; 〈한〉
U+3009 Right angle bracket &#12297;
U+300A Left double angle bracket &#12298; 《한》
U+300B Right double angle bracket &#12299;
U+300C Left corner bracket &#12300; 「白八櫨」
U+300D Right corner bracket &#12301;
U+300E Left white corner bracket &#12302; 『カタカナ』
U+300F Right white corner bracket &#12303;
U+3010 Left black lenticular bracket &#12304; 【ひらがな】
U+3011 Right black lenticular bracket &#12305;
General purpose
(fullwidth East-Asian)[44]
U+FF08 Fullwidth left parenthesis &#65288; (Wiki)
U+FF09 Fullwidth right parenthesis &#65289;
U+FF3B Fullwidth left square bracket &#65339; sic
U+FF3D Fullwidth right square bracket &#65341;
Technical/mathematical
(fullwidth East-Asian)[44]
U+FF1C Fullwidth less-than sign &#65308; <HTML>
U+FF1E Fullwidth greater-than sign &#65310;
U+FF5B Fullwidth left curly bracket &#65371; {1、2}
U+FF5D Fullwidth right curly bracket &#65373;
U+FF5F Fullwidth left white parenthesis &#65375; ⦅…⦆
U+FF60 Fullwidth right white parenthesis &#65376;
  1. ^ a b c d &lang; and &rang; were tied to the deprecated symbols U+2329 and U+232A in HTML4 and MathML2, but are being migrated to U+27E8 and U+27E9 for HTML5 and MathML3, as defined in XML Entity Definitions for Characters.
  2. ^ This is fullwidth version of U+2033 DOUBLE PRIME. In vertical texts, U+301F LOW DOUBLE PRIME QUOTATION MARK is preferred.

Braces (curly brackets) first became part of a character set with the 8-bit code of the IBM 7030 Stretch.[45]

The angle brackets or chevrons at U+27E8 and U+27E9 are for mathematical use and Western languages, whereas U+3008 and U+3009 are for East Asian languages. The chevrons at U+2329 and U+232A are deprecated in favour of the U+3008 and U+3009 East Asian angle brackets. Unicode discourages their use for mathematics and in Western texts,[26] because they are canonically equivalent to the CJK code points U+300x and thus likely to render as double-width symbols. The less-than and greater-than symbols are often used as replacements for chevrons.

See also



This article uses material from the Wikipedia article "Angle bracket", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD