Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 4.0 (Amin).
A toilet[n 1] is a piece of hardware used for the collection or disposal of human urine and feces. In other words: "Toilets are sanitation facilities at the user interface that allow the safe and convenient urination and defecation".[1] Toilets can be with or without flushing water (flush toilet or dry toilet). They can be set up for a sitting posture or for a squatting posture (squat toilet). Flush toilets are usually connected to a sewer system in urban areas and to septic tanks in less built-up areas. Dry toilets are connected to a pit, removable container, composting chamber or other storage and treatment device. Toilets are commonly made of ceramic (porcelain), concrete, plastic or wood.
In private homes, the toilet, sink, bath or shower may be in the same room. Another option is to have one room for body washing (bathroom) and a separate room for the toilet and handwashing sink (toilet room). Public toilets consist of one or more toilets (and commonly urinals) which are available for use by the general public. Portable toilets or chemical toilets may be brought in for large but temporary gatherings.
Many poor households in developing countries use very basic, and often unhygienic toilets, for example simple pit latrines and bucket toilets which are usually placed in outhouses. Globally, nearly one billion people even have no access to a toilet at all, and are forced to do open defecation (particularly in India).[2] Diseases transmitted via the fecal-oral route or via water, such as cholera and diarrhea can be spread by open defecation. They can also be spread by unsafe toilets which cause pollution of surface water or groundwater. Historically, sanitation has been a concern from the earliest stages of human settlements. The Sustainable Development Goal Number 6 calls for "adequate and equitable sanitation and hygiene for all and end open defecation by 2030".[2]
A typical flush toilet is a ceramic bowl (pan) connected on the "up" side to a cistern (tank) that enables rapid filling with water, and on the "down" side to a drain pipe that removes the effluent. When a toilet is flushed, the sewage should flow into a septic tank or into a system connected to a sewage treatment plant. However, in many developing countries, this treatment step does not take place.
The water in the toilet bowl is connected to a pipe shaped like an upside-down U. One side of the U channel is arranged as a siphon tube longer than the water in the bowl is high. The siphon tube connects to the drain. The bottom of the drain pipe limits the height of the water in the bowl before it flows down the drain. The water in the bowl acts as a barrier to sewer gas entering the building. Sewer gas escapes through a vent pipe attached to the sewer line.
The amount of water used by conventional flush toilets usually makes up a significant portion of personal daily water usage. However, modern low flush toilet designs allow the use of much less water per flush. Dual flush toilets allow the user to select between a flush for urine or feces, saving a significant amount of water over conventional units. The flush handle on these toilets is pushed up for one kind of flush and down for the other.[3] In some places, users are encouraged not to flush after urination. Flush toilets can be plumbed to use greywater (previously used for washing dishes, laundry and bathing) rather than potable water (drinking water). Some modern toilets pressurize the water in the tank, which initiates flushing action with less water usage.
Another variant is the pour-flush toilet (often a type of pit latrine).[1] This type of flush toilet has no cistern, but is flushed manually with a few litres of a small bucket. This type of low-cost toilet is common in many Asian countries. It can use as little as 2–3 litres, and this can be greywater or rainwater.[1]
Flush toilets, when used on ships, are typically flushed with seawater.
"High-tech" toilets include features such as: automatic-flushing mechanisms; water jets or "bottom washers"; blow dryers; or artificial flush sounds to mask noises. Others include medical monitoring features such as urine and stool analysis and the checking of blood pressure, temperature, and blood sugar. Some toilets have automatic lid operation, heated seats, deodorizing fans or automated replacement of paper toilet-seat-covers. Interactive urinals have been developed in several countries, allowing users to play video games. The "Toylet", produced by Sega, uses pressure sensors to detect the flow of urine and translates that into on-screen action.[4]
Astronauts on the International Space Station use a space toilet with urine diversion which can recover potable water.[5]
A vacuum toilet is a flush toilet that requires very little flushing water and is connected to a vacuum sewer system. For example, they are used on planes (aircraft lavatories) and on trains (passenger train toilets).
Many types of toilets without a water seal (also called dry toilets or "non-flush toilets") exist. These types of toilets do not use water as an odor seal or to move excreta along. For example, from simple to more complex: a bucket toilet (honey bucket), a tree bog or arborloo (two simple systems for converting excrement to direct fertiliser for trees), a pit latrine (a deep hole in the ground), a vault toilet (which keeps all the waste underground until it is pumped out), a container-based toilet, a composting toilet (which mixes excreta with carbon-rich materials for faster decomposition), a urine-diverting dry toilet (which keeps urine separate from feces), and incinerating and freezing toilets.
Dry toilets use no water for flushing. They also do not produce wastewater. Some of these devices are high-tech but many are quite basic.[6]
A simple pit latrine uses no water seal and collects human excreta in a pit or trench. This type of toilet can range from a simple slit trench to more elaborate systems with seating or squatting pans and ventilation systems. In developed countries they are associated with camping and wilderness areas, whereas they are common in rural or peri-urban areas of much of the developing world. Pit latrines are used in emergency situations.
The pit or trench can be dug large enough so that the pit can be used for many years before it fills up. When the pit becomes full, it may be emptied or the hole covered with earth and the pit latrine relocated. Pit latrines have to be located away from drinking water sources (wells, streams, etc.) to minimize the possibility of disease spread via groundwater pollution.
A ventilation improved pit (VIP) latrine adds certain design features to the simple pit latrine which reduces flies from exiting the latrine, thereby reducing the spread of diseases.[1]
A vault toilet is a non-flush toilet with a sealed container (or vault) buried in the ground to receive the excreta, all of which is contained underground until it is removed by pumping. A vault toilet is distinguished from a pit latrine because the waste accumulates in the vault instead of seeping into the underlying soil.
Urine diversion toilets have two compartments, one for urine and one for feces. A urine-diverting dry toilet uses no water for flushing, and keeps urine and feces separate. It can be linked to systems which reuse excreta as a fertilizer.
The portable toilet is used on construction sites, film locations, and large outdoor gatherings where there are no other facilities. They are typically self-contained units that are made to be easily moved. Most portable toilets are Unisex single units with privacy ensured by a simple lock on the door. The units are usually light weight and easily transported by a flatbed truck and loaded and unloaded by a small forklift. Many portable toilets are small molded plastic or fiberglass portable rooms with a lockable door and a receptacle to catch waste in a chemically treated container. If used for an extended period of time, they have to be cleaned out and new chemicals put in the waste receptacle. For servicing multiple portable toilets, tanker trucks (vacuum trucks or honeywagons) are equipped with large vacuums to evacuate the waste and replace the chemicals. Portable toilets can also be urine-diverting dry toilets.
A bucket toilet, also known as a honey bucket, is a very simple type of portable toilet.
Chemical toilets collect human excreta in a holding tank and use chemicals to minimize odors. They do not require a connection to a water supply and are used in a variety of situations.
Aircraft lavatories and passenger train toilets were in the past often designed as chemical toilets but are nowadays more likely to be vacuum toilets.[citation needed]
Toilets can be designed to be used either in a sitting or in a squatting posture.
Sitting toilets are often referred to as "western-style toilets".[7] Sitting toilets are more convenient than squat toilets for people with disabilities and the elderly.
A squat toilet (also called "squatting toilet", "natural position toilet", or by many national names) is a toilet of any technology type (i.e. pit latrine, urine-diverting dry toilet, flush toilet etc.) which is used in a Squatting position rather than sitting. This means that the Defecation posture used is to place one foot on each side of the toilet drain or hole and to squat over it.
Squatting toilets are the norm in many Asian and African countries, but can also occasionally be found in some European and South American countries. They are common in most Muslim countries. They can be used in conjunction with anal cleansing with water in accordance with Islamic toilet etiquette.
In 1976, squatting toilets were said to be used by the majority of the world's population.[8] However, there is a general trend in many countries to move from squatting toilets to sitting toilets (particularly in urban areas) as the latter are often regarded as more modern.[9]
|
In the Western world, the most common method of cleaning the anal area after defecation is by toilet paper or sometimes by using a bidet. In many Muslim countries, the faciliites are designed to enable people to follow Islamic toilet etiquette Qaḍāʼ al-Ḥājah.[11] For example, a bidet shower may be plumbed in. The left hand is used for cleansing, for which reason that hand is considered impolite or polluted in many Asian countries.[12]
There are toilets on the market where the seats have integrated spray mechanicms for anal and genital water sprays (see for example Toilets in Japan). This can be useful for the elderly or people with disabilities.
A public toilet is accessible to the general public. It may be municipally owned or managed, entered directly from the street. It may be within a building that, while privately owned, allows public access, such as a department store, or it may be limited to the business's customers, such as a restaurant. If its use requires a fee, it is also called a pay toilet.
Depending on culture, there may be varying degrees of separation between men and women and different levels of privacy. Typically, the entire room, or a stall or cubicle containing a toilet, is lockable. Urinals, if present in a men's toilet, are typically mounted on a wall with or without a divider between them. In the most basic form, a public toilet may be not much more than an open latrine. Another form is a street urinal known as a pissoir, after the French term.
To this day, 1 billion people in developing countries have no toilets in their homes and are resorting to Open defecation instead.[13] The Joint Monitoring Programme (JMP) for Water Supply and Sanitation by WHO and UNICEF is the official United Nations mechanism tasked with monitoring progress towards the Millennium Development Goal relating to drinking-water and sanitation (MDG 7, Target 7c). One target of this goal is to: "Halve, by 2015, the proportion of people without sustainable access to safe drinking-water and basic sanitation" and publishes figures on access to sanitation worldwide on a regular basis.[14] Another organisation which focuses on toilet and sanitation is the World Toilet Organisation which has its founding date, November 19, used for the UN's International World Toilet Day.[15]
Toilets are one important element of a sanitation system, although other elements are also needed: transport, treatment, disposal or reuse.[1] Diseases, including Cholera, which still affects some 3 million people each year, can be largely prevented when effective sanitation and water treatment prevents fecal matter from contaminating waterways, groundwater and drinking water supplies.
There have been five main Cholera outbreaks and pandemics since 1825. In London alone, the second killed 14,137 people in 1849, and the third took 10,738 lives in 1853–54. In 1849 the English physician John Snow published a paper On the Mode of Communication of Cholera, in which he suggested that cholera might be waterborne. During the 1854 epidemic, he collected and analyzed data establishing that people who drank water from contaminated sources such as the Broad Street pump died of cholera at much higher rates than those who got water elsewhere.
A floating toilet is essentially a toilet on a platform built above or floating on the water. Instead of excreta going into the ground they are collected in a tank or barrel. To reduce the amount of excreta that needs to hauled to shore, many use urine diversion. The floating toilet was developed for residents without quick access to land or connection to a sewer systems.[17] It is also used in areas subjected to prolonged flooding.[18] The need for this type of toilet is high in areas like Cambodia.[19]
The pig toilet, which consists of a toilet linked to a pigsty by a chute, is still in use to a limited extent.[20] It was common in rural China, and was known in Japan, Korea, and India. The "fish pond toilet" depends on the same principle, of livestock (often carp) eating human excreta directly.
During the third millennium BC, toilets and sewers were invented throughout the world. Mohenjo-Daro circa 2800 BC is cited as having some of the most advanced, with toilets built into outer walls of homes. These toilets were Western-style, albeit a primitive form, with vertical chutes, via which waste was disposed of into cesspits or street drains.[21]
These toilets were only used by the affluent classes; most people would have squatted over old pots set into the ground or used open pits.[22] The people of the Harappan civilization in Pakistan and northwestern India had primitive water-cleaning toilets that used flowing water in each house that were linked with drains covered with burnt clay bricks. The flowing water removed the human waste.[23] The Indus Valley civilisation had a rudimentary network of sewers built under grid pattern streets.[24]
Other very early toilets that used flowing water to remove the waste are found at Skara Brae in Orkney, Scotland, which was occupied from about 3100 BC until 2500 BC. Some of the houses there have a drain running directly beneath them, and some of these had a cubicle over the drain. Around the 18th century BC, toilets started to appear in Minoan Crete, Pharaonic Egypt, and ancient Persia.
In 2012, archaeologists found what is believed to be Southeast Asia's earliest latrine during the excavation of a neolithic village in the Rạch Núi archaeological site, southern Vietnam. The toilet, dating back 1500 BC, yielded important clues about early Southeast Asian society. More than 30 coprolites, containing fish and shattered animal bones, provided information on the diet of humans and dogs, and on the types of parasites each had to contend with.[25][26][27]
In Roman civilization, toilets using flowing water were sometimes part of public bath houses. Roman toilets, like the ones pictured here, are commonly thought to have been used in the sitting position. The Roman toilets were probably elevated to raise them above open sewers which were periodically "flushed" with flowing water, rather than elevated for sitting. Romans and Greeks also used chamber pots, which they brought to meals and drinking sessions.[28] Johan J. Mattelaer said, "Plinius has described how there were large receptacles in the streets of cities such as Rome and Pompeii into which chamber pots of urine were emptied. The urine was then collected by fullers." (Fulling was a vital step in Textile manufacture.)
The Han dynasty in China two thousand years ago used pig toilets.
Garderobes were toilets used in the Post-classical history, most commonly found in upper-class dwellings. Essentially, they were flat pieces of wood or stone spanning from one wall to the other, with one or more holes to sit on. These were above chutes or pipes that discharged outside the castle or Manor house.[29] Garderobes would be placed in areas away from bedrooms to shun the smell[30] and also near kitchens or fireplaces to keep the enclosure warm.[29]
|
The other main way of handling toilet needs was the chamber pot, a receptacle, usually of ceramic or metal, into which one would excrete waste. This method was used for hundreds of years; shapes, sizes, and decorative variations changed throughout the centuries.[31] Chamber pots were in common use in Europe from ancient times, even being taken to the Middle East by medieval pilgrims.[32]
By the Early Modern era, chamber pots were frequently made of china or copper and could include elaborate decoration. They were emptied into the gutter of the street nearest to the home.
In pre-modern Denmark, people generally defecated on farmland or other places where the human waste could be collected as fertilizer.[33] The Old Norse language had several terms for referring to outhouses, including garðhús (yard house), náð-/náða-hús (house of rest), and annat hús (the other house). In general, toilets were functionally non-existent in rural Denmark until the 18th century.[33]
By the 16th century, cesspits and cesspools were increasingly dug into the ground near houses in Europe as a means of collecting waste, as urban populations grew and street gutters became blocked with the larger volume of human waste. Rain was no longer sufficient to wash away waste from the gutters. A pipe connected the latrine to the cesspool, and sometimes a small amount of water washed waste through. Cesspools were cleaned out by tradesmen, who pumped out liquid waste, then shovelled out the solid waste and collected it during the night. This solid waste, euphemistically known as Nightsoil, was sold as fertilizer for agricultural production (similarly to the closing-the-loop approach of ecological sanitation).
The garderobe was replaced by the Privy midden and Pail closet in early industrial Europe.[34]
In the early 19th century, public officials and public hygiene experts studied and debated sanitation for several decades. The construction of an underground network of pipes to carry away solid and liquid waste was only begun in the mid 19th-century, gradually replacing the cesspool system, although cesspools were still in use in some parts of Paris into the 20th century.[35]
Even London, at that time the world's largest city, did not require indoor toilets in its building codes until after the First World War.
Before the introduction of indoor toilets, it was common to use the chamber pot under one's bed at night and then to dispose of its contents in the morning. During the Victorian era, British housemaids collected all of the household's chamber pots and carried them to a room known as the housemaids' cupboard. This room contained a "slop sink", made of wood with a lead lining to prevent chipping china chamber pots, for washing the "bedroom ware" or "chamber utensils". Once running water and flush toilets were plumbed into British houses, servants were sometimes given their own lavatory downstairs, separate from the family lavatory.[36] The practice of emptying one's own chamber pot, known as Slopping out, continued in British prisons until recently[year needed] and is still in use in the Republic of Ireland.[year needed]
With rare exceptions, chamber pots are no longer used. Modern related implements are bedpans and commodes, used in hospitals and the homes of invalids.
Before the flush toilet became as popular as it is, there were inventors, scientists, and public health officials in Europe who supported the use of "dry earth closets". One person developing these was the English clergyman Henry Moule, who dedicated his life to improving public sanitation after witnessing the horrors of the cholera epidemics of 1849 and 1854. He invented what he called the dry earth system, somewhat similar to a composting toilet or a bucket toilet. In partnership with James Bannehr, in 1860 he took out a patent for the process (No. 1316).[37]
His system was adopted in private houses, in rural districts, in military camps, in many hospitals, and extensively in the British Raj.[37]
Ultimately, however, it failed to gain the same public support in Europe as the water closet, although variations of the design remain today in use (see dry toilet).
Although a precursor to the flush toilet system which is widely used nowadays was designed in 1596 by John Harington,[38] such systems did not come into widespread use until the late nineteenth century.[39] With the onset of the industrial revolution and related advances in technology, the flush toilet began to emerge into its modern form. A crucial advance in plumbing, was the S-trap, invented by the Scottish mechanic Alexander Cummings in 1775, and still in use today. This device uses the standing water to seal the outlet of the bowl, preventing the escape of foul air from the sewer. It was only in the mid-19th century, with growing levels of urbanisation and industrial prosperity, that the flush toilet became a widely used and marketed invention. This period coincided with the dramatic growth in the sewage system, especially in London, which made the flush toilet particularly attractive for health and sanitation reasons.
Flush toilets were also known as "water closets", as opposed to the earth closets described above. WCs first appeared in Britain in the 1880s, and soon spread to Continental Europe. In America, the chain-pull indoor toilet was introduced in the homes of the wealthy and in hotels in the 1890s. William Elvis Sloan invented the Flushometer in 1906, which used pressurized water directly from the supply line for faster recycle time between flushes.
Toilet was originally a French loanword (first attested in 1540) that referred to the toilette ("little cloth") draped over one's shoulders during hairdressing.[41] During the late 17th century,[41] the term came to be used by metonymy in both languages for the whole complex of grooming and body care that centered at a dressing table (also covered by a cloth) and for the equipment composing a toilet service, including a mirror, hairbrushes, and containers for powder and makeup. The time spent at such a table also came to be known as one's "toilet"; it came to be a period during which close friends or tradesmen were received as "toilet-calls".[41][44]
The use of "toilet" to describe a special room for grooming came much later (first attested in 1819), following the French cabinet de toilet. Similar to "powder room", "toilet" then came to be used as a euphemism for rooms dedicated to urination and defecation, particularly in the context of signs for public toilets, as on trains. Finally, it came to be used for the plumbing fixtures in such rooms (apparently first in the United States) as these replaced chamber pots, outhouses, and latrines. These two uses, the fixture and the room, completely supplanted the other senses of the word during the 20th century[41] except in the form "toiletries".[n 2]
The word "toilet", for the plumbing fixture or for the room, is considered impolite in some varieties of English, while elsewhere the word is used without any embarrassment. "Toilet" was by etymology a euphemism, but is no longer understood as such. As old euphemisms have become the standard term, they have been progressively replaced by newer ones, an example of the euphemism treadmill at work.[45] The choice of word relies not only on regional variation, but also on social situation and level of formality (register) or social class. American manufacturers show an uneasiness with the word and its class attributes: American Standard, the largest firm, sells them as "toilets", yet the higher priced products of the Kohler Company, often installed in more expensive housing, are sold as commodes or closets, words which also carry other meanings. Confusingly, products imported from Japan such as TOTO are referred to as "toilets", even though they carry the cachet of higher cost and quality. (Toto, an abbreviation of Tōyō Tōki (東洋陶器 Oriental Ceramics), is used in Japanese comics to visually indicate toilets or other things that look like toilets; see Toilets in Japan.)
Different dialects use "bathroom" and "restroom" (American English), "bathroom" and "washroom" (Canadian English), and "WC" (an initialism for "water closet"), "lavatory" and its abbreviation "lav" (British English).
"Crapper" was already in use as a coarse name for a toilet, but it gained currency from the work of Thomas Crapper, who popularized flush toilets in England.
"The Jacks" is Irish slang for toilet.[46] It perhaps derives from "jacques" and "jakes", an old English term.[47]
"Loo" – The etymology of loo is obscure. The Oxford English Dictionary notes the 1922 appearance of "How much cost? Waterloo. Watercloset." in James Joyce's novel Ulysses and defers to Alan S. C. Ross's arguments that it derived in some fashion from the site of Napoleon's 1815 defeat.[48][49] In the 1950s the use of the word "loo" was considered one of the markers of British upper-class speech, featuring in a famous essay, "U and non-U English".[50] "Loo" may have derived from a corruption of French l'eau ("water"), gare à l'eau ("mind the water", used in reference to emptying chamber pots into the street from an upper-story window), lieu ("place"), lieu d'aisance ("place of ease", used euphemistically for a toilet), or lieu à l'anglaise ("English place", used from around 1770 to refer to English-style toilets installed for travelers).[48][51][52] Other proposed etymologies include a supposed tendency to place toilets in room 100 (hence "loo") in English hotels,[53] a dialectical corruption of the nautical term "lee" in reference to the need to urinate and defecate with the wind prior to the advent of head pumps,[n 3] or the 17th-century preacher Louis Bourdaloue, whose long sermons at Paris's Saint-Paul-Saint-Louis prompted his parishioners to bring along chamber pots.[54]
|
Wikivoyage has travel information for Toilets. |
This article uses material from the Wikipedia article "Toilet", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted