powered by CADENAS

Social Share

DC-to-DC converter (9302 views - Electronics & PCB)

A DC-to-DC converter is an electronic circuit or electromechanical device that converts a source of direct current (DC) from one voltage level to another. It is a type of electric power converter. Power levels range from very low (small batteries) to very high (high-voltage power transmission).
Go to Article

Explanation by Hotspot Model

DC-to-DC converter

DC-to-DC converter

A DC-to-DC converter is an electronic circuit or electromechanical device that converts a source of direct current (DC) from one voltage level to another. It is a type of electric power converter. Power levels range from very low (small batteries) to very high (high-voltage power transmission).

History

Before the development of power semiconductors and allied technologies, one way to convert the voltage of a DC supply to a higher voltage, for low-power applications, was to convert it to AC by using a vibrator, followed by a step-up transformer and rectifier.[1][2] For higher power an electric motor was used to drive a generator of the desired voltage (sometimes combined into a single "dynamotor" unit, a motor and generator combined into one unit, with one winding driving the motor and the other generating the output voltage). These were relatively inefficient and expensive procedures used only when there was no alternative, as to power a car radio (which then used thermionic valves/tubes requiring much higher voltages than available from a 6 or 12 V car battery).[1] The introduction of power semiconductors and integrated circuits made it economically viable to use techniques as described below, for example to convert the DC power supply to high-frequency AC, use a transformer—small, light, and cheap due to the high frequency—to change the voltage, and rectify back to DC.[3] Although by 1976 transistor car radio receivers did not require high voltages, some amateur radio operators continued to use vibrator supplies and dynamotors for mobile transceivers requiring high voltages, although transistorised power supplies were available.[4]

While it was possible to derive a lower voltage from a higher with a linear electronic circuit, or even a resistor, these methods dissipated the excess as heat; energy-efficient conversion only became possible with solid-state switch-mode circuits.

Uses

DC to DC converters are used in portable electronic devices such as cellular phones and laptop computers, which are supplied with power from batteries primarily. Such electronic devices often contain several sub-circuits, each with its own voltage level requirement different from that supplied by the battery or an external supply (sometimes higher or lower than the supply voltage). Additionally, the battery voltage declines as its stored energy is drained. Switched DC to DC converters offer a method to increase voltage from a partially lowered battery voltage thereby saving space instead of using multiple batteries to accomplish the same thing.

Most DC to DC converter circuits also regulate the output voltage. Some exceptions include high-efficiency LED power sources, which are a kind of DC to DC converter that regulates the current through the LEDs, and simple charge pumps which double or triple the output voltage.

DC to DC converters developed to maximize the energy harvest for photovoltaic systems and for wind turbines are called power optimizers.

Transformers used for voltage conversion at mains frequencies of 50–60 Hz must be large and heavy for powers exceeding a few watts. This makes them expensive, and they are subject to energy losses in their windings and due to eddy currents in their cores. DC-to-DC techniques that use transformers or inductors work at much higher frequencies, requiring only much smaller, lighter, and cheaper wound components. Consequently these techniques are used even where a mains transformer could be used; for example, for domestic electronic appliances it is preferable to rectify mains voltage to DC, use switch-mode techniques to convert it to high-frequency AC at the desired voltage, then, usually, rectify to DC. The entire complex circuit is cheaper and more efficient than a simple mains transformer circuit of the same output.

Electronic conversion

Practical electronic converters use switching techniques. Switched-mode DC-to-DC converters convert one DC voltage level to another, which may be higher or lower, by storing the input energy temporarily and then releasing that energy to the output at a different voltage. The storage may be in either magnetic field storage components (inductors, transformers) or electric field storage components (capacitors). This conversion method can increase or decrease voltage. Switching conversion is more power efficient (often 75% to 98%) than linear voltage regulation, which dissipates unwanted power as heat. Fast semiconductor device rise and fall times are required for efficiency; however, these fast transitions combine with layout parasitic effects to make circuit design challenging.[5] The higher efficiency of a switched-mode converter reduces the heatsinking needed, and increases battery endurance of portable equipment. Efficiency has improved since the late 1980s due to the use of power FETs, which are able to switch more efficiently with lower switching losses at higher frequencies than power bipolar transistors, and use less complex drive circuitry. Another important improvement in DC-DC converters is replacing the flywheel diode by synchronous rectification[6] using a power FET, whose "on resistance" is much lower, reducing switching losses. Before the wide availability of power semiconductors, low-power DC-to-DC synchronous converters consisted of an electro-mechanical vibrator followed by a voltage step-up transformer feeding a vacuum tube or semiconductor rectifier, or synchronous rectifier contacts on the vibrator.

Most DC-to-DC converters are designed to move power in only one direction, from dedicated input to output. However, all switching regulator topologies can be made bidirectional and able to move power in either direction by replacing all diodes with independently controlled active rectification. A bidirectional converter is useful, for example, in applications requiring regenerative braking of vehicles, where power is supplied to the wheels while driving, but supplied by the wheels when braking.

Although they require few components, switching converters are electronically complex. Like all high-frequency circuits, their components must be carefully specified and physically arranged to achieve stable operation and to keep switching noise (EMI / RFI) at acceptable levels[7]. Their cost is higher than linear regulators in voltage-dropping applications, but their cost has been decreasing with advances in chip design.

DC-to-DC converters are available as integrated circuits (ICs) requiring few additional components. Converters are also available as complete hybrid circuit modules, ready for use within an electronic assembly.

Linear regulators which are used to output a stable DC independent of input voltage and output load from a higher but less stable input by dissipating excess volt-amperes as heat, could be described literally as DC-to-DC converters, but this is not usual usage. (The same could be said of a simple voltage dropper resistor, whether or not stabilised by a following voltage regulator or Zener diode.)

There are also simple capacitive voltage doubler and Dickson multiplier circuits using diodes and capacitors to multiply a DC voltage by an integer value, typically delivering only a small current.

Magnetic

In these DC-to-DC converters, energy is periodically stored within and released from a magnetic field in an inductor or a transformer, typically within a frequency range of 300 kHz to 10 MHz. By adjusting the duty cycle of the charging voltage (that is, the ratio of the on/off times), the amount of power transferred to a load can be more easily controlled, though this control can also be applied to the input current, the output current, or to maintain constant power. Transformer-based converters may provide isolation between input and output. In general, the term DC-to-DC converter refers to one of these switching converters. These circuits are the heart of a switched-mode power supply. Many topologies exist. This table shows the most common ones.

Forward (energy transfers through the magnetic field) Flyback (energy is stored in the magnetic field)
No transformer (non-isolated)
  • Step-down (buck) - The output voltage is lower than the input voltage, and of the same polarity.
  • Non-inverting: The output voltage is the same polarity as the input.
    • Step-up (boost) - The output voltage is higher than the input voltage.
    • SEPIC - The output voltage can be lower or higher than the input.
  • Inverting: the output voltage is of the opposite polarity as the input.
  • True buck-boost - The output voltage is the same polarity as the input and can be lower or higher.
  • Split-pi (boost-buck) - Allows bidirectional voltage conversion with the output voltage the same polarity as the input and can be lower or higher.
With transformer (isolatable)

In addition, each topology may be:

Hard switched
Transistors switch quickly while exposed to both full voltage and full current
Resonant
An LC circuit shapes the voltage across the transistor and current through it so that the transistor switches when either the voltage or the current is zero

Magnetic DC-to-DC converters may be operated in two modes, according to the current in its main magnetic component (inductor or transformer):

Continuous
The current fluctuates but never goes down to zero
Discontinuous
The current fluctuates during the cycle, going down to zero at or before the end of each cycle

A converter may be designed to operate in continuous mode at high power, and in discontinuous mode at low power.

The half bridge and flyback topologies are similar in that energy stored in the magnetic core needs to be dissipated so that the core does not saturate. Power transmission in a flyback circuit is limited by the amount of energy that can be stored in the core, while forward circuits are usually limited by the I/V characteristics of the switches.

Although MOSFET switches can tolerate simultaneous full current and voltage (although thermal stress and electromigration can shorten the MTBF), bipolar switches generally can't so require the use of a snubber (or two).

High-current systems often use multiphase converters, also called interleaved converters.[8][9][10] Multiphase regulators can have better ripple and better response times than single-phase regulators.[11]

Many laptop and desktop motherboards include interleaved buck regulators, sometimes as a voltage regulator module.[12]

Capacitive

Switched capacitor converters rely on alternately connecting capacitors to the input and output in differing topologies. For example, a switched-capacitor reducing converter might charge two capacitors in series and then discharge them in parallel. This would produce the same output power (less that lost to efficiency of under 100%) at, ideally, half the input voltage and twice the current. Because they operate on discrete quantities of charge, these are also sometimes referred to as charge pump converters. They are typically used in applications requiring relatively small currents, as at higher currents the increased efficiency and smaller size of switch-mode converters makes them a better choice.[13] They are also used at extremely high voltages, as magnetics would break down at such voltages.

Electromechanical conversion

A motor-generator set, mainly of historical interest, consists of an electric motor and generator coupled together. A dynamotor combines both functions into a single unit with coils for both the motor and the generator functions wound around a single rotor; both coils share the same outer field coils or magnets.[4] Typically the motor coils are driven from a commutator on one end of the shaft, when the generator coils output to another commutator on the other end of the shaft. The entire rotor and shaft assembly is smaller in size than a pair of machines, and may not have any exposed drive shafts.

Motor-generators can convert between any combination of DC and AC voltage and phase standards. Large motor-generator sets were widely used to convert industrial amounts of power while smaller units were used to convert battery power (6, 12 or 24 V DC) to a high DC voltage, which was required to operate vacuum tube (thermionic valve) equipment.

For lower-power requirements at voltages higher than supplied by a vehicle battery, vibrator or "buzzer" power supplies were used. The vibrator oscillated mechanically, with contacts that switched the polarity of the battery many times per second, effectively converting DC to square wave AC, which could then be fed to a transformer of the required output voltage(s).[1] It made a characteristic buzzing noise.

Electrochemical conversion

A further means of DC to DC conversion in the kilowatts to megawatts range is presented by using redox flow batteries such as the vanadium redox battery.

Chaotic behavior

DC-to-DC converters are subject to different types of chaotic dynamics such as bifurcation,[14] crisis, and intermittency.[15][16]

Terminology

Step-down
A converter where output voltage is lower than the input voltage (such as a buck converter).
Step-up
A converter that outputs a voltage higher than the input voltage (such as a boost converter).
Continuous current mode
Current and thus the magnetic field in the inductive energy storage never reach zero.
Discontinuous current mode
Current and thus the magnetic field in the inductive energy storage may reach or cross zero.
Noise
Unwanted electrical and electromagnetic signal noise, typically switching artifacts.
RF noise
Switching converters inherently emit radio waves at the switching frequency and its harmonics. Switching converters that produce triangular switching current, such as the Split-Pi, forward converter, or Ćuk converter in continuous current mode, produce less harmonic noise than other switching converters.[17] RF noise causes electromagnetic interference (EMI). Acceptable levels depend upon requirements, e.g. proximity to RF circuitry needs more suppression than simply meeting regulations.
Input noise
The input voltage may have non-negligible noise. Additionally, if the converter loads the input with sharp load edges, the converter can emit RF noise from the supplying power lines. This should be prevented with proper filtering in the input stage of the converter.
Output noise
The output of an ideal DC-to-DC converter is a flat, constant output voltage. However, real converters produce a DC output upon which is superimposed some level of electrical noise. Switching converters produce switching noise at the switching frequency and its harmonics. Additionally, all electronic circuits have some thermal noise. Some sensitive radio-frequency and analog circuits require a power supply with so little noise that it can only be provided by a linear regulator.[citation needed] Some analog circuits which require a power supply with relatively low noise can tolerate some of the less-noisy switching converters, e.g. using continuous triangular waveforms rather than square waves.[17][not in citation given]

See also



This article uses material from the Wikipedia article "DC-to-DC converter", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electronics & PCB

Cadence, Mentor Graphics, Eagle CAD, Altium Designer, AUTODESK EAGLE, Cadence Allegro, DesignSpark PCB , Mentor PADS, Mentor Xpedition, Novarm DipTrace, Pulsonix, TARGET 3001!, Xpedition xDX Designer, Zuken CADSTAR, Altium P-CAD, Agnisys, Altera Quartus, OrCAD, kiCAD, Solido Design Automation, ELectronics, PCB, Curcuit Board, 3D drawings, 3D library, 3D content, PCB Design, 2D symbols, 2D drawings, 2D icons, 2D schematics