This article has multiple issues. Please help improve it or discuss these issues on the talk page. (Learn how and when to remove these template messages)
(Learn how and when to remove this template message)
|
A juicer (also known as juicing machine or juice extractor) is a tool used to extract juice from fruits, herbs, leafy greens and other types of vegetables in a process called juicing.[1] It crushes, grinds, and/or squeezes the juice out of the pulp.[2]
Some types of juicers can also function as a food processor.[3] Most of the twin gear and horizontal masticating juicers have attachments for crushing herbs and spices, extruding pasta, noodles or bread sticks, making baby food and nut butter, grinding coffee, making nut milk, etc.
Reamers are used for squeezing juice from citrus such as grapefruits, lemons, limes, and oranges.[4] Juice is extracted by pressing or grinding a halved citrus along a juicer's ridged conical center and discarding the rind. Some reamers are stationary and require a user to press and turn the fruit, while others are electrical, automatically turning the ridged center when fruit is pressed upon.
A centrifugal juicer cuts up the fruit or vegetable with a flat cutting blade.[5] It then spins the produce at a high speed to separate the juice from the pulp.
A masticating juicer known as cold press juicer or slow juicer uses a single auger to compact and crush produce into smaller sections before squeezing out its juice along a static screen while the pulp is expelled through a separate outlet.[5]
Triturating juicers (twin gear juicers) have twin augers to crush and press produce.
A juicing press, such as a fruit press or wine press, is a larger scale that are used in agricultural production. These presses can be stationary or mobile. A mobile press has the advantage that it can be moved from one orchard to another. The process is primarily used for apples and involves a stack of apple mash, wrapped in fine mesh cloth, which is then pressed under approx 40 tonnes. These machines are popular in Europe and have now been introduced to North America.
A stovetop steam juice extractor is typically a pot to generate steam that used to heat a batch of berries (or other fruit) in a perforated pot stacked on top of a juice collecting container that is above the steam pot. The juice is extracted without mechanical means so it is remarkably clear and because of the steam heating it is also pasteurized for long term storage.
This article uses material from the Wikipedia article "Juicer", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
food,liquor,alcohol,drink,beverage,coke