Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In jewelry, a collar is an ornament for the neck.
Collar is an older word for necklace, and is usually reserved today for a necklace that lies flat to the body rather than hanging freely.
In contemporary fine jewelry, collar necklaces are 14 inches in chain length. In street fashion, collars are more commonly referred to as dog collars. Dog collars are associated with the punk scene and the BDSM scene.[1]
Specifically, collar may refer to:
This fashion-related article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "Collar (jewelry)", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D, jewellery,jewelry