Organelle | |
---|---|
Details | |
Identifiers | |
Latin | organella |
Code | TH H1.00.01.0.00009 |
TH | H1.00.01.0.00009 |
FMA | 63832 |
Anatomical terminology |
In cell biology, an organelle (/ɔːrɡəˈnɛl/) is a specialized subunit within a cell that has a specific function. Individual organelles are usually separately enclosed within their own lipid bilayers.
The name organelle comes from the idea that these structures are parts of cells, as organs are to the body, hence organelle, the suffix -elle being a diminutive. Organelles are identified by microscopy, and can also be purified by cell fractionation. There are many types of organelles, particularly in eukaryotic cells. While prokaryotes do not possess organelles per se, some do contain protein-based bacterial microcompartments, which are thought to act as primitive organelles.[1]
Cell biology | |
---|---|
The animal cell | |
Components of a typical animal cell:
|
In biology organs are defined as confined functional units within an organism.[2] The analogy of bodily organs to microscopic cellular substructures is obvious, as from even early works, authors of respective textbooks rarely elaborate on the distinction between the two.
In the 1830s, Félix Dujardin refuted Ehrenberg theory which said that microorganisms have the same organs of multicellular animals, only minor.[3]
Credited as the first[4][5][6] to use a diminutive of organ (i.e., little organ) for cellular structures was German zoologist Karl August Möbius (1884), who used the term organula (plural of organulum, the diminutive of Latin organum).[7] In a footnote, which was published as a correction in the next issue of the journal, he justified his suggestion to call organs of unicellular organisms "organella" since they are only differently formed parts of one cell, in contrast to multicellular organs of multicellular organisms.[citation needed]
While most cell biologists consider the term organelle to be synonymous with "cell compartment", other cell biologists choose to limit the term organelle to include only those that are containing deoxyribonucleic acid (DNA), having originated from formerly autonomous microscopic organisms acquired via endosymbiosis.[8][9][10]
Under this definition, there would only be two broad classes of organelles (i.e. those that contain their own DNA, and have originated from endosymbiotic bacteria):
Other organelles are also suggested to have endosymbiotic origins, but do not contain their own DNA (notably the flagellum – see evolution of flagella).
Under the more restricted definition of membrane-bound structures, some parts of the cell do not qualify as organelles. Nevertheless, the use of organelle to refer to non-membrane bound structures such as ribosomes is common.[12] This has led some texts to delineate between membrane-bound and non-membrane bound organelles.[13] The non-membrane bound organelles, also called large biomolecular complexes, are large assemblies of macromolecules that carry out particular and specialized functions, but they lack membrane boundaries. Such cell structures include:
Eukaryotic cells are structurally complex, and by definition are organized, in part, by interior compartments that are themselves enclosed by lipid membranes that resemble the outermost cell membrane. The larger organelles, such as the nucleus and vacuoles, are easily visible with the light microscope. They were among the first biological discoveries made after the invention of the microscope.
Not all eukaryotic cells have each of the organelles listed below. Exceptional organisms have cells that do not include some organelles that might otherwise be considered universal to eukaryotes (such as mitochondria).[14] There are also occasional exceptions to the number of membranes surrounding organelles, listed in the tables below (e.g., some that are listed as double-membrane are sometimes found with single or triple membranes). In addition, the number of individual organelles of each type found in a given cell varies depending upon the function of that cell.
Organelle | Main function | Structure | Organisms | Notes |
---|---|---|---|---|
chloroplast (plastid) | photosynthesis, traps energy from sunlight | double-membrane compartment | plants, protists (rare kleptoplastic organisms) | has own DNA; theorized to be engulfed by the ancestral eukaryotic cell (endosymbiosis) |
endoplasmic reticulum | translation and folding of new proteins (rough endoplasmic reticulum), expression of lipids (smooth endoplasmic reticulum) | single-membrane compartment | all eukaryotes | rough endoplasmic reticulum is covered with ribosomes, has folds that are flat sacs; smooth endoplasmic reticulum has folds that are tubular |
flagellum | locomotion, sensory | some eukaryotes | ||
Golgi apparatus | sorting, packaging, processing and modification of proteins | single-membrane compartment | all eukaryotes | cis-face (convex) nearest to rough endoplasmic reticulum; trans-face (concave) farthest from rough endoplasmic reticulum |
mitochondrion | energy production from the oxidation of glucose substances and the release of adenosine triphosphate | double-membrane compartment | most eukaryotes | constituting element of the chondriome; has own DNA; theorized to be engulfed by an ancestral eukaryotic cell (endosymbiosis) |
nucleus | DNA maintenance, controls all activities of the cell, RNA transcription | double-membrane compartment | all eukaryotes | contains bulk of genome |
vacuole | storage, transportation, helps maintain homeostasis | single-membrane compartment | eukaryotes |
Mitochondria and chloroplasts, which have double-membranes and their own DNA, are believed to have originated from incompletely consumed or invading prokaryotic organisms, which were adopted as a part of the invaded cell. This idea is supported in the Endosymbiotic theory.
Organelle/Macromolecule | Main function | Structure | Organisms |
---|---|---|---|
acrosome | helps spermatozoa fuse with ovum | single-membrane compartment | many animals |
autophagosome | vesicle that sequesters cytoplasmic material and organelles for degradation | double-membrane compartment | all eukaryotes |
centriole | anchor for cytoskeleton, organizes cell division by forming spindle fibers | Microtubule protein | animals |
cilium | movement in or of external medium; "critical developmental signaling pathway".[15] | Microtubule protein | animals, protists, few plants |
cnidocyst | stinging | coiled hollow tubule | cnidarians |
eyespot apparatus | detects light, allowing phototaxis to take place | green algae and other unicellular photosynthetic organisms such as euglenids | |
glycosome | carries out glycolysis | single-membrane compartment | Some protozoa, such as Trypanosomes. |
glyoxysome | conversion of fat into sugars | single-membrane compartment | plants |
hydrogenosome | energy & hydrogen production | double-membrane compartment | a few unicellular eukaryotes |
lysosome | breakdown of large molecules (e.g., proteins + polysaccharides) | single-membrane compartment | animals |
melanosome | pigment storage | single-membrane compartment | animals |
mitosome | probably plays a role in Iron-sulfur cluster (Fe-S) assembly | double-membrane compartment | a few unicellular eukaryotes that lack mitochondria |
myofibril | myocyte contraction | bundled filaments | animals |
nucleolus | pre-ribosome production | protein-DNA-RNA | most eukaryotes |
parenthesome | not characterized | not characterized | fungi |
peroxisome | breakdown of metabolic hydrogen peroxide | single-membrane compartment | all eukaryotes |
proteasome | degradation of unneeded or damaged proteins by proteolysis | very large protein complex | All eukaryotes, all archaea, some bacteria |
ribosome (80S) | translation of RNA into proteins | RNA-protein | all eukaryotes |
stress granule | mRNA storage[16] | membraneless
(mRNP complexes) |
Most eukaryotes |
vesicle | material transport | single-membrane compartment | all eukaryotes |
Other related structures:
Prokaryotes are not as structurally complex as eukaryotes, and were once thought not to have any internal structures enclosed by lipid membranes. In the past, they were often viewed as having little internal organization, but slowly, details are emerging about prokaryotic internal structures. An early false turn was the idea developed in the 1970s that bacteria might contain membrane folds termed mesosomes, but these were later shown to be artifacts produced by the chemicals used to prepare the cells for electron microscopy.[18]
However, more recent research has revealed that at least some prokaryotes have microcompartments such as carboxysomes. These subcellular compartments are 100–200 nm in diameter and are enclosed by a shell of proteins.[1] Even more striking is the description of membrane-bound magnetosomes in bacteria, reported in 2006,[19][20] as well as the nucleus-like structures of the Planctomycetes that are surrounded by lipid membranes, reported in 2005.[21]
Organelle/Macromolecule | Main function | Structure | Organisms |
---|---|---|---|
carboxysome | carbon fixation | protein-shell compartment | some bacteria |
chlorosome | photosynthesis | light harvesting complex | green sulfur bacteria |
flagellum | movement in external medium | protein filament | some prokaryotes and eukaryotes |
magnetosome | magnetic orientation | inorganic crystal, lipid membrane | magnetotactic bacteria |
mesosomes | functions of Golgi bodies, centrioles, etc. | small irregular shaped organelle containing ribosomes | present in most prokaryotic cells |
nucleoid | DNA maintenance, transcription to RNA | DNA-protein | prokaryotes |
pilus | Adhesion to other cells for conjugation or to a solid substrate to create motile forces. | a hair-like appendage sticking out (though partially embedded into) the plasma membrane | prokaryotic cells |
plasmid | DNA exchange | circular DNA | some bacteria |
ribosome (70S) | translation of RNA into proteins | RNA-protein | bacteria and archaea |
thylakoid | photosynthesis | photosystem proteins and pigments | mostly cyanobacteria |
The function of a protein is closely correlated with the organelle in which it resides. Some methods were proposed for predicting the organelle in which an uncharacterized protein is located according to its amino acid composition[22][23] and some methods were based on pseudo amino acid composition.[24][25][26][27]
This article uses material from the Wikipedia article "Organelle", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,virus,bacteria,medicine, molecule,atom,chemistry,labor