powered by CADENAS

Social Share

Amazon

Constant-current diode (9750 views - Electronics & PCB)

Constant-current diode is an electronic device that limits current to a maximum specified value for the device. It is known as current-limiting diode (CLD), current-regulating diode (CRD). These diodes consist of an n-channel JFET-transistor with the gate shorted to the source, which functions like a two-terminal current limiter or current source (analogous to a voltage-limiting Zener diode). They allow a current through them to rise to a certain value, and then level off at a specific value. Unlike Zener diodes, these diodes keep the current constant instead of the voltage constant. These devices keep the current flowing through them unchanged when the voltage changes. An example is the 1N5312. Note the negative VGS is required, as an example on the n-type junction-gate field-effect transistor 2N5457.
Go to Article

Constant-current diode

Constant-current diode

Constant-current diode is an electronic device that limits current to a maximum specified value for the device. It is known as current-limiting diode (CLD), current-regulating diode (CRD).

These diodes consist of an n-channel JFET-transistor with the gate shorted to the source, which functions like a two-terminal current limiter or current source (analogous to a voltage-limiting Zener diode). They allow a current through them to rise to a certain value, and then level off at a specific value. Unlike Zener diodes, these diodes keep the current constant instead of the voltage constant. These devices keep the current flowing through them unchanged when the voltage changes. An example is the 1N5312. Note the negative VGS is required, as an example on the n-type junction-gate field-effect transistor 2N5457.

Diode
JFET


This article uses material from the Wikipedia article "Constant-current diode", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electronics & PCB

Cadence, Mentor Graphics, Eagle CAD, Altium Designer, AUTODESK EAGLE, Cadence Allegro, DesignSpark PCB , Mentor PADS, Mentor Xpedition, Novarm DipTrace, Pulsonix, TARGET 3001!, Xpedition xDX Designer, Zuken CADSTAR, Altium P-CAD, Agnisys, Altera Quartus, OrCAD, kiCAD, Solido Design Automation, ELectronics, PCB, Curcuit Board, 3D drawings, 3D library, 3D content, PCB Design, 2D symbols, 2D drawings, 2D icons, 2D schematics