powered by CADENAS

Social Share

Electronic symbol (11179 views - Electrical Engineering)

An electronic symbol is a pictogram used to represent various electrical and electronic devices (such as wires, batteries, resistors, and transistors) in a schematic diagram of an electrical or electronic circuit. These symbols can (because of remaining traditions) vary from country to country, but are today to a large extent internationally standardized. Some symbols represent components (such as vacuum tubes) which ceased to be used routinely as newer technologies were introduced.
Go to Article

Electronic symbol

Electronic symbol

An electronic symbol is a pictogram used to represent various electrical and electronic devices (such as wires, batteries, resistors, and transistors) in a schematic diagram of an electrical or electronic circuit. These symbols can (because of remaining traditions) vary from country to country, but are today to a large extent internationally standardized. Some symbols represent components (such as vacuum tubes) which ceased to be used routinely as newer technologies were introduced.

Standards for symbols

There are several national and international standards for graphical symbols in circuit diagrams, in particular:

  • IEC 60617 (also known as British Standard BS 3939).
  • ANSI Y32.2-1975 (also known as IEEE Std 315-1975 or CSA Z99-1975)
  • IEEE Std 91/91a: graphic symbols for logic functions (used in digital electronics). It is referenced in ANSI Y32.2/IEEE Std 315.
  • Australian Standard AS 1102.

Different symbols may be used depending on the discipline using the drawing. For example, lighting and power symbols used as part of architectural drawings may be different from symbols for devices used in electronics. National and local variations to international standards also exist.

Gallery of common electronic symbols

Symbols shown are typical examples, not a complete list.[1][2]

Traces

Circuit Return

Sources

Resistors

Capacitors

Inductors

Transistors

Unipolar

Bipolar

Diodes

Antennas

Vacuum tubes

Switches

Relays

Lamps

Current Limiters

Transformers

Acoustic Devices

Miscellaneous

Gallery of historical electronic symbols

The shape of electronic symbols have changed over time. Some symbols were more prevalent in some countries. The following are historic electronic symbols that might be found in old electronic books and schematics.

Capacitors (historical)

See also



This article uses material from the Wikipedia article "Electronic symbol", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electrical Engineering

EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced