Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Developer(s) | Logic Design Inc. |
---|---|
Stable release |
V12.0
/ February 2017; 9 months ago (2017-02) |
Operating system | Windows (XP, Vista, Windows 7, Windows 8, Windows 10) |
Type | Electronic circuit simulation |
License | Proprietary |
Website |
www |
CircuitLogix is a software electronic circuit simulator which uses PSpice to simulate thousands of electronic devices, models, and circuits. CircuitLogix supports analog, digital, and mixed-signal circuits, and its SPICE simulation gives accurate real-world results. The graphic user interface allows students to quickly and easily draw, modify and combine analog and digital circuit diagrams. CircuitLogix was first launched in 2005, and its popularity has grown quickly since that time. In 2012, it reached the milestone of 250,000 licensed users, and became the first electronics simulation product to have a global installed base of a quarter-million customers in over 100 countries. [1]
CircuitLogix was developed by Dr. Colin Simpson, an electronics professor at George Brown College, in Toronto, Canada, and John (Bud) Skinner, a computer programmer. The electronics program has won awards including the Award of Excellence from the Association of Canadian Community Colleges (ACCC).[2]
The professional version of CircuitLogix (CircuitLogix Pro) includes over 10,000 device models, as well as 8 virtual instruments.[3] It also includes 3DLab, which is a software product that combines an interactive 3-dimensional learning environment and electronic devices and tools to enhance the user's comprehension of electronics. 3DLab virtual components include batteries, switches, motors, lamps, resistors, inductors, capacitors and instruments including oscilloscopes, Signal generators, and frequency counters.[4]
Fast, accurate simulation of electronic circuits is essential because it provides the information needed to perform accurate analysis of circuit behavior. SPICE simulators are used to verify that analog and mixed-signal circuits will yield the expected outputs. A schematic netlist file and circuit input values are fed to the SPICE software, which simulates the circuit's behavior for a specified length of time. CircuitLogix allows for the observation of voltage and current levels at any circuit node as they change with frequency and time. It allows for obtaining accurate results even when simulating complex circuits where hierarchical blocks are reused. The CircuitLogix simulation engine is based on Berkeley SPICE, and contains a GUI to make circuit design easier and more efficient.
The CircuitLogix 32-bit SPICE engine is interactive, allowing, for example, the frequency of sources to be changed, potentiometers adjusted, and switches thrown during simulation. The SPICE engine is fully integrated with the schematic capture and waveform tools; CircuitLogix passes schematic edits to the simulator automatically while running. Components such as fuses, LEDs and controlled switches are automatically updated in the schematic as the simulation runs.
CircuitLogix simulates analog, digital, and mixed analog-digital circuits. The simulator first divides the circuit into analog and digital portions. The analog circuitry is simulated with the time-step driven SPICE engine, while the digital parts are simulated separately with an event-driven simulation engine. The CircuitLogix digital engine was developed directly in .NET, faster than SPICE macros. Because the simulator automatically performs signal conversion, it is possible to connect any analog or digital part to any other. The system’s model library contains hybrid parts for analog-to-digital and digital-to-analog conversion.
CircuitLogix is a mixed-mode schematic editor, and includes both analog and event-driven simulation capabilities: any simulation may contain components that are analog, event driven (digital or sampled-data), or a combination of both. An entire mixed signal analysis can be driven from one integrated schematic. All the digital models in CircuitLogix provide accurate specification of propagation time and rise/fall time delays.
The event-driven algorithm used by CircuitLogix is general-purpose and supports non-digital types of data. For example, elements can use real or integer values to simulate DSP functions or sampled data filters. Because the event-driven algorithm is faster than the standard SPICE matrix, simulation time is greatly reduced for circuits that use event-driven models in place of analog models.
Mixed-mode simulation is handled on three levels by CircuitLogix: (a) with primitive digital elements that use timing models and a built-in 12-state digital logic simulator, (b) with subcircuit models that use the actual transistor topology of the integrated circuit, and finally, (c) with In-line Boolean logic expressions. These two modeling techniques use SPICE to solve a problem while the third method, digital primitives, uses mixed-mode capability.
The component library includes:
This article uses material from the Wikipedia article "CircuitLogix", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D