powered by CADENAS

Social Share

Bar table (5049 views - Interior Design)

A bar table is a table in a common law courtroom at which advocates sit or stand. It is generally situated between the Bench and the well of the court, where the public sit. Advocates such as barristers sit facing the Bench with their backs to the well. Usually the witness box and, if there is one, the jury box, will be to the sides of the room, between the bar table and the bench. In some jurisdictions, solicitors sit on a table behind the bar table. In others, they sit at the bar table facing the barristers and with their backs to the judge.
Go to Article

Explanation by Hotspot Model

Bar table

Bar table

A bar table is a table in a common law courtroom at which advocates sit or stand.[1] It is generally situated between the Bench and the well of the court, where the public sit. Advocates such as barristers sit facing the Bench with their backs to the well. Usually the witness box and, if there is one, the jury box, will be to the sides of the room, between the bar table and the bench.

In some jurisdictions, solicitors sit on a table behind the bar table. In others, they sit at the bar table facing the barristers and with their backs to the judge.

  1. ^ "Archived copy". Archived from the original on 2009-05-01. Retrieved 2009-05-10. 


This article uses material from the Wikipedia article "Bar table", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Interior Design

3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art