powered by CADENAS

Social Share

Beach furniture (5666 views - Interior Design)

Beach furniture is furniture designed for use with or in an urban beach or natural beach.
Go to Article

Explanation by Hotspot Model

Beach furniture

Beach furniture

Beach furniture is furniture designed for use with or in an urban beach or natural beach.

Standard beach furniture

Typically beach furniture is made of plastic, concrete, or of stainless steel.

For example, the Dundas Square beach area includes a number of stainless steel chairs that are placed on the beach area during the day and stored at night (even though the urbeach, including the aquatic play features, remain open 24 hours a day).

Installation art beach furniture

The Teluscape beach incorporates beach furniture into the design of the water-pipe-organ (hydraulophone) by way of the South Division of the pipe organ's pipes being incorporated/incorporating seating made of cast-in-place concrete. In this beach, the area was excavated and an underground sounding chamber was constructed for the pipe organ, wherein part of the sounding chamber extends out as a hollow snakelike "creature" upon which the "head" of the snake forms a seating surface all the way around the largest pipes of the organ, and the "tail" of the snake provides partial seating on the side of the organ pipes that face the playing surface (fountain jets).




This article uses material from the Wikipedia article "Beach furniture", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Interior Design

3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art