Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Retro-Computing Society of Rhode Island).
Computer hardware is the physical parts or components of a computer, such as the monitor, keyboard, computer data storage, graphic card, sound card and motherboard.[1] By contrast, software is instructions that can be stored and ran by hardware.
Hardware is directed by the software to execute any command or instruction. A combination of hardware and software forms a usable computing system.
The template for all modern computers is the Von Neumann architecture, detailed in a 1945 paper by Hungarian mathematician John von Neumann. This describes a design architecture for an electronic digital computer with subdivisions of a processing unit consisting of an arithmetic logic unit and processor registers, a control unit containing an instruction register and program counter, a memory to store both data and instructions, external mass storage, and input and output mechanisms.[2] The meaning of the term has evolved to mean a stored-program computer in which an instruction fetch and a data operation cannot occur at the same time because they share a common bus. This is referred to as the Von Neumann bottleneck and often limits the performance of the system.[3]
For the third consecutive year, U.S. business-to-business channel sales (sales through distributors and commercial resellers) increased, ending 2013 up nearly 6 percent at $61.7 billion. The impressive growth was the fastest sales increase since the end of the recession. Sales growth accelerated in the second half of the year peaking in fourth quarter with a 6.9 percent increase over the fourth quarter of 2012.[4]
There are a number of different types of computer system in use today.
The personal computer, also known as the PC, is one of the most common types of computer due to its versatility and relatively low price. Laptops are generally very similar, although they may use lower-power or reduced size components, thus lower performance.
The computer case encloses most of the components of the system. It provides mechanical support and protection for internal elements such as the motherboard, disk drives, and power supplies, and controls and directs the flow of cooling air over internal components. The case is also part of the system to control electromagnetic interference radiated by the computer, and protects internal parts from electrostatic discharge. Large tower cases provide extra internal space for multiple disk drives or other peripherals and usually stand on the floor, while desktop cases provide less expansion room. All-in-one style designs from Apple, namely the iMac, and similar types, include a video display in the same case. Portable and laptop computers require cases that provide impact protection for the unit. A current development in laptop computers is a detachable keyboard, which allows the system to be configured as a touch-screen tablet. Hobbyists may decorate the cases with colored lights, paint, or other features, in an activity called case modding.
A power supply unit (PSU) converts alternating current (AC) electric power to low-voltage DC power for the internal components of the computer. Laptops are capable of running from a built-in battery, normally for a period of hours.[5]
The motherboard is the main component of a computer. It is a board with integrated circuitry that connects the other parts of the computer including the CPU, the RAM, the disk drives (CD, DVD, hard disk, or any others) as well as any peripherals connected via the ports or the expansion slots.
Components directly attached to or to part of the motherboard include:
An expansion card in computing is a printed circuit board that can be inserted into an expansion slot of a computer motherboard or backplane to add functionality to a computer system via the expansion bus. Expansions cards can be used to obtain or expand on features not offered by the motherboard.
A storage device is any computing hardware and digital media that is used for storing, porting and extracting data files and objects. It can hold and store information both temporarily and permanently, and can be internal or external to a computer, server or any similar computing device. Data storage is a core function and fundamental component of computers.
Data is stored by a computer using a variety of media. Hard disk drives are found in virtually all older computers, due to their high capacity and low cost, but solid-state drives are faster and more power efficient, although currently more expensive than hard drives in terms of dollar per gigabyte,[6] so are often found in personal computers built post-2007.[7] Some systems may use a disk array controller for greater performance or reliability.
To transfer data between computers, a USB flash drive or optical disc may be used. Their usefulness depends on being readable by other systems; the majority of machines have an optical disk drive, and virtually all have at least one USB port.
Input and output devices are typically housed externally to the main computer chassis. The following are either standard or very common to many computer systems.
Input devices allow the user to enter information into the system, or control its operation. Most personal computers have a mouse and keyboard, but laptop systems typically use a touchpad instead of a mouse. Other input devices include webcams, microphones, joysticks, and image scanners.
Output devices display information in a human readable form. Such devices could include printers, speakers, monitors or a Braille embosser.
In the 1960s and 1970s, more and more departments started to use cheaper and dedicated systems for specific purposes like process control and laboratory automation.
A supercomputer is superficially similar to a mainframe, but is instead intended for extremely demanding computational tasks. As of June 2016[update], the fastest supercomputer in the world is the Sunway TaihuLight, in Jiangsu, China.[8]
The term supercomputer does not refer to a specific technology. Rather it indicates the fastest computations available at any given time. In mid 2011, the fastest supercomputers boasted speeds exceeding one petaflop, or 1 quadrillion (10^15 or 1,000 trillion) floating point operations per second. Super computers are fast but extremely costly so they are generally used by large organizations to execute computationally demanding tasks involving large data sets. Super computers typically run military and scientific applications. Although they cost millions of dollars, they are also being used for commercial applications where huge amounts of data must be analyzed. For example, large banks employ supercomputers to calculate the risks and returns of various investment strategies, and healthcare organizations use them to analyze giant databases of patient data to determine optimal treatments for various diseases and problems incurring to the country.
When using computer hardware, an upgrade means adding new hardware to a computer that improves its performance, adds capacity or new features. For example, a user could perform a hardware upgrade to replace the hard drive with a SSD to get a boost in performance or increase the amount of files that may be stored. Also, the user could increase the RAM so the computer may run more smoothly. The user could add a USB 3.0 expansion card in order to fully use USB 3.0 devices, or could upgrade the GPU for extra rendering power. Performing such hardware upgrades may be necessary for older computers to meet a programs' system requirements.
Because computer parts contain hazardous materials, there is a growing movement to recycle old and outdated parts.[9] Computer hardware contain dangerous chemicals such as: lead, mercury, nickel, and cadmium. According to the EPA these e-wastes have a harmful effect on the environment unless they are disposed of properly. Making hardware requires energy, and recycling parts will reduce air pollution, water pollution, as well as greenhouse gas emissions.[10] Disposing unauthorized computer equipment is in fact illegal. Legislation makes it mandatory to recycle computers through the government approved facilities. Recycling a computer can be made easier by taking out certain reusable parts. For example, the RAM, DVD drive, the graphics card, hard drive or SSD, and other similar removable parts can be reused.
The central processing unit contains many toxic materials. It contains lead and chromium in the metal plates. Resistors, semi-conductors, infrared detectors, stabilizers, cables, and wires contain cadmium. The circuit boards in a computer contain mercury, and chromium.[11] When these types of materials, and chemicals are disposed improperly will become hazardous for the environment.
According to the United States Environmental Protection Agency only around 15% of the e-waste actually is recycled. When e-waste byproducts leach into ground water are burned or get mishandled during recycling it causes harm. Health problems associated with such toxins include impaired mental development, cancer, and damage to the lungs, liver, and kidneys.[12] That's why even wires have to be recycled. Different companies have different techniques to recycle a wire. The most popular one is the grinder that separates the copper wires form the plastic/rubber casing. When the processes is done there are two different piles left; one containing the copper powder, and the other containing plastic/rubber pieces.[13] Computer monitors, mice, and keyboards all have a similar way of being recycled. For example, first each of the parts are taken apart then all of the inner parts get separated and placed into its own bin.[14]
Recycling a computer is made easier by a few of the national services, such as Dell and Apple. Both companies will take back the computer of their make or any other make. Otherwise a computer can be donated to Computer Aid International which is an organization that recycles and refurbishes old computers for hospitals, schools, universities, etc.[15]
This article uses material from the Wikipedia article "Computer hardware", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Computer, Hardware, Software