Licensed under Creative Commons Attribution-Share Alike 3.0 (Makemake at the German language Wikipedia).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (December 2016) (Learn how and when to remove this template message) |
Natural resources are resources that exist without actions of humankind. This includes all valued characteristics such as magnetic, gravitational, and electrical properties and forces etc. On earth it includes: sunlight, atmosphere, water, land (includes all minerals) along with all vegetation, crops and animal life that naturally subsists upon or within the heretofore identified characteristics and substances.[1][2][3][4]
Particular areas such as the rainforest in Fatu-Hiva are often characterized by the biodiversity and geodiversity existent in their ecosystems. Natural resources may be further classified in different ways. Natural resources are materials and components (something that can be used) that can be found within the environment. Every man-made product is composed of natural resources (at its fundamental level). A natural resource may exist as a separate entity such as fresh water, air, and as well as a living organism such as a fish, or it may exist in an alternate form that must be processed to obtain the resource such as metal ores, rare earth metals, petroleum, and most forms of energy.
There is much debate worldwide over natural resource allocations, this is particularly true during periods of increasing scarcity and shortages (depletion and overconsumption of resources) but also because the exportation of natural resources is the basis for many economies (particularly for developed countries).
Some natural resources such as sunlight and air can be found everywhere, and are known as ubiquitous resources. However, most resources only occur in small sporadic areas, and are referred to as localised resources. There are very few resources that are considered inexhaustible (will not run out in foreseeable future) – these are solar radiation, geothermal energy, and air (though access to clean air may not be). The vast majority of resources are theoretically exhaustible, which means they have a finite quantity and can be depleted if managed improperly.
There are various methods of categorizing natural resources, these include source of origin, stage of development, and by their renewability.
On the basis of origin, natural resources may be divided into two types:
Considering their stage of development, natural resources may be referred to in the following ways:
Many natural resources can be categorized as either renewable or non-renewable:
Resource extraction involves any activity that withdraws resources from nature. This can range in scale from the traditional use of preindustrial societies, to global industry. Extractive industries are, along with agriculture, the basis of the primary sector of the economy. Extraction produces raw material which is then processed to add value. Examples of extractive industries are hunting, trapping, mining, oil and gas drilling, and forestry. Natural resources can add substantial amounts to a country's wealth,[7] however a sudden inflow of money caused by a resource boom can create social problems including inflation harming other industries ("Dutch disease") and corruption, leading to inequality and underdevelopment, this is known as the "resource curse".
Extractive industries represent a large growing activity in many less-developed countries but the wealth generated does not always lead to sustainable and inclusive growth. Extractive industry businesses often are assumed to be interested only in maximizing their short-term value, implying that less-developed countries are vulnerable to powerful corporations. Alternatively, host governments are often assumed to be only maximizing immediate revenue. Researchers argue there are areas of common interest where development goals and business cross. These present opportunities for international governmental agencies to engage with the private sector and host governments through revenue management and expenditure accountability, infrastructure development, employment creation, skills and enterprise development and impacts on children, especially girls and women.[8]
In recent years, the depletion of natural resources has become a major focus of governments and organizations such as the United Nations (UN). This is evident in the UN's Agenda 21 Section Two, which outlines the necessary steps to be taken by countries to sustain their natural resources.[9] The depletion of natural resources is considered to be a sustainable development issue.[10] The term sustainable development has many interpretations, most notably the Brundtland Commission's 'to ensure that it meets the needs of the present without compromising the ability of future generations to meet their own needs',[11] however in broad terms it is balancing the needs of the planet's people and species now and in the future.[9] In regards to natural resources, depletion is of concern for sustainable development as it has the ability to degrade current environments[12] and potential to impact the needs of future generations.[10]
Depletion of natural resources is associated with social inequity. Considering most biodiversity are located in developing countries,[14] depletion of this resource could result in losses of ecosystem services for these countries.[15] Some view this depletion as a major source of social unrest and conflicts in developing nations.[16]
At present, with it being the year of the forest,[17] there is particular concern for rainforest regions which hold most of the Earth's biodiversity.[17] According to Nelson[18] deforestation and degradation affect 8.5% of the world's forests with 30% of the Earth's surface already cropped. If we consider that 80% of people rely on medicines obtained from plants and ¾ of the world's prescription medicines have ingredients taken from plants,[15] loss of the world's rainforests could result in a loss of finding more potential life saving medicines.[19]
The depletion of natural resources is caused by 'direct drivers of change'[18] such as Mining, petroleum extraction, fishing and forestry as well as 'indirect drivers of change' such as demography, economy, society, politics and technology.[18] The current practice of Agriculture is another factor causing depletion of natural resources. For example, the depletion of nutrients in the soil due to excessive use of nitrogen[18] and desertification.[9] The depletion of natural resources is a continuing concern for society. This is seen in the cited quote given by Theodore Roosevelt, a well-known conservationist and former United States president, who was opposed to unregulated natural resource extraction.
In 1982, the UN developed the World Charter for Nature, which recognized the need to protect nature from further depletion due to human activity. It states that measures need to be taken at all societal levels, from international to individual, to protect nature. It outlines the need for sustainable use of natural resources and suggests that the protection of resources should be incorporated into national and international systems of law.[20] To look at the importance of protecting natural resources further, the World Ethic of Sustainability, developed by the IUCN, WWF and the UNEP in 1990,[21] set out eight values for sustainability, including the need to protect natural resources from depletion. Since the development of these documents, many measures have been taken to protect natural resources including establishment of the scientific field and practice of conservation biology and habitat conservation, respectively.
Conservation biology is the scientific study of the nature and status of Earth's biodiversity with the aim of protecting species, their habitats, and ecosystems from excessive rates of extinction.[22][23] It is an interdisciplinary subject drawing on science, economics and the practice of natural resource management.[24][25][26][27] The term conservation biology was introduced as the title of a conference held at the University of California, San Diego, in La Jolla, California, in 1978, organized by biologists Bruce A. Wilcox and Michael E. Soulé.
Habitat conservation is a land management practice that seeks to conserve, protect and restore, habitat areas for wild plants and animals, especially conservation reliant species, and prevent their extinction, fragmentation or reduction in range.[28]
Natural resource management is a discipline in the management of natural resources such as land, water, soil, plants and animals, with a particular focus on how management affects the quality of life for both present and future generations.Hence sustainable development can be followed where there is a judicial use of resources which compromises the needs of the present generations as well as the future generations.
Management of natural resources involves identifying who has the right to use the resources and who does not for defining the boundaries of the resource.[29] The resources are managed by the users according to the rules governing of when and how the resource is used depending on local condition.[30]
A successful management of natural resources should[neutrality is disputed] engage the community because of the nature of the shared resources the individuals who are affected by the rules can participate in setting or changing them.[29] The users have rights to devise their own management institutions and plans under the recognition by the government. The right to resources includes land, water, fisheries and pastoral rights.[30] The users or parties accountable to the users have to actively monitor and ensure the utilisation of the resource compliance with the rules and to impose penalty on those peoples who violates the rules.[29] These conflicts are resolved in a quick and low cost manner by the local institution according to the seriousness and context of the offence.[30] The global science-based platform to discuss natural resources management is the World Resources Forum, based in Switzerland.
Value of Natural Resources by country (in USD Trillions), 2016[31] | ||
---|---|---|
Country | Value | |
Russia | 75 | |
United States | 45 | |
Saudi Arabia | 34.4 | |
Canada | 33.2 | |
Iran | 27.3 | |
China | 23 | |
Brazil | 21.8 | |
Australia | 19.9 | |
Iraq | 15.9 | |
Venezuela | 14.3 |
This article uses material from the Wikipedia article "Natural resource", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
database,rohs,reach,compliancy,directory,listing,information,substance,material