Licensed under Creative Commons Attribution-Share Alike 2.0 fr (Rama).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (June 2012) (Learn how and when to remove this template message) |
Artillery is a class of large military weapons built to fire munitions far beyond the range and power of infantry's small arms. Early artillery development focused on the ability to breach fortifications, and led to heavy, fairly immobile siege engines. As technology improved, lighter, more mobile field artillery developed for battlefield use. This development continues today; modern self-propelled artillery vehicles are highly mobile weapons of great versatility providing the largest share of an army's total firepower.
In its earliest sense, the word artillery referred to any group of soldiers primarily armed with some form of manufactured weapon or armour. Since the introduction of gunpowder and cannon, the word "artillery" has largely meant cannon, and in contemporary usage, it usually refers to shell-firing guns, howitzers, mortars, rockets and guided missiles. In common speech, the word artillery is often used to refer to individual devices, along with their accessories and fittings, although these assemblages are more properly called "equipments". However, there is no generally recognised generic term for a gun, howitzer, mortar, and so forth: the United States uses "artillery piece", but most English-speaking armies use "gun" and "mortar". The projectiles fired are typically either "shot" (if solid) or "shell" (if not). "Shell" is a widely used generic term for a projectile, which is a component of munitions.
By association, artillery may also refer to the arm of service that customarily operates such engines. In some armies one arm has operated field, coast, anti-aircraft artillery and some anti-tank artillery, in others these have been separate arms and in some nations coast has been a naval or marine responsibility. In the 20th Century technology based target acquisition devices, such as radar, and systems, such as sound ranging and flash spotting, emerged to acquire targets, primarily for artillery. These are usually operated by one or more of the artillery arms. The widespread adoption of indirect fire in the early 20th century introduced the need for specialist data for field artillery, notably survey and meteorological, in some armies provision of these are the responsibility of the artillery arm.
Artillery originated for use against ground targets—against infantry, cavalry and other artillery. An early specialist development was coastal artillery for use against enemy ships. The early 20th Century saw the development of a new class of artillery for use against aircraft: anti-aircraft guns.
Artillery is arguably the most lethal form of land-based armament currently employed, and has been since at least the early Industrial Revolution. The majority of combat deaths in the Napoleonic Wars, World War I, and World War II were caused by artillery.[1] In 1944, Joseph Stalin said in a speech that artillery was "the God of War".[1]
Although not called as such, machines performing the role recognizable as artillery have been employed in warfare since antiquity. Historical references show artillery was first employed by the Roman legions at Syracuse in 399 BC,[citation needed] well before the Christian era. Until the introduction of gunpowder into western warfare, artillery was dependent upon mechanical energy which not only severely limited the kinetic energy of the projectiles, it also required the construction of very large engines to store sufficient energy. A 1st-century BC Roman catapult launching 6.55 kg (14.4 lb) stones achieved a kinetic energy of 16,000 joules, compared to a mid-19th-century 12-pounder gun, which fired a 4.1 kg (9.0 lb) round, with a kinetic energy of 240,000 joules, or a late 20th century US battleship that fired a 1,225 kg (2,701 lb) projectile from its main battery with an energy level surpassing 350,000,000 joules.
From the Middle Ages through most of the modern era, artillery pieces on land were moved by horse-drawn gun carriages. In the contemporary era, artillery pieces and their crew relied on wheeled or tracked vehicles as transportation. These land versions of artillery were dwarfed by railway guns, which includes the largest super-gun ever conceived, theoretically capable of putting a satellite into orbit. Artillery used by naval forces has also changed significantly, with missiles replacing guns in surface warfare.
Over the course of military history, projectiles were manufactured from a wide variety of materials, into a wide variety of shapes, using many different methods in which to target structural/defensive works and inflict enemy casualties. The engineering applications for ordnance delivery have likewise changed significantly over time, encompassing some of the most complex and advanced technologies in use today.
In some armies, the weapon of artillery is the projectile, not the equipment that fires it. The process of delivering fire onto the target is called gunnery. The actions involved in operating an artillery piece are collectively called "serving the gun" by the "detachment" or gun crew, constituting either direct or indirect artillery fire. The manner in which gunnery crews (or formations) are employed is called artillery support. At different periods in history this may refer to weapons designed to be fired from ground-, sea-, and even air-based weapons platforms.
The term "gunner" is used in some armed forces for the soldiers and sailors with the primary function of using artillery.
The gunners and their guns are usually grouped in teams called either "crews" or "detachments". Several such crews and teams with other functions are combined into a unit of artillery, usually called a battery, although sometimes called a company. In gun detachments, each role is numbered, starting with "1" the Detachment Commander, and the highest number being the Coverer, the second-in-command. "Gunner" is also the lowest rank and junior non-commissioned officers are "Bombardiers" in some artillery arms.
Batteries are roughly equivalent to a company in the infantry, and are combined into larger military organizations for administrative and operational purposes, either battalions or regiments, depending on the army. These may be grouped into brigades; the Russian army also groups some brigades into artillery divisions, and the People's Liberation Army has artillery corps.
The term "artillery" is also applied to a combat arm of most military services when used organizationally to describe units and formations of the national armed forces that operate the weapons.
During military operations, the role of field artillery is to provide support to other arms in combat or to attack targets, particularly in depth. Broadly, these effects fall into two categories, either to suppress or neutralize the enemy, or to cause casualties, damage, and destruction. This is mostly achieved by delivering high-explosive munitions to suppress, or inflict casualties on the enemy from casing fragments and other debris and blast, or by destroying enemy positions, equipment, and vehicles. Non-lethal munitions, notably smoke, can also be used to suppress or neutralize the enemy by obscuring their view.
Fire may be directed by an artillery observer or other observer, including manned and unmanned aircraft pilots, or called onto map coordinates.
Military doctrine has played a significant influence on the core engineering design considerations of artillery ordnance through its history, in seeking to achieve a balance between delivered volume of fire with ordnance mobility. However, during the modern period, the consideration of protecting the gunners also arose due to the late-19th-century introduction of the new generation of infantry weapons using conoidal bullet, better known as the Minié ball, with a range almost as long as that of field artillery.
The gunners' increasing proximity to and participation in direct combat against other combat arms and attacks by aircraft made the introduction of a gun shield necessary. The problems of how to employ a fixed or horse-towed gun in mobile warfare necessitated the development of new methods of transporting the artillery into combat. Two distinct forms of artillery developed: the towed gun, which was used primarily to attack or defend a fixed line; and the self-propelled gun, which was designed to accompany a mobile force and provide continuous fire support. These influences have guided the development of artillery ordnance, systems, organisations, and operations until the present, with artillery systems capable of providing support at ranges from as little as 100 m to the intercontinental ranges of ballistic missiles. The only combat in which artillery is unable to take part in is close quarters combat, with the possible exception of artillery reconnaissance teams.[2]
The word as used in the current context originated in the Middle Ages. One suggestion is that it comes from the Old French atellier, meaning "to arrange", and attillement, meaning "equipment".
From the 13th century, an artillier referred to a builder of any war equipment; and, for the next 250 years, the sense of the word "artillery" covered all forms of military weapons. Hence, the naming of the Honourable Artillery Company an essentially infantry unit until the 19th century. Another suggestion is that it comes from the Italian arte de tirare (art of shooting), coined by one of the first theorists on the use of artillery, Niccolò Tartaglia.
Mechanical systems used for throwing ammunition in ancient warfare, also known as "engines of war", like the catapult, onager, trebuchet, and ballista, are also referred to by military historians as artillery.
Early Chinese artillery had vase-like shapes. This includes the "long range awe inspiring" cannon dated from 1350 and found in the 14th century Ming Dynasty treatise Huolongjing.[3] With the development of better metallurgy techniques, later cannons abandoned the vase shape of early Chinese artillery. This change can be seen in the bronze "thousand ball thunder cannon," an early example of field artillery.[4] These small, crude weapons diffused into the Middle East (the madfaa, see also the German Wikipedia and midfa) and reached Europe in the 13th century, in a very limited manner.
In Asia, Mongols adopted the Chinese artillery and used it effectively in the great conquest. By the late 14th century, Chinese rebels used organized artillery and cavalry to push Mongols out.
As small smooth-bore tubes these were initially cast in iron or bronze around a core, with the first drilled bore ordnance recorded in operation near Seville in 1247.[citation needed] They fired lead, iron, or stone balls, sometimes large arrows and on occasions simply handfuls of whatever scrap came to hand. During the Hundred Years' War, these weapons became more common, initially as the bombard and later the cannon. Cannon were always muzzle-loaders. While there were many early attempts at breech-loading designs, a lack of engineering knowledge rendered these even more dangerous to use than muzzle-loaders.
In 1415, the Portuguese invaded the Mediterranean port town of Ceuta. While it is difficult to confirm the use of firearms in the siege of the city, it is known the Portuguese defended it thereafter with firearms, namely bombardas, colebratas, and falconetes. In 1419, Sultan Abu Sa'id led an army to reconquer the fallen city, and Moroccans brought cannons and used them in the assault on Ceuta. Finally, hand-held firearms and riflemen appear in Morocco, in 1437, in an expedition against the people of Tangiers.[7][page needed] It is clear these weapons had developed into several different forms, from small guns to large artillery pieces.
The artillery revolution in Europe caught on during the Hundred Years' War and changed the way that battles were fought. In the preceding decades, the English had even used a gunpowder-like weapon in military campaigns against the Scottish.[8] However, at this time, the cannons used in battle were very small and not particularly powerful. Cannons were only useful for the defense of a castle, as demonstrated at Breteuil in 1356, when the besieged English used a cannon to destroy an attacking French assault tower. By the end of the 14th century, cannon were only powerful enough to knock in roofs, and could not penetrate castle walls.
However, a major change occurred between 1420 and 1430, when artillery became much more powerful and could now batter strongholds and fortresses quite efficiently. The English, French, and Burgundians all advanced in military technology, and as a result the traditional advantage that went to the defense in a siege was lost. The cannon during this period were elongated, and the recipe for gunpowder was improved to make it three times as powerful as before.[9] These changes led to the increased power in the artillery weapons of the time.
Joan of Arc encountered gunpowder weaponry several times. When she led the French against the English at the Battle of Tourelles, in 1430, she faced heavy gunpowder fortifications, and yet her troops prevailed in that battle. In addition, she led assaults against the English-held towns of Jargeau, Meung, and Beaugency, all with the support of large artillery units. When she led the assault on Paris, Joan faced stiff artillery fire, especially from the suburb of St. Denis, which ultimately led to her defeat in this battle. In April 1430, she went to battle against the Burgundians, whose support was purchased by the English. At this time, the Burgundians had the strongest and largest gunpowder arsenal among the European powers, and yet the French, under Joan of Arc's leadership, were able to beat back the Burgundians and defend themselves.[11] As a result, most of the battles of the Hundred Years' War that Joan of Arc participated in were fought with gunpowder artillery.
The army of Mehmet the Conqueror, which conquered Constantinople in 1453, included both artillery and foot soldiers armed with gunpowder weapons.[12] The Ottomans brought to the siege sixty-nine guns in fifteen separate batteries and trained them at the walls of the city. The barrage of Ottoman cannon fire lasted forty days, and they are estimated to have fired 19,320 times.[13] Artillery also played a decisive role in the Battle of St. Jakob an der Birs of 1444.
The new Ming Dynasty established the "Divine Engine Battalion" (神机营), which specialized in various types of artillery. Light cannons and cannons with multiple volleys were developed. In a campaign to suppress a local minority rebellion near today's Burmese border, the Ming army used a 3-line formation of arquebuses/muskets to destroy an elephant formation.[citation needed]
Between 1593 and 1597, about 200,000 Korean and Chinese troops which fought against Japan in Korea actively used heavy artillery in both siege and field combat. Korean forces mounted artillery in ships as naval guns, providing an advantage against Japanese navy which used Kunikuzushi (国崩し – Japanese breech-loading swivel gun) and Ōzutsu (大筒 – large size Tanegashima) as their largest firearms.[14][15]
Bombards were of value mainly in sieges. A famous Turkish example used at the siege of Constantinople in 1453 weighed 19 tons[vague], took 200 men and sixty oxen to emplace, and could fire just seven times a day. The Fall of Constantinople was perhaps "the first event of supreme importance whose result was determined by the use of artillery" when the huge bronze cannons of Mehmed II breached the city's walls, ending the Byzantine Empire, according to Sir Charles Oman.[16]
Bombards developed in Europe were massive smoothbore weapons distinguished by their lack of a field carriage, immobility once emplaced, highly individual design, and noted unreliability (in 1460 James II, King of Scots, was killed when one exploded at the siege of Roxburgh). Their large size precluded the barrels being cast and they were constructed out of metal staves or rods bound together with hoops like a barrel, giving their name to the gun barrel.[17][page needed]
The use of the word "cannon" marks the introduction in the 15th century of a dedicated field carriage with axle, trail and animal-drawn limber—this produced mobile field pieces that could move and support an army in action, rather than being found only in siege and static defences. The reduction in the size of the barrel was due to improvements in both iron technology and gunpowder manufacture, while the development of trunnions – projections at the side of the cannon as an integral part of the cast – allowed the barrel to be fixed to a more movable base, and also made raising or lowering the barrel much easier.[17]
The first land-based mobile weapon is usually credited to Jan Žižka, who deployed his oxen-hauled cannon during the Hussite Wars of Bohemia (1418–1424). However cannons were still large and cumbersome. With the rise of musketry in the 16th century, cannon were largely (though not entirely) displaced from the battlefield—the cannon were too slow and cumbersome to be used and too easily lost to a rapid enemy advance.
The combining of shot and powder into a single unit, a cartridge, occurred in the 1620s with a simple fabric bag, and was quickly adopted by all nations. It speeded loading and made it safer, but unexpelled bag fragments were an additional fouling in the gun barrel and a new tool—a worm—was introduced to remove them. Gustavus Adolphus is identified as the general who made cannon an effective force on the battlefield—pushing the development of much lighter and smaller weapons and deploying them in far greater numbers than previously. The outcome of battles was still determined by the clash of infantry.
Shells, explosive-filled fused projectiles, were also developed in the 17th century.[citation needed] The development of specialized pieces—shipboard artillery, howitzers and mortars—was also begun in this period. More esoteric designs, like the multi-barrel ribauldequin (known as "organ guns"), were also produced.
The 1650 book by Kazimierz Siemienowicz Artis Magnae Artilleriae pars prima[18] was one of the most important contemporary publications on the subject of artillery. For over two centuries this work was used in Europe as a basic artillery manual.[citation needed]
One of the most significant effects of artillery during this period was however somewhat more indirect – by easily reducing to rubble any medieval-type fortification or city wall (some which had stood since Roman times), it abolished millennia of siege-warfare strategies and styles of fortification building.[17] This led, among other things, to a frenzy of new bastion-style fortifications to be built all over Europe and in its colonies, but also had a strong integrating effect on emerging nation-states, as kings were able to use their newfound artillery superiority to force any local dukes or lords to submit to their will, setting the stage for the absolutist kingdoms to come.[17]
Modern rocket artillery can trace its heritage back to the Mysorean rockets of India. Their first recorded use was in 1780 during the battles of the Second, Third and Fourth Mysore Wars. The wars fought between the British East India Company and the Kingdom of Mysore in India made use of the rockets as a weapon. In the Battle of Pollilur, the Siege of Seringapatam (1792) and in Battle of Seringapatam in 1799 these rockets were used with considerable effect against the British."[19] After the wars, several Mysore rockets were sent to England, and from 1801, William Congreve copied the rockets with minor modifications as the Congreve rocket which were used effectively during the Napoleonic Wars and the War of 1812.[20]
Cannons continued to become smaller and lighter—Frederick II of Prussia deployed the first genuine light artillery during the Seven Years' War.
Jean-Baptiste de Gribeauval, a French artillery engineer, introduced the standardization of cannon design in the mid-18th century. He developed a 6-inch (150 mm) field howitzer whose gun barrel, carriage assembly and ammunition specifications were made uniform for all French cannons. The standardized interchangeable parts of these cannons down to the nuts, bolts and screws made their mass production and repair much easier.
These improvements in the French artillery were essential for the later military successes of Napoleon. Napoleon, himself a former artillery officer, perfected the tactic of massed artillery batteries unleashed upon a critical point in his enemies' line as a prelude to a decisive infantry and cavalry assault.
The development of modern artillery occurred in the mid to late 19th century as a result of the convergence of various improvements in the underlying technology. Advances in metallurgy allowed for the construction of breech-loading rifled guns that could fire at a much greater muzzle velocity.
After the British artillery was shown up in the Crimean War as having barely changed since the Napoleonic Wars the industrialist William Armstrong was awarded a contract by the government to design a new piece of artillery. Production started in 1855 at the Elswick Ordnance Company and the Royal Arsenal at Woolwich, and the outcome was the revolutionary Armstrong Gun, which marked the birth of modern artillery.[21][22] Three of its features particularly stand out.
First, the piece was rifled, which allowed for a much more accurate and powerful action. Although rifling had been tried on small arms since the 15th century, the necessary machinery to accurately rifle artillery was only available by the mid-19th century. Martin von Wahrendorff, and Joseph Whitworth independently produced rifled cannon in the 1840s, but it was Armstrong's gun that was first to see widespread use during the Crimean War.[23] The cast iron shell of the Armstrong gun was similar in shape to a Minié ball and had a thin lead coating which made it fractionally larger than the gun's bore and which engaged with the gun's rifling grooves to impart spin to the shell. This spin, together with the elimination of windage as a result of the tight fit, enabled the gun to achieve greater range and accuracy than existing smooth-bore muzzle-loaders with a smaller powder charge.
His gun was also a breech-loader. Although attempts at breech-loading mechanisms had been made since medieval times, the essential engineering problem was that the mechanism couldn't withstand the explosive charge. It was only with the advances in metallurgy and precision engineering capabilities during the Industrial Revolution that Armstrong was able to construct a viable solution. The gun combined all the properties that make up an effective artillery piece. The gun was mounted on a carriage in such a way as to return the gun to firing position after the recoil.
What made the gun really revolutionary lay in the technique of the construction of the gun barrel that allowed it to withstand much more powerful explosive forces. The "built-up" method involved assembling the barrel with wrought-iron (later mild steel was used) tubes of successively smaller diameter.[24] The tube would then be heated to allow it to expand and fit over the previous tube. When it cooled the gun would contract although not back to its original size, which allowed an even pressure along the walls of the gun which was directed inward against the outward forces that the gun firing exerted on the barrel.[25]
Another innovative feature, more usually associated with 20th-century guns, was what Armstrong called its "grip", which was essentially a squeeze bore; the 6 inches of the bore at the muzzle end was of slightly smaller diameter, which centered the shell before it left the barrel and at the same time slightly swaged down its lead coating, reducing its diameter and slightly improving its ballistic qualities.
Armstrong's system was adopted in 1858, initially for "special service in the field" and initially he only produced smaller artillery pieces, 6-pounder (2.5 in/64 mm) mountain or light field guns, 9-pounder (3 in/76 mm) guns for horse artillery, and 12-pounder (3 inches /76 mm) field guns.
The first cannon to contain all 'modern' features is generally considered to be the French 75 of 1897.[26][27] It was the first field gun to include a hydro-pneumatic recoil mechanism, which kept the gun's trail and wheels perfectly still during the firing sequence. Since it did not need to be re-aimed after each shot, the crew could fire as soon as the barrel returned to its resting position. In typical use, the French 75 could deliver fifteen rounds per minute on its target, either shrapnel or melinite high-explosive, up to about 5 miles (8,500 m) away. Its firing rate could even reach close to 30 rounds per minute, albeit only for a very short time and with a highly experienced crew. These were rates that contemporary bolt action rifles could not match. The gun used cased ammunition, was breech-loading, had modern sights, a self-contained firing mechanism and hydro-pneumatic recoil dampening.
Indirect fire, the firing of a projectile without relying on direct line of sight between the gun and the target, possibly dates back to the 16th century.[28] Early battlefield use of indirect fire may have occurred at Paltzig in July 1759, when the Russian artillery fired over the tops of trees,[29] and at the Battle of Waterloo, where a battery of the Royal Horse Artillery fired Shrapnel indirectly against advancing French troops.[30]
In 1882, Russian Lieutenant Colonel KG Guk published Indirect Fire for Field Artillery, which provided a practical method of using aiming points for indirect fire by describing, "all the essentials of aiming points, crest clearance, and corrections to fire by an observer".[31]
A few years later, the Richtfläche (lining-plane) sight was invented in Germany and provided a means of indirect laying in azimuth, complementing the clinometers for indirect laying in elevation which already existed. Despite conservative opposition within the German army, indirect fire was adopted as doctrine by the 1890s. In the early 1900s, Goertz in Germany developed an optical sight for azimuth laying. It quickly replaced the lining-plane; in English, it became the 'Dial Sight' (UK) or 'Panoramic Telescope' (US).
The British halfheartedly experimented with indirect fire techniques since the 1890s, but with the onset of the Boer War, they were the first to apply the theory in practice in 1899, although they had to improvise without a lining-plane sight.[32]
In the next 15 years leading up to World War I, the techniques of indirect fire became available for all types of artillery. Indirect fire was the defining characteristic of 20th-century artillery and led to undreamt of changes in the amount of artillery, its tactics, organisation, and techniques, most of which occurred during World War I.
An implication of indirect fire and improving guns was increasing range between gun and target, this increased the time of flight and the vertex of the trajectory. The result was decreasing accuracy (the increasing distance between the target and the mean point of impact of the shells aimed at it) caused by the increasing effects of non-standard conditions. Indirect firing data was based on standard conditions including a specific muzzle velocity, zero wind, air temperature and density, and propellant temperature. In practice, this standard combination of conditions almost never existed, they varied throughout the day and day to day, and the greater the time of flight, the greater the inaccuracy. An added complication was the need for survey to accurately fix the coordinates of the gun position and provide accurate orientation for the guns. Of course, targets had to be accurately located, but by 1916, air photo interpretation techniques enabled this, and ground survey techniques could sometimes be used.
In 1914, the methods of correcting firing data for the actual conditions were often convoluted, and the availability of data about actual conditions was rudimentary or non-existent, the assumption was that fire would always be ranged (adjusted). British heavy artillery worked energetically to progressively solve all these problems from late 1914 onwards, and by early 1918, had effective processes in place for both field and heavy artillery. These processes enabled 'map-shooting', later called 'predicted fire'; it meant that effective fire could be delivered against an accurately located target without ranging. Nevertheless, the mean point of impact was still some tens of yards from the target-centre aiming point. It was not precision fire, but it was good enough for concentrations and barrages. These processes remain in use into the 21st Century with refinements to calculations enabled by computers and improved data capture about non-standard conditions.The British major-general Henry Hugh Tudor pioneered armour and artillery cooperation at the breakthrough Battle of Cambrai. The improvements in providing and using data for non-standard conditions (propellant temperature, muzzle velocity, wind, air temperature, and barometric pressure) were developed by the major combatants throughout the war and enabled effective predicted fire.[33] The effectiveness of this was demonstrated by the British in 1917 (at Cambrai) and by Germany the following year (Operation Michael).
Major General J. B. A. Bailey, British Army (retired) wrote:
From the middle of the eighteenth century to the middle of the nineteenth, artillery is judged to have accounted for perhaps 50% of battlefield casualties. In the sixty years preceding 1914, this figure was probably as low as 10 percent. The remaining 90 percent fell to small arms, whose range and accuracy had come to rival those of artillery. ... [By WWI] The British Royal Artillery, at over one million men, grew to be larger than the Royal Navy. Bellamy (1986), pp. 1–7, cites the percentage of casualties caused by artillery in various theaters since 1914: in the First World War, 45 percent of Russian casualties and 58 percent of British casualties on the Western Front; in the Second World War, 75 percent of British casualties in North Africa and 51 percent of Soviet casualties (61 percent in 1945) and 70 percent of German casualties on the Eastern Front; and in the Korean War, 60 percent of US casualties, including those inflicted by mortars.[34]— J. B. A. Bailey (2004). Field artillery and firepower
An estimated 75,000 French soldiers were casualties of friendly artillery fire in the four years of World War I.[35]
Modern artillery is most obviously distinguished by its long range, firing an explosive shell or rocket and a mobile carriage for firing and transport. However, its most important characteristic is the use of indirect fire, whereby the firing equipment is aimed without seeing the target through its sights. Indirect fire emerged at the beginning of the 20th century and was greatly enhanced by the development of predicted fire methods in World War I. However, indirect fire was area fire; it was and is not suitable for destroying point targets; its primary purpose is area suppression. Nevertheless, by the late 1970s precision-guided munitions started to appear, notably the US 155 mm Copperhead and its Soviet 152 mm Krasnopol equivalent that had success in Indian service. These relied on laser designation to 'illuminate' the target that the shell homed onto. However, in the early 21st Century, the Global Positioning System (GPS) enabled relatively cheap and accurate guidance for shells and missiles, notably the US 155 mm Excalibur and the 227 mm GMLRS rocket. The introduction of these led to a new issue, the need for very accurate three dimensional target coordinates – the mensuration process.
Weapons covered by the term 'modern artillery' include "cannon" artillery (such as howitzer, mortar, and field gun) and rocket artillery. Certain smaller-caliber mortars are more properly designated small arms rather than artillery, albeit indirect-fire small arms. This term also came to include coastal artillery which traditionally defended coastal areas against seaborne attack and controlled the passage of ships. With the advent of powered flight at the start of the 20th century, artillery also included ground-based anti-aircraft batteries.
The term "artillery" has traditionally not been used for projectiles with internal guidance systems, preferring the term "missilery",[citation needed] though some modern artillery units employ surface-to-surface missiles. Advances in terminal guidance systems for small munitions has allowed large-caliber guided projectiles to be developed, blurring this distinction.
One of the most important roles of logistics is the supply of munitions as a primary type of artillery consumable, their storage (ammunition dump, arsenal, magazine ) and the provision of fuses, detonators and warheads at the point where artillery troops will assemble the charge, projectile, bomb or shell.
A round of artillery ammunition comprises four components:
Wikimedia Commons has media related to Fuzes. |
Fuzes are the devices that initiate an artillery projectile, either to detonate its high explosive (HE) filling or eject its cargo (illuminating flare or smoke canisters being examples). The official military spelling is "fuze".[36] Broadly there are four main types:
Most artillery fuzes are nose fuzes. However, base fuzes have been used with armour piercing shells and for squash head (HESH or HEP) anti-tank shells. At least one nuclear shell and its non-nuclear spotting version also used a multi-deck mechanical time fuze fitted into its base.
Impact fuzes were, and in some armies remain, the standard fuze for HE projectiles. Their default action is normally 'superquick', some have had a 'graze' action which allows them to penetrate light cover and others have 'delay'. Delay fuzes allow the shell to penetrate the ground before exploding. Armor- or concrete-piercing fuzes are specially hardened. During World War I and later, ricochet fire with delay or graze fuzed HE shells, fired with a flat angle of descent, was used to achieve airburst.
HE shells can be fitted with other fuzes. Airburst fuzes usually have a combined airburst and impact function. However, until the introduction of proximity fuzes, the airburst function was mostly used with cargo munitions—for example, shrapnel, illumination, and smoke. The larger calibers of anti-aircraft artillery are almost always used airburst. Airburst fuzes have to have the fuze length (running time) set on them. This is done just before firing using either a wrench or a fuze setter pre-set to the required fuze length.
Early airburst fuzes used igniferous timers which lasted into the second half of the 20th century. Mechanical time fuzes appeared in the early part of the century. These required a means of powering them. The Thiel mechanism used a spring and escapement (i.e. 'clockwork'), Junghans used centrifugal force and gears, and Dixi used centrifugal force and balls. From about 1980, electronic time fuzes started replacing mechanical ones for use with cargo munitions.
Proximity fuzes have been of two types: photo-electric or radar. The former was not very successful and seems only to have been used with British anti-aircraft artillery 'unrotated projectiles' (rockets) in World War II. Radar proximity fuzes were a big improvement over the mechanical (time) fuzes which they replaced. Mechanical time fuzes required an accurate calculation of their running time, which was affected by non-standard conditions. With HE (requiring a burst 20 to 30 feet (9.1 m) above the ground), if this was very slightly wrong the rounds would either hit the ground or burst too high. Accurate running time was less important with cargo munitions that burst much higher.
The first radar proximity fuzes (codenamed 'VT') were initially used against aircraft in World War II. Their ground use was delayed for fear of the enemy recovering 'blinds' (artillery shells which failed to detonate) and copying the fuze. The first proximity fuzes were designed to detonate about 30 feet (9.1 m) above the ground. These air-bursts are much more lethal against personnel than ground bursts because they deliver a greater proportion of useful fragments and deliver them into terrain where a prone soldier would be protected from ground bursts.
However, proximity fuzes can suffer premature detonation because of the moisture in heavy rain clouds. This led to 'controlled variable time' (CVT) after World War II. These fuzes have a mechanical timer that switched on the radar about 5 seconds before expected impact, they also detonated on impact.
The proximity fuze emerged on the battlefields of Europe in late December 1944. They have become known as the U.S. Artillery's "Christmas present", and were much appreciated when they arrived during the Battle of the Bulge. They were also used to great effect in anti-aircraft projectiles in the Pacific against kamikaze as well as in Britain against V-1 flying bombs.[37]
Electronic multi-function fuzes started to appear around 1980. Using solid-state electronics they were relatively cheap and reliable, and became the standard fitted fuze in operational ammunition stocks in some western armies. The early versions were often limited to proximity airburst, albeit with height of burst options, and impact. Some offered a go/no-go functional test through the fuze setter.
Later versions introduced induction fuze setting and testing instead of physically placing a fuze setter on the fuze. The latest, such as Junghan's DM84U provide options giving, superquick, delay, a choice of proximity heights of burst, time and a choice of foliage penetration depths.
A new type of artillery fuze will appear soon. In addition to other functions these offer some course correction capability, not full precision but sufficient to significantly reduce the dispersion of the shells on the ground.
The projectile is the munition or "bullet" fired downrange. This may or may not be an explosive device. Traditionally, projectiles have been classified as "shot" or "shell", the former being solid and the latter having some form of "payload".
Shells can also be divided into three configurations: bursting, base ejection or nose ejection. The latter is sometimes called the shrapnel configuration. The most modern is base ejection, which was introduced in World War I. Both base and nose ejection are almost always used with airburst fuzes. Bursting shells use various types of fuze depending on the nature of the payload and the tactical need at the time.
Payloads have included:
Most forms of artillery require a propellant to propel the projectile at the target. Propellant is always a low explosive, this means it deflagrates instead of detonating, as with high explosives. The shell is accelerated to a high velocity in a very short time by the rapid generation of gas from the burning propellant. This high pressure is achieved by burning the propellant in a contained area, either the chamber of a gun barrel or the combustion chamber of a rocket motor.
Until the late 19th century, the only available propellant was black powder. Black powder had many disadvantages as a propellant; it has relatively low power, requiring large amounts of powder to fire projectiles, and created thick clouds of white smoke that would obscure the targets, betray the positions of guns, and make aiming impossible. In 1846, nitrocellulose (also known as guncotton) was discovered, and the high explosive nitroglycerin was discovered at much the same time. Nitrocellulose was significantly more powerful than black powder, and was smokeless. Early guncotton was unstable, however, and burned very fast and hot, leading to greatly increased barrel wear. Widespread introduction of smokeless powder would wait until the advent of the double-base powders, which combine nitrocellulose and nitroglycerin to produce powerful, smokeless, stable propellant.
Many other formulations were developed in the following decades, generally trying to find the optimum characteristics of a good artillery propellant; low temperature, high energy, non-corrosive, highly stable, cheap, and easy to manufacture in large quantities. Broadly, modern gun propellants are divided into three classes: single-base propellants which are mainly or entirely nitrocellulose based, double-base propellants composed of a combination of nitrocellulose and nitroglycerin, and triple base composed of a combination of nitrocellulose and nitroglycerin and Nitroguanidine.
Artillery shells fired from a barrel can be assisted to greater range in three ways:
Propelling charges for tube artillery can be provided in one of two ways: either as cartridge bags or in metal cartridge cases. Generally, anti-aircraft artillery and smaller-caliber (up to 3" or 76.2 mm) guns use metal cartridge cases that include the round and propellant, similar to a modern rifle cartridge. This simplifies loading and is necessary for very high rates of fire. Bagged propellant allows the amount of powder to be raised or lowered, depending on the range to the target. It also makes handling of larger shells easier. Each requires a totally different type of breech to the other. A metal case holds an integral primer to initiate the propellant and provides the gas seal to prevent the gases leaking out of the breech; this is called obturation. With bagged charges, the breech itself provides obturation and holds the primer. In either case, the primer is usually percussion, but electrical is also used, and laser ignition is emerging. Modern 155 mm guns have a primer magazine fitted to their breech.
Artillery ammunition has four classifications according to use:
This section does not cite any sources. Please help improve this section by adding citations to reliable sources. Unsourced material may be challenged and removed. (May 2017) (Learn how and when to remove this template message) |
Because field artillery mostly uses indirect fire the guns have to be part of a system that enables them to attack targets invisible to them in accordance with the combined arms plan.
The main functions in the field artillery system are:
Organisationally and spatially, these functions can be arranged in many ways. Since the creation of modern indirect fire, different armies have done it differently at different times and in different places. Technology is often a factor, but so are military–social issues, the relationships between artillery and other arms, and the criteria by which military capability, efficiency, and effectiveness are judged. Cost is also an issue because artillery is expensive due to the large quantities of ammunition that it uses and its level of manpower.
Communications underpin the artillery system, as it must be reliable and available in real-time. During the 20th century communications often used flags, morse code by radio, line and lights (which could include voice and teleprinter, to name a few contrivances). Radio has included HF, VHF, satellite and radio relay as well as modern tactical trunk systems. In western armies radio communications are now usually encrypted.[citation needed]
The emergence of mobile and man-portable radios after World War I had a major impact on artillery because it enabled fast and mobile operations with observers accompanying the infantry or armoured troops. In World War II, some armies fitted their self-propelled guns with radios. However, sometimes in the first half of the 20th century, hardcopy artillery fire plans and map traces were distributed.
Data communications can be especially important for artillery because by using structured messages and defined data types fire control messages can be automatically routed and processed by computers. For example, a target acquisition element can send a message with target details which is automatically routed through the tactical and technical fire control elements to deliver firing data to the gun's laying system and the gun automatically laid. As tactical data networks become pervasive, they will provide any connected soldier with a means for reporting target information and requesting artillery fire.
Command is the authority to allocate resources, typically by assigning artillery formations or units. Terminology and its implications vary widely. However, very broadly, artillery units are assigned in direct support or in general support. Typically, the former mostly provide close support to manoeuvre units, while the latter may provide close support and or depth fire, notably counter-battery. Generally, 'direct support' also means that the artillery unit provides artillery observation and liaison teams to the supported units. Sometimes, direct support units are placed under command of the regiment/brigade they support. General support units may be grouped into artillery formations; for example, brigades, even divisions, or multi-battalion regiments, and usually under command of division, corps, or higher HQs. General support units tend to be moved to where they are most required at any particular time. Artillery command may impose priorities and constraints to support their combined arms commander's plans.
Target acquisition can take many forms, it is usually observation in real time, but may be the product of analysis. Artillery observation teams are the most common means of target acquisition. However, air observers have been use since the beginning of indirect fire and were quickly joined by air photography. Target acquisition may also be by anyone that can get the information into the artillery system. Targets may be visible to forward troops or in depth and invisible to them.
Observation equipment can vary widely in its complexity.
Control, sometimes called tactical fire control, is primarily concerned with 'targeting' and the allotment of fire units to targets. This is vital when a target is within range of many fire units and the number of fire units needed depends on the nature of the target, and the circumstances and purpose of its engagement. Targeting is concerned with selecting the right weapons in the right quantities to achieve the required effects on the target. Allotment attempts to address the artillery dilemma—important targets are rarely urgent and urgent targets are rarely important. Of course importance is a matter of perspective; what is important to a divisional commander is rarely the same as what is important to an infantry platoon commander.
Broadly, there are two situations: fire against opportunity targets, and targets whose engagement is planned as part of a particular operation. In the latter situation, command assigns fire units to the operation and an overall artillery fire planner makes a plan, possibly delegating resources for some parts of it to other planners. Fire plans may also involve use of non-artillery assets, such as mortars and aircraft.
Control of fire against opportunity targets is an important differentiator between different types of artillery system. In some armies, only designated artillery HQs have the tactical fire control authority to order fire units to engage a target, all 'calls for fire' being requests to these HQs. This authority may also extend to deciding the type and quantity of ammunition to be used. In other armies, an 'authorised observer' (for example, artillery observation team or other target acquisition element) can order fire units to engage. In the latter case, a battery observation team can order fire to their own battery and may be authorised to order fire to their own battalion, and sometimes to many battalions. For example, a divisional artillery commander may authorise selected observers to order fire to the entire divisional artillery. When observers or cells are not authorised, they can still request fire.
Armies that apply forward tactical control generally put the majority of the more senior officers of artillery units forward in command observation posts or with the supported arm. Those that do not use this approach tend to put these officers close to the guns. In either case, the observation element usually controls fire in detail against the target, such as adjusting it onto the target, moving it, and coordinating it with the supported arm as necessary to achieve the required effects.
Firing data has to be calculated and is the key to indirect fire; the arrangements for this have varied widely. Firing data has two components: quadrant elevation and azimuth, to these may be added the size of propelling charge and the fuze setting. The process to produce firing data is sometimes called technical fire control. Before computers, some armies set the range on the gun's sights, which mechanically corrected it for the gun's muzzle velocity. For the first few decades of indirect fire, firing data were calculated by the observer, who then adjusted the fall of shot onto the target.
The need to engage targets at night, in depth, or hit the target with the first rounds led to predicted fire being quickly developed in World War I. Predicted fire existed alongside the older method. After World War II, predicted methods were invariably applied, but the fall of shot usually needed adjustment because of inaccuracy in locating the target, the proximity of friendly troops, or the need to engage a moving target. Target location errors were significantly reduced once laser rangefinders, orientation, and navigation devices were issued to observation parties.
In predicted fire, the basic geospatial data of range, angle of sight, and azimuth between a fire unit and its target was produced and corrected for variations from the 'standard conditions'. These variations included barrel wear, propellant temperature, different projectiles weights that all affected the muzzle velocity, and air temperature, density, wind speed & direction, and rotation of the Earth that affect the shell in flight. The net effect of variations can also be determined by shooting at an accurately known point, a process called 'registration'.
All these calculations to produce a quadrant elevation (or range) and azimuth were done manually using instruments, tablulated, data of the moment, and approximations until battlefield computers started appearing in the 1960s and 1970s. While some early calculators copied the manual method (typically substituting polynomials for tabulated data), computers use a different approach. They simulate a shell's trajectory by 'flying' it in short steps and applying data about the conditions affecting the trajectory at each step. This simulation is repeated until it produces a quadrant elevation and azimuth that lands the shell within the required 'closing' distance of the target coordinates. NATO has a standard ballistic model for computer calculations and has expanded the scope of this into the NATO Armaments Ballistic Kernel (NABK)[44] within the SG2 Shareable (Fire Control) Software Suite (S4).
Technical fire control has been performed in various places, but mostly in firing batteries. However, in the 1930s, the French moved it to battalion level and combined it with some tactical fire control. This was copied by the US. Nevertheless, most armies seemed to have retained it within firing batteries, and some duplicated the technical fire control teams in a battery to give operational resilience and tactical flexibility. Computers reduced the number of men needed and enabled decentralisation of technical fire control to autonomous sub-battery fire units, such as platoons, troops, or sections, although some armies had sometimes done this with their manual methods. Computation on the gun or launcher, integrated with their laying system, is also possible. MLRS led the way in this.
A fire unit is the smallest artillery element, consisting of one or more weapon systems, capable of being employed to execute a fire assigned by a tactical fire controller. Generally it is a battery, but sub-divided batteries are also used. On occasions a battery of 6 guns has been 6 fire units. Fire units may or may not occupy separate positions.
Specialist services provide data need for predicted fire. Increasingly, they are provided from within firing units. These services include:
Supply of artillery ammunition has always been a major component of military logistics. Up until World War I some armies made artillery responsible for all forward ammunition supply because the load of small arms ammunition was trivial compared to artillery. Different armies use different approaches to ammunition supply, which can vary with the nature of operations. Differences include where the logistic service transfers artillery ammunition to artillery, the amount of ammunition carried in units and extent to which stocks are held at unit or battery level. A key difference is whether supply is 'push' or 'pull'. In the former the 'pipeline' keeps pushing ammunition into formations or units at a defined rate. In the latter units fire as tactically necessary and replenish to maintain or reach their authorised holding (which can vary), so the logistic system has to be able to cope with surge and slack.
Artillery types can be categorised in several ways, for example by type or size of weapon or ordnance, by role or by organizational arrangements.
The types of cannon artillery are generally distinguished by the velocity at which they fire projectiles. Types of artillery:
Modern field artillery can also be split into two other subcategories: towed and self-propelled. As the name suggests, towed artillery has a prime mover, usually an artillery tractor or truck, to move the piece, crew, and ammunition around. Towed artillery is in some cases equipped with an APU for small displacements. Self-propelled artillery is permanently mounted on a carriage or vehicle with room for the crew and ammunition and is thus capable of moving quickly from one firing position to another, both to support the fluid nature of modern combat and to avoid counter-battery fire. It includes mortar carrier vehicles, many of which allow the mortar to be removed from the vehicle and be used dismounted, potentially in terrain in which the vehicle cannot navigate, or in order to avoid detection.
At the beginning of the modern artillery period, the late 19th century, many armies had three main types of artillery, in some case they were sub-branches within the artillery branch in others they were separate branches or corps. There were also other types excluding the armament fitted to warships:
After World War I many nations merged these different artillery branches, in some cases keeping some as sub-branches. Naval artillery disappeared apart from that belonging to marines. However, two new branches of artillery emerged during that war and its aftermath, both used specialised guns (and a few rockets) and used direct not indirect fire, in the 1950s and 1960s both started to make extensive use of missiles:
However, the general switch by artillery to indirect fire before and during World War I led to a reaction in some armies. The result was accompanying or infantry guns. These were usually small, short range guns, that could be easily man-handled and used mostly for direct fire but some could use indirect fire. Some were operated by the artillery branch but under command of the supported unit. In World War II they were joined by self-propelled assault guns, although other armies adopted infantry or close support tanks in armoured branch units for the same purpose, subsequently tanks generally took on the accompanying role.
The three main types of artillery "gun" are guns, howitzers and mortars. During the 20th century, guns and howitzers have steadily merged in artillery use, making a distinction between the terms somewhat meaningless. By the end of the 20th century, true guns with calibers larger than about 60 mm had become very rare in artillery use, the main users being tanks, ships, and a few residual anti-aircraft and coastal guns. The term "cannon" is a United States generic term that includes guns, howitzers and mortars; it is not used in other English speaking armies.
The traditional definitions differentiated between guns and howitzers in terms of maximum elevation (well less than 45° as opposed to close to or greater than 45°), number of charges (one or more than one charge), and having higher or lower muzzle velocity, sometimes indicated by barrel length. These three criteria give eight possible combinations, of which guns and howitzers are but two. However, modern "howitzers" have higher velocities and longer barrels than the equivalent "guns" of the first half of the 20th century.
True guns are characterized by long range, having a maximum elevation significantly less than 45°, a high muzzle velocity and hence a relatively long barrel, smooth bore (no rifling) and a single charge. The latter often led to fixed ammunition where the projectile is locked to the cartridge case. There is no generally accepted minimum muzzle velocity or barrel length associated with a gun.Howitzers can fire at maximum elevations at least close to 45°; elevations up to about 70° are normal for modern howitzers. Howitzers also have a choice of charges, meaning that the same elevation angle of fire will achieve a different range depending on the charge used. They have rifled bores, lower muzzle velocities and shorter barrels than equivalent guns. All this means they can deliver fire with a steep angle of descent. Because of their multi-charge capability, their ammunition is mostly separate loading (the projectile and propellant are loaded separately).
That leaves six combinations of the three criteria, some of which have been termed gun howitzers. A term first used in the 1930s when howitzers with a relatively high maximum muzzle velocities were introduced, it never became widely accepted, most armies electing to widen the definition of "gun" or "howitzer". By the 1960s, most equipments had maximum elevations up to about 70°, were multi-charge, had quite high maximum muzzle velocities and relatively long barrels.
Mortars are simpler. The modern mortar originated in World War I and there were several patterns. After that war, most mortars settled on the Stokes pattern, characterized by a short barrel, smooth bore, low muzzle velocity, elevation angle of firing generally greater than 45°, and a very simple and light mounting using a "baseplate" on the ground. The projectile with its integral propelling charge was dropped down the barrel from the muzzle to hit a fixed firing pin. Since that time, a few mortars have become rifled and adopted breech loading.
There are other recognized typifying characteristics for artillery. One such characteristic is the type of obturation used to seal the chamber and prevent gases escaping through the breech. This may use a metal cartridge case that also holds the propelling charge, a configuration called "QF" or "quickfiring" by some nations. The alternative does not use a metal cartridge case, the propellant being merely bagged or in combustible cases with the breech itself providing all the sealing. This is called "BL" or "breech loading" by some nations.
A second characteristic is the form of propulsion. Modern equipment can either be towed or self-propelled (SP). A towed gun fires from the ground and any inherent protection is limited to a gun shield. Towing by horse teams lasted throughout World War II in some armies, but others were fully mechanized with wheeled or tracked gun towing vehicles by the outbreak of that war. The size of a towing vehicle depends on the weight of the equipment and the amount of ammunition it has to carry.
A variation of towed is portee, where the vehicle carries the gun which is dismounted for firing. Mortars are often carried this way. A mortar is sometimes carried in an armored vehicle and can either fire from it or be dismounted to fire from the ground. Since the early 1960s it has been possible to carry lighter towed guns and most mortars by helicopter. Even before that, they were parachuted or landed by glider from the time of the first airborne trials in the USSR in the 1930s.
In an SP equipment, the gun is an integral part of the vehicle that carries it. SPs first appeared during World War I, but did not really develop until World War II. They are mostly tracked vehicles, but wheeled SPs started to appear in the 1970s. Some SPs have no armor and carry little or no ammunition. Armoured SPs usually carry a useful ammunition load. Early armoured SPs were mostly a "casemate" configuration, in essence an open top armored box offering only limited traverse. However, most modern armored SPs have a full enclosed armored turret, usually giving full traverse for the gun. Many SPs cannot fire without deploying stabilizers or spades, sometimes hydraulic. A few SPs are designed so that the recoil forces of the gun are transferred directly onto the ground through a baseplate. A few towed guns have been given limited self-propulsion by means of an auxiliary engine.
Two other forms of tactical propulsion were used in the first half of the 20th century: Railways or transporting the equipment by road, as two or three separate loads, with disassembly and re-assembly at the beginning and end of the journey. Railway artillery took two forms, railway mountings for heavy and super-heavy guns and howitzers and armored trains as "fighting vehicles" armed with light artillery in a direct fire role. Disassembled transport was also used with heavy and super heavy weapons and lasted into the 1950s.
A third form of artillery typing is to classify it as "light", "medium", "heavy" and various other terms. It appears to have been introduced in World War I, which spawned a very wide array of artillery in all sorts of sizes so a simple categorical system was needed. Some armies defined these categories by bands of calibers. Different bands were used for different types of weapons—field guns, mortars, anti-aircraft guns and coast guns.
List of countries in order of amount of artillery:[45]
Artillery is used in a variety of roles depending on its type and caliber. The general role of artillery is to provide fire support—"the application of fire, coordinated with the manoeuvre of forces to destroy, neutralize or suppress the enemy". This NATO definition, of course, makes artillery a supporting arm although not all NATO armies agree with this logic. The italicised terms are NATO's.[57]
Unlike rockets, guns (or howitzers as some armies still call them) and mortars are suitable for delivering close supporting fire. However, they are all suitable for providing deep supporting fire although the limited range of many mortars tends to exclude them from the role. Their control arrangements and limited range also mean that mortars are most suited to direct supporting fire. Guns are used either for this or general supporting fire while rockets are mostly used for the latter. However, lighter rockets may be used for direct fire support. These rules of thumb apply to NATO armies.
Modern mortars, because of their lighter weight and simpler, more transportable design, are usually an integral part of infantry and, in some armies, armor units. This means they generally do not have to concentrate their fire so their shorter range is not a disadvantage. Some armies also consider infantry operated mortars to be more responsive than artillery, but this is a function of the control arrangements and not the case in all armies. However, mortars have always been used by artillery units and remain with them in many armies, including a few in NATO.
In NATO armies artillery is usually assigned a tactical mission that establishes its relationship and responsibilities to the formation or units it is assigned to. It seems that not all NATO nations use the terms and outside NATO others are probably used. The standard terms are: direct support, general support, general support reinforcing and reinforcing. These tactical missions are in the context of the command authority: operational command, operational control, tactical command or tactical control.
In NATO direct support generally means that the directly supporting artillery unit provides observers and liaison to the manoeuvre troops being supported, typically an artillery battalion or equivalent is assigned to a brigade and its batteries to the brigade's battalions. However, some armies achieve this by placing the assigned artillery units under command of the directly supported formation. Nevertheless, the batteries' fire can be concentrated onto a single target, as can the fire of units in range and with the other tactical missions.
There are several dimensions to this subject. The first is the notion that fire may be against an opportunity target or may be prearranged. If it is the latter it may be either on-call or scheduled. Prearranged targets may be part of a fire plan. Fire may be either observed or unobserved, if the former it may be adjusted, if the latter then it has to be predicted. Observation of adjusted fire may be directly by a forward observer or indirectly via some other target acquisition system.
NATO also recognises several different types of fire support for tactical purposes:
These purposes have existed for most of the 20th century, although their definitions have evolved and will continue to do so, lack of suppression in counterbattery is an omission. Broadly they can be defined as either:
Two other NATO terms also need definition:
The tactical purposes also include various "mission verbs", a rapidly expanding subject with the modern concept of "effects based operations".
Targeting is the process of selecting target and matching the appropriate response to them taking account of operational requirements and capabilities. It requires consideration of the type of fire support required and the extent of coordination with the supported arm. It involves decisions about:
The targeting process is the key aspect of tactical fire control. Depending on the circumstances and national procedures it may all be undertaken in one place or may be distributed. In armies practicing control from the front, most of the process may be undertaken by a forward observer or other target acquirer. This is particularly the case for a smaller target requiring only a few fire units. The extent to which the process is formal or informal and makes use of computer based systems, documented norms or experience and judgement also varies widely armies and other circumstances.
Surprise may be essential or irrelevant. It depends on what effects are required and whether or not the target is likely to move or quickly improve its protective posture. During World War II UK researchers concluded that for impact fuzed munitions the relative risk were as follows:
Airburst munitions significantly increase the relative risk for lying men, etc. Historically most casualties occur in the first 10–15 seconds of fire, i.e. the time needed to react and improve protective posture, however, this is less relevant if airburst is used.
There are several ways of making best use of this brief window of maximum vulnerability:
Modern counter-battery fire developed in World War I, with the objective of defeating the enemy's artillery. Typically such fire was used to suppress enemy batteries when they were or were about to interfere with the activities of friendly forces (such as to prevent enemy defensive artillery fire against an impending attack) or to systematically destroy enemy guns. In World War I the latter required air observation. The first indirect counter-battery fire was in May 1900 by an observer in a balloon.
Enemy artillery can be detected in two ways, either by direct observation of the guns from the air or by ground observers (including specialist reconnaissance), or from their firing signatures. This includes radars tracking the shells in flight to determine their place of origin, sound ranging detecting guns firing and resecting their position from pairs of microphones or cross-observation of gun flashes using observation by human observers or opto-electronic devices, although the widespread adoption of 'flashless' propellant limited the effectiveness of the latter.
Once hostile batteries have been detected they may be engaged immediately by friendly artillery or later at an optimum time, depending on the tactical situation and the counter-battery policy. Air strike is another option. In some situations the task is to locate all active enemy batteries for attack using a counter-battery fire at the appropriate moment in accordance with a plan developed by artillery intelligence staff. In other situations counter-battery fire may occur whenever a battery is located with sufficient accuracy.
Modern counter-battery target acquisition uses unmanned aircraft, counter-battery radar, ground reconnaissance and sound-ranging. Counter-battery fire may be adjusted by some of the systems, for example the operator of an unmanned aircraft can 'follow' a battery if it moves. Defensive measures by batteries include frequently changing position or constructing defensive earthworks, the tunnels used by North Korea being an extreme example. Counter-measures include air defence against aircraft and attacking counter-battery radars physically and electronically.
'Field Artillery Team' is a US term and the following description and terminology applies to the US, other armies are broadly similar but differ in significant details. Modern field artillery (post–World War I) has three distinct parts: the forward observer (or FO), the fire direction center (FDC) and the actual guns themselves. The forward observer observes the target using tools such as binoculars, laser rangefinders, designators and call back fire missions on his radio, or relays the data through a portable computer via an encrypted digital radio connection protected from jamming by computerized frequency hopping. A lesser known part of the team is the FAS or Field Artillery Survey team which setups up the "Gun Line" for the cannons. Today most artillery battalions use a(n) "Aiming Circle" which allows for faster setup and more mobility. FAS teams are still used for checks and balances purposes and if a gun battery has issues with the "Aiming Circle" a FAS team will do it for them.
The FO can communicate directly with the battery FDC, of which there is one per each battery of 4–8 guns. Otherwise the several FOs communicate with a higher FDC such as at a Battalion level, and the higher FDC prioritizes the targets and allocates fires to individual batteries as needed to engage the targets that are spotted by the FOs or to perform preplanned fires.
The Battery FDC computes firing data—ammunition to be used, powder charge, fuse settings, the direction to the target, and the quadrant elevation to be fired at to reach the target, what gun will fire any rounds needed for adjusting on the target, and the number of rounds to be fired on the target by each gun once the target has been accurately located—to the guns. Traditionally this data is relayed via radio or wire communications as a warning order to the guns, followed by orders specifying the type of ammunition and fuse setting, direction, and the elevation needed to reach the target, and the method of adjustment or orders for fire for effect (FFE). However, in more advanced artillery units, this data is relayed through a digital radio link.
Other parts of the field artillery team include meteorological analysis to determine the temperature, humidity and pressure of the air and wind direction and speed at different altitudes. Also radar is used both for determining the location of enemy artillery and mortar batteries and to determine the precise actual strike points of rounds fired by battery and comparing that location with what was expected to compute a registration allowing future rounds to be fired with much greater accuracy.
A technique called Time on Target was developed by the British Army in North Africa at the end of 1941 and early 1942 particularly for counter-battery fire and other concentrations, it proved very popular. It relied on BBC time signals to enable officers to synchronize their watches to the second because this avoided the need to use military radio networks and the possibility of losing surprise, and the need for field telephone networks in the desert.[58] With this technique the time of flight from each fire unit (battery or troop) to the target is taken from the range or firing tables, or the computer and each engaging fire unit subtracts its time of flight from the TOT to determine the time to fire. An executive order to fire is given to all guns in the fire unit at the correct moment to fire. When each fire unit fires their rounds at their individual firing time all the opening rounds will reach the target area almost simultaneously. This is especially effective when combined with techniques that allow fires for effect to be made without preliminary adjusting fires.
This is a modern version of the earlier "time on target" concept in which fire from different weapons was timed to arrive on target at the same time. It is possible for artillery to fire several shells per gun at a target and have all of them arrive simultaneously, which is called MRSI (Multiple Rounds Simultaneous Impact). This is because there is more than one trajectory for the rounds to fly to any given target: typically one is below 45 degrees from horizontal and the other is above it, and by using different size propelling charges with each shell, it is possible to create multiple trajectories. Because the higher trajectories cause the shells to arc higher into the air, they take longer to reach the target and so if the shells are fired on these trajectories for the first volleys (starting with the shell with the most propellant and working down) and then after the correct pause more volleys are fired on the lower trajectories, the shells will all arrive at the same time. This is useful because many more shells can land on the target with no warning. With traditional volleys along the same trajectory, anybody at the target area may have time (however long it takes to reload and re-fire the guns) to take cover between volleys. However, guns capable of burst fire can deliver several rounds in 10 seconds if they use the same firing data for each, and if guns in more than one location are firing on one target they can use Time on Target procedures so that all their shells arrive at the same time and target.
To engage targets using MRSI requires two things, firstly guns with the requisite rate of fire and sufficiently different size propelling charges, secondly a fire control computer that has been designed to compute such missions and the data handling capability that allows all the firing data to be produced, sent to each gun and then presented to the gun commander in the correct order. The number of rounds that can be delivered in MRSI depends primarily on the range to the target and the rate of fire, for maximum rounds the range is limited to that of lowest propelling charge that will reach the target.
Examples of guns with a rate of fire that makes them suitable for MRSI includes UK's AS-90, South Africa's Denel G6-52 (which can land six rounds simultaneously at targets at least 25 km (16 mi) away), Germany's Panzerhaubitze 2000 (which can land five rounds simultaneously at targets at least 17 km (11 mi) away) Slovakia's 155 mm SpGH ZUZANA model 2000. The Archer project (developed by BAE-Systems in Sweden) is a 155 mm howitzer on a wheeled chassis which is claimed to be able to deliver up to six shells on target simultaneously from the same gun. The 120 mm twin barrel AMOS mortar system, joint developed by Hägglunds (Sweden) and Patria (Finland),[59] is capable of 7 + 7 shells MRSI. The United States Crusader program (now cancelled) was slated to have MRSI capability. It is unclear how many fire control computers have the necessary capabilities.
Two-round MRSI firings were a popular artillery demonstration in the 1960s, where well trained detachments could show off their skills for spectators.
The destructiveness of artillery bombardments can be enhanced when some or all of the shells are set for airburst, meaning that they explode in the air above the target instead of upon impact. This can be accomplished either through time fuses or proximity fuses. Time fuses use a precise timer to detonate the shell after a preset delay. This technique is tricky and slight variations in the functioning of the fuse can cause it to explode too high and be ineffective, or to strike the ground instead of exploding above it. Since December 1944 (Battle of the Bulge), proximity fuzed artillery shells have been available that take the guesswork out of this process. These embody a miniature, low powered radar transmitter in the fuse to detect the ground and explode them at a predetermined height above it. The return of the weak radar signal completes an electrical circuit in the fuze which explodes the shell. The proximity fuse itself was developed by the British to increase the effectiveness of anti-aircraft warfare.
This is a very effective tactic against infantry and light vehicles, because it scatters the fragmentation of the shell over a larger area and prevents it from being blocked by terrain or entrenchments that do not include some form of robust overhead cover. Combined with TOT or MRSI tactics that give no warning of the incoming rounds, these rounds are especially devastating because many enemy soldiers are likely to be caught in the open. This is even more so if the attack is launched against an assembly area or troops moving in the open rather than a unit in an entrenched tactical position.
This article uses material from the Wikipedia article "Artillery", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,model,library,rendering,Inca,Maya,Egypt,Pyramids,Bible, Quoran,Gizeh,Greek,Ancient,Medival Times, Stone Age