powered by CADENAS

Social Share

Amazon

Chain conveyor (14777 views - Mechanical Engineering)

A chain conveyor is a type of conveyor system for moving material through production lines. Chain conveyors utilize a powered continuous chain arrangement, carrying a series of single pendants. The chain arrangement is driven by a motor, and the material suspended on the pendants are conveyed. Chain conveyors are used for moving products down an assembly line and/or around a manufacturing or warehousing facility. Chain conveyors are primarily used to transport heavy unit loads, e.g. pallets, grid boxes, and industrial containers. These conveyors can be single or double chain strand in configuration. The load is positioned on the chains, the friction pulls the load forward. Chain conveyors are generally easy to install and have very minimum maintenance for users. Many industry sectors use chain conveyor technology in their production lines. The automotive industry commonly uses chain conveyor systems to convey car parts through paint plants. Chain conveyors also have widespread use in the white and brown goods, metal finishing and distribution industries. Chain conveyors are also used in the painting and coating industry, this allows for easier paint application. The products are attached to an above head chain conveyor, keeping products off of the floor allows for higher productivity levels.
Go to Article

Explanation by Hotspot Model

Youtube


    

Chain conveyor

Chain conveyor

A chain conveyor is a type of conveyor system for moving material through production lines.

Chain conveyors utilize a powered continuous chain arrangement, carrying a series of single pendants. The chain arrangement is driven by a motor, and the material suspended on the pendants are conveyed. Chain conveyors are used for moving products down an assembly line and/or around a manufacturing or warehousing facility.

Chain conveyors are primarily used to transport heavy unit loads, e.g. pallets, grid boxes, and industrial containers. These conveyors can be single or double chain strand in configuration. The load is positioned on the chains, the friction pulls the load forward.[1] Chain conveyors are generally easy to install and have very minimum maintenance for users.

Many industry sectors use chain conveyor technology in their production lines. The automotive industry commonly uses chain conveyor systems to convey car parts through paint plants.[2] Chain conveyors also have widespread use in the white and brown goods, metal finishing and distribution industries. Chain conveyors are also used in the painting and coating industry, this allows for easier paint application. The products are attached to an above head chain conveyor, keeping products off of the floor allows for higher productivity levels.

Multiflexing chain conveyor

The multiflexing conveyor systems use the plastic chains in many configurations. The flexible conveyor chain design permits horizontal as well as vertical change of direction.

Drag chain conveyor

The drag chain conveyor system, used for dry bulk solids and powder processing, moves powders and granules, particularly fragile materials such as cereals, nuts, coffee beans and food ingredients inside a hygienic, sealed tube. Material is fed into the pockets formed between discs inside of the conveying tube and is pulled through until it reaches the outlet. This is important particularly for food products as it minimizes product degradation and ensures dust-free transfer.[3]

See also



This article uses material from the Wikipedia article "Chain conveyor", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD