Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (May 2008) (Learn how and when to remove this template message) |
A C-clamp or G-clamp is a type of clamp device typically used to hold a wood or metal workpiece, and often used in, but are not limited to, carpentry and welding. These clamps are called "C" clamps because of their C-shaped frame, but are otherwise often called G-clamps or G-cramps[1] because including the screw part they are shaped like an uppercase letter G.
C-clamps or G-clamps are typically made of steel or cast iron, though smaller clamps may be made of pot metal. At the top of the "C" is usually a small flat edge. At the bottom is a threaded hole through which a large threaded screw protrudes. One end of this screw contains a flat edge of similar size to the one at the top of the frame, and the other end usually a small metal bar, perpendicular to the screw itself, which is used to gain leverage when tightening the clamp. When the clamp is completely closed, the flat end of the screw is in contact with the flat end on the frame.[2] When the clamp is actually used, it is very rare that this occurs. Generally some other object or objects will be contained between the top and bottom flat edges.
A G-clamp is used by means of turning the screw through the bottom of the frame until the desired state of pressure or release is reached. In the case that the clamp is being tightened, this is when the objects being secured are satisfactorily secured between the flat end of the screw and the flat end of the frame. If the clamp is being loosened, this is when a sufficient amount of force is released to allow the secured objects to be moved.
While a G-clamp is a useful tool for woodworking, special care should be taken when working with any woods. The flat gripping edges of the frame, generally no larger than half an inch or a centimetre (depending on the size of the clamp) can cause indentations and marring of the surfaces being clamped. This can be avoided by buffering between the clamp and the timber using two pieces of scrap wood. As each piece of scrap wood is directly in contact with the flat edges of the frame and with the items being clamped, this allows the scrap wood to receive the damage from the clamping, while dispersing the clamping force across the piece of scrap wood into the clamped objects. Deep-throated clamps are also available and provide greater reach for smaller jobs.
C-clamps are frequently used to hang stage lighting instruments.
This article uses material from the Wikipedia article "C-clamp", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD