Licensed under Creative Commons Attribution-Share Alike 3.0 (Unkown).
The dumbbell, a type of free weight, is a piece of equipment used in weight training. It can be used individually or in pairs, with one in each hand.
The forerunner of the dumbbell, halteres, were used in ancient Greece as lifting weights[1][2] and also as weights in the ancient Greek version of the long jump.[3] A kind of dumbbell was also used in India for more than a millennium, shaped like a club – so it was named Indian club. Despite their common English name implying an Indian origin, the so-called Indian clubs were in fact created in the Near East. Properly referred to as meels, they are first recorded as being used by wrestlers in ancient Persia, Egypt and the Middle East.[citation needed] The practice has continued to the present day, notably in the Varzesh-e Bastan tradition practiced in the zurkaneh of Iran. From Persia, the Mughals brought the meels to South Asia where are still used by pehlwan (wrestlers). British colonists first came across Persian meels in India, and erroneously referred to them as "Indian clubs" despite their Middle Eastern origin. The design of the "Nal", as the equipment was referred to, can be seen as a halfway point between a barbell and a dumbbell. It was generally used in pairs, in workouts by wrestlers, bodybuilders, sports players, and others wishing to increase strength and muscle size.
The term "dumbbell" or "dumb bell" originated in late Stuart England. In 1711 the poet Joseph Addison mentioned exercising with a "dumb bell" in an essay published in The Spectator (1711).[4] Although Addison elsewhere in the same publication describes having used equipment similar to the modern understanding of dumbbells, according to sport historian Jan Todd, the form of the first dumbbells remains unclear.[4] The Oxford English Dictionary describes "apparatus similar to that used to ring a church bell, but without the bell, so noiseless or ‘dumb’", implying the action of pulling a bell rope to practise English bellringing.[5]
By the early 17th century, the familiar shape of the dumbbell, with two equal weights attached to a handle, had appeared.[6] There are currently three main types of dumbbell:
This article uses material from the Wikipedia article "Dumbbell", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
.max, Maya, Challenge, Competition, Rendering, 3D, Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D, 3D library