Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article has multiple issues. Please help improve it or discuss these issues on the talk page. (Learn how and when to remove these template messages)
(Learn how and when to remove this template message)
|
A dress (also known as a frock or a gown) is a garment consisting of a skirt with an attached bodice (or a matching bodice giving the effect of a one-piece garment).[1] It consists of a top piece that covers the torso and hangs down over the legs. A dress can be any one-piece garment containing a skirt of any length. Dresses can be formal or informal. In many cultures, dresses are more often worn by women and girls.
The hemlines of dresses vary depending on the whims of fashion and the modesty or personal taste of the wearer.[2]
This section needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (January 2017) (Learn how and when to remove this template message) |
This section possibly contains original research. Please improve it by verifying the claims made and adding inline citations. Statements consisting only of original research should be removed. (January 2017) (Learn how and when to remove this template message) |
Before the Victorian period, the word "dress" usually referred to a general overall mode of attire for either men or women, as reflected today in such phrases "evening dress", "morning dress", "travelling dress", "full dress", and so on, rather than to any specific garment. At that time, the most-often used English word for a woman's skirted garment was gown. By the early 20th century, both "gown" and "frock" were essentially synonymous with "dress", although gown was more often used for a formal, heavy or full-length garment, and frock or dress for a lightweight, shorter, or informal one. Only in the last few decades has "gown" lost its general meaning of a woman's garment in the United States in favor of "dress".
In the ancient world, for example Ancient Greece and Rome, both men and women wore a similar dress-like garment termed generically a tunic. From this developed the dress worn by women and male clothing such as cassocks and Fustanella worn by priests and soldiers respectively. An ancient Greek tunic, appearing on the Charioteer of Delphi inspired an early twentieth gown designer, Mariano Fortuny to create the Delphos gown in 1907.
Dresses increased dramatically to the hoopskirt and crinoline-supported styles of the 1860s, then fullness was draped and drawn to the back. Dresses had a "day" bodice with a high neckline and long sleeves, and an "evening" bodice with a low neckline (decollete) and very short sleeves.
Throughout this period, the length of fashionable dresses varied only slightly, between ankle-length and floor-sweeping.[2]
Beginning around 1915, hemlines for daytime dresses left the floor for good. For the next fifty years fashionable dresses became short (1920s), then long (1930s), then shorter (the War Years with their restrictions on fabric), then long (the "New Look").
Since the 1970s, no one dress type or length has dominated fashion for long, with short and ankle-length styles often appearing side-by-side in fashion magazines and catalogs.[3]
In most varieties of formal dress codes in Western cultures, a dress of an appropriate style is mandatory for women. They are also very popular for special occasions such as proms or weddings.[4] For such occasions they, together with blouse and skirt, remain the de facto standard attire for many girls and women.
Gown or Long Dress - a woman's formal dress, usually having a floor-length skirt.[5]
Midi dress - a “midi” is used to refer to any dress or skirt that has a hem which hits at mid-calf – halfway between the knee and ankle.[5]
Knee length dress- Hemline ends at knee height.[5]
Mini dress (1960s) - a very short dress that terminates above the knee.[5][7]
Micro dress (right) with minidresses, 2008.- A microdress is an extremely short version of a mini.[8]
This article uses material from the Wikipedia article "Dress", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted