powered by CADENAS

Social Share

Useless machine (3969 views - Mechanism & Kinematics)

A useless machine is a device which has a function but no direct purpose. It may be intended to make a philosophical point, as an amusing engineering "hack", or as an intellectual joke. Devices which have no function or which malfunction are not considered to be "useless machines". The most well-known "useless machines" are those inspired by Marvin Minsky's design, in which the device's sole function is to switch itself off by operating its own "off" switch. More elaborate devices and novelty toys, having some obvious function or entertainment value, have been based on these simple "useless machines".
Go to Article

Explanation by Hotspot Model

Useless machine

Useless machine

A useless machine is a device which has a function but no direct purpose. It may be intended to make a philosophical point, as an amusing engineering "hack", or as an intellectual joke. Devices which have no function or which malfunction are not considered to be "useless machines".

The most well-known "useless machines" are those inspired by Marvin Minsky's design, in which the device's sole function is to switch itself off by operating its own "off" switch. More elaborate devices and novelty toys, having some obvious function or entertainment value, have been based on these simple "useless machines".

History

The Italian artist Bruno Munari began building "useless machines" (macchine inutili) in the 1930s. He was a "third generation" Futurist and did not share the first generation's boundless enthusiasm for technology, but sought to counter the threats of a world under machine rule by building machines that were artistic and unproductive.[1]

The version of the useless machine that became famous in information theory (basically a box with a simple switch which, when turned "on", causes a hand or lever to appear from inside the box that switches the machine "off" before disappearing inside the box again[2]) appears to have been invented by MIT professor and artificial intelligence pioneer Marvin Minsky, while he was a graduate student at Bell Labs in 1952.[3] Minsky dubbed his invention the "ultimate machine", but that sense of the term did not catch on.[3] The device has also been called the "Leave Me Alone Box".[4]

Minsky's mentor at Bell Labs, information theory pioneer Claude Shannon (who later also became an MIT professor), made his own versions of the machine. He kept one on his desk, where science fiction author Arthur C. Clarke saw it. Clarke later wrote, "There is something unspeakably sinister about a machine that does nothing—absolutely nothing—except switch itself off", and he was fascinated by the concept.[3]

Minsky also invented a "gravity machine" that would ring a bell if the gravitational constant were to change, a theoretical possibility that is not expected to occur in the foreseeable future.[3]

Commercial products

In the 1960s, a novelty toy maker called "Captain Co." sold a "Monster Inside the Black Box", featuring a mechanical hand that emerged from a featureless plastic black box and flipped a toggle switch, turning itself off. This version may have been inspired in part by "Thing", the disembodied hand featured in the television sitcom The Addams Family.[3] Other versions have been produced.[5] In their conceptually purest form, these machines do nothing except switch themselves off.

A closely related design is a coin snatching black box machine called "The Thing". It activates when a conductive metal coin is placed in a holder. The box begins to whir and vibrate, then a small plastic hand slowly emerges from under a trapdoor. The hand snatches the coin, pulls it in, and slams the door shut, ending the performance. It can be argued that this machine is not strictly useless, acting as a type of piggy bank, in a way that acts like a Rube Goldberg machine.

It is claimed that Don Poynter, who graduated from the University of Cincinnati in 1949 and founded Poynter Products, Inc., first produced and sold the "Little Black Box", which simply switched itself off. He then added the coin snatching feature, dubbed his invention "The Thing", arranged licensing with the producers of the television show, The Addams Family, and later sold "Uncle Fester's Mystery Light Bulb" as another show spinoff product.[6][7] Robert J. Whiteman, owner and president of Liberty Library Corporation, also claims credit for developing "The Thing".[8][9] (Both companies were later to be co-defendants in landmark litigation initiated by Theodor Geisel ("Dr. Seuss") over copyright issues related to figurines).[10][6]

Both the plain black box and the bank version were widely sold by Spencer Gifts, and appeared in its mail-order catalogs through the 1960s and early 1970s. As of 2015, a version of the coin snatching black box is being sold as the "Black Box Money Trap Bank" or "Black Box Bank".[citation needed]

Do-it-yourself versions of the useless machine (often modernized with microprocessor controls) have been featured in a number of web videos[11] and inspired more complex machines that are able to move or which use more than one switch.[12] As of 2015, there are several completed or kit form devices being offered for sale.[13]

Conceptual significance

Columbia University professor Lydia H. Liu wrote in her 2010 book The Freudian Robot that the useless machine reflects an "intuitive grasp of a fundamental problem of the unconscious that Freud has termed the death drive."[3]

Cultural references

In 2009, the artist David Moises exhibited his reconstruction of The Ultimate Machine aka Shannon's Hand, and explained the interactions of Claude Shannon, Marvin Minsky, and Arthur C. Clarke regarding the device.[14]

Episode 3 of the third season of the FX show Fargo, "The Law of Non-Contradiction", features a useless machine[15] (and, in a story within the story, an android named Minsky after Marvin Minsky).[16]

See also



This article uses material from the Wikipedia article "Useless machine", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanism & Kinematics

3D,Geneva double,mechanism,kinematics,rotation,translation