powered by CADENAS

Social Share

Dispenser (3913 views - Interior Design)

Dispenser may refer to:
Go to Article

Explanation by Hotspot Model

Dispenser

Dispenser

Dispenser may refer to:

Devices

Candy

Hygiene

Medicine

Others

  • Cash dispenser, automated teller machine
  • Label dispenser, machines built to simplify the process of removing a label from its liner or backing tape
  • Tape dispenser, an object that holds a roll of tape and has a mechanism at one end to shear the tape
  • Vending machines, which dispense beverages, candy, chips, sandwiches, and other foods
  • Water dispenser, a device designed to dispense hot or cold water
  • Wine dispenser, a device designed to serve and preserve wines
  • Media dispenser, a device for dispensing small units of liquid laboratory media
  • An automated dispenser used for order picking in warehouses

People

  • Le Despenser, a surname, most commonly associated with Norman-English barons

See also



This article uses material from the Wikipedia article "Dispenser", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Interior Design

3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art